web counter

What's the Difference between the BMP280 and the BME280 Atmospheric Sensors?

Sophie

Published: 06 July 2022 | Last Updated: 06 July 2022

11607

BME280

BME280

Bosch Sensortec

Pressure, Temperature and Humidity Sensor Digital Output 1.8V 8-Pin LGA T/R

Unit Price: $6.275209

Ext Price: $6.28

Purchase Guide

Pressure, Temperature and Humidity Sensor Digital Output 1.8V 8-Pin LGA T/R

In terms of BMP280 vs. BME280, When purchasing BME280 on eBay, there is a good chance you may receive BMP280 instead. Many sellers do not distinguish between the two. In this article, we will explain the features and specs of each so that you can distinguish between the two. Aside from their differences, we'll run a tutorial to see how well they interface with other libraries. When completing a complex project, you will know which choice is superior.

In this video, the author introduces the differences between the BMP280 and the BME280 atmospheric sensors.

What's the difference between the BMP280 and the BME280 atmospheric sensors

What is BMP280 ?

BMP280 is a barometric pressure sensor that measures air pressure and temperature. In contrast to the BME280, which monitors air pressure, temperature, and humidity, the BMP280 just measures air pressure and temperature. The unit's low power consumption and small size enable the implementation of battery-powered devices such as watches, GPS devices, and mobile phones. MBP280 additionally supports SPI and I2C connection and functions as a precision altimeter.


What is BME280 ?

BME280 is a precision environmental sensor that measures humidity, temperatures, and barometric pressures. The device syndicates high exactitude and linearity and is impeccably practical for high EMC sturdiness and long-term stability. 


BMP280 vs BME280 Pinout

BMP280 pinout.jpg

BMP280 Pinout

Pin No.Pin NamePin Description
1VCCThis is the power pin. Connect 3.3V DC supply at this pin.
2GNDGround pin
3SCLThis is the serial clock pin for the I2C interface.
4SDAThis is the serial data pin for the I2C interface.
5CSBThe chip select pin selects the I2C or SPI interface. It selects the SPI interface when provided with a low signal or grounded. On applying a HIGH signal of 3.3V, this pin will select the I2C interface.
6SDOIt is the serial data output pin that sends out the output value.

BME280 PINOUT.jpg

BME280 Pinout


Pin NumberPin NamePin Description
1GNDGround
2CSBChip Select
3SDISerial Data Interface
4SCKSerial Clock Interface
5SDOSerial Data Output
6VDDIODigital/Interface Supply
7GNDGround
8VDDAnalog Supply




BMP280 vs BME280 Specifications


BME280BMP280
Measuresair pressure
temperature
humidity
air pressure
temperature
Supply
voltage
1.7 to 3.6V (for the chip) 3.3 to 5V for the board1.7 to 3.6V (for the chip) 3.3 to 5V for the board
Temperature
range
-40 to 85ºC-40 to 85ºC
Weight G.W 10g3g
Accuracy of Air Pressure±1.0 hPa±1.0 hPa
Range of Air pressure300 – 1100 hPa300 – 1100 hPa
Dimensions40mm x20mm x15mm20mm x 40mm
Current Consumption 0.4 mA 0.6 mA
Accuracy of Temperature±1±1


BMP280 vs BME280Applications

BMP280 Applications

You may be wondering where the BMP280 sensor comes in handy. Because of its characteristics and capabilities, such as SPI and I2C compatibility, the BMP280 sensor is ideal for weather and environmental sensing. Some of the BMP280's applications are listed below.

  • Monitoring of fitness

  • Control of home automation

  • Forecast of weather

  • Indoor  navigation (elevator detection, floor detection)

  • Outdoor navigation (sports and leisure applications)

  • Indicating vertical velocity

  • GPS navigation enhancement (dead-reckoning, detection of slopes, etc)

  • Applications relating to health care i.e. spirometry

  • All other projects requiring the appropriate reading of the atmospheric pressure





BME280 Applications

You might be wondering where the BME280 sensor can be used. Because of its characteristics and capabilities, such as SPI and I2C compatibility, the BME280 sensor is ideal for weather and environmental sensing. Some of the BME280's uses are listed below.

  • Monitoring of fitness

  • Control of home automation

  • Forecast of weather

  • Indoor or outdoor navigation

  • GPS navigation enhancement

  • All other projects requiring the appropriate reading of the atmospheric pressure

 


BMP280 & BME280 Manufacturer

Bosch Sensortec GmbH is a fully owned subsidiary of Robert Bosch GmbH dedicated to the world of consumer electronics; offering a complete portfolio of micro-electro-mechanical systems (MEMS) based sensors and solutions that enable mobile devices to feel and sense the world around them. Bosch Sensortec develops and markets a broad portfolio of MEMS sensors, solutions, and systems for applications in smartphones, tablets, wearable devices, and various products within the IoT (Internet of Things).


BMP28 vs BME280 PCB 

PCB.jpg

Looking at the rear of the PCB, it seems the purple PCB may be the “genuine” and the blue PCB a “clone” – notice the poor printing by comparison and the M which became I1. Regardless, it seems the PCB was designed for BME280 and BMP280 – the black dot on the left module on the P text indicates it’s a BMP280. This was, however, confusing to the seller who insisted this meant it was a BME280 as the E was showing. The purple module on the right didn’t have any marks.


BME280 use with Arduino

You can use the environmental sensor Grove-BME280 with different microcontrollers such as Arduino, LinkIt ONE, and Beaglebone. You can achieve this through SPI or I2C. For our example today, we will be explaining to you how to connect your Grove environmental sensor BM280 to the Arduino.

Step by Step Guide


Step One: Connect the BME280 sensor to touch the Grove Base Shield V2 I2C port. After that, plug or insert it into Seeeduino. However, if you lack a Grove Base Shield, the module can be connected directly to the Seeeduino.


Step Two: Using a USB cable, connect Seeeduino to the PC


Step Three: Here is the software aspect of the tutorial. First of all, visit Github to download the example and library code.


Step Four: Create a brand new sketch for the Arduino and then paste some codes to it. You can also get access to the code directly just by following this path: File – Example – Barometer_Sensor – Barometer_Sensor.


Step Five: This step requires that you upload this code gotten in step five into your Arduino


Step Six: Open the serial monitor in order to receive the data of the sensor, which includes humidity, altitude, the value of barometric pressure, and temperature.


BMP28 vs BME280 Package

Finally, you can know the difference between bmp280 vs bme280 just by inspecting the package visually. If you check the datasheet of the BME280, you will see the markings for devices requiring mass production. This marking has to have ??? U? format. Here, the U signifies BME280. Now, the last ? you are seeing here just a P, while the final two characters are supposed to be UP.

Compared with the datasheet of BMP280, the format ought to be ??? K?. Here, the final “?” should be either W, N, U, or P. Therefore, KW, KN, KU, and KP are all devices of BMP280.


BME280 Equivalents

BME180, BMP280, HTU21D


BMP28 vs BME280 Datasheet

Conclusion

If you try to buy a Bosch Sensortec BME280 module on eBay, there’s a good chance you will get the lesser BMP280 instead. The reason seems to be sellers that don’t know what they are selling, a supply chain that doesn’t understand the difference between a BME280 and the BMP280, and a PCB break-out design that is shared between the two types of sensors. As a result, buying these sensors can get quite frustrating, as the sellers often get away with them.

If you want to be sure you get what you ordered, you’ll probably have to spend quite a bit more for a proper module from the likes of Adafruit, where everything is clearly labeled and controlled.


Frequently Asked Questions

What is BMP280?

The BMP280 is an absolute barometric pressure sensor, which is especially feasible for mobile applications. Its small dimensions and its low power consumption allow for the implementation in battery-powered devices such as mobile phones, GPS modules, or watches.

What is bme280?

The BME280 is a humidity sensor specially developed for mobile applications and wearables where size and low power consumption are key design parameters. The unit combines high linearity and high accuracy sensors and is perfectly feasible for low current consumption, long-term stability, and high EMC robustness.

How does bme280 work?

The BME280 sensor module reads barometric pressure, temperature, and humidity. Because pressure changes with altitude, you can also estimate altitude. There are several versions of this sensor module. The BME280 sensor uses I2C or SPI communication protocol to exchange data with a microcontroller.

What are i2c sensors?

The I2C bus is a simple and flexible way to transfer digital data between two electronic devices which may be physically separate or contained on the same printed circuit board (PCB).

How Does a Barometric Sensor Work? How Do I Connect My BMP180 to Arduino?

An aneroid barometer consists of an aneroid cell inside. The aneroid cell expands/contracts when there are small changes to atmospheric pressure. This movement from the aneroid cell causes mechanical levers to amplify, resulting in display pointers triggering and registering as readings on the front display.