WS2813 LED Light Source: Datasheet, Power and Wiring

UTMEL

Published: 30 September 2021 | Last Updated: 30 September 2021

4976

WS2813C

WS2813C

Worldsemi

WS2813C datasheet pdf and Unclassified product details from Worldsemi stock available at Utmel

Purchase Guide

WS2813 is an intelligent control integrated LED light source. This article mainly covers the datasheet, power, wiring diagram, pinout, and other details about WS2813. Furthermore, there is a huge range of semiconductors, capacitors, resistors, and ICs in stock. Welcome RFQ!

In This Video we are going to show you what is the Difference of WS2812b and WS2813 including an detailed data sheet of the WS2813 Schematics WS2811 Mechanical Drawing

What is the Difference of WS2812b and WS2813 datasheet?

WS2813 Pinout

WS2813 PINOUT.jpg

WS2813 Pinout

NO.SymbolPINFunction   description
1NCHANGINGSuspended in PCB   layout, the circuit will be out of operation when it connects to other   circuits
2VDDPOWER VOLTAGEPower Voltage,   connect to "+5V"
3DODATA CUTControl data signal   output
4DINDATA INControl data signal   input
5GNDGROUNDData& Power   Grounding
6BINBACKUP DATA INBackup Control data   signal input


WS2813 CAD Model

Symbol

WS2813 symbol.jpg

Symbol

Footprint

WS2813 footprint.jpg

Footprint

What is WS2813?

WS2813 is an intelligent control LED light source that the control circuit and RGB chip are integrated into a package of 5050 components. Its internal includes intelligent digital port data latch and signal reshaping amplification drive circuit. A precision internal oscillator and a 12V voltage programmable constant current control portion are also included, resulting in an exceedingly consistent color effect.


Specifications

Worldsemi WS2813C technical specifications, attributes, parameters and parts with similar specifications to Worldsemi WS2813C.
  • Type
    Parameter
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    SMD,5x5mm
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • Illumination Color

    Illumination Color refers to the specific color of light emitted by an LED or display component when it is activated. It is an important parameter as it affects the visibility and aesthetics of the electronic device. Common illumination colors include red, green, blue, yellow, and white, among others. The chosen illumination color can influence user experience and product design, making it a critical consideration in electronics engineering.

    RGB
  • Dominant Wavelength / Coordinate rank

    The parameter "Dominant Wavelength / Coordinate rank" in electronic components refers to the measurement of the dominant wavelength of light emitted by a component, typically an LED or a display. Dominant wavelength is the perceived color of the light emitted by the component, and it is measured in nanometers (nm). The coordinate rank indicates the color purity or saturation of the emitted light, with higher values indicating a more pure color. This parameter is important in applications where accurate color representation is crucial, such as in displays, signage, and lighting systems.

    620~625nmRed 515~525nmGreen 465~475nmBlue
  • Luminous Intensity (IF=20mA)

    Luminous Intensity (IF=20mA) is a parameter used to measure the brightness of light emitted by an electronic component, typically an LED (Light Emitting Diode). It specifies the intensity of light produced by the component when a current of 20mA (milliamperes) is passed through it. This parameter helps in determining the brightness level of the LED under specific operating conditions, allowing designers to select the appropriate component for their application based on the desired level of brightness. In general, a higher luminous intensity value indicates a brighter light output from the LED.

    60mcd@5mARed,245mcd@5mAGreen,60mcd@5mABlue
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

WS2813 Features and Benefits

  • The control circuit and the LED share the only power source.

  • The control circuit and RGB chip are integrated into 5050 components, to form an external control pixel.

  • Using the built-in signal reshaping circuit to achieve the signal waveform shaping, and no distortion of waveform of the signal takes place.

  • Built-in power-on reset and brown-out reset circuits.

  • The gray levels of each pixel are 256 levels, which achieves “256*256*256=16777216” full-color display, and the refresh frequency reaches 2 KHz/s.

  • Serial cascade interface, data receiving, and decoding depend on just one signal line.

  • Dual-signal wires version, signal break-point continuous transmission.

  • Any two points the distance more than 3m transmission signal without any increase circuit.

  • When the refresh rate is 30fps, cascade numbers are far more than 1024 points.

  • Data transmitting at speeds of up to 800Kbps.

  • Good color consistency reliability, high cost-effective.


WS2813 Applications

  • Guardrail tube series, point light display series, flexible/rigid strips series, module series applications.

  • Lighting stage costumes, innovative gadgets, or any other electronic products.


WS2813 Wiring

Only one power supply is shared by the control circuit and the LED.

To create an external control pixel, the control circuit and RGB chip are incorporated in 5050 components.

The signal waveform shaping is achieved using the built-in signal reshaping circuit, with no signal waveform distortion.

Power-on reset and brown-out reset circuits are built-in.

A full-color display of 256 * 256 * 256=16777216 and a refresh frequency of 2 kHz / s are achieved by each pixel having a gray level of 256 levels.

A single line of the signal is used to receive and decode data in the serial cascade interface. Its continuous transmitting signal break-point is in the dual-signal wires version.

ws2813 wiring diagram.jpg

WS2813 Wiring Diagram

How to use WS2813

A single NZR communication mode is used in the data transfer protocol.

After the pixel power-on reset, the DIN port gets data from the controller; the first pixel gathers initial 24bit data and delivers it to the internal data latch; the other data is reshaped by the internal signal reshaping amplification circuit and sent to the next cascade pixel via the DO port.

After transmission, each pixel's signal is reduced to 24 bits.

Each WS2813 LED pixel uses auto-reshaping transmission technology, which means that the pixel cascade numbers do not refer to the signal's transmission, but merely to the speed at which it is transmitted.

After 24bit data phagocytosis, the BIN gets the data signal and compares it to the DIN side; if DIN does not receive the signal, the BIN switches to accepting the input signal, guaranteeing that any IC damage does not disrupt signal cascade transmission.

Ensure that the BIN is in the receiving signal mode until it resumes after powering down.


WS2813 vs. WS2812B

ws2813 vs.ws2812.jpg

The LED bypass property of the two LED strips is the most significant distinction between WS2813 and WS2812B. One of the most significant advantages of the WS2813 over the WS2812B is that it operates on dual-signal cables with continuous signal break-point transmission.

This implies that if one of the LEDs in the middle of the chain burns out, the circuit will remain closed and the other LEDs will continue to light up. The remaining LEDs will continue to function normally as long as no other adjacent LEDs are broken. When one LED in a WS2812B strip is broken or burnt, the circuit is interrupted, and the remaining LEDs in the chain will not work.

This is because the earlier WS1812B only has one data signal; therefore a broken LED would prohibit the other LEDs from functioning. The WS2813 LED, on the other hand, has two data signals, which implies that until two neighboring LEDs are destroyed, any pixel failure in the chain will not impair signal flow. It's not so bad if only one of the LEDs fails. While you consider repairs, the rest might continue to flash as usual.

 


WS2813 Dimension

WS2813 dimensions.jpg

WS2813 Dimension

WS2813 Manufacturer

WorldSemi was founded in 2007, we work as the leading LED specialist in IC designer for Constant Current LED Driver IC, Chip Driver LED, we are recognized as the product development and delivery of LED lighting industry leader and we’ve expanded offerings to the inclusion of LED strip lights, LED point lights and LED controllers, etc.


Frequently Asked Questions

How do I control WS2813?

How to control WS2813 LED with Arduino? From the FastLED library, you can control WS2813 LED Strips. Use the type “WS2812” and set the LED strip by specifying the DATA PIN. The LED strip's DIN (data input) pin goes to Arduino PIN 6 with an optional 470 in between resistors.

How does the reset time of the WS2813 compare to that of the WS2812B?

The WS2813 has a reset time of 250μs, enabling the WS2813 LED to work better at lower frequencies and less expensive microcontrollers.

What is WS2813 used for?

WS2813 LED is widely used in guardrail tubes, pixel displays, flexible/rigid strips, modular lighting applications, stage lighting, and electronic gadgets for innovation.
WS2813C

Worldsemi

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe