web counter

2SK3878 Field Effect Transistor: Equivalent, Datasheet and Diagram

Sophie

Published: 24 February 2022 | Last Updated: 24 February 2022

14492

2SK3878

2SK3878

TOSHIBA

2SK3878 datasheet pdf and Unclassified product details from TOSHIBA stock available at Utmel

Purchase Guide

2SK3878 is a three-terminal silicon device. This article is going to introduce 2SK3878 pinout, equivalents, applications, and other details.

This video is about how to test mosfet on easy way.

Test mosfet on easy way!!

2SK3878 Description

2SK3878 is a three-terminal silicon device with current conduction capability of 9A, fast switching speed, l ow on-state resistance, breakdown voltage rating of 900V, and max.

threshold voltage of 4 volts.

They are designed for use in applications  such as switched mode power supplies, DC to DC converters, motor control circuits,UPS, switching regulator  and general purpose switching applications  .


2SK3878 Pinout

2SK3878 PINOUT.jpg

2SK3878 Pinout

2SK3878 Features

  • Marking Code: K3878

  • Type of Transistor  : MOSFET 

  • Type of Control Channel: N -Channel 

  • Maximum Power Dissipation  (Pd): 150 W

  • Maximum Drain-Source Voltage |Vds|: 900 V

  • Maximum Gate-Source Voltage |Vgs|: 30 V

  • Maximum Gate-Threshold Voltage |Vgs(th)|: 4 V

  • Maximum Drain Current |Id|: 9 A

  • Maximum Junction Temperature (Tj): 150 °C

  • Total Gate Charge (Qg): 60 nC

  • Rise Time (tr): 25 nS

  • Drain-Source Capacitance (Cd): 190 pF

  • Maximum Drain-Source On-State Resistance  (Rds): 1.3  Ohm 

  • Package: SC65 TO3P 


Specifications

TOSHIBA 2SK3878 technical specifications, attributes, parameters and parts with similar specifications to TOSHIBA 2SK3878.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    TO-3P
  • Current - Continuous Drain (Id) @ 25℃
    9A
  • Power Dissipation (Max)
    150W
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube-packed
  • FET Type

    "FET Type" refers to the type of Field-Effect Transistor (FET) being used in an electronic component. FETs are three-terminal semiconductor devices that can be classified into different types based on their construction and operation. The main types of FETs include Metal-Oxide-Semiconductor FETs (MOSFETs), Junction FETs (JFETs), and Insulated-Gate Bipolar Transistors (IGBTs).Each type of FET has its own unique characteristics and applications. MOSFETs are commonly used in digital circuits due to their high input impedance and low power consumption. JFETs are often used in low-noise amplifiers and switching circuits. IGBTs combine the high input impedance of MOSFETs with the high current-carrying capability of bipolar transistors, making them suitable for high-power applications like motor control and power inverters.When selecting an electronic component, understanding the FET type is crucial as it determines the device's performance and suitability for a specific application. It is important to consider factors such as voltage ratings, current handling capabilities, switching speeds, and power dissipation when choosing the right FET type for a particular circuit design.

    N-Channel
  • Rds On (Max) @ Id, Vgs

    Rds On (Max) @ Id, Vgs refers to the maximum on-resistance of a MOSFET or similar transistor when it is fully turned on or in the saturation region. It is specified at a given drain current (Id) and gate-source voltage (Vgs). This parameter indicates how much resistance the component will offer when conducting, impacting power loss and efficiency in a circuit. Lower Rds On values are preferred for better performance in switching applications.

    1.3Ω@4A,10V
  • Vgs(th) (Max) @ Id

    The parameter "Vgs(th) (Max) @ Id" in electronic components refers to the maximum gate-source threshold voltage at a specified drain current (Id). This parameter is commonly found in field-effect transistors (FETs) and is used to define the minimum voltage required at the gate terminal to turn on the transistor and allow current to flow from the drain to the source. The maximum value indicates the upper limit of this threshold voltage under specified operating conditions. It is an important parameter for determining the proper biasing and operating conditions of the FET in a circuit to ensure proper functionality and performance.

    4V@1mA
  • Drain to Source Voltage (Vdss)

    The Drain to Source Voltage (Vdss) is a key parameter in electronic components, particularly in field-effect transistors (FETs) such as MOSFETs. It refers to the maximum voltage that can be applied between the drain and source terminals of the FET without causing damage to the component. Exceeding this voltage limit can lead to breakdown and potentially permanent damage to the device.Vdss is an important specification to consider when designing or selecting components for a circuit, as it determines the operating range and reliability of the FET. It is crucial to ensure that the Vdss rating of the component is higher than the maximum voltage expected in the circuit to prevent failures and ensure proper functionality.In summary, the Drain to Source Voltage (Vdss) is a critical parameter that defines the maximum voltage tolerance of a FET component and plays a significant role in determining the overall performance and reliability of electronic circuits.

    900V
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

2SK3878 Applications

  • Low drain-source  ON resistance: RDS  (ON) = 1.0 Ω (typ.)

  • High forward transfer admittance  : ⎪Yfs⎪ = 7.0 S (typ.)

  • Low leakage current: IDSS = 100 μA (max) (VDS = 720 V)

  • Enhancement model: Vth = 2.0~4.0 V (VDS = 10 V, ID = 1 mA)

 


2SK3878 Equivalents

2SK3757 , 2SK3766 , 2SK3767 , 2SK3798 , 2SK3799 , 2SK3842 , 2SK3843 , 2SK3845 , 2SK4106 , 2SK3880 , 2SK3940 , 2SK4003 , 2SK4013 , 2SK4014 , 2SK4017 , 2SK4023 , 2SK4026

 


2SK3878 Package

2sk3878 package.png

2SK3878 Package 

2SK3878 Manufacturer

Toshiba is a world leader and innovator in pioneering high technology, a diversified manufacturer and marketer of advanced electronic and electrical products spanning information & communications systems; digital consumer products; electronic devices and components; power systems, including nuclear energy; industrial and social infrastructure systems; and home appliances. Toshiba was founded in 1875, and today operates a global network of more than 740 companies, with 204,000 employees worldwide and annual sales surpassing 6.3 trillion yen (US$68 billion).

Frequently Asked Questions

What is the breakdown voltage rating of a three-terminal silicon device?

900V

What is 2SK3878?

2SK3878 is a three-terminal silicon device.

What is 2SK3878 used for?

It is designed for use in switched-mode power supplies.
2SK3878

TOSHIBA

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe