web counter

A3144 Hall Effect Sensor: Datasheet, Circuit and Pinout

UTMEL

Published: 11 November 2021 | Last Updated: 11 November 2021

77064

A3144EU

A3144EU

ALLEGRO MICROSYSTEMS LLC

A3144EU datasheet pdf and Unclassified product details from ALLEGRO MICROSYSTEMS LLC stock available at Utmel

Purchase Guide

A3144 is a small, versatile, linear unipolar hall-effect sensor that acts as a magnetic switch. This article mainly covers datasheet, pinout, applications, working, and other details about the A3144 hall effect sensor.

Here we have used an NPN transistor that acts as a switch and as an amplifier. The whole circuitry can be controlled using a bar magnet having both the poles north-south.

Hall Effect Sensor A3144 Magnetic Switch || Circuit Diagram & Working

Overview of A3144 Hall Effect Sensor

A3144 is a small, versatile, linear unipolar hall-effect sensor that acts as a magnetic switch. Because of the semiconductor type case and lack of glass encapsulation, this Hall Effect sensor is similar to a switch but is more sensitive to magnetic flux and ideal for severe environments. When one pole of a magnet comes close to this type of unipolar Hall Effect sensor, it changes its state. This is appropriate for commercial, consumer, and industrial use.


A3144 Hall Effect Sensor Pinout

A3144 hall effect sensor consists of three pins which are shown in the following diagram.

The first pin is the power pin, which is used to power this sensor. On this sensor, 5V dc voltages are employed for power. The ground pin, on the other hand, is utilized to provide ground to this sensor. The digital output pin, on the other hand, is connected to an interface controller such as a microcontroller or an Arduino. However, between pins 1 and 3, a 10k ohm pull-up resistor is required to keep the output high when there is no magnetic field. A capacitor with a value of 0.1F is also required between pins 2 and 3 for filtering the digital output because noise may be linked with it.

A3144 PIN1.jpg

a3144 pin.jpg

A3144 Pinout

NoPin NameDescription
1'+5V (Vcc)Used to power the   hall sensor, typically +5V is used
2GroundConnect to the ground   of the circuit
3OutputThis pin goes high if a magnet is detected. The output voltage is equal to the Operating voltage.


A3144 Hall Sensor Specifications and Features

  • Power Consumption of 3.5mA at VCC = 5V for Energy Efficiency

  • Miniature Construction

  • Single Current Sourcing Output

  • Linear Output for Circuit Design Flexibility

  • Low Noise Output Virtually Eliminates the Need for Filtering

  • A Stable and Accurate Output

  • Temperature Range of -40°C to +85°C

  • Responds to either Positive or Negative Gauss


Alternatives for A3144 Hall Effect Sensor

A3141, A3142, A3143, US1881, OH090U


A3144 Hall Effect Sensor Applications

  • Used to detect magnets (objects) in automation systems

  • Used in a magnetic door alarm system

  • Measure speed in automobiles

  • Detect the pole of magnets in BLDC motors


Working Principle of A3144 Hall Effect Sensor

Every A3144 Hall Effect Sensor is made up of a material with a magnetic field. However, the magnetic field's charges are not active. When voltages are added to the input pins of the device, these changes become active. When a beam of charged particles passes through this magnetic field, a force is applied to the particles, and the beam is reflected in its original path. This beam is a conductor that carries current.

As a result of this entire process, two planes are formed: one with a magnetic field and the other with a deflected back beam or a current-carrying conductor. As a result, one plane has a positive charge while the other has a negative charge. Hall Effect voltages are the voltages that exist between these two planes. The gap between these two planes will be stopped if the force between the current carry conductor and the magnetic field is equal. If there is no current change, the flux density is measured by the hall voltages.

working principle.jpg

A3144 Working Principle


Where to Use A3144 Hall Effect Sensor

A hall-effect sensor, as the name implies, works on the hall-effect principle and is used to detect magnets. One pole can be detected on each side of the sensor. Because it uses transistor logic, it can be easily interfaced with a microcontroller.

So, if you need a sensor to detect magnets to measure the speed of a moving object or simply to identify objects, this sensor could be the right fit for your project.

 


How to Use A3144 Hall Effect Sensor

There are two types of hall-effect sensors: one that outputs an analog signal and the other that outputs a digital signal. The A3144 is a digital output hall sensor, which means that if it senses a magnet, the output will fall low, however, if it detects nothing, the output will stay high. A pull-up resistor, as illustrated below, is also required to maintain the output high when no magnet is detected.

a3144 circuit.jpg

A3144 Circuit

In the above circuit diagram, the resistor R1 (10K) is used as a pull-up resistor and the capacitor C1 (0.1uF) is used to filter any noise that might be coupled with the digital output.


Dimensions of A3144 Hall Effect Sensor

a3144 dimensions.jpg

 Dimensions of A3144 Hall Effect Sensor

Manufacturer of A3144 Hall Effect Sensor

As a leading company in the development, manufacture, and market of high-performance semiconductors, Allegro MicroSystems, LLC provides high-growth applications for the automotive market and also stays focused on consumer/communications, automation, and industrial solutions. Headquartered in Worcester, Massachusetts (USA) Allegro locates its design, applications, and sales support centers worldwide.


Frequently Asked Questions

What is the use of A3144?

A3144 is a digital output hall sensor, meaning if it detects a magnet the output will go low else the output will remain high. It is also mandatory to use a pull-up resistor as shown below to keep the output high when no magnet is detected.

How does A3144 work?

The A3144 is an integrated Hall Effect non-latching sensor. Holding a magnet near the sensor will cause the output pin to toggle. This makes for a robust presence sensor.A3144 is a digital output hall sensor, meaning if it detects a magnet the output will go low else the output will remain high.

Is CS3144 the same as A3144?

It is a type of Hall element, the specific parameters may be slightly different, and the pin definitions are the same.
A3144EU

ALLEGRO MICROSYSTEMS LLC

In Stock: 285

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe