Advantech Corp 96MPXE-2.6-19M36: A Comprehensive Guide to the Discontinued Skylake Microprocessor Module
Xeon Gold 6126 Microprocessor Skylake Series 3647-LGA Module
This article provides a detailed overview of the Advantech Corp 96MPXE-2.6-19M36 microprocessor module, a Skylake series product that has been discontinued. The article covers the general description, key features, primary and secondary applications, applicable specific modules, reference designs, alternative parts, and frequently asked questions related to this product.
Product Introduction
1. Description:
The Advantech Corp 96MPXE-2.6-19M36 is a high-performance microprocessor module that belongs to the Skylake series. It features a Xeon Gold 6126 core processor with a speed of 2.6GHz and 12 cores/64-bit bus width. The module comes in a 3647-LGA package and supports DDR4 RAM controllers. Despite being discontinued, it offers advanced processing capabilities for various applications.
2. Features:
- 2.6GHz speed for high processing performance
- 12 cores/64-bit bus width for multitasking and parallel processing
- DDR4 RAM controllers for efficient memory management
- Compact 3647-LGA package for easy integration into systems
3. Applications:
Primary Applications:
- Industrial automation
- Embedded computing
- Networking equipment
Secondary Applications:
- Medical devices
- Aerospace and defense systems
- Telecommunications infrastructure
Applicable Specific Modules:
- Advantech SOM-5899
- Advantech SOM-6883
4. Reference Designs:
The Advantech Corp 96MPXE-2.6-19M36 microprocessor module has been used in the following reference designs:
- Industrial IoT Gateway
- Embedded Vision System
- Network Security Appliance
5. Alternative Parts:
While the Advantech Corp 96MPXE-2.6-19M36 is discontinued, users can consider the following alternative parts with similar capabilities:
- Intel Xeon Gold 6126F
- Advantech Corp 96MPXE-2.8-19M36
6. FAQs:
Q: Is the Advantech Corp 96MPXE-2.6-19M36 still available for purchase?
A: No, this product has been discontinued by the manufacturer. Users may consider alternative parts with similar specifications.
Q: Can the Advantech Corp 96MPXE-2.6-19M36 be used in rugged environments?
A: While not specifically designed for rugged environments, this module can be used with proper environmental protection measures in place.
Q: What is the maximum supported RAM capacity of the Advantech Corp 96MPXE-2.6-19M36?
A: This module supports up to 128GB of DDR4 RAM.
In conclusion, the Advantech Corp 96MPXE-2.6-19M36 microprocessor module, despite being discontinued, offers advanced processing capabilities suitable for various industrial and embedded applications. Users can explore alternative parts with similar features for their projects.
Specifications
- TypeParameter
- Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
3647-LGA Module - Series
In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.
Skylake - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Discontinued - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Speed
In electronic components, "Speed" typically refers to the rate at which data can be processed or transferred within the component. It is a measure of how quickly the component can perform its functions, such as executing instructions or transmitting signals. Speed is often specified in terms of frequency, such as clock speed in processors or data transfer rate in memory modules. Higher speed components can perform tasks more quickly, leading to improved overall performance in electronic devices. It is an important parameter to consider when designing or selecting electronic components for specific applications.
2.6GHz - Core Processor
The term "Core Processor" typically refers to the central processing unit (CPU) of a computer or electronic device. It is the primary component responsible for executing instructions, performing calculations, and managing data within the system. The core processor is often considered the brain of the device, as it controls the overall operation and functionality. It is crucial for determining the speed and performance capabilities of the device, as well as its ability to handle various tasks and applications efficiently. In modern devices, core processors can have multiple cores, allowing for parallel processing and improved multitasking capabilities.
Xeon Gold 6126 - Number of Cores/Bus Width12 Core 64-Bit
- Graphics Acceleration
Graphics accelerators speed up the displaying of images on the monitor making it possible to achieve effects not otherwise possible - for example, the presentation of very large images or of interactive games in which images need to change quickly in response to user input.
No - RAM Controllers
RAM controllers are electronic components responsible for managing the flow of data to and from random access memory (RAM) in a computer system. They control the timing and data transfer between the CPU and RAM, ensuring efficient communication and data access. RAM controllers play a crucial role in determining the speed and performance of a computer system by optimizing memory access and utilization. These controllers are typically integrated into the motherboard or processor and are essential for the overall functioning of the system's memory subsystem.
DDR4
Parts with Similar Specs
Datasheet PDF
- Datasheets :
SST25VF040B 4-Mbit SPI Serial Flash: Pinout, Equivalent and Datasheet31 March 20221017
ADXL345 3-Axis Digital Accelerometer: Technical Design Guide and Datasheet Analysis17 January 2026342
AD7524: A High-Performance Digital to Analog Converter for Precise Signal Conversion05 March 2024262
M95020-W EEPROM: Pinout, Features and Datasheet07 January 20221939
SG3524 Modulators: Price, Circuit and Pinout19 July 20215935
IRLZ44N Power MOSFET: Datasheet, Pinout, IRLZ44N MOSFET24 November 202132176
MIC2026 1YM Power Switch: Dual USB High-Side 500mA, MIC2026 Current Limiting Power Switch14 January 2022963
Understanding the dsPIC33EVXXXGM00X/10X Family of Digital Signal Controller Devices29 February 2024133
Multivibrator: Circuits, Types and Application08 September 202024367
MediaTek, Qualcomm Announce Joining Russia Sanctions10 March 20224350
13 Semiconductor Startups Poised for Success in 2024, According to Investors11 December 20234304
The Energy Internet - A New Era of Energy Management and Distribution11 July 20233481
Inductance Basis: Definition, Structure and Applications18 April 20227444
Basic Introduction to Memristor12 January 202110305
Global Semiconductor Market Share Continues to Grow27 October 2023576
What is an Auto Transformer and Its Working?01 April 20216921
Advantech Corp
In Stock