web counter

CR2016 Battery: Pinout, Equivalents, CR2016 vs. CR2032

Sophie

Published: 06 October 2021 | Last Updated: 06 October 2021

4727

CR2016

CR2016

ZEUS Battery Products

BATTERY LITHIUM 3V CR2016

Purchase Guide

BATTERY LITHIUM 3V CR2016

This article will unlock more details about CR2016, a lithium coin cell battery

This video is about the differences between CR2032 and CR2016.

CR2032 vs CR2016 – What is the Difference Between These Batteries

CR2016 Pinout

CR2016 Pinout.jpg

CR2016 Pinout


CR2016 Description

The CR2016 is a lithium coin battery commonly used in automotive applications, sensors, medical thermometers, and other electronics applications. It uses a lithium/manganese dioxide (Li/MnO2) chemical system. The nominal voltage for a cell is around 3V. And typical power capacity is approximately 90-100 mAh.


Specifications

ZEUS Battery Products CR2016 technical specifications, attributes, parameters and parts with similar specifications to ZEUS Battery Products CR2016.
  • Type
    Parameter
  • Factory Lead Time
    12 Weeks
  • Voltage Rated

    RATED voltage is the voltage on the nameplate - the "design point" for maximum power throughput and safe thermal operation.

    3V
  • Size / Dimension

    In electronic components, the parameter "Size / Dimension" refers to the physical dimensions of the component, such as its length, width, and height. These dimensions are crucial for determining how the component will fit into a circuit or system, as well as for ensuring compatibility with other components and the overall design requirements. The size of a component can also impact its performance characteristics, thermal properties, and overall functionality within a given application. Engineers and designers must carefully consider the size and dimensions of electronic components to ensure proper integration and functionality within their designs.

    0.79Dia x 0.06 H 20.0mmx1.6mm
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    Not Applicable
  • Termination Style

    "Termination style" in electronic components refers to the method used to connect the component to a circuit board or other electronic devices. It determines how the component's leads or terminals are designed for soldering or mounting onto the circuit board. Common termination styles include through-hole, surface mount, and wire lead terminations.Through-hole components have leads that are inserted through holes in the circuit board and soldered on the other side. Surface mount components have flat terminals that are soldered directly onto the surface of the circuit board. Wire lead terminations involve attaching wires to the component for connection.The choice of termination style depends on factors such as the type of component, the manufacturing process, and the space available on the circuit board. Different termination styles offer various advantages in terms of ease of assembly, reliability, and space efficiency in electronic designs.

    Requires Holder
  • Storage/Refrigeration Temperature

    The parameter "Storage/Refrigeration Temperature" in electronic components refers to the recommended temperature range at which the components should be stored to maintain their integrity and functionality. This parameter indicates the temperature limits within which the components can be safely stored without risking damage or degradation. Storage temperature is crucial for preserving the performance and reliability of electronic components over time, especially for sensitive components such as integrated circuits and semiconductors. Refrigeration temperature may be specified for certain components that require lower temperatures to prevent degradation or prolong shelf life. It is important to adhere to the recommended storage/refrigeration temperature guidelines to ensure the longevity and proper functioning of electronic components.

    32°F~86°F 0°C~30°C
  • Battery Chemistry

    A battery is a device that stores chemical energy, and converts it to electricity. This is known as electrochemistry and the system that underpins a battery is called an electrochemical cell. A battery can be made up of one or several (like in Volta's original pile) electrochemical cells.

    Lithium Manganese Dioxide
  • Battery Cell Size

    The most common lithium-ion cell is the 18650 (the numbers define the physical dimensions and shape as follows: 18mm in diameter, 65mm long and the 0 means it has a round cross-section) which is due to its widespread use in laptop battery packs.

    Coin 20.0mm
  • Capacity

    In electronic components, "Capacity" typically refers to the maximum amount of electrical charge that a component can store. It is measured in units called farads (F). Capacitors are the most common components that have a capacity rating. The capacity of a capacitor determines how much energy it can store and release when connected in a circuit. Higher capacity capacitors can store more charge and are often used in applications requiring larger energy storage or filtering capabilities. It is important to select a capacitor with the appropriate capacity to ensure proper functioning of the circuit.

    80mAh
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

CR2016 Features

●Good pulse and high discharge rate performance

●Wide operating temperature range

●Stable discharge voltage

●No passivation

●Long operating life and shelf life

●Self-discharge rate less than 3% per year at 20°C

●Excellent safety in a hermetically sealed case

●Ability to provide a variety of welded termination tabs for all cell types


CR2016 Applications

  • Digital watch

  • Automobile applications (smart key, keyless entry, etc.)

  • Laser pens

  • Fitness applications

  • Medical devices


CR2016 Equivalents

CR2032, CR1220.


How to use CR2016

As per the below circuit diagram, you can power up a 3V DC motor by using a CR2016 battery. These batteries are used in many modules also like the RTC module. The output voltage is 3V so you can also power up your devices, module, electronic equipment which operates on 3V.

How to use CR2016.jpg

How to use CR2016



CR2016 vs. CR2032

Although CR2032 battery and CR2016 battery share similarities, there are actually differences in battery thickness and battery capacity. Therefore, we cannot simply use the two batteries.

CR2016 and CR2032 may vary in thickness, but they are identical in several ways.

They're both 3-volt versions, and none of them is rechargeable. However, it is important to remember that there are variations inability. CR 2032 has a capacity of 240 mAh, while CR2016 has a capacity of just 90 mAh. The CR2032 can provide 10 hours of use, while you only get about six hours from the CR2016, depending on the power you're using, of course.

Due to their equivalent voltage, there are several cases where CR2016 and CR2032 can be interchanged. However, the fact that they have different capacities and therefore different runtimes can cause problems. You will not get the power from the CR2016 that you will get from the CR2032, and some devices won't function at all.


CR2016 Dimensions

CR2016 Dimensions.jpg

CR2016 Dimensions


CR2016 Manufacturer

ZEUS Battery Products, founded in 2001 and located in the Midwest, emerges as a leading battery manufacturer dedicated to meeting the evolving demands of domestic and global primary and rechargeable battery markets.


Datasheet PDF

Download datasheets and manufacturer documentation for ZEUS Battery Products CR2016.
Frequently Asked Questions

Can You Use CR2016 instead of CR2032?

No, the CR2016 is thinner and a bit smaller than the CR2032.

What Does CR Mean in Batteries?

CR is the generic designation that is used by the entire batteries maker but lithium batteries are also having chromium. All the batteries that have this chemical substance in their batteries can use this abbreviation CR. On the other DL is the short abbreviation of the battery making company Duracell.

How long do CR2016 batteries last?

10 years.

How do you stack CR2016 batteries?

Remove the two batteries from the remote by sliding batteries out of the battery holder. 4.) Stack the new CR2016 batteries as shown with (+) facing up on both and slide back into the battery holder. Re-attach the cover with the three Phillips screws.

Can you use a 2025 battery in place of a 2016?

2016 is 20mm in diameter and 1.6mm thick. 2025 is 20mm in diameter and 2.5mm thick. The added thickness of 2025 would prevent it from fitting properly in the watches you mention.
CR2016

ZEUS Battery Products

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe