How LM324 Comparator Applied in a Circuit?
20nA 80 dB Instrumentational OP Amps 0.3μA 3V~30V ±1.5V~15V LM324 14-SOIC (0.154, 3.90mm Width)









20nA 80 dB Instrumentational OP Amps 0.3μA 3V~30V ±1.5V~15V LM324 14-SOIC (0.154, 3.90mm Width)
The LM324 operational amplifier IC can be worked as a comparator. On a single chip, this IC contains four independent operational amplifiers. In this article, we'll look at the widely used LM 324 IC. We'll look at the pin configuration, key features, and technical specs, and then we'll look at examples of the most basic application circuits that use the LM324.

Top 4 LM324 awesome diy electronics projects, 4 useful diy circuits
What is LM324 Comparator?
The LM324 comparator circuit consists of sensor voltage, reference voltage, Vcc, ground, and output pins. The LM324 operational amplifier IC can be worked as a comparator. On a single chip, this IC contains four independent operational amplifiers. This is a Low Power Quad Operational Amplifier with good stability and bandwidth that was designed to operate over a wide range of voltages from a single power supply.
The quad amplifier can run at supply voltages as low as 3.0 V and as high as 3.2 V, with quiescent currents roughly a quarter of the MC174's.

LM324 Circuit
LM324 Comparator Pinout
The pin configuration of the IC LM324 is shown below, along with a description of each pin's function.

LM324 Comparator Pinout
| Pin No. | The function of the Pin |
| 1 | The output of the first comparator |
| 2 | Inverting input of the first comparator |
| 3 | The non-inverting input of the first comparator |
| 4 | Supply voltage 5V |
| 5 | The non-inverting input of the second comparator |
| 6 | Inverting input of the second comparator |
| 7 | The output of the second comparator |
| 8 | The output of the third comparator |
| 9 | Inverting input of the third comparator |
| 10 | The non-inverting input of the third comparator |
| 11 | Ground |
| 12 | The non-inverting input of the fourth comparator |
| 13 | Inverting input of the fourth comparator |
| 14 | The output of the fourth comparator |
LM324 Comparator Features
It can operate from 3 V to 30 V single power supply.
It can operate from +/- 1.5 V to +/- 15 V for dual supply.
It has bandwidth up to 1.3 MHz
The large voltage gain of 100 dB
4 independent amplifiers
Some of the variants are short circuit protected at the output.
Rue differential input stages
Very low current consumption: 375 uA.
Low input bias current: 20 nA.
LM324 Electronics Characteristics
Input offset voltage: typical: 2 mV, maximum: 7 mV.
Input offset current typical: 2 nA, maximum: 20 nA.
Input bias current typical: 20 nA, maximum: 100 nA.
Large signal voltage gain ( Vcc = 15 v, RL, = 2 kohm, Vo = 1.4 V to 11.4 V): min: 50 V/mV, max: 100 V/mV.
Slew rate (Vcc = 15 V, VI = 0.5 V to 3 V, RL = 2 Kohm, CL = 100pF, unity gain) typical: 0.4 V/uS
Output current source [Vid = 1 V] (Vcc = 15 V, VO = 2V): minimum: 20 mA, Typical: 40 mA, Maximum: 70 mA.
Output sink current [Vid = -1 V] (Vcc = 15 V, VO = 2V) Minimum: 10mA, Typical: 20 mA.
High Level Output Voltage (Vcc = 30 V, RL = 2 K ohm) minimum: 26 V, Typical: 27 V.
High Level Output Voltage (Vcc = 5 V, RL = 2 K ohm) minimum: 3 V.
Low Level Output Voltage (RL = 10 k Ohm) Typical: 5 mV, Maximum: 20mV.
Total harmonic distortion (f = 1 kHz, Av = 20 dB, RL = 2 kΩ, VO = 2 Vpp, CL = 100 pF, VCC = 30 V) typical: 0.015 %.
Gain Bandwidth Product (VCC = 30 V, f = 100 kHz, Vin = 10 mV, RL = 2 kΩ, CL = 100 pF) Typical : 1.3 MHz.
LM324 Comparator Advantages
The LM324 is utilized as a comparator as well as an op-amp.
The LM324 is an electronic voltage amplifier with a high gain.
LM324 Comparator Applications
The LM324 comparator is generally used in the line following robot
The applications of the conventional op-amp can easily be implemented by using the LM324
The LM324 is applicable for oscillators, amplifiers, rectifiers, comparators, etc.
How to Apply LM324 in a Circuit?
The voltage comparator is shown in the following schematic. The LM324 comparator and two 10K ohm resistors are required for this circuit. The two inputs, input A and input B come from the line sensor circuit's output, and the two resistors are utilized to establish the voltage reference so that the optimal digital output may be produced.

Comparator Circuit Using LM324
We can see that Node A and Node B are connected to the non-inverting inputs of the left and right comparators in the aforementioned circuit. The left comparator's output is connected to Microcontroller P1.0, while the right comparator's output is connected to Microcontroller P1.1. The non-inverting mode is used by both comparators.
How does LM324 Comparator Work?
The LM324 comparator circuit is made up of three LM324 comparators as well as other components such as resistors, capacitors, and ground. The following circuit demonstrates the operation of this comparator in easy steps.

Working of LM324 Comparator
When a voltage smaller than the op-inverting amp's voltage is applied to the non-inverting terminal, the output becomes zero, indicating that no current flows. We already know that "+ > – = 1" when "+ > – = 1". The '+' sign denotes a non-inverting terminal, while the '-' sign denotes an inverting terminal.
The output will be high if the non-inverting voltage is greater than the inverting voltage.
This LM324 output is internally coupled to resistance and has some internal structure, which distinguishes it from other comparators.
It is internally pulled up; therefore there is no need for a power supply resistor connection.
What is LM324 used for?
By using this IC, the conventional op-amp applications can be implemented very simply. This IC can be used as oscillators, rectifiers, amplifiers, comparators, etc.
What is the gain of LM324?
It operates from a single positive power supply of 3 to 32V, and can also operate from a split supply of ± 1.5 to ±16V like typical Op-Amp. 1MHz unity-gain bandwidth. Open-loop gain of 100x.
What is the meaning of LM in LM324?
The prefix LM stands for linear monolithic, referring to the analog components integrated onto a single piece of silicon.
The prefix LM stands for linear monolithic, referring to the analog components integrated onto a single piece of silicon.
When the power is applied to the non-inverting terminal which is less than the inverting voltage of the op-amp then the output becomes zero which means there is no current flow. If the non-inverting voltage is greater than the inverting voltage then the output will be high.
6N139 Optocoupler: Pinout, Applications and Datasheet13 August 20212815
DRV8835 IC: Pinout, Feature and Application03 August 20214619
STM32H750VBT6: Features, Applications, and Datasheet31 October 20237631
BB18 POWR-BAR Distribution: Datasheet, Features, Equivalents12 January 20222039
TC1044SCPA Charge Pump Switching Regulator IC: Pinout, Equivalent, TC1044SCPA VS LM2574N-ADJG09 February 20222790
BME280 Sensor: Datasheet, Pinout and Applications08 July 202116864
SI4410DY: datasheet, package,pinout and applications14 March 2022670
TIP120 NPN Transistor: Pinout, Datasheet, and Schematic Diagram30 June 202110579
Semiconductor Industry's Water Risk Underpriced, Warn Fund Managers14 September 20234013
What is An Optoisolator?09 January 20218732
Introduction to Flyback Transformer29 January 202112172
What is an ASIC Chip?07 January 202616080
Varistor: Definition, Function, Working and Testing03 April 202585417
What are the Testing Method and Types of Transistors?21 October 202514915
Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications25 June 20261046
Aluminum Electrolytic Capacitor Basis: Definition, Characteristics and Life03 March 20226936
STMicroelectronics
In Stock: 377500
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools