web counter

LM35 Sensor: Pinout, Alternatives and Datasheet

Sophie

Published: 26 August 2021 | Last Updated: 26 August 2021

14189

LM35DZ/LFT1

LM35DZ/LFT1

Texas Instruments

Bulk Analog, Local 4V~30V Through Hole 0°C~100°C Analog Voltage ±1.5°C 10mV/°C 1 (Unlimited)

Unit Price: $2.139035

Ext Price: $2.14

Purchase Guide

Bulk Analog, Local 4V~30V Through Hole 0°C~100°C Analog Voltage ±1.5°C 10mV/°C 1 (Unlimited)

Hello everyone, I am Rose. Today we will have a discussion about LM35. LM35 is a precision centigrade temperature sensors. This article mainly introduce pinout, alternatives, datasheet and other detailed information about Texas Instruments LM35.

This video will show you how to convert ADC counts into degree centigrade with LM35 Sensor.

LM35 Temperature Sensor with Arduino Uno

LM35 Description

LM35 is a precision centigrade temperature sensors, It shows values in the form of output voltages instead of degree Celsius.  LM35 shows high voltage values than thermocouples and may not need that the output voltage is amplified. 


The output voltage of LM35 is proportional to the Celsius temperature. The scale factor is .01 V/°C. One most important characteristic is that it draws just 60 microamps from its supply and acquires a low self-heating capacity. 


LM35 temperature sensor available in many different packages like T0-46 metal transistor-like package, TO-92 plastic transistor-like package, 8-lead surface mount SO-8 small outline package.


LM35 Pinout

LM35 Pinout.jpg

Pinout2.png

LM35 CAD Model

Symbol

Symbol.png

Footprint

Footprint.png

3D Model

LM35 3D Model.jpg

LM35 Features

●Minimum and Maximum Input Voltage is 35V and -2V respectively. Typically operates at 5V.

●Can measure temperature ranging from -55°C to 150°C

●Output voltage is directly proportional (Linear) to temperature (i.e.) there will be a rise of 10mV (0.01V) for every 1°C rise in temperature.

●±0.5°C  Accuracy

●Drain current is less than 60uA  

●Low cost temperature sensor

●Small and hence suitable for remote applications

●Available in TO-92, TO-220, TO-CAN and SOIC package


Specifications

Texas Instruments LM35DZ/LFT1 technical specifications, attributes, parameters and parts with similar specifications to Texas Instruments LM35DZ/LFT1.
  • Type
    Parameter
  • Lifecycle Status

    Lifecycle Status refers to the current stage of an electronic component in its product life cycle, indicating whether it is active, obsolete, or transitioning between these states. An active status means the component is in production and available for purchase. An obsolete status indicates that the component is no longer being manufactured or supported, and manufacturers typically provide a limited time frame for support. Understanding the lifecycle status is crucial for design engineers to ensure continuity and reliability in their projects.

    ACTIVE (Last Updated: 5 days ago)
  • Factory Lead Time
    6 Weeks
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    Through Hole
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Through Hole
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    TO-226-3, TO-92-3 (TO-226AA)
  • Number of Pins
    3
  • Test Conditions
    25°C
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    0°C~100°C
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Bulk
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e3
  • Pbfree Code

    The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.

    yes
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    3
  • ECCN Code

    An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.

    EAR99
  • Temperature Coefficient

    The resistance-change factor per degree Celsius of temperature change is called the temperature coefficient of resistance. This factor is represented by the Greek lower-case letter “alpha” (α). A positive coefficient for a material means that its resistance increases with an increase in temperature.

    POSITIVE ppm/°C
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Matte Tin (Sn)
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    4V~30V
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    LM35
  • Output Type

    The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.

    Analog Voltage
  • Interface

    In electronic components, the term "Interface" refers to the point at which two different systems, devices, or components connect and interact with each other. It can involve physical connections such as ports, connectors, or cables, as well as communication protocols and standards that facilitate the exchange of data or signals between the connected entities. The interface serves as a bridge that enables seamless communication and interoperability between different parts of a system or between different systems altogether. Designing a reliable and efficient interface is crucial in ensuring proper functionality and performance of electronic components and systems.

    Analog
  • Termination Type

    Termination Type in electronic components refers to the method used to connect the component to a circuit board or other electronic devices. It specifies how the component's leads or terminals are designed for soldering or mounting onto a PCB. Common termination types include through-hole, surface mount, and wire lead terminations. The termination type is an important consideration when selecting components for a circuit design, as it determines how the component will be physically connected within the circuit. Different termination types offer varying levels of durability, ease of assembly, and suitability for specific applications.

    SOLDER
  • Nominal Supply Current

    Nominal current is the same as the rated current. It is the current drawn by the motor while delivering rated mechanical output at its shaft.

    82A
  • Output Current

    The rated output current is the maximum load current that a power supply can provide at a specified ambient temperature. A power supply can never provide more current that it's rated output current unless there is a fault, such as short circuit at the load.

    10mA
  • Quiescent Current

    The quiescent current is defined as the current level in the amplifier when it is producing an output of zero.

    56μA
  • Resolution

    Resolution in electronic components refers to the smallest increment of measurement or change that can be detected or represented by the component. It is a crucial specification in devices such as sensors, displays, and converters, as it determines the level of detail or accuracy that can be achieved. For example, in a digital camera, resolution refers to the number of pixels that make up an image, with higher resolution indicating a greater level of detail. In analog-to-digital converters, resolution is the number of discrete values that can be represented in the digital output, determining the precision of the conversion process. Overall, resolution plays a significant role in determining the performance and capabilities of electronic components in various applications.

    10mV/°C
  • Sensor Type

    In electronic components, the parameter "Sensor Type" refers to the specific type of sensor technology used in a particular component to detect and measure physical phenomena such as light, temperature, pressure, motion, or proximity. Different sensor types utilize various principles and mechanisms to convert the detected input into an electrical signal that can be processed by the electronic component. Common sensor types include photodiodes, thermistors, accelerometers, and proximity sensors, each designed for specific applications and environments. Understanding the sensor type is crucial for selecting the right component for a given task and ensuring accurate and reliable sensing capabilities in electronic systems.

    Analog, Local
  • Max Supply Voltage (DC)

    The parameter "Max Supply Voltage (DC)" in electronic components refers to the maximum voltage that can be safely applied to the component without causing damage. This specification is crucial for ensuring the reliable operation and longevity of the component within a given circuit. Exceeding the maximum supply voltage can lead to overheating, breakdown of internal components, or even permanent damage. It is important to carefully adhere to this specification when designing or using electronic circuits to prevent potential failures and ensure the safety of the components.

    30V
  • Min Supply Voltage (DC)

    The parameter "Min Supply Voltage (DC)" in electronic components refers to the minimum voltage level required for the component to operate properly. It indicates the lowest voltage that can be safely applied to the component without causing damage or malfunction. This parameter is crucial for ensuring the reliable and stable operation of the component within its specified operating range. It is important for designers and engineers to adhere to the specified minimum supply voltage to prevent potential issues such as erratic behavior, reduced performance, or permanent damage to the component.

    4V
  • Housing

    Housing in electronic components refers to the physical enclosure that protects the internal circuitry and components from environmental factors such as dust, moisture, and mechanical damage. It provides structural support and electrical insulation while facilitating heat dissipation. The design and materials used for housing are crucial for the reliability and performance of the electronic device, as they impact factors like thermal management, electromagnetic interference, and overall aesthetics.

    PLASTIC
  • Accuracy - Highest (Lowest)

    In electronic components, "Accuracy - Highest (Lowest)" refers to the range within which the actual value of a parameter can deviate from the ideal or specified value. The term "Highest" indicates the upper limit of this range, while "Lowest" indicates the lower limit. For example, if a component has an accuracy of ±5%, the highest accuracy would mean that the actual value could be within 5% above the specified value, while the lowest accuracy would mean it could be within 5% below the specified value. This parameter is crucial for ensuring the reliability and performance of electronic devices by determining how closely the component's output matches the desired value.

    ±1.5°C
  • Sensing Temperature - Local

    Sensing Temperature - Local refers to the capability of an electronic component to measure the temperature in its immediate environment or vicinity. This parameter is crucial for applications that require monitoring of temperature for performance, safety, or stability purposes. It often involves temperature sensors integrated within components like microcontrollers, power regulators, or other integrated circuits. The local sensing allows for accurate temperature readings that help in adjusting operational conditions, ensuring optimal performance, and preventing thermal-related failures.

    0°C~100°C
  • Accuracy-Max

    Accuracy-Max refers to the maximum permissible error in the output of an electronic component or system, typically expressed as a percentage of the nominal value. It indicates the extent to which the measured or calculated value can deviate from the true value under specified conditions. This parameter is crucial for ensuring reliable performance, especially in applications where precision is critical. A lower Accuracy-Max signifies better accuracy and higher quality in measurement and control processes.

    1.5 Cel
  • R0-Nom

    R0-Nom is a parameter commonly found in electronic components, particularly resistors. It refers to the nominal resistance value of the component under standard operating conditions. This value is typically specified by the manufacturer and represents the resistance that the component is designed to have within a certain tolerance range. Knowing the R0-Nom value is important for accurately calculating and designing circuits, as it ensures that the component will perform as expected within the specified parameters. It is essential to consider the R0-Nom value when selecting components for a circuit to ensure proper functionality and performance.

    0.4 Ω
  • Height
    5.34mm
  • Length
    4.3mm
  • Width
    4.3mm
  • Thickness

    Thickness in electronic components refers to the measurement of how thick a particular material or layer is within the component structure. It can pertain to various aspects, such as the thickness of a substrate, a dielectric layer, or conductive traces. This parameter is crucial as it impacts the electrical, mechanical, and thermal properties of the component, influencing its performance and reliability in electronic circuits.

    3.6mm
  • REACH SVHC

    The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.

    No SVHC
  • Radiation Hardening

    Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.

    No
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
  • Lead Free

    Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.

    Lead Free
0 Similar Products Remaining

LM35 Alternatives

Alternatives.png

LM35 Functional Block Diagram

Functional Block Diagram.png

How to use LM35?

LM35 is a precession Integrated circuit Temperature sensor, whose output voltage varies, based on the temperature around it. It is a small and cheap IC which can be used to measure temperature anywhere between -55°C to 150°C. It can easily be interfaced with any Microcontroller that has ADC function or any development platform like Arduino.

Power the IC by applying a regulated voltage like +5V (VS) to the input pin and connected the ground pin to the ground of the circuit. Now, you can measure the temperate in form of voltage as shown below.

how to use.png

If the temperature is 0°C, then the output voltage will also be 0V. There will be rise of 0.01V (10mV) for every degree Celsius rise in temperature.  The voltage can converted into temperature using the below formulae.

how to use2.png



LM35 Layout Example

Layout Example.png

LM35 Applications

●Used for measuring the temperature of a particular environment.

●Used in Power Supplies

●Used in Battery Management

●Used in HVAC

●Used in Appliances

●Used in Monitoring Battery Temperature

●Used in HVAC applications as a temperature measurement device.

●It provides thermal shutdown for a circuit/component

●It provides thermal shutdown for a circuit or component used in a specific project.

●It provides battery protection from overheating.




LM35 Package

Package.png

LM35 Manufacturer

Texas Instruments Incorporated (TI) is an American technology company headquartered in Dallas, Texas, that designs and manufactures semiconductors and various integrated circuits, which it sells to electronics designers and manufacturers globally. It is one of the top 10 semiconductor companies worldwide based on sales volume.The company's focus is on developing analog chips and embedded processors, which account for more than 80% of its revenue.TI also produces TI digital light processing technology and education technology products including calculators, microcontrollers and multi-core processors. 


Trend Analysis

Datasheet PDF

Download datasheets and manufacturer documentation for Texas Instruments LM35DZ/LFT1.

Parts with Similar Specs

The three parts on the right have similar specifications to Texas Instruments & LM35DZ/LFT1.
Frequently Asked Questions

1.What’s the working principle of LM35?

LM35 is a widely used temperature sensor. Because it uses internal compensation, the output can start from 0°C.
Its basic working principle: The temperature sensor circuit converts the measured temperature signal into a voltage signal and outputs it to the signal amplifying circuit. The voltage signal corresponding to the temperature value is amplified and then output to the A/D conversion circuit to convert the voltage signal into a digital signal. For the SCM system, the SCM system processes the digital quantity according to the display needs, and then sends the temperature display system to display.

2.Can LM35 temperature sensor replace DS18B20 temperature sensor?

The two cannot be directly substituted, because the working process and output of the two are different.
LM35 is a direct output linear analog quantity, which can be adjusted by the circuit to become the required voltage or current analog quantity for subsequent applications. If it is to be used on a single-chip microcomputer, it can be used after analog conversion; DS18B20 outputs a digital quantity, which can be directly connected with The single-chip microcomputer performs digital processing.
The working voltage of LM35 is larger and wider, while DS18B20 works intelligently under the voltage of 2.5V~5V of single-chip microcomputer.

3.How to convert LM35 output signal to binary?

The output of LM35 is an analog voltage signal, which needs an A/D converter to convert it into a binary digital signal.