LM393 Dual Comparator vs. LM358 Dual Op-Amp: Are they interchangeable?
Surface Mount Cut Tape (CT) 1.3 μs μs Linear Comparators 106.02dB dB 250nA pA 2006 5mV mV









Surface Mount Cut Tape (CT) 1.3 μs μs Linear Comparators 106.02dB dB 250nA pA 2006 5mV mV
The LM358 Op-Amp and the LM393 Comparator are two common jellybean components that are characterized by their ease of use and availability. Outwardly, the LM358 and LM393 are very similar–they come in the same package and with the same pinout, but there are fundamental differences to both chips, which we will be taking a look at in this article. Furthermore, Huge range of Semiconductors, Capacitors, Resistors and IcS in stock. Welcome RFQ.

Powerful 12v Audio Amplifier using LM358 IC
LM393 vs. LM358: Overview
LM393 Overview
The LM393 is a Dual in package comparator IC, meaning the IC has two comparators inside a single 8-pin package. The LM393 IC can be considered as the equivalent comparator version of the most popular LM358 Op-Amp. While any Op-Amp can be made to work as a voltage comparator, the LM393 proves itself to be advantages by providing an open collector output making it suitable to drive loads.
The LM393 series are dual independent precision voltage comparators capable of single or split supply operation. These devices are designed to permit a common mode range−to−ground level with single supply operation. Input offset voltage specifications as low as 2.0 mV make this device an excellent selection for many applications in consumer, automotive, and industrial electronics.
LM358 Overview
LM358 is a dual op-amp IC integrated with two op-amps powered by a common power supply. It can be considered as one half of LM324 Quad op-amp which contains four op-amps with common power supply. The LM358 series consists of two independent, high gain, internally frequency compensated operational amplifiers which were designed specifically to operate from a single power supply over a wide range of voltages.
Utilizing the circuit designs perfected for Quad Operational Amplifiers, these dual operational amplifiers feature low power drain, a common mode input voltage range extending to ground/VEE, and single supply or split supply operation. The LM358 series is equivalent to one−half of an LM324. These amplifiers have several distinct advantages over standard operational amplifier types in single supply applications.
LM393 vs. LM358: Pinout

LM393 vs. LM358: Pinout
LM393 vs. LM358: Specifications
| Specification | LM358 | LM393 |
| Supply Voltage | 32V, +/-16V | 36V, +/-18V |
| Differential Input Voltage | 32V | 36V |
| Input Offset Voltage | 3mV max. | 5mV max. |
| Input Bias Current | 100nA max. | 250nA max. |
| Input Common Mode Range | 0V to V+ - 2V | 0V to V+ - 1.5V |
| Large Signal Voltage Gain | 100V/mV typ. | 200V/mV typ. |
| Bandwidth | 1MHz | Not specified |
Although the input specifications seem similar, it is clear that the LM358 Op-Amp has a lower bias current and offset voltage, since it is designed to be used as an amplifier where these parameters matter. On the other hand, the LM393 has slightly worse input bias and offset performance, because for a comparator these parameters are not usually critical, since it is designed to be used only to compare voltages and not amplify them.
This is also reflected in the large signal voltage gain. The op-amp has a smaller gain, whereas the comparator's gain is much higher to make the output transition as fast as possible. The bandwidth of the comparator is also not specified, since it is not compensated.
LM393 vs. LM358: Features
LM393 Features
● Wide Single−Supply Range: 2.0 Vdc to 36 Vdc
● Split−Supply Range: ±1.0 Vdc to ±18 Vdc
● Very Low Current Drain Independent of Supply Voltage: 0.4 mA
● Low Input Bias Current: 25 nA
● Low Input Offset Current: 5.0 nA
● Low Input Offset Voltage: 5.0 mV (max)
● Input Common Mode Range to Ground Level
● Differential Input Voltage Range Equal to Power Supply Voltage
● Output Voltage Compatible with DTL, ECL, TTL, MOS, and CMOS Logic Levels
● ESD Clamps on the Inputs Increase the Ruggedness of the Device without Affecting Performance
● NCV Prefix for Automotive and Other Applications Requiring Unique Site and Control Change Requirements; AEC−Q100 Qualified and PPAP Capable
● These Devices are Pb−Free, Halogen Free/BFR Free and are RoHS Compliant
LM358 Features
● Short Circuit Protected Outputs
● True Differential Input Stage
● Single Supply Operation: 3.0 V to 32 V
● Low Input Bias Currents
● Internally Compensated
● Common Mode Range Extends to Negative Supply
● Single and Split Supply Operation
● ESD Clamps on the Inputs Increase Ruggedness of the Device without Affecting Operation
● Pb−Free Package May be Available. The G−Suffix Denotes a Pb−Free Lead Finish
LM393 vs. LM358: Internal Circuitry

LM393 Comparator Internal Circuit

LM358 Op-Amp Internal Circuit
At first glance, the internal circuits of the LM358 and the LM393 look similar, but taking a closer look we can find the differences that explain the different specifications mentioned above.
The input stages are similar to "Darlington-connected" PNPs, which explains the ground sensing capability of both the LM358 and LM393. The differential stages run at different currents, however – the LM393 runs at a higher current to increase the gain and output switching speed. Since the LM358 is a linear amplifier, this is not so important.
The largest difference is the output stages. The output stage of the LM393 is much simpler than that of the LM358 because it is designed to switch the output between the rails as fast as possible, spending the smallest amount of time between the rails. The output stage is also open-collector. The LM358 has a fully linear output stage, since it is an op-amp and designed to be used as a linear amplifier, where the output scales linearly with the input.
Parts with Similar Specs
- ImagePart NumberManufacturerPackage / CaseNumber of PinsInput Offset Voltage (Vos)Supply VoltageVoltage GainQuiescent CurrentCurrent - Input Bias (Max)Lead FreeView Compare
LM393DR2G
8-SOIC (0.154, 3.90mm Width)
8
5 mV
5 V
106.02 dB
2.5 mA
0.25μA @ 5V
Lead Free
8-SOIC (0.154, 3.90mm Width)
8
2 mV
5 V
106.02 dB
2.5 mA
0.25μA @ 5V
Lead Free
8-SOIC (0.154, 3.90mm Width)
8
5 mV
5 V
106.02 dB
2.5 mA
0.25μA @ 5V
Lead Free
8-SOIC (0.154, 3.90mm Width)
8
5 mV
5 V
106.02 dB
2.5 mA
0.25μA @ 5V
Lead Free
8-SOIC (0.154, 3.90mm Width)
8
5 mV
5 V
106.02 dB
2.5 mA
0.25μA @ 5V
Lead Free
LM393 vs. LM358: Applications
LM393 Applications
● Voltage Comparator Circuits
● Can drive Relay, Lamp, Motor Etc
● Peak Voltage Detector
● High Voltage Protection/Warning
● Oscillator Circuits
● Zero Crossing Detector (Single Supply)
● Zero Crossing Detector (Split Supply)
● Free−Running Square−Wave Oscillator
● Time Delay Generator
● Comparator with Hysteresis
LM358 Applications
● Transducer Amplifiers
● Conventional Op-amp Circuits
● Integrator, Differentiator, Summer, Adder, Voltage follower, etc.,
● DC gain blocks, Digital multimeters, Oscilloscopes
● Comparators (Loop control & regulation)
● Active Filters
● General Signal Conditioning and Amplification
● 4- to 20-mA Current Loop Transmitters
LM393 vs. LM358: Package

LM393/LM358 SOIC−8 Package
Major Differences Between LM358 and LM393
| LM358 | LM393 |
| Dual operational amplifier | Dual comparator |
| Relatively better input specifications | Relatively worse input specifications |
| Output linear with input | Non-linear output |
| Stable with negative feedback | Stable with positive feedback |
Conclusion
The LM358 and LM393 might seem outwardly similar, but the LM358 is an operational amplifier with linear output, and the LM393 is a comparator with a digital output, and they cannot be interchanged.
The pin functions of LM393 and LM358 are the same, I want to know whether they can be directly interchanged?
Generally not directly interchangeable. Although the Op Amp can be used as a voltage comparator in some circuits that require less precision, the Op Amp cannot be replaced by a comparator because there is no amplification function; When LM358 is replaced with LM393, the original 393 output terminal should be removed, pull-resistance comparator; Although the symbols of the comparator and the Op Amp are the same on the circuit diagram, the two devices do have very big differences and generally cannot be interchanged.
What is the difference between LM258 and LM393?
One is an operational amplifier and the other is a voltage comparator. Of course, LM258 can also be used as a voltage comparator. LM393 must be used as a comparator output terminal to add a pull-up resistor, using LM258 as a comparator can eliminate the need for an external pull-up resistor.
Can LM324 and LM358 be replaced?
358 is an 8-pin dual op amp, and 324 is a 14-pin quad op amp. Their parameters are the same. It can be replaced, but the circuit board needs to be changed. If it is used as a comparator in the inverter, it is no problem. Personally, I think it is better to use 358, because it is easier to design the circuit board. If the op amp is used as an oscillator, it is recommended to replace it with TL082 and 084, which are high-speed op amps.
What are the advantages of LM258 compared to LM358?
LM258 is an industrial grade, and LM358 is a commercial grade. LM258 is a grade higher than LM358, and LM258 parameters are better than LM358. One type of chip with good performance is 258.
TPS92638QPWPRQ1 LED Lighting Driver: Alternatives, Pinout, Datasheet18 March 20221248
PIC16F876 Microcontroller: Features, Pinout, and Datasheet23 November 20218533
A Comprehensive Guide to LTM8005HY#PBF LED Driver by Linear Technology/Analog Devices06 March 2024214
MIC29302WU Voltage Regulator: Pinout, Applications and Datasheet24 October 20232555
STM32F103VCT6 Microcontroller: 72MHz, 100-LQFP, Pinout and Datasheet09 February 20225189
2P4M SCR: Datasheet, Pin and Circuit09 November 202110586
CD4001BE: Overview, Applications and Datasheet09 November 20232299
A Comprehensive Guide to LTC6946IUFD-1 Clock/Frequency Synthesizer06 March 2024338
Using SiC-GaN to Create Two-Phase Interleaved DC-DC Converters for Plug-in Electric Vehicles03 February 20233050
MLCC: Applications and Future Development20 December 202110534
Semiconductor Memory Market to See More Significant Price Declines17 August 20222368
How Fast is Wi-Fi 6?07 June 20217722
FPGA: A Highly Customised Type of Chip Based on Digital Circuits22 February 20234890
What Sensors does a Car Engine Have?28 March 202526993
Design and Implementation of High Frequency Inverter for Printer Based on IR211013 April 202210268
L1154F Battery Features and What Makes It Unique22 August 20252339
ON Semiconductor
In Stock: 29198
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools