RC4558P Operational Amplifier: Layout, Pinout, and Datasheet
2 Channels 150nA 70 dB Instrumentational OP Amps 10V~30V ±5V~15V RC4558 8 Pins 8-DIP (0.300, 7.62mm)









2 Channels 150nA 70 dB Instrumentational OP Amps 10V~30V ±5V~15V RC4558 8 Pins 8-DIP (0.300, 7.62mm)
The RC4558P is a dual general-purpose operational amplifier with each half electrically comparable to the μA741, with the exception of offset null capabilities. This article mainly introduces Layout, Pinout, Datasheet and other detailed information about Texas Instruments RC4558P.

#4558D,4558 ic full diagram /4558D circuit diagram/Mr electro
RC4558P Description
The RC4558P is a dual general-purpose operational amplifier with each half electrically comparable to the μA741, with the exception of offset null capabilities.
This amplifier is suited for voltage-follower applications because of its wide common-mode input voltage range and lack of latch-up. Short-circuit protection is built in, and internal frequency adjustment assures stability without the use of additional components.
RC4558P Pinout
The RC4558P Pinout is shown as follows.

Pinout
| Pin Number | Pin Name | Description |
| 3 | 1IN+ | Noninverting input |
| 2 | 1IN- | Inverting Input |
| 1 | 1OUT | Output |
| 5 | 2IN+ | Noninverting input |
| 6 | 2IN- | Inverting Input |
| 7 | 2OUT | Output |
| 8 | VCC+ | Positive Supply |
| 4 | VCC- | Negative Supply |
RC4558P CAD Model
RC4558P Features
• Continuous Short-Circuit Protection
• Wide Common-Mode and Differential Voltage Ranges
• No Frequency Compensation Required
• Low Power Consumption
• No Latch-Up
• Unity-Gain Bandwidth . . . 3 MHz Typ
• Gain and Phase Match Between Amplifiers
• Low Noise . . . 8 nV/√Hz Typ at 1 kHz
Specifications
- TypeParameter
- Lifecycle Status
Lifecycle Status refers to the current stage of an electronic component in its product life cycle, indicating whether it is active, obsolete, or transitioning between these states. An active status means the component is in production and available for purchase. An obsolete status indicates that the component is no longer being manufactured or supported, and manufacturers typically provide a limited time frame for support. Understanding the lifecycle status is crucial for design engineers to ensure continuity and reliability in their projects.
ACTIVE (Last Updated: 2 days ago) - Factory Lead Time6 Weeks
- Contact Plating
Contact plating (finish) provides corrosion protection for base metals and optimizes the mechanical and electrical properties of the contact interfaces.
Gold - Mounting Type
The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.
Through Hole - Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
8-DIP (0.300, 7.62mm) - Surface Mount
having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.
NO - Number of Pins8
- Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
0°C~70°C - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tube - JESD-609 Code
The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.
e4 - Pbfree Code
The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.
yes - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Number of Terminations8
- ECCN Code
An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.
EAR99 - Terminal Position
In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.
DUAL - Number of Functions2
- Supply Voltage
Supply voltage refers to the electrical potential difference provided to an electronic component or circuit. It is crucial for the proper operation of devices, as it powers their functions and determines performance characteristics. The supply voltage must be within specified limits to ensure reliability and prevent damage to components. Different electronic devices have specific supply voltage requirements, which can vary widely depending on their design and intended application.
15V - Base Part Number
The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.
RC4558 - Pin Count
a count of all of the component leads (or pins)
8 - Power Supplies
an electronic circuit that converts the voltage of an alternating current (AC) into a direct current (DC) voltage.?
+-15V - Number of Channels2
- Operating Supply Current
Operating Supply Current, also known as supply current or quiescent current, is a crucial parameter in electronic components that indicates the amount of current required for the device to operate under normal conditions. It represents the current drawn by the component from the power supply while it is functioning. This parameter is important for determining the power consumption of the component and is typically specified in datasheets to help designers calculate the overall power requirements of their circuits. Understanding the operating supply current is essential for ensuring proper functionality and efficiency of electronic systems.
2.5mA - Nominal Supply Current
Nominal current is the same as the rated current. It is the current drawn by the motor while delivering rated mechanical output at its shaft.
5.6mA - Max Supply Current
Max Supply Current refers to the maximum amount of electrical current that a component can draw from its power supply under normal operating conditions. It is a critical parameter that ensures the component operates reliably without exceeding its thermal limits or damaging internal circuitry. Exceeding this current can lead to overheating, performance degradation, or failure of the component. Understanding this parameter is essential for designing circuits that provide adequate power while avoiding overload situations.
5.6mA - Slew Rate
the maximum rate of output voltage change per unit time.
1.7V/μs - Architecture
In electronic components, the parameter "Architecture" refers to the overall design and structure of the component. It encompasses the arrangement of internal components, the layout of circuitry, and the physical form of the component. The architecture of an electronic component plays a crucial role in determining its functionality, performance, and compatibility with other components in a system. Different architectures can result in variations in power consumption, speed, size, and other key characteristics of the component. Designers often consider the architecture of electronic components carefully to ensure optimal performance and integration within a larger system.
VOLTAGE-FEEDBACK - Amplifier Type
Amplifier Type refers to the classification or categorization of amplifiers based on their design, functionality, and characteristics. Amplifiers are electronic devices that increase the amplitude of a signal, such as voltage or current. The type of amplifier determines its specific application, performance capabilities, and operating characteristics. Common types of amplifiers include operational amplifiers (op-amps), power amplifiers, audio amplifiers, and radio frequency (RF) amplifiers. Understanding the amplifier type is crucial for selecting the right component for a particular circuit or system design.
General Purpose - Common Mode Rejection Ratio
Common Mode Rejection Ratio (CMRR) is a measure of the ability of a differential amplifier to reject input signals that are common to both input terminals. It is defined as the ratio of the differential gain to the common mode gain. A high CMRR indicates that the amplifier can effectively eliminate noise and interference that affects both inputs simultaneously, enhancing the fidelity of the amplified signal. CMRR is typically expressed in decibels (dB), with higher values representing better performance in rejecting common mode signals.
70 dB - Current - Input Bias
The parameter "Current - Input Bias" in electronic components refers to the amount of current required at the input terminal of a device to maintain proper operation. It is a crucial specification as it determines the minimum input current needed for the component to function correctly. Input bias current can affect the performance and accuracy of the device, especially in precision applications where small signal levels are involved. It is typically specified in datasheets for operational amplifiers, transistors, and other semiconductor devices to provide users with important information for circuit design and analysis.
150nA - Voltage - Supply, Single/Dual (±)
The parameter "Voltage - Supply, Single/Dual (±)" in electronic components refers to the power supply voltage required for the proper operation of the component. This parameter indicates whether the component requires a single power supply voltage (e.g., 5V) or a dual power supply voltage (e.g., ±15V). For components that require a single power supply voltage, only one voltage level is needed for operation. On the other hand, components that require a dual power supply voltage need both positive and negative voltage levels to function correctly.Understanding the voltage supply requirements of electronic components is crucial for designing and integrating them into circuits to ensure proper functionality and prevent damage due to incorrect voltage levels.
10V~30V ±5V~15V - Input Offset Voltage (Vos)
Input Offset Voltage (Vos) is a key parameter in electronic components, particularly in operational amplifiers. It refers to the voltage difference that must be applied between the two input terminals of the amplifier to nullify the output voltage when the input terminals are shorted together. In simpler terms, it represents the voltage required to bring the output of the amplifier to zero when there is no input signal present. Vos is an important parameter as it can introduce errors in the output signal of the amplifier, especially in precision applications where accuracy is crucial. Minimizing Vos is essential to ensure the amplifier operates with high precision and accuracy.
6mV - Neg Supply Voltage-Nom (Vsup)
The parameter "Neg Supply Voltage-Nom (Vsup)" in electronic components refers to the nominal negative supply voltage that the component requires to operate within its specified performance characteristics. This parameter indicates the minimum voltage level that must be provided to the component's negative supply pin for proper functionality. It is important to ensure that the negative supply voltage provided to the component does not exceed the maximum specified value to prevent damage or malfunction. Understanding and adhering to the specified negative supply voltage requirements is crucial for the reliable operation of the electronic component in a circuit.
-15V - Unity Gain BW-Nom
Unity Gain Bandwidth, often abbreviated as Unity Gain BW or UGBW, refers to the frequency at which an amplifier can provide a gain of one (0 dB). It is a critical parameter in assessing the performance of operational amplifiers and other amplifying devices, indicating the range of frequencies over which the amplifier can operate without distortion. Unity Gain BW is particularly important in applications where signal fidelity is crucial, as it helps determine the maximum frequency of operation for a given gain level. As the gain is reduced, the bandwidth typically increases, ensuring that the amplifier can still operate effectively across various signal frequencies.
3000 kHz - Voltage Gain
Voltage gain is a measure of how much an electronic component or circuit amplifies an input voltage signal to produce an output voltage signal. It is typically expressed as a ratio or in decibels (dB). A higher voltage gain indicates a greater amplification of the input signal. Voltage gain is an important parameter in amplifiers, where it determines the level of amplification provided by the circuit. It is calculated by dividing the output voltage by the input voltage and is a key factor in determining the overall performance and functionality of electronic devices.
109.54dB - Low-Offset
Low-offset is a parameter used to describe the level of offset voltage in electronic components, particularly in operational amplifiers. Offset voltage refers to the small voltage difference that exists between the input terminals of the amplifier when the input voltage is zero. A low-offset value indicates that this voltage difference is minimal, which is desirable for accurate signal processing and amplification. Components with low-offset specifications are preferred in applications where precision and accuracy are critical, such as in instrumentation and measurement systems. Minimizing offset voltage helps reduce errors and ensures the faithful reproduction of input signals by the amplifier.
NO - Frequency Compensation
Frequency compensation is implemented by modifying the gain and phase characteristics of the amplifier's open loop output or of its feedback network, or both, in such a way as to avoid the conditions leading to oscillation. This is usually done by the internal or external use of resistance-capacitance networks.
YES - Voltage - Input Offset
Voltage - Input Offset is a parameter that refers to the difference in voltage between the input terminals of an electronic component, such as an operational amplifier, when the input voltage is zero. It is an important characteristic that can affect the accuracy and performance of the component in various applications. A low input offset voltage is desirable as it indicates that the component will have minimal error in its output when the input signal is near zero. Manufacturers typically provide this specification in the component's datasheet to help users understand the component's behavior and make informed decisions when designing circuits.
500μV - Low-Bias
Low-bias in electronic components refers to a design or configuration that minimizes the amount of bias current flowing through the component. Bias current is a small, steady current that is used to establish the operating point of a component, such as a transistor or amplifier. By reducing the bias current to a low level, the component can operate with lower power consumption and potentially lower distortion. Low-bias components are often used in applications where power efficiency and signal fidelity are important, such as in audio amplifiers or battery-powered devices. Overall, the low-bias parameter indicates the ability of the component to operate efficiently and accurately with minimal bias current.
NO - Micropower
the use of very small electric generators and prime movers or devices to convert heat or motion to electricity, for use close to the generator.
NO - Bias Current-Max (IIB) @25C
The parameter "Bias Current-Max (IIB) @25C" in electronic components refers to the maximum input bias current that the component can handle at a specified temperature of 25 degrees Celsius. Bias current is the current flowing into the input terminal of a device when no signal is applied. This parameter is important because excessive bias current can affect the performance and stability of the component, leading to potential issues such as distortion or offset errors in the output signal. By specifying the maximum bias current allowed at a certain temperature, manufacturers provide users with important information to ensure proper operation and reliability of the component in their circuit designs.
0.5μA - Programmable Power
A programmable power supply provides remote control capability of the output voltage(s) via an analog control signal controlled by keypad or rotary switch from the front panel of the power supply or via a computer interface such as RS232, GPIB, or USB.
NO - Dual Supply Voltage
Dual Supply Voltage refers to an electronic component's requirement for two separate power supply voltages, typically one positive and one negative. This configuration is commonly used in operational amplifiers, analog circuits, and certain digital devices to allow for greater signal handling capabilities and improved performance. The use of dual supply voltages enables the device to process bipolar signals, thereby enhancing its functionality in various applications.
9V - Nominal Gain Bandwidth Product
The Nominal Gain Bandwidth Product is a key parameter in electronic components, particularly in operational amplifiers. It represents the product of the gain and the bandwidth at which that gain is achieved. In simpler terms, it indicates the frequency range over which the amplifier can provide a specified level of gain. A higher Nominal Gain Bandwidth Product implies that the amplifier can operate over a wider range of frequencies while maintaining a consistent level of amplification. Designers often consider this parameter when selecting components for applications that require specific bandwidth and gain requirements.
3MHz - Max I/O Voltage
Max I/O Voltage refers to the maximum input/output voltage that an electronic component can safely handle without causing damage. This parameter is crucial for ensuring the proper functioning and longevity of the component. Exceeding the specified maximum I/O voltage can lead to electrical overstress, which may result in permanent damage or failure of the component. It is important to carefully adhere to the manufacturer's guidelines and specifications to prevent any potential issues related to voltage levels.
6mV - Power
Power in electronic components refers to the rate at which electrical energy is transferred or converted by a device. It is typically measured in watts and can be calculated using the formula Power equals voltage multiplied by current. In circuits, power can represent the energy consumed by devices such as resistors, or the energy output by sources like batteries. Understanding power is crucial for ensuring components operate within safe limits and for designing efficient electronic systems.
NO - Height5.08mm
- Length9.81mm
- Width6.35mm
- Thickness
Thickness in electronic components refers to the measurement of how thick a particular material or layer is within the component structure. It can pertain to various aspects, such as the thickness of a substrate, a dielectric layer, or conductive traces. This parameter is crucial as it impacts the electrical, mechanical, and thermal properties of the component, influencing its performance and reliability in electronic circuits.
3.9mm - REACH SVHC
The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.
No SVHC - Radiation Hardening
Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.
No - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
ROHS3 Compliant - Lead Free
Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.
Lead Free
Parts with Similar Specs
- ImagePart NumberManufacturerPackage / CaseNumber of PinsSlew RateInput Offset Voltage (Vos)Common Mode Rejection RatioOperating Supply CurrentNumber of TerminationsMicropowerView Compare
RC4558P
8-DIP (0.300, 7.62mm)
8
1.7V/μs
6 mV
70 dB
2.5 mA
8
NO
8-DIP (0.300, 7.62mm)
8
1.7V/μs
500 μV
70 dB
2.5 mA
8
NO
PDIP
8
13 V/μs
6 mV
75 dB
1.4 mA
8
NO
PDIP
8
1.7 V/μs
6 mV
70 dB
2.5 mA
8
NO
RC4558P Functional Block Diagram
RC4558P Typical Application
Differential signals are required in several applications. On a single 15-V supply, the following circuit converts a single-ended input of 2 V to 10 V into a differential output of 8 V. To maximize linearity, the output range has been purposefully constrained. There are two amplifiers in the circuit. One amplifier serves as a buffer, generating the voltage VOUT+. To generate VOUT–, the second amplifier inverts the input and adds a reference voltage. VOUT+ and VOUT– have a voltage range of 2 to 10 volts. The difference between VOUT+ and VOUT– is known as VDIFF .

Schematic for Single-Ended Input to Differential Output Conversion
The design requirements are as follows:
• Supply voltage: 15 V
• Reference voltage: 12V
• Input: 2 V to 10 V
• Output differential: ±8 V
RC4558P Noninverting Amplifier Schematic
RC4558P Layout
Use good PCB layout practices for the device's optimal operating performance, such as:
• Noise can enter analog circuitry through the circuit's overall power pins and the operational amplifier. Bypass capacitors provide low impedance power sources close to the analog circuitry, reducing coupling noise.
— Place low-ESR, 0.1-μF ceramic bypass capacitors as close to the device as possible between each supply pin and ground. For single-supply applications, a single bypass capacitor from V+ to ground is sufficient.
• One of the simplest and most effective methods of noise suppression is to separate the analog and digital sections of the circuitry. Ground planes are frequently dedicated to one or more layers on multilayer PCBs . A ground plane aids in the distribution of heat and the reduction of EMI noise pickup. Make sure that the digital and analog grounds are physically separated, and that the ground current is flowing in the right direction. Refer to Circuit Board Layout Techniques for further details (SLOA089).
• Run the input lines as far away from the supply or output traces as feasible to reduce parasitic coupling. If keeping them separate isn't practicable, it's far better to cross the sensitive trace perpendicular to the loud trace rather than parallel to it.
• Keep the external components as close as possible to the device. As seen in Layout Example, keeping RF and RG close to the inverting input reduces parasitic capacitance.
• As much as possible, keep input traces short. Always keep in mind that the circuit's input traces are the most vulnerable.
• Consider encircling the important traces with a driven, low-impedance protection ring. A guard ring can reduce leakage currents from surrounding traces with varying potentials greatly.

Operational Amplifier Schematic for Noninverting Configuration

Operational Amplifier Board Layout for Noninverting Configuration
RC4558P Applications
• DVD Recorders and Players
• Pro Audio Mixers
RC4558P Package
RC4558P Manufacturer
Texas Instruments Incorporated (TI) is an American technology corporation based in Dallas, Texas, that creates and manufactures semiconductors and integrated circuits for electronic designers and manufacturers around the world. Based on sales volume, it is one of the top ten semiconductor businesses in the world. Analog chips and embedded processors, which account for more than 80% of the company's revenue, are the company's main focus. TI also makes calculators, microcontrollers, and multi-core processors, as well as TI digital light processing technologies and education technology.
Trend Analysis
Datasheet PDF
- Datasheets :
RC4558P-Texas-Instruments-datasheet-81472256.pdf
RC4558P-Texas-Instruments-datasheet-20723.pdf
RC4558P-Texas-Instruments-datasheet-14137623.pdf
RC4558P-Texas-Instruments-datasheet-151357.pdf
RC4558P-Texas-Instruments-datasheet-5395492.pdf
RC4558P-Texas-Instruments-datasheet-17597776.pdf
RC4558P-Texas-Instruments-datasheet-7268156.pdf
RC4558P-Texas-Instruments-datasheet-66748.pdf
- PCN Design/Specification :
What is operational amplifier?
An operational amplifier is an integrated circuit that can amplify weak electric signals. An operational amplifier has two input pins and one output pin. Its basic role is to amplify and output the voltage difference between the two input pins.
What is operational amplifier and its types?
Op-amps can be classified into 3 main types based on the input/output voltage range: Dual Supply, Single-Supply, and Rail-to-Rail.
What is the exception to the RC4558P?
Offset null capabilities.
Why is the RC4558P suited for voltage-follower applications?
Wide common-mode input voltage range and lack of latch-up.
What type of protection is built in?
Short-circuit protection
ATMEGA8-16PU 8-bit Microcontroller: Circuit, Pinout, and Datasheet11 February 202210834
AD202 2000V Isolation Amplifier: Datasheet, Pinout, and Performance Deep Dive03 March 202619
Advantech Corp 96MPXE-2.6-19M36: A Comprehensive Guide to the Discontinued Skylake Microprocessor Module07 March 2024484
2N3904 NPN Transistor:Pinout, Datasheet and Circuit07 July 202117475
LME49600 Audio Buffer: Datasheet, Pinout and Schematic31 August 20212455
BTA12 Triacs: Features, Pinout, and Datasheet [Video&FAQ]04 December 202114771
LMR400 VS LMR300: Which one to choose?|LMR® -400 VS LMR® -30012 June 20248877
The Comprehensive Introduction to SS14 Diode [Video]02 September 20226293
Solar Inverter: Definition, Types and Costs01 February 20215588
Low Temperature Drift Resistors Increase the Accuracy of Analog Circuits11 February 20251105
What is a Monostable Multivibrator?16 January 20216253
Types, Structure, and Packages of Integrated Circuits23 October 202512301
What is a USB Type-C Connector?28 October 20255580
Development Board History and Differences from Single Board Computers (SBCs)16 May 20225533
Several Steps to Choose a Microcontroller MCU17 June 20224255
BYD Semiconductor Terminates IPO Application for the Fourth Time22 February 20233571
Texas Instruments
In Stock: 342