SR621SW Silver Oxide Watch Battery 1.55V, 23 mAh : SR621SW VS SR626SW, Datasheet and Equivalents
BATTERY SLVR OX 1.55V COIN 6.8MM
The SR621SW is a Silver-Oxide cell that is commonly used in timepieces. This article is going to talk about more detailed information about SR621SW.

How To Change A Watch Battery - Watch and Learn #43
Overview of SR621SW
The SR621SW is a Silver-Oxide cell that is commonly used in timepieces and has a 5-year shelf life. Calculators, film cameras, medical instruments, cash registers, and FA instruments are examples of other applications (measuring instruments, onboard microcomputers, sensors). This is a low-drain "SW" battery. Low-drain batteries are ideal for devices that require a tiny amount of power over a long period of time, such as analog timepieces, TV remote controls, and alarm clocks. This is in contrast to high-drain batteries, which are used in devices with constant low power consumption and occasional high peaks, such as analog and digital watches with additional functions (backlight, alarm), pocket calculators, electronic games, cameras, and so on. Specifications Chemistry: Oxide of silver 1.55V voltage 6.8 mm in diameter Dimensions: 2.2 mm Dimensions: 2.2 mm Dimensions: 2.2 mm Low-Drainage Style.
SR621SW Dimensions

SR621SW Dimensions
Specifications
- TypeParameter
- Factory Lead Time14 Weeks
- Weight0.32g
- Voltage Rated
RATED voltage is the voltage on the nameplate - the "design point" for maximum power throughput and safe thermal operation.
1.55V - Size / Dimension
In electronic components, the parameter "Size / Dimension" refers to the physical dimensions of the component, such as its length, width, and height. These dimensions are crucial for determining how the component will fit into a circuit or system, as well as for ensuring compatibility with other components and the overall design requirements. The size of a component can also impact its performance characteristics, thermal properties, and overall functionality within a given application. Engineers and designers must carefully consider the size and dimensions of electronic components to ensure proper integration and functionality within their designs.
0.27Dia x 0.08 H 6.8mmx2.0mm - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
Not Applicable - Termination Style
"Termination style" in electronic components refers to the method used to connect the component to a circuit board or other electronic devices. It determines how the component's leads or terminals are designed for soldering or mounting onto the circuit board. Common termination styles include through-hole, surface mount, and wire lead terminations.Through-hole components have leads that are inserted through holes in the circuit board and soldered on the other side. Surface mount components have flat terminals that are soldered directly onto the surface of the circuit board. Wire lead terminations involve attaching wires to the component for connection.The choice of termination style depends on factors such as the type of component, the manufacturing process, and the space available on the circuit board. Different termination styles offer various advantages in terms of ease of assembly, reliability, and space efficiency in electronic designs.
Requires Holder - Battery Chemistry
A battery is a device that stores chemical energy, and converts it to electricity. This is known as electrochemistry and the system that underpins a battery is called an electrochemical cell. A battery can be made up of one or several (like in Volta's original pile) electrochemical cells.
Silver Oxide - Battery Cell Size
The most common lithium-ion cell is the 18650 (the numbers define the physical dimensions and shape as follows: 18mm in diameter, 65mm long and the 0 means it has a round cross-section) which is due to its widespread use in laptop battery packs.
Coin 6.8mm - Capacity
In electronic components, "Capacity" typically refers to the maximum amount of electrical charge that a component can store. It is measured in units called farads (F). Capacitors are the most common components that have a capacity rating. The capacity of a capacitor determines how much energy it can store and release when connected in a circuit. Higher capacity capacitors can store more charge and are often used in applications requiring larger energy storage or filtering capabilities. It is important to select a capacitor with the appropriate capacity to ensure proper functioning of the circuit.
23mAh - Discharge Rate
The "Discharge Rate" in electronic components refers to the rate at which a component can release stored energy or power. This parameter is particularly important in devices that use batteries or capacitors, as it determines how quickly these components can discharge their stored energy. A high discharge rate means that the component can release energy quickly, while a low discharge rate indicates a slower release of energy. Understanding the discharge rate of electronic components is crucial for designing circuits and systems that require specific power delivery characteristics.
40μA - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
ROHS3 Compliant
SR621SW Electrical Characteristics

SR621SW Electrical Characteristics
SR621SW Applications
Timepieces
TV remote controls
Alarm clocks
Pocket calculators
Electronic games
Cameras
SR621SW VS SR626SW
| SR621SW | SR626SW | |
| Weight | 0.32g | 0.39g |
| Capacity | 23mAh | 28mAh |
| Size / Dimension | 0.27Dia x 0.08 H 6.8mmx2.0mm | 0.27Dia x 0.10 H 6.8mmx2.6mm |
| Images | ![]() |
|
Conclusions of SR621SW VS SR626SW:
The SR626SW and SR621SW batteries are only 0.5 mm apart in height, which isn't much; however, while battery compartments designed for SR626SW batteries may accommodate smaller SR621SW batteries, contact with the SR621SW battery may not be completely dependable. Because the SR621SW is the same width as the SR626SW, it will fit in the battery slot perfectly, but it will be somewhat shorter. The SR626W was a silver oxide battery meant for high drain use in older LED digital watches, while the SR626SW is a less expensive alkaline battery designed for newer low drain watches.
SR621SW Equivalents
SR60
280-34
D364
SB-AG
SB-DG
TR621SW
Warnings about SR621SW
Forbid short-circuit, charge between”+” and”-“.
Forbid over-discharge, fire, damage.
Finish sealing less more than 5 seconds at 200 C~250 C;
Take out the battery when discharging to cut-off voltage, and embed it under the ground or jump in the deep water.
SR621SW Manufacturer
Seiko Instruments Inc. (SII) was founded in 1937 as the Seiko Group's primary watch manufacturer. The company provides micro mechatronics products and services, such as watch and HDD components, semiconductors, FPD and electronic devices, network solutions systems, nanotechnology equipment, scientific instruments, and large-format inkjet printers, based on sophisticated micro mechatronics and nanotechnology techniques developed through decades of experience in precision machinery manufacturing and low-power consumption technologies.
Datasheet PDF
- Datasheets :
- MSDS Material Safety Datasheet :
Popularity by Region
What battery replaces SR621SW?
364 Battery is a direct replacement for SR621SW, SR60, SR621, SB-AG/DG, 280-34, T, V364, D364, 602, S621E, GP364, AG1, AG-1, 364, L621, LR621, SG1, LR60, LR620, SW621, GP164, 364X, 364A, AG1/364A, SB-AG, E364 batteries.
What’s the Impedance of SR621SW?
5 to 15 ohms.
What’s the Nominal Voltage of SR621SW?
1.55 Volts.
What’s the capacity of SR621SW?
23mAh.
What’s the Discharge Rate of SR621SW?
40μA.
What’s the battery material of SR621SW?
Silver Oxide.
SG3524 Modulators: Price, Circuit and Pinout19 July 20216014
LM3671MF-2.8 DC-DC converter: Pinout, Specification, and Datasheet24 June 20211904
LM334D Adjustable Current Source: Feature, Specification, and Datasheet03 July 2021789
LM340 Voltage Regulator: Datasheet, Pinout and Circuit28 September 20216845
ATMEGA168 Microcontrollers: Features, Pinout, and Datasheet07 December 20218312
STM8L151G6U6 vs STM8L152K4: Complete Microcontroller Comparison11 June 2025118
How to Utilize the TLP250 Isolated MOSFET Driver?10 March 202219223
UC3842 PWM controller: Datasheet, Application, Circuit19 October 202166614
Amkor Technology to Invest $2 Billion in Semiconductor Testing Plant in Peoria, Creating 2,000 Jobs11 December 20234077
Automatic Voltage Regulator: Ultimate Guide to Stable Power and Equipment Protection06 May 20257590
Huawei Responded How to Solve the Problem of Chip Supply29 March 20224055
What are the Applications of Filters?17 January 202616122
Global Semiconductor Market Share Continues to Grow27 October 20231934
What Are Wi-Fi Modules and Their Uses in IoT Today04 June 20252370
What are TPMS Sensors?21 November 20204662
Beginners Guide to FPGA Design29 December 2021946
Seiko Instruments
In Stock