The Rj9 VS Rj11 Connectors-Who is the winner?

Sophie

Published: 26 March 2022 | Last Updated: 26 March 2022

19203

RJ11-2L-S

RJ11-2L-S

TE Connectivity Corcom Filters

L Jack Bulk Unshielded 6p2c (RJ11) 1 Port 90° Angle (Right) Solder Through Hole

Purchase Guide

L Jack Bulk Unshielded 6p2c (RJ11) 1 Port 90° Angle (Right) Solder Through Hole

The purpose of these two little gadgets is to connect phone cables to networks. They may appear to be similar, yet there are several differences that distinguish them. This article is going to find their differences separately and decide the winner.

This is an Instructional Video showing you how to Install RJLOCKDOWNS RJ12 RJ11 RJ9 Patch Lock Telephone Cord Hand Set CordLock.

RJ12 RJ11 RJ9 Patch Lock Telephone Cord Hand Set Cord made by RJLOCKDOWN

Introduction


Most of the time, when we pick up the phone to make a call, we don't consider the intricate intricacies that allow us to do so. Connectors, for example, are relatively little devices, yet they are quite important. Different connectors exist for various cables, including Ethernet cablestelephone lines, and modems.

There are two configuration variants for the Rj11, which are most typically used for telephone and modem connections. The Rj9  connector isn't something you'll come across every day. It is sometimes referred to as the Rj10  or Rj22, and it has its own configuration type.


Overview of Rj9

rj9.jpg

This connector has a compact square design and is widely used. It's composed of tough plastic, so it'll endure a long time. The material utilized is interesting because it is see-through, which makes for an aesthetically appealing device. This connector is available in two different configurations.

The 6P2C  connection is the first configuration type. There are 6   locations and 2  connecting points on this gadget. The conductors are the components that make contact with the copper wires and hence are the connection sites. The Rj11 connector in this configuration type can only send data at slow speeds. It's a device that connects phone lines.


Overview of Rj11

rj11.jpg

There's a lot of misunderstanding about this connector. It's sometimes referred to as the Rj10, and it's also known as the Rj22. Because all of these connector types have comparable dimensions and configurations, this is the case.

This connector has a rectangular shape rather than a square shape. It measures 7.6  mm in width, making it slightly smaller than the Rj11   connector,  It does, however, have a very comparable build. It's made of clear plastic that's both robust and durable. The connection of wires is exposed by this plastic.

The 4P4C   configuration of this connection is identical to that of the Rj10  and Rj22.  which is why they are regarded as the same. It has four places and four connection points, according to its arrangement. It's perfect for securing phone handset cords.


Rj9 VS. Rj11

The key distinction between RJ9  and RJ11  is that the RJ9  is only available in one configuration, namely the 4  P4C connection typeRJ11, on the other hand, has two different configurations. The connection types are 6  P2C and 6P4C, respectively.

Differences between Rj9 and Rj11

Parameters of Comparison
Rj9Rj11
FunctionalityTelephone handset cablesPhones and modem cables
Configuration4p4C Configuration6p2C/64pC Configuration
Shape and structureRectangular Square
sizeRj9 is smaller in comparison to Rj11.Rj11 is bigger in size.
VersatilityLess as it has only one configuration type to connect.More versatile as it comes with two configuration types.


Pros and Cons of Rj9 and Rj11

RJ11

Pros

It has two configuration types

It is made with durable material

It is aesthetically pleasing

It is easy to attach and terminate

Its pins are gold coated to prevent rusting


Cons

It may not be ideal for heavy transmissions and cables with many wires


RJ9

Pros

It is made with durable see-through plastic

It has pins that are gold and nickel coated to prevent them from rusting

It is aesthetically appealing

It is easy to attach and terminate


Cons

It can only take 4 wires at a time


Conclusion

The fact that the Rj11  and Rj9  are connections designed for distinct uses makes determining which is superior nearly difficult. The Rj11, on the other hand, appears to be a more planned connector because it comes in two different builds with two different configuration options. This increases the connector's adaptability by allowing it to connect to a wider range of cables. As a result, it stands out as the superior performer.

Frequently Asked Questions

What is RJ9 used for?

The RJ9 connector is used for telephone handset cables, while the RJ12 connector is used in system phones. The 4P4C connector on RJ9 is different from the 6P6C connector on RJ12. Registered Jack 9 is abbreviated as RJ9.

What is the connector on a phone handset?

The four-position four-conductor (4P4C) connection is sometimes referred to as a handset connector since it is used on both ends of telephone handset cords. Because it was not designed to connect directly to telephone lines, this handset connector is not a registered jack.

What kind of connectors does the RJ9 have?

The Rj9 has only one connector type, 4P4C, which means it has four positions and four connection points, making it perfect for connecting phone lines. Because phone handsets/headsets aren't always directly associated with the government, they don't have a unique enlisted jack code.

Are RJ9 and RJ11 the same size?

Rj9 is smaller in comparison to Rj11. Rj11 is bigger in size. There are fewer because there is only one configuration type to connect.

Is it possible to utilize RJ9 instead of RJ11?

RJ12 and RJ11 are backward compatible, although RJ11 will not operate with RJ12. RJ9 or RJ22 connectors are used in coiled handset wires (both names refer to the same thing). These have four conductors and are physically smaller than RJ11/RJ12.
RJ11-2L-S

TE Connectivity Corcom Filters

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More
  • RJ45-8X
    RJ45-8X

    TE Connectivity Corcom Filters