TL082 JFET Dual Op-Amp: Where & How to Use TL082?

Sophie

Published: 08 December 2021 | Last Updated: 08 December 2021

12335

TL082CDT

TL082CDT

STMicroelectronics

2 Channels 40mA per Channel 20pA 70 dB Instrumentational OP Amps 18V 6V~36V ±3V~18V TL082 8 Pins 8-SOIC (0.154, 3.90mm Width)

Purchase Guide

2 Channels 40mA per Channel 20pA 70 dB Instrumentational OP Amps 18V 6V~36V ±3V~18V TL082 8 Pins 8-SOIC (0.154, 3.90mm Width)

The TL082 is high speed JFET input dual operational amplifier incorporating well-matched, high voltage JFET and bipolar transistors in a monolithic integrated circuit. This device features high slew rates, low input bias and offset current, and low offset voltage temperature coefficient. Furthermore, Huge range of Semiconductors, Capacitors, Resistors and IcS in stock. Welcome RFQ.

This video shows that a really easy circuit to make with an op amp, even with a dual power supply.

Dual supply op amp voltage follower circuit using TL082 electronics tutorial

TL082 Pinout

Pinout.png

Pinout


TL082 Pinout.png

TL082 Pinout


TL082 CAD Model

PCB Symbol.png

PCB Symbol

PCB Footprint.png

PCB Footprint

3D Model.png

3D Model


TL082 Overview

The TL082 Op-Amp is a low cost, high speed, dual JFET input operational amplifier with an internally trimmed input offset voltage. This device requires a low supply current yet maintains a large gain bandwidth product and fast slew rate. In addition, well-matched high voltage JFET input devices provide very low input bias and offset currents. The TL082 is high speed JFET input dual operational amplifier incorporating well-matched, high voltage JFET and bipolar transistors in a monolithic integrated circuit. This device features high slew rates, low input bias and offset current, and low offset voltage temperature coefficient.

This article provides you with a basic overview of the TL082 JFET Dual Operation Amplifier, including its pin descriptions, features and specifications, etc., to help you quickly understand what TL082 is.


TL082 Features

● Wide common-mode (up to VCC+) and differential voltage range

● Low input bias and offset current

● Output short-circuit protection

● High input impedance JFET input stage

● Internal frequency compensation

● Latch up free operation

● High slew rate: 16 V/µs (typical)


Specifications

STMicroelectronics TL082CDT technical specifications, attributes, parameters and parts with similar specifications to STMicroelectronics TL082CDT.
  • Type
    Parameter
  • Lifecycle Status

    Lifecycle Status refers to the current stage of an electronic component in its product life cycle, indicating whether it is active, obsolete, or transitioning between these states. An active status means the component is in production and available for purchase. An obsolete status indicates that the component is no longer being manufactured or supported, and manufacturers typically provide a limited time frame for support. Understanding the lifecycle status is crucial for design engineers to ensure continuity and reliability in their projects.

    ACTIVE (Last Updated: 6 months ago)
  • Factory Lead Time
    10 Weeks
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    Surface Mount
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    8-SOIC (0.154, 3.90mm Width)
  • Number of Pins
    8
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    0°C~70°C
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Cut Tape (CT)
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e3
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    8
  • ECCN Code

    An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.

    EAR99
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Matte Tin (Sn) - annealed
  • Packing Method

    The packing method in electronic components refers to the technique used to package and protect the component during shipping and handling. It encompasses various forms including tape and reel, tray, tube, or bulk packaging, each suited for different types of components and manufacturing processes. The choice of packing method can affect the ease of handling, storage, and the efficiency of assembly in automated processes. Additionally, it plays a crucial role in ensuring the reliability and integrity of the components until they are used in electronic devices.

    TR
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    DUAL
  • Terminal Form

    Occurring at or forming the end of a series, succession, or the like; closing; concluding.

    GULL WING
  • Peak Reflow Temperature (Cel)

    Peak Reflow Temperature (Cel) is a parameter that specifies the maximum temperature at which an electronic component can be exposed during the reflow soldering process. Reflow soldering is a common method used to attach electronic components to a circuit board. The Peak Reflow Temperature is crucial because it ensures that the component is not damaged or degraded during the soldering process. Exceeding the specified Peak Reflow Temperature can lead to issues such as component failure, reduced performance, or even permanent damage to the component. It is important for manufacturers and assemblers to adhere to the recommended Peak Reflow Temperature to ensure the reliability and functionality of the electronic components.

    260
  • Number of Functions
    2
  • Supply Voltage

    Supply voltage refers to the electrical potential difference provided to an electronic component or circuit. It is crucial for the proper operation of devices, as it powers their functions and determines performance characteristics. The supply voltage must be within specified limits to ensure reliability and prevent damage to components. Different electronic devices have specific supply voltage requirements, which can vary widely depending on their design and intended application.

    15V
  • Time@Peak Reflow Temperature-Max (s)

    Time@Peak Reflow Temperature-Max (s) refers to the maximum duration that an electronic component can be exposed to the peak reflow temperature during the soldering process, which is crucial for ensuring reliable solder joint formation without damaging the component.

    30
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    TL082
  • Pin Count

    a count of all of the component leads (or pins)

    8
  • Operating Supply Voltage

    The voltage level by which an electrical system is designated and to which certain operating characteristics of the system are related.

    18V
  • Power Supplies

    an electronic circuit that converts the voltage of an alternating current (AC) into a direct current (DC) voltage.?

    +-15V
  • Number of Channels
    2
  • Operating Supply Current

    Operating Supply Current, also known as supply current or quiescent current, is a crucial parameter in electronic components that indicates the amount of current required for the device to operate under normal conditions. It represents the current drawn by the component from the power supply while it is functioning. This parameter is important for determining the power consumption of the component and is typically specified in datasheets to help designers calculate the overall power requirements of their circuits. Understanding the operating supply current is essential for ensuring proper functionality and efficiency of electronic systems.

    1.4mA
  • Nominal Supply Current

    Nominal current is the same as the rated current. It is the current drawn by the motor while delivering rated mechanical output at its shaft.

    2.5mA
  • Power Dissipation

    the process by which an electronic or electrical device produces heat (energy loss or waste) as an undesirable derivative of its primary action.

    680mW
  • Output Current

    The rated output current is the maximum load current that a power supply can provide at a specified ambient temperature. A power supply can never provide more current that it's rated output current unless there is a fault, such as short circuit at the load.

    40mA
  • Slew Rate

    the maximum rate of output voltage change per unit time.

    16V/μs
  • Architecture

    In electronic components, the parameter "Architecture" refers to the overall design and structure of the component. It encompasses the arrangement of internal components, the layout of circuitry, and the physical form of the component. The architecture of an electronic component plays a crucial role in determining its functionality, performance, and compatibility with other components in a system. Different architectures can result in variations in power consumption, speed, size, and other key characteristics of the component. Designers often consider the architecture of electronic components carefully to ensure optimal performance and integration within a larger system.

    VOLTAGE-FEEDBACK
  • Amplifier Type

    Amplifier Type refers to the classification or categorization of amplifiers based on their design, functionality, and characteristics. Amplifiers are electronic devices that increase the amplitude of a signal, such as voltage or current. The type of amplifier determines its specific application, performance capabilities, and operating characteristics. Common types of amplifiers include operational amplifiers (op-amps), power amplifiers, audio amplifiers, and radio frequency (RF) amplifiers. Understanding the amplifier type is crucial for selecting the right component for a particular circuit or system design.

    J-FET
  • Common Mode Rejection Ratio

    Common Mode Rejection Ratio (CMRR) is a measure of the ability of a differential amplifier to reject input signals that are common to both input terminals. It is defined as the ratio of the differential gain to the common mode gain. A high CMRR indicates that the amplifier can effectively eliminate noise and interference that affects both inputs simultaneously, enhancing the fidelity of the amplified signal. CMRR is typically expressed in decibels (dB), with higher values representing better performance in rejecting common mode signals.

    70 dB
  • Current - Input Bias

    The parameter "Current - Input Bias" in electronic components refers to the amount of current required at the input terminal of a device to maintain proper operation. It is a crucial specification as it determines the minimum input current needed for the component to function correctly. Input bias current can affect the performance and accuracy of the device, especially in precision applications where small signal levels are involved. It is typically specified in datasheets for operational amplifiers, transistors, and other semiconductor devices to provide users with important information for circuit design and analysis.

    20pA
  • Voltage - Supply, Single/Dual (±)

    The parameter "Voltage - Supply, Single/Dual (±)" in electronic components refers to the power supply voltage required for the proper operation of the component. This parameter indicates whether the component requires a single power supply voltage (e.g., 5V) or a dual power supply voltage (e.g., ±15V). For components that require a single power supply voltage, only one voltage level is needed for operation. On the other hand, components that require a dual power supply voltage need both positive and negative voltage levels to function correctly.Understanding the voltage supply requirements of electronic components is crucial for designing and integrating them into circuits to ensure proper functionality and prevent damage due to incorrect voltage levels.

    6V~36V ±3V~18V
  • Output Current per Channel

    Output Current per Channel is a specification commonly found in electronic components such as amplifiers, audio interfaces, and power supplies. It refers to the maximum amount of electrical current that can be delivered by each individual output channel of the component. This parameter is important because it determines the capacity of the component to drive connected devices or loads. A higher output current per channel means the component can deliver more power to connected devices, while a lower output current may limit the performance or functionality of the component in certain applications. It is crucial to consider the output current per channel when selecting electronic components to ensure they can meet the power requirements of the intended system or setup.

    40mA
  • Input Offset Voltage (Vos)

    Input Offset Voltage (Vos) is a key parameter in electronic components, particularly in operational amplifiers. It refers to the voltage difference that must be applied between the two input terminals of the amplifier to nullify the output voltage when the input terminals are shorted together. In simpler terms, it represents the voltage required to bring the output of the amplifier to zero when there is no input signal present. Vos is an important parameter as it can introduce errors in the output signal of the amplifier, especially in precision applications where accuracy is crucial. Minimizing Vos is essential to ensure the amplifier operates with high precision and accuracy.

    10mV
  • Neg Supply Voltage-Nom (Vsup)

    The parameter "Neg Supply Voltage-Nom (Vsup)" in electronic components refers to the nominal negative supply voltage that the component requires to operate within its specified performance characteristics. This parameter indicates the minimum voltage level that must be provided to the component's negative supply pin for proper functionality. It is important to ensure that the negative supply voltage provided to the component does not exceed the maximum specified value to prevent damage or malfunction. Understanding and adhering to the specified negative supply voltage requirements is crucial for the reliable operation of the electronic component in a circuit.

    -15V
  • Unity Gain BW-Nom

    Unity Gain Bandwidth, often abbreviated as Unity Gain BW or UGBW, refers to the frequency at which an amplifier can provide a gain of one (0 dB). It is a critical parameter in assessing the performance of operational amplifiers and other amplifying devices, indicating the range of frequencies over which the amplifier can operate without distortion. Unity Gain BW is particularly important in applications where signal fidelity is crucial, as it helps determine the maximum frequency of operation for a given gain level. As the gain is reduced, the bandwidth typically increases, ensuring that the amplifier can still operate effectively across various signal frequencies.

    4000 kHz
  • Voltage Gain

    Voltage gain is a measure of how much an electronic component or circuit amplifies an input voltage signal to produce an output voltage signal. It is typically expressed as a ratio or in decibels (dB). A higher voltage gain indicates a greater amplification of the input signal. Voltage gain is an important parameter in amplifiers, where it determines the level of amplification provided by the circuit. It is calculated by dividing the output voltage by the input voltage and is a key factor in determining the overall performance and functionality of electronic devices.

    106.02dB
  • Low-Offset

    Low-offset is a parameter used to describe the level of offset voltage in electronic components, particularly in operational amplifiers. Offset voltage refers to the small voltage difference that exists between the input terminals of the amplifier when the input voltage is zero. A low-offset value indicates that this voltage difference is minimal, which is desirable for accurate signal processing and amplification. Components with low-offset specifications are preferred in applications where precision and accuracy are critical, such as in instrumentation and measurement systems. Minimizing offset voltage helps reduce errors and ensures the faithful reproduction of input signals by the amplifier.

    NO
  • Frequency Compensation

    Frequency compensation is implemented by modifying the gain and phase characteristics of the amplifier's open loop output or of its feedback network, or both, in such a way as to avoid the conditions leading to oscillation. This is usually done by the internal or external use of resistance-capacitance networks.

    YES
  • Voltage - Input Offset

    Voltage - Input Offset is a parameter that refers to the difference in voltage between the input terminals of an electronic component, such as an operational amplifier, when the input voltage is zero. It is an important characteristic that can affect the accuracy and performance of the component in various applications. A low input offset voltage is desirable as it indicates that the component will have minimal error in its output when the input signal is near zero. Manufacturers typically provide this specification in the component's datasheet to help users understand the component's behavior and make informed decisions when designing circuits.

    3mV
  • Low-Bias

    Low-bias in electronic components refers to a design or configuration that minimizes the amount of bias current flowing through the component. Bias current is a small, steady current that is used to establish the operating point of a component, such as a transistor or amplifier. By reducing the bias current to a low level, the component can operate with lower power consumption and potentially lower distortion. Low-bias components are often used in applications where power efficiency and signal fidelity are important, such as in audio amplifiers or battery-powered devices. Overall, the low-bias parameter indicates the ability of the component to operate efficiently and accurately with minimal bias current.

    YES
  • Bias Current-Max (IIB) @25C

    The parameter "Bias Current-Max (IIB) @25C" in electronic components refers to the maximum input bias current that the component can handle at a specified temperature of 25 degrees Celsius. Bias current is the current flowing into the input terminal of a device when no signal is applied. This parameter is important because excessive bias current can affect the performance and stability of the component, leading to potential issues such as distortion or offset errors in the output signal. By specifying the maximum bias current allowed at a certain temperature, manufacturers provide users with important information to ensure proper operation and reliability of the component in their circuit designs.

    0.0004μA
  • Dual Supply Voltage

    Dual Supply Voltage refers to an electronic component's requirement for two separate power supply voltages, typically one positive and one negative. This configuration is commonly used in operational amplifiers, analog circuits, and certain digital devices to allow for greater signal handling capabilities and improved performance. The use of dual supply voltages enables the device to process bipolar signals, thereby enhancing its functionality in various applications.

    9V
  • Input Offset Current-Max (IIO)

    Input Offset Current-Max (IIO) is a parameter that describes the maximum difference in input bias currents between two input terminals of an electronic component, such as an operational amplifier. Input offset current can cause errors in the output of the component, especially in precision applications where accuracy is crucial. The IIO specification provides a limit on the maximum allowable difference in input currents to ensure that the component operates within its specified performance range. Designers need to consider the IIO value when selecting components and designing circuits to minimize errors and ensure reliable operation.

    0.01μA
  • Height
    1.25mm
  • Length
    4.9mm
  • Width
    3.9mm
  • REACH SVHC

    The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.

    No SVHC
  • Radiation Hardening

    Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.

    No
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
  • Lead Free

    Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.

    Lead Free
0 Similar Products Remaining

TL082 Functional Block Diagram

Schematic diagram.png

Schematic diagram


TL082 Equivalent

     Model number                             Manufacturer                                       Description
TL082IPTSTMicroelectronicsJFET inputs, low input bias current
NJM2162DNew Japan Radio Co LtdOperational Amplifier, 2 Func, 15000uV Offset-Max, BIPolar, PDIP8, DIP-8
TL072IDTexas InstrumentsDual, 30-V, 3-MHz, high slew rate (13-V/µs), In to V+, JFET-input op amp 8-SOIC -40 to 85
MC34002DRochester Electronics LLCDUAL OP-AMP, 13000uV OFFSET-MAX, 4MHz BAND WIDTH, PDSO8, PLASTIC, SO-8
LF353HNational Semiconductor CorporationIC DUAL OP-AMP, 13000 uV OFFSET-MAX, 4 MHz BAND WIDTH, MBCY8, METAL CAN-8, Operational Amplifier
LF253HSTMicroelectronicsDUAL OP-AMP, 13000uV OFFSET-MAX, 4MHz BAND WIDTH, MBCY8, TO-99, 8 PIN
TL072MNSTMicroelectronicsDUAL OP-AMP, 13000uV OFFSET-MAX, 4MHz BAND WIDTH, PDIP8, ROHS COMPLIANT, PLASTIC, DIP-8
TL082CHSTMicroelectronicsDUAL OP-AMP, 13000uV OFFSET-MAX, 4MHz BAND WIDTH, MBCY8, TO-99, 8 PIN
TL082IDTexas InstrumentsDual, 30-V, 3-MHz, 13-V/µs slew rate, In to V+, JFET-input op amp 8-SOIC -40 to 85
NJM2162MNew Japan Radio Co LtdOperational Amplifier, 2 Func, 15000uV Offset-Max, BIPolar, PDSO8, DMP-8


Where to use TL082 Op-Amp?

The TL082 is a Dual Package Operational Amplifier, meaning it has two Op-Amps inside it and each Op-Amp can be used independently.

Pin connections (top view).png

The main distinguishing feature of the TL082 Op-Amp is that they incorporate high-voltage JFET and bipolar transistors which helps the transistor to have very high input impedance and low bias current. Also, this Op-Amp has low noise and harmonic distortion making it an ideal choice for audio pre-amplifiers. Other than that, these amplifiers may be used in applications such as high-speed integrators, fast D/A converters, sample and hold circuits and many other circuits requiring low input offset voltage, low input bias current, high input impedance, high slew rate and wide bandwidth. These devices also exhibit low noise and offset voltage drift. So, if you are looking for an Op-Amp IC with Quad package and JFET driven then this IC might be the right choice for you.


How to use TL082 Op-Amp?

TL082 Op-Amp IC can be used for audio pre-amplification and it can provide an edge in terms of sound quality because of its price compared to its specs. As a test, a non-inverting op-amp configuration is shown below.

e24360fa4ef40475b60e37050d7fc33c_TL082-Op-Amp-Circuit-Diagram.jpg

In the above the TL082 Op-amp is configured as a non-inverting configuration. The gain of the op-amp is set to 10. For that we have used a 1K resistor and a 9.1K resistor, as you can see for the simulation, we have used a variable potentiometer. By varying the potentiometer, we can vary the input voltage and the output voltage will also vary, to power the op-amp we have used +12V and -12V supply, as the gain of the op-amp is 10 so if we provide 1V at the input we will get 10V at the output and the simulated circuit shows exactly that.


Parts with Similar Specs

The three parts on the right have similar specifications to STMicroelectronics & TL082CDT.

TL082 Applications

● Circuit requiring high input impedance

● Buffer application

● Filter circuits, Voltage followers

● Integrator, Differentiator, Summer, adder, Voltage follower, etc.

● DC gain blocks

● Comparators (Loop control & regulation)

● Audio Amplifier


TL082 Typical Application

100 kHz quadruple oscillator.png

100 kHz quadruple oscillator


TL082 Parameter Measurement Information

Voltage follower.png

Voltage follower


Gain-of-10 inverting amplifier.png

Gain-of-10 inverting amplifier


TL082 Package

SO8 package outline.png

SO8 package outline


TL082 Manufacturer

STMicroelectronics is a globally recognized semiconductor company. They are dedicated to developing semiconductor solutions for various microelectronics applications. STMicroelectronics enjoys unrivaled silicon and system expertise, strong manufacturing strength, IP portfolio,and solid relationships with their strategic partners. Based on these advantages, STMicroelectronics has become a pioneer in System-on-Chip (SoC) technology and its products has a positive effect in realizing today's convergence trends.


Trend Analysis

Frequently Asked Questions

What is the better supply voltage for TL082?

The power supply voltage of the integrated circuit has been determined during the design. If it exceeds or is too low, it will affect the use effect of the circuit. Here, it mainly affects the stability of the circuit operating point in the integrated circuit. TL082 is a dual op amp integrated circuit, using plus or minus 15V is its best working condition, the deviation of the power supply voltage will affect its stability characteristics. Therefore, it should be used according to the requirements provided by the manufacturer.

What is the difference between TL084 and TL082? Are there any substitutions for each?

TL084 is a four op amp, and TL082 is a dual op amp. The replacement of TL084 is TL064, and the replacement of TL082 is TL062. The power consumption of TL064 and TL062 is lower than that of TL084 and TL082, and the load capacity is also lower, depending on what load you are.

What is the difference between TL082 and LM393?

TL082 is a dual op amp, and LM393 is a dual voltage comparator. There is a difference between the two. LM393 is specially used as a comparator and cannot be used as an op amp. The TL082 is an op amp, and the op amp can also be used as a comparator by principle, but it is not as ideal as a dedicated comparator.

What IC can be used instead of TL082?

TL082 is JFET input. If high input impedance is not required, other dual operational amplifiers can be used instead. Such as NE5532 or TL072. TL072 is a little more precise than TL082, it saves a little power, and only a little bit, there is even no difference. However, it should be noted that the electrical performance of the same model products of different manufacturers are quite different.
TL082CDT

STMicroelectronics

In Stock: 3015000