What is Amplifier?

Amplifier Working ? | Classes A, B, AB, C & D | Technical Difference
Last Updated: November 2025 | This article has been updated to reflect the latest developments in amplifier technology, including advances in optical fiber amplifiers, operational amplifiers, and power amplifier designs.
Topics Covered in This Article:
Ⅰ. Basic Principles of Amplifier Circuits Ⅱ. Basic Characteristics of Amplifiers Ⅲ. Optical Fiber Amplifier Ⅳ. Operational Amplifier Ⅴ. Power Amplifier
An amplifier is a device that uses tubes or transistors, power supplies, transformers, and other electrical components to increase the voltage or power of an input signal. The amplifier's amplification effect is achieved by regulating the energy source with the input signal, while the energy source provides the power consumption required for amplification. Communications, broadcasting, radar, television, automation, and other systems all employ amplifiers extensively.
An amplifier boosts a signal's amplitude or strength, making it a crucial component of signal processing in automation technology applications. The amplification is achieved by controlling the energy source with the input signal. Linear amplifiers produce outputs that are replications and augmentations of the input signal, while nonlinear amplifiers produce outputs that are functions of the input signal.
Ⅰ. Basic Principles of Amplifier Circuits
The term "amplification" refers to the process of passing a weak electrical signal through a device to produce a signal output with the same waveform as the weak signal but significantly higher amplitude. A transistor amplifier circuit accomplishes this function.
The amplifier circuit's amplification effect primarily transfers energy from the DC power supply (VCC) to the output signal. The transistor is the heart of the amplifier circuit. For the amplifier circuit to amplify the input signal effectively, the transistor must operate in the amplifying region.
Transistor amplifier circuits are typically configured in three ways:
Common emitter configuration
Common base configuration
Common collector configuration
Regardless of the amplifying circuit's configuration, the goal is to transmit the input weak signal through the amplifying circuit, where its signal amplitude will be significantly increased at the output.
In electronic technology, the common emitter amplifier circuit is the most extensively used type. The circuit's general structure consists of input coupling, biasing network, transistor amplification stage, and output coupling components.

Figure 1: Common Emitter Amplifier Circuit
Ⅱ. Basic Characteristics of Amplifiers
1. Gain
The gain of an amplifier measures how much it can boost the amplitude of a signal. This parameter is frequently expressed in decibels (dB). Mathematically, gain is defined as the ratio of output amplitude to input amplitude. In 2025, modern amplifiers achieve gains ranging from 20 dB for low-gain applications to over 120 dB for precision instrumentation amplifiers.
2. Output Dynamic Range
The output dynamic range represents the range between the maximum and minimum useful output amplitudes, commonly expressed in decibels (dB). The dynamic range of an amplifier is limited at the lower end by output noise and at the upper end by signal clipping or distortion. Contemporary high-performance amplifiers can achieve dynamic ranges exceeding 140 dB.
3. Bandwidth and Rise Time
Bandwidth: The difference between the low-frequency and high-frequency half-power points (-3dB points) defines an amplifier's bandwidth (BW). For example, a quality audio amplifier's -3dB bandwidth typically spans approximately 20 Hz to 20 kHz (the frequency range of normal human hearing). Modern wideband amplifiers used in telecommunications can achieve bandwidths exceeding several GHz.
Rise Time: When a step signal is input, the rise time refers to the time required for the output to change from 10% to 90% of the final output amplitude value. Rise time is inversely proportional to bandwidth.
4. Ideal Frequency Characteristics
In an ideal amplifier, the phase shift is proportional to frequency and the gain remains constant across all frequencies. This means the amplifier provides uniform amplification for signals of different frequencies with minimal phase distortion.
5. Settling Time
Settling time is the duration required for the output amplitude to stabilize within a specified percentage of the final amplitude (typically 0.1% to 1%). This parameter is crucial for high-speed data acquisition and signal processing applications.
6. Efficiency
Efficiency measures the proportion of input energy that is delivered to the amplifier output:
Class A amplifiers: 10-25% efficiency (maximum theoretical: 25%)
Class AB amplifiers: 35-55% efficiency (maximum theoretical: 78.5%)
Class D amplifiers: 85-97% efficiency in modern designs
Class GaN amplifiers (2024-2025): Up to 98% efficiency using gallium nitride technology
Higher efficiency means less heat generation and reduced cooling requirements, which is particularly important in portable and high-power applications.
7. Slew Rate
The slew rate is the maximum rate of change of the output voltage, typically expressed in volts per microsecond (V/μs). Modern high-speed operational amplifiers can achieve slew rates exceeding 10,000 V/μs, enabling them to handle very fast signal transitions.
8. Noise Figure
The noise figure quantifies how much noise the amplification process introduces. It can be measured as the output noise voltage with zero input or calculated from the degradation of the signal-to-noise ratio between input and output. Lower noise figures indicate better performance, with state-of-the-art low-noise amplifiers achieving noise figures below 0.5 dB.
9. Linearity
While perfect linear amplifiers don't exist, real amplifiers maintain linearity within specific limits. Beyond these limits, distortion occurs. Common types of distortion include:
Clipping distortion: Occurs when the output reaches saturation
Crossover distortion: Common in Class B amplifiers
Harmonic distortion: Measured as Total Harmonic Distortion (THD)
Modern high-fidelity amplifiers achieve THD values below 0.001% (0.00001 or -100 dB).
Ⅲ. Optical Fiber Amplifier
The development of optical amplifiers represents a significant milestone in optical fiber communication technology, enabling optical multiplexing, long-distance communication, and all-optical networks. As of 2025, optical amplifiers have become indispensable components in modern telecommunications infrastructure, supporting data rates exceeding 400 Gbps per wavelength channel.
Fiber amplifiers typically consist of a gain medium, pump light source, and input/output coupling structures. The three main categories are:
Erbium-Doped Fiber Amplifiers (EDFA)
Semiconductor Optical Amplifiers (SOA)
Fiber Raman Amplifiers (FRA)
Optical amplifiers can serve three primary functions in fiber networks:
Power amplifiers (Boosters): Placed after the transmitter to increase signal power
In-line amplifiers: Positioned along the transmission line to compensate for fiber losses
Pre-amplifiers: Located before the receiver to improve detection sensitivity
Erbium-Doped Fiber Amplifier (EDFA)
Principle of Operation: EDFAs utilize a three-level energy system in erbium ions (Er³⁺). When pump light (typically at 980 nm or 1480 nm wavelengths) is injected into the erbium-doped fiber, Er³⁺ ions in the ground state are excited to higher energy levels. These ions quickly transition to a metastable state through non-radiative decay. The long lifetime of this metastable state (approximately 10 ms) enables population inversion, allowing signal photons at 1550 nm to stimulate emission and achieve amplification.
Key Advantages of EDFA (2025):
High gain: 20-40 dB typical, up to 50 dB in specialized designs
Low noise figure: 3-6 dB
Wide bandwidth: C-band (1530-1565 nm) and L-band (1565-1625 nm) coverage
High output power: +20 to +30 dBm
Polarization-independent operation
Low insertion loss
Simultaneous amplification of multiple wavelength channels
Modern EDFA Developments: As of 2025, advanced EDFAs incorporate:
Dynamic gain equalization for flat spectral response
Automatic gain control (AGC) for stable operation
Multi-stage designs with mid-stage access for dispersion compensation
Integration with wavelength-selective switches for reconfigurable optical networks
Semiconductor Optical Amplifier (SOA)
Semiconductor Optical Amplifiers are compact, traveling-wave amplifiers constructed using semiconductor laser technology. When operated below the lasing threshold, these devices provide optical amplification for coherent input light.
Advantages of SOA:
Compact size and easy integration with other photonic components
Wide gain bandwidth covering both 1300 nm and 1550 nm windows
Low power consumption
Fast response time enabling signal processing functions
Cost-effective for mass production
Suitable for wavelength conversion and optical switching
2025 Applications: SOAs are increasingly used in:
Data center interconnects
Metro and access networks
All-optical signal processing (wavelength conversion, clock recovery)
Optical packet switching
Silicon photonics integration
Limitations: Compared to EDFAs, SOAs have higher noise figures (6-10 dB), lower output power, polarization sensitivity, and faster gain dynamics that can cause crosstalk in WDM systems.
Fiber Raman Amplifier (FRA)
Fiber Raman Amplifiers exploit stimulated Raman scattering (SRS), a nonlinear optical effect in which pump photons transfer energy to signal photons at longer wavelengths. The Raman gain spectrum peaks approximately 13 THz (100 nm at 1550 nm) below the pump wavelength.
Key Advantages of FRA:
Flexible gain wavelength determined by pump wavelength
Ultra-wide bandwidth: can cover 1292-1660 nm range
Distributed amplification reduces nonlinear effects
Low noise figure when used as distributed amplifier
Excellent temperature stability
Can amplify wavelength bands not covered by EDFA
Modern FRA Technology (2025):
Multi-wavelength pumping for broadband flat gain
Counter-propagating and bi-directional pumping schemes
Hybrid EDFA-Raman amplifiers for extended bandwidth
Advanced pump lasers with output powers exceeding 1W per wavelength
Application in ultra-long-haul submarine cable systems (>10,000 km)
Ⅳ. Operational Amplifier
An operational amplifier (op-amp) is a versatile integrated circuit that combines multiple transistors, resistors, capacitors, and other components on a single chip to perform high-precision amplification. Modern op-amps offer exceptional performance characteristics including high gain, low noise, wide bandwidth, and excellent stability.
How Operational Amplifiers Work
An operational amplifier has two input terminals and one output terminal:
Non-inverting input (+): Signals applied here appear in-phase at the output
Inverting input (-): Signals applied here appear inverted at the output
Output: Provides the amplified signal
Ideal Op-Amp Characteristics:
Infinite open-loop gain: Any voltage difference between inputs drives the output to the rail voltage
Infinite input impedance: No current flows into the input terminals
Zero output impedance: Output voltage is independent of load
Infinite bandwidth: Gain is constant at all frequencies
Zero offset voltage: Output is zero when inputs are equal
Virtual Short Concept: In negative feedback configurations, the op-amp adjusts its output to maintain nearly equal voltages at both inputs, creating a "virtual short" between the input terminals while maintaining infinite input impedance.
Classification of Operational Amplifiers (2025)
1. General-Purpose Op-Amps: Cost-effective devices suitable for non-critical applications (e.g., LM358, TL072, MCP6002)
2. Precision Op-Amps: Feature low offset voltage (<50 μV), low drift (<0.5 and="" high="" cmrr="">120 dB). Examples include LTC2057, OPA2188, and AD8628.
3. High-Speed Op-Amps: Offer wide bandwidth (>100 MHz) and high slew rates (>1000 V/μs). Modern examples include LMH6881, THS4551, and ADA4960.
4. Low-Noise Op-Amps: Achieve voltage noise below 1 nV/√Hz. Examples: AD797, LT1028, OPA2134.
5. Low-Power Op-Amps: Consume<100 μA per amplifier, ideal for battery-powered applications. Examples: MAX4475, OPA2333, LPV521.
6. Rail-to-Rail Op-Amps: Input and output ranges extend to within millivolts of supply rails, maximizing dynamic range in low-voltage applications.
7. Instrumentation Amplifiers: Specialized op-amp configurations with very high CMRR (>100 dB) and precise gain setting for sensor interfacing.
8. Programmable Gain Amplifiers (PGA): Digitally controlled gain settings enable flexible signal conditioning. Modern PGAs offer gains from 1 to 128 with<0.01% accuracy.
2025 Innovations:
Zero-drift amplifiers with auto-calibration
GaN-based op-amps for extreme environments
Integrated op-amps in advanced CMOS processes (7nm and below)
AI-assisted op-amp design optimization
Ⅴ. Power Amplifier
Power amplifiers are essential components in audio systems, RF transmitters, and motor control applications where significant output power is required. A power amplifier's primary function is to increase the power level of a signal while maintaining fidelity to the original waveform.
Power Amplifier Principles
Power amplifiers utilize the current control characteristics of bipolar junction transistors (BJTs) or the voltage control characteristics of field-effect transistors (FETs) to modulate power from the DC supply according to the input signal. The amplified output current or voltage is then delivered to the load.
Classification of Power Amplifiers
Class A Amplifiers:
Transistor conducts for entire 360° of input cycle
Excellent linearity and lowest distortion (<0.01% THD achievable)
Low efficiency (20-25% maximum)
High heat dissipation
Best sound quality for audio applications
Used in high-end audio equipment
Class B Amplifiers:
Each transistor conducts for 180° of input cycle
Two complementary transistors handle positive and negative half-cycles
Higher efficiency (50-70%)
Suffers from crossover distortion
Rarely used alone in audio applications
Class AB Amplifiers:
Combines advantages of Class A and Class B
Small bias current eliminates crossover distortion
Efficiency: 50-70%
Good linearity (THD < 0.1%)
Most common in audio power amplifiers
Excellent balance of performance and efficiency
Class D Amplifiers (2025 Technology):
Switching amplifier using pulse-width modulation (PWM)
Very high efficiency (85-97%)
Compact size and low heat generation
Modern designs achieve THD < 0.01% with advanced filtering
Switching frequencies now exceed 1 MHz for improved audio performance
Dominant in portable devices, automotive audio, and professional sound systems
GaN and SiC devices enable higher power density and efficiency
Class G and H Amplifiers:
Use multiple power supply rails for improved efficiency
Class G: Switches between supply voltages based on signal amplitude
Class H: Modulates supply voltage to track signal envelope
Efficiency: 60-80%
Common in professional audio and high-power applications
Modern Power Amplifier Topologies (2025)
1. Output Transformerless (OTL) Amplifiers:
Use coupling capacitor instead of output transformer
Common in low to medium power applications
Simpler design and lower cost
Limited by capacitor size at low frequencies
2. Output Capacitorless (OCL) Amplifiers:
Use dual power supplies (±V)
Direct coupling to load
Excellent frequency response down to DC
Most common topology in modern audio amplifiers
Requires protection circuitry to prevent DC offset damage
3. Bridge-Tied Load (BTL) Amplifiers:
Two amplifiers drive load differentially
Doubles output voltage swing
Four times the power of single-ended configuration
Common in automotive and portable audio
Requires floating load (no ground connection)
2025 Innovations in Power Amplifiers
GaN Technology: Gallium Nitride transistors enable higher frequencies, greater efficiency, and smaller size
Digital Power Amplifiers: All-digital signal path with integrated DSP for advanced features
Adaptive Bias: Dynamic adjustment of bias current based on signal conditions
Envelope Tracking: Real-time supply voltage modulation for maximum efficiency
Self-Oscillating Class D: Eliminates need for external PWM modulator
Multi-Level Switching: Three or more voltage levels reduce filtering requirements
AI-Based Distortion Correction: Machine learning algorithms predict and compensate for nonlinearities
Key Specifications for Power Amplifiers
Output Power: Measured in watts (W) at specified load impedance and distortion level
Total Harmonic Distortion (THD): Modern amplifiers:<0.01% to 0.1%
Signal-to-Noise Ratio (SNR): High-end amplifiers: >110 dB
Damping Factor: Ratio of load impedance to output impedance; higher is better (>100 typical)
Frequency Response: Audio amplifiers: 20 Hz to 20 kHz (±0.1 dB or better)
Intermodulation Distortion (IMD): Should be<0.01% for high-fidelity applications
Conclusion: Amplifier technology continues to evolve rapidly in 2025, with advances in semiconductor materials (GaN, SiC), digital signal processing, and circuit topologies enabling unprecedented levels of performance, efficiency, and integration. Whether for audio, RF, optical, or instrumentation applications, modern amplifiers deliver exceptional specifications while consuming less power and occupying less space than ever before.
Article last updated: November 2025
1. What is an amplifier?
An amplifier is a device that can amplify the voltage or power of an input signal and is composed of tubes or transistors, power transformers, and other electrical components. Used in communication, broadcasting, radar, television, automatic control, and other devices.
2. What is the difference between an amplifier and a repeater?
First, Different functions. The amplifier simply amplifies the signal and suppresses noise and interference. The repeater plays the role of signal forwarding, which is equivalent to the role of a microphone. It is not only for data forwarding but also for advanced relays for sessions and application services. Second, the principle is different. The amplifier is actually an analog Fourier transformer. The output of the amplifier is a DC voltage, which is proportional to the signal amplitude of a specific frequency (parameter input frequency) in the input signal. And other frequency components in the input signal will not make any contribution to the output voltage. The purpose of the repeater design is to push the network signal to make the transmission farther. Digital or analog signals carrying information can only travel a limited distance due to the effects of transmission line noise.
3. What is the difference between audio amplifier and general amplifier?
Audio amplification has high requirements for the working frequency of the amplifier, because the range of human hearing sound is 20-20000 Hz, so the amplifier requires that the amplification factor should be kept stable within this range, so that undistorted sound can be heard. If it is required to have a better effect on the bass, then the amplification of the low frequency should be larger. To sum up, audio amplification generally uses a special audio amplifier, otherwise the effect will not be good.
Introduction to MD8002A Audio AmplifierUTMEL27 March 20259705The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.
Read More
Understanding the Low Noise Amplifier (LNA)UTMEL20 March 202526398A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.
Read More
Introduction to Optical AmplifierUTMEL27 March 202510374An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.
Read More
What is an Inverting Amplifier?UTMEL25 April 202512285An inverting amplifier is a fundamental configuration of operational amplifiers where the output signal has opposite polarity to the input signal. This configuration uses an operational amplifier with its inverting input terminal receiving the input signal, while the non-inverting terminal is typically connected to ground. The primary function of this circuit is to amplify the input signal while inverting its phase by 180 degrees.
Read More
Low-Power Design of Operational AmplifiersUTMEL27 March 20257629Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.
Read More
Subscribe to Utmel !
MP6KE20A/TRMicrochip Technology
MSMCG26CA/TRMicrochip Technology
1N5636A/TRMicrochip Technology
JANS1N6108A/TRMicrochip Technology
LT4363HMS-1#PBFLinear Technology/Analog Devices
LT4356CS-1#TRPBFLinear Technology/Analog Devices
65600001009Littelfuse Inc.
RD12S-T1-ATRenesas
JANTXV1N5907/TRMicrochip Technology
JANTX1N6048A/TRMicrochip Technology


Product
Brand
Articles
Tools