18650 vs. 21700: What Difference is between them?
BATTERY LITHIUM 3.7V 2.6AH
This post will unlock the differences between 18650 and 27100 from different angles.

21700 vs 18650 for Nanolongrange
18650 vs. 21170: Overview
18650 Overview
A lithium-ion battery is a 18650 battery. The name is derived from the battery's dimensions: 18mm x 65mm. That's about the size of an AA battery. The 18650 battery has a 3.6v voltage and a capacity of 2600mAh to 3500mAh (mili-amp-hours).
21170 Overview
The cylindrical 21700 battery has a diameter of 21mm and a height of 70.0mm. It has the best energy density and lowest cost battery in the world at the moment, and it is cost-effective.
18650 vs. 21170: Characteristic
18650 Characteristic
Large capacity: A lithium battery has a capacity of at least 1200mah, if not 3600mah, but the ordinary battery cell has a capacity of just 500mah.
High energy storage efficiency and stability: It can still sustain full performance output at temperatures below 70°, and there is usually a protection circuit within to keep the battery from burning out.
No memory effect: There is no need to discharge all leftover power before charging, and it may be charged and discharged at any moment, making it comfortable to use.
High charge and discharge cycle life: Lithium batteries have tens of thousands of cycles and high-temperature resistance.
Environmental safeguards, no hazardous substances: Non-toxic, non-polluting, and RoHS quality certified.
21170 Characteristic
Because the positive electrode has been converted to nickel, the performance is unaffected, the consistency is good, and it may be used immediately as a battery pack.
Lithium-ion Rechargeable Cell
Size: Diameter: 21mm, Length: 70mm
Weight: around 65g
Rated voltage: 3.6V
Standard capacity: 4800mAh
Internal resistance: approximately 13 milliohms
Charging voltage: 4.2V
Discharge cut-off voltage: 2.5V
Discharge current: 10A (15-20A can be discharged instantaneously).
Flashlights, scooters, LED lights, miner's lamps, lighting products, power banks, mobile power supplies, backup power supplies, computers, mobile devices, automobiles, bicycles, communications, medical, energy storage, solar energy, and so on.
18650 vs. 21170: Advantage
18650 Advantage
1) Large storage capacity
The capacity of a 18650 battery ranges from 1200mah to 3600mah, while the capacity of a standard battery is just about 800mah. When paired with a 18650 battery pack, it can easily exceed 5000mah.
2) Prolonged Life
The 18650 battery has a long service life, with a cycle life of more than 500 times during typical operation, which is more than double that of standard batteries.
4) Very High Voltage
The voltage of a 18650 lithium battery is typically 3.6V, 3.8V, or 4.2V, which is significantly higher than the 1.2V voltage of nickel-cadmium or nickel-metal hydride batteries.
5) There is no memory effect.
It is not necessary to drain the remaining power before charging, making it more convenient to use.
6)Internal Resistance Is Low
The internal resistance of the polymer battery is lower than that of the general liquid battery, and the internal resistance of the domestic polymer battery can be as low as 35m, which significantly reduces self-consumption of the battery and increases the standby life of the mobile phone. This polymer lithium battery with a high discharge current is perfect for remote control models and has emerged as the most promising replacement for nickel-metal hydride batteries.
7) It can be connected in series or parallel to make a lithium battery pack with 18650 cells.
8) Broad Applicability
Notebook computers, walkie-talkies, portable DVD players, instrumentation, audio equipment, model aeroplanes, toys, video cameras, digital cameras, and other electronic devices can all use 18650 batteries.
21170 Advantage
1) The 21700 type battery has a better energy density than the well-known 18650 type battery. After grouping, the number of single cells in use can be considerably decreased, as can the cost. A 18650 battery has a capacity of roughly 2600-3600 mAh, whereas a 21700 battery has a capacity of more than 4000 mAh, and even 5000mAh has surfaced on the market. Furthermore, a bigger capacity is becoming increasingly useful for extending the battery life of current devices.
2) The rechargeable battery's single volume has been raised by 35%. Using the Tesla 21700 rechargeable battery as an example, a single battery's energy can be enhanced by 34.8ah, a 35% increase.
3) It is expected that the net weight of the system software will be lowered by 10%. The total capacity exceeds 21700. The total number of batteries required under the same kinetic energy can be reduced by about 1/3 with an increase in a single volume and an increase in single energy ratio, and the total number of metal components and electrical components selected for the battery pack can reduce the difficulty of managing information systems coefficient. After changing the SDI (Samsung Digital Interface) to the new 21700 rechargeable battery, the system software discovered that the net weight was lowered by 10% over the current battery.
18650 vs. 21170: Specification
18650 Battery | 21700 Battery |
Nominal Voltage: 3.6V | Voltage: 3.7V |
Nominal Capacity: 2,850 mAh | Capacity: 3500- 5600mAh |
Minimum Discharge Voltage: 3V | Operating voltage: 2.5- 4.2V |
Maximum Discharge current: 1C | Cutoff voltage: 2 - 2.5V |
Charging Voltage: 4.2V (maximum) | Weight: 55gms to 75gms |
Charging current: 0.5C | Charge density (Energy per cell): 10.5- 13.7Wh |
Charging Time: 3 hours (approx) | Charge discharge cycle: 500 to 2000 |
Charging Method: CC and CV | Continuous discharge current: 20- 35 amps |
Cell Weight: 48g (approx) | Optimum /Minimum charging time: 2.5 hrs to 3.5 hrs |
Cell Dimension: 18.4mm (dia) and 65mm (height) | Charging voltage: 4.2V- 5V |
18650 vs. 21170: Conclusion
Many people question what the main difference is between a 21700 battery and a 18650 battery. Physically, the difference is simple; the size is the only difference. The 21700 battery is slightly larger than the 18650 battery. Both are available in flat top and button top styles. One, though, is smaller than the other. Because the 21700 battery is slightly larger, it has higher energy/power and runtime. The mAh of these batteries is an important factor to consider. The mAh capacity of 18650 batteries will range from 2000 to 3500. On 21700 batteries, you can expect mAhs ranging from 3000 to 5000. You may come across advertisements for 18650 batteries that claim to have capacities of up to 9000 mAH.
The 18650 rechargeable battery offers strong dependability and stability, whereas the 21700 battery has a substantially higher performance index than the 18650 battery. Furthermore, when compared to other battery models, the raw materials, production technology, and technological processes of the 21700 rechargeable battery level are more advanced than the level of the 18650 rechargeable battery. As a result, the best fit is between the 18650 and 21700 production lines.
18650 Datasheet PDF
Can I use AA batteries instead of 18650?
In brief: No, the 18650 cells can not be used in place of standard AA batteries, rechargeable or otherwise: The nominal voltage of the 18650 is significantly different from the 1.5x3=4.5V of the three AA cells, assuming those are connected in series.
What can I use instead of an 18650 battery-performance and replacement?
21700 batteries. These are rechargeable lithium-ion cells which are used to power vaping accessories and flashlights. ... 26650 batteries. Many people confuse between 18650 and 26650 batteries. ... 20700 batteries.
Are 21700 batteries better than 18650?
Because 21700 cells heat up faster and have lower resistance than 18650 cells, there is more polarization in the 18650 and variations between the voltage curves for the two formats at higher C rates. For discharge rates up to 3.75C, the 21700 has approximately 50% more capacity and energy density than the 18650.
Does Tesla use 21700 batteries?
When Tesla and Panasonic revealed the 21700 cells in 2017, it made enormous headlines. Tesla, on the other hand, no longer uses 18650 cells; instead, it now employs the 21700 standards, with cells measuring 21mm by 70mm. The new Tesla battery has grown in size yet again, this time by a substantial margin to 4680, or 46mm x 80mm.
Does Tesla use 18650 batteries?
Currently, Tesla mostly employs the Panasonic 18650 lithium-cobalt-acid battery, which has thousands of independent cells and costs approximately 135 $ / kWh to generate 233 W / kg of energy. Tesla's future plans call for the release of a new 20,700 lithium battery pack.
Are all 21700 Batteries the same?
No, not all 21700 batteries are created equal. Some of these lithium-ion cells might be protected, while others might not be. PCB and overheat protection are standard features on most 21700 batteries. These safeguards keep the battery from overcharging or overheating. Unprotected batteries are more harmful since they lack this protective measure. The design and mAh's are two other distinctions between 21700 batteries. Some 21700 cells will be available in flat variants, while others will be available in button top versions. They also offer a variety of mAh ranges, some lower and others greater.
What other products use 21700 batteries?
Many devices, including cars, electric motorcycles, and vapes, employ 21700 batteries. Because 21700 batteries can supply greater power, they are becoming more used in gadgets, particularly flashlights.
Cypress PSoC® 3: CY8C38 Family Datasheet Overview29 February 2024186
LMG5200 Half-Bridge Power Stage: Feature, Application, and Datasheet16 June 20214717
LM2901 Quad Comparator: Pinout, Equivalent and Datasheet28 December 20214668
MIC5205 150mA Low-Noise LDO Regulator: Pinout, Datasheet pdf and Circuit25 November 20213198
CA3130EZ BiMOS Operational Amplifier: Schematic, Pinout, and Datasheet14 February 20222620
ST2001FX Transistor: Datasheet, Pinout, Application09 August 20212015
FDG6335N N-Channel MOSFET: Diagram, Pinout, and Datasheet [Video&FAQ]28 April 20223629
The Comprehensive Introduction to AD8310 [FAQ]27 May 20222830
Introduction to MSP430 Microcontroller26 December 202512810
Semiconductor Market Expected to Surge, Driven by Rising Number of Data Centers04 June 20242952
How to read Resistors Color Code?16 October 202525139
Filter Circuit: Types, Characteristics and Principles01 December 20219909
Humidity Sensor: Classification, Package and Application13 November 20255641
What is MCU Decryption?17 January 20222101
3-D Printing as Part of the Next Industrial Revolution15 November 20191724
LDR/Light Dependent Resistor: Working Principle, Types and Applications19 January 202634254
SparkFun Electronics
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools