1N4001 vs 1N4007: What’s the Differences?
Standard Diode Rectifier Standard Recovery >500ns, > 200mA (Io) 1.1V @ 1A -55°C~175°C 5μA @ 50V Tape & Reel (TR) DO-204AL, DO-41, Axial Through Hole
Unit Price: $0.131516
Ext Price: $0.13









Standard Diode Rectifier Standard Recovery >500ns, > 200mA (Io) 1.1V @ 1A -55°C~175°C 5μA @ 50V Tape & Reel (TR) DO-204AL, DO-41, Axial Through Hole
1N4001 and 1N4007 are both diodes of the 1N400x series. What do “1” and “7” mean separately? Can I use the 1N4001 instead of 1N4007? Where can I use them? In this passage, I will show you the details.

Electronics circuit. Full wave bridge rectifier. LEDs and 1N4001 diodes. Rectifier component shown.
1N4001
A 1N4001 is a diode of the 1N400x series, all diodes of this series are widely used in electronic devices.
The 1N4001 diode is manufactured with good specifications, such as 1A upstream current, 3W power dissipation, and small in size with low price, which makes it ideal for a wide variety of electronic applications.
1N4007
1N4007 is a PN junction rectifier diode. These types of diodes only allow the flow of electric current in one direction. Therefore, it can be used for the conversion of alternating current to direct current. The 1N4007 is electrically compatible with other rectifier diodes and can be used instead of any diode of the 1N400X series.
The 1N4007 has various applications in real life. For example, applications of freewheeling diodes, general rectifying of power supplies, inverters, converters, etc.
1N4001 VS 1N4007: Pinout
Just shown below, The 1N4007 and 1N4001 both have two pins, the anode, and cathode respectively. Both pins have opposite charges on them. The two pins and their names and charges are shown in the table below.
The 1N4007 and 1N4001 diodes have a cathode (-) and anode (+). In the schematic symbol, the tip of the triangle with the line on top of it is the cathode.

| Pin No. | Pin Name | Description |
| 1 | Anode | Current always Enters through Anode |
| 2 | Cathode | Current always Exits through Cathode |
1N4001 VS 1N4007: Features
1N4001 Features
The average forward current is 1A
Non-repetitive peak current is 30A
The reverse current is 5uA.
RMS reverse voltage is 35V
Peak repetitive reverse voltage is 50V
Available in DO-41 Package
1N4007 Features
Operating Junction Temperature : -550C – 1750C
Forward Voltage: 1.1 Volts
The average forward current is 1A
Non-repetitive Peak current is 30A
The reverse current is 5uA.
Peak repetitive reverse voltage is 1000V
Power dissipation 3W
Available in DO-41 Package
1N4001 VS 1N4007 Application
1N4001 Application
Can be used to prevent reverse polarity problem
Half Wave and Full Wave rectifiers
Used as a protection device
Current flow regulators
1N4007 Application
For use in general purpose rectification of power supplies, inverters, converters, and freewheeling diodes application.
Power Supplies
Battery Chargers
Voltage Doublers
Adapters
Rectification
Components protection
Blocking incoming voltage were not required
1N4001 & 1N4007 Meaning
1N4001 series diodes are 1 Ampere current handling general purpose rectifier diodes. 1N stands for American standard semiconductor (Generic name) with ONE JUNCTION.
400X Series like 4001, 4002 to 4007 indicate the diodes' voltage, current, and power rating.
1N= Means One Junction between P-type and N-Type.
400= Means the Serial number of the rectifier.
1= Means Defines its (1 A) current rating.
How to Safely Long Run 1N4007 in a Circuit
To obtain the maximum operating time of the diode, it is recommended to stay between 30 and 40 V below its maximum repetitive reverse voltage and other values. Always connect with correct polarity, and do not exceed a load of 1A. Do not operate and store at a temperature below -55 centigrade and above +175 centigrade.
1N4001 & 1N4007 Manufacturer
onsemi (legally ON Semiconductor Corporation; formerly ON Semiconductor until August 5, 2021) is an American semiconductor supplier company, formerly in the Fortune 500, but dropping into the Fortune 1000 (ranked 512) in 2020. Products include power and signal management, logic, discrete, and custom devices for automotive, communications, computing, consumer, industrial, LED lighting, medical, military/aerospace, and power applications. onsemi runs a network of manufacturing facilities, sales offices, and design centers in North America, Europe, and the Asia Pacific. Headquartered in Phoenix, Arizona, onsemi has revenues of $3.907 billion (2016), which puts it among the top 20 semiconductor sales leaders worldwide.
1N4001 & 1N4007 Datasheet
What is purpose of a diode?
It allows current to flow easily in one direction but severely restricts current from flowing in the opposite direction. Diodes are rectifiers that change alternating current (ac) into pulsating direct current (dc). Diodes are rated according to their type, voltage, and current capacity.
Is 1N4007 a Schottky Diode?
1N4007 is a rectifier diode with a PN junction.
What is a 1N4001 Diode Used for?
The 1N400x (or 1N4001 or 1N4000) series is a prominent one-ampere general-purpose silicon rectifier diode family that is widely utilized in AC adapters for common household appliances. Its blocking voltage ranges from 50 to 1000 volts (1N4001) (1N4007).
Can I Replace 1N4001 with 1N4007?
Yes. The 1N4007 can sustain a larger reverse voltage (Vr), 1000V compared to 50V.
Where we can Use 1N4007?
1N4007 can be used in several circuits; it is often designed for general-purpose rectification, but it can also be used in any circuit that requires voltage blocking, voltage spike blocking, and so on. It's also useful in digital logic circuits.
TPS92630QPWPRQ1 LED Driver: Pinout, Manufacturer, and Datasheet23 March 2022443
2N2907A Bipolar Transistor PNP TO-18: Datasheet, Pinout, and Equivalents09 February 20222653
LM358 Dual Op-Amp vs LM393 Dual Comparator12 August 20228547
ATmega16: 8-bit Microcontroller29 February 2024641
AD7794 Integration Notes: Resolving SPI Drops, Gain Errors, and ADC Replacement Constraints27 April 2026500
SHT15 Humidity Sensor: Datasheet, Pinout and Features06 September 20212700
Analog Devices Inc. 5962-8851301PA: A Versatile Instrumentation Amplifier for Military Applications06 March 2024250
LM1875T/NOPB Audio Amplifier: Feature,Specification,Datasheet17 May 20215159
What is Instrument Transformer?08 January 20228026
How does the CPU Calculate 1+1?12 January 20225186
An Overview of Bipolar Transistors27 August 20209525
Understanding of Coaxial Cable06 August 202140176
sar-adc-reference-driver-selection-managing-dynamic-kickback-noise-loop-stability17 September 2026514
Global Semiconductor Sales Experience a 2.3% Surge in July 202309 September 20233978
MCU Crystal Selection & Startup Verification: Load Capacitance, ESR, and Oscillation Margin Guide29 September 2026547
What to Know Before Buying CR1225 Battery Equivalent05 September 20252544
ON Semiconductor
In Stock: 3000
Minimum: 1 Multiples: 1
Qty
Unit Price
Ext Price
1
$0.131516
$0.13
500
$0.096703
$48.35
1000
$0.080585
$80.58
2000
$0.073932
$147.86
5000
$0.069095
$345.48
10000
$0.064274
$642.74
15000
$0.062161
$932.42
50000
$0.061122
$3,056.10
Not the price you want? Send RFQ Now and we'll contact you ASAP.
Inquire for More Quantity


Product
Brand
Articles
Tools