web counter

LM358 Dual Op-Amp vs LM393 Dual Comparator

Sophie

Published: 12 August 2022 | Last Updated: 12 August 2022

8488

LM393N

LM393N

ON Semiconductor

Through Hole Tube 1.4 μs μs Linear Comparators 106.02dB dB 250nA pA 2006 5mV mV Through Hole

Purchase Guide

Through Hole Tube 1.4 μs μs Linear Comparators 106.02dB dB 250nA pA 2006 5mV mV Through Hole

The LM358 Op-Amp and the LM393 Comparator are two typical jellybean components that stand out for their simplicity and availability. Outwardly, the LM358 and LM393 are extremely similar - they come in the same packaging and have the same pinout - but there are significant variations between the two chips, which we shall examine in this article.

This is a video about some similar Op amps ic.

Op amps ic lm358, lm393, tl072, ne5532 tester circuit

LM358 overview

The LM358 is a dual op-amp integrated circuit having two op-amps supplied by a single power source. It is one-half of the LM324 Quad op-amp, which has four op-amps with a shared power supply. The differential input voltage range can be the same as the power supply voltage range. The default input offset voltage is incredibly low, measuring only 2mV. The standard supply current is 500uA and has a maximum current of 700uA regardless of the supply voltage range. The operational temperature ranges from 0˚C to 70˚C at ambient, with a maximum junction temperature of 150 C.


LM393 overview

The LM393 integrated circuit is the comparator version of the popular LM358 Op-Amp. While any Op-Amp may be made to serve as a voltage comparator, the LM393 has a benefit in that it has an open collector output, making it suited for driving loads.

 

The output transistor can drive loads up to 50V and 50mA, which is sufficient for typical TTL, MOS, and RTL loads. The transistor can also separate the load from the system ground. So, if you need a Voltage comparator to drive loads with these characteristics, this IC could be a good fit.


LM358 vs LM393: Features

LM358 Dual Op-Amp IC Features and Specifications


  • Integrated with two Op-Amps in a single package

  • Wide power supply Range

  • Singe supply: 3V to 32V

  • Dual supply: ±1.5V to ±16V

  • Low Supply current: 700uA

  • A single supply for two op-amps enables reliable operation

  • Short circuit protected outputs

  • Operating ambient temperature: 0˚C to 70˚C

  • Soldering pin temperature: 260 ˚C (for 10 seconds – prescribed)

  • Available packages: TO-99, CDIP, DSBGA, SOIC, PDIP, DSBGA

 

LM393 Differential Comparator features and specifications


  • Dual Comparator in a single package

  • Wide power supply Range

     -Singe supply – 2V to 36V

     -Dual supply – ±1V to ±18V

  • Drain Current of only 0.4mA

  • Input Offset Voltage is ±5mV maximum

  • Power Dissipation: 660mW

  • Can Drive most of the TTL and MOS loads

  • Output can be Isolated from System Ground

  • Low Offset Voltage and current


LM358 vs LM393: Pinouts

lm358 pinout.jpg       lm393 pinout.jpg

                          LM358 pinout                                                              LM393 pinout


As shown in the two pinouts above, LM358 and LM393 share the same pinout configurations. 


Pin NumberPin NameDescription
1OUTPUT1The output of Op-Amp 1
2INPUT1-Inverting Input of Op-Amp 1
3INPUT1+Non-Inverting Input of Op-Amp 1
4V EE, GNDGround or Negative Supply Voltage
5INPUT2+Non-Inverting Input of Op-Amp 2
6INPUT2-Inverting Input of Op-Amp 2
7OUTPUT2The output of Op-Amp 2
8V CCPositive Supply Voltage


LM358 vs LM393: Applications

LM358 Applications


  • Transducer Amplifiers

  • Conventional op-amp circuits

  • Integrator, Differentiator, Summer, adder, Voltage follower, etc.,

  • DC gain blocks, Digital multimeters, Oscilloscopes

  • Comparators (Loop control & regulation)

 


LM393 Applications


  • Voltage Comparator circuits

  • Can drive Relay, Lamp, Motor Etc

  • Zero Crossing detector

  • Peak voltage Detector

  • High Voltage Protection/Warning

  • Oscillator circuits


LM358 vs LM393: Equivalents

LM358 Equivalents

LM358A, LM358E, LM358-N, LM358W

 

LM393 Equivalents

LM358, TL082, LM311


LM358 & LM393: Manufacturer

onsemi (legally ON Semiconductor Corporation; formerly ON Semiconductor until August 5, 2021) is an American semiconductor supplier company, formerly in the Fortune 500, but dropping into the Fortune 1000 (ranked 512) in 2020. Products include power and signal management, logic, discrete, and custom devices for automotive, communications, computing, consumer, industrial, LED lighting, medical, military/aerospace, and power applications. onsemi runs a network of manufacturing facilities, sales offices, and design centers in North America, Europe, and the Asia Pacific regions. Headquartered in Phoenix, Arizona, onsemi has revenues of $3.907 billion (2016), which puts it among the worldwide top 20 semiconductor sales leaders.


Major Differences Between LM358 and LM393

SpecificationLM358LM393
Supply Voltage32V, +/-16V36V, +/-18V
Differential Input Voltage32V36V
Input Offset Voltage3mV max.5mV max.
Input Bias Current100nA max.250nA max.
Input Common Mode Range0V to V + - 2V0V to V + - 1.5V
Large Signal Voltage Gain100V/mV typ.200V/mV typ.
Bandwidth1MHzNot specified


LM358 vs LM393: Internal Circuit

lm358 circuit.jpg

lm358 circuit

lm393 circuit.jpg

lm393 circuit

The internal circuitry of the LM358 and LM393 appear similar at first glance, but deeper inspection reveals variances that explain the varied specs indicated above.

 

The input stages are analogous to "Darlington-connected" PNPs, which explains why both the LM358 and LM393 have ground sensing capabilities. The differential stages, however, operate at different currents; the LM393 operates at a higher current to boost the gain and output switching speed. Because the LM358 is a linear amplifier, this is unimportant.

The output stages are the most noticeable change. The LM393 output stage is substantially simpler than the LM358 output stage because it is designed to switch the output between the rails as quickly as possible while spending the least amount of time between the rails. The output stage is open-collector as well. Because the LM358 is an op-amp meant to be used as a linear amplifier, its output scales linearly with the input, it has a fully linear output stage.


LM358 vs LM393: Datasheet

Frequently Asked Questions

Can I use LM393 instead of LM358?

The LM358 and LM393 might seem outwardly similar, but the LM358 is an operational amplifier with linear output, and the LM393 is a comparator with a digital output, and they cannot be interchanged.

What is the difference between a comparator and an op amp?

Unlike operational amplifiers that usually operate with the input voltages at the same level, comparators typically see large differential voltage swings at their inputs. But some comparators without rail-to-rail inputs are specified to have a limited common mode input voltage range.

What are the applications of an op-amp in real life?

Op amps are used in a wide variety of applications in electronics. Some of the more common applications are a voltage follower, selective inversion circuit, current-to-voltage converter, active rectifier, integrator, a whole wide variety of filters, and a voltage comparator.

What is the use of LM358 in IR sensor?

Here operational amplifier (op-amp) of LM 358 is used as a comparator. When the IR receiver does not receive the signal the potential at the inverting input goes higher than that at the non-inverting input of the comparator (LM 358). Thus the output of the comparator goes low and the LED does not glow.

What is LM393 used for?

The LM393 IC is a low-power, single-supply, low-offset voltage, double, differential comparator. Generally, a common comparator IC is a tiny voltmeter with included switches. It is used to calculate the voltages at two dissimilar terminals and contrasts the dissimilarity in voltage quantity.
LM393N

ON Semiconductor

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More