CR2450 VS LIR2450[FAQ+Video]: Are they interchangeable?
BATTERY LITHIUM 3V COIN 24.5MM
LiR2450 batteries and CR2450 batteries are both round, flat, and shaped like small silver buttons, appearing to be the same. Can they all be used generically because they all look the same? This article will answer your questions and show you how they are similar and different, as well as how they can be used interchangeably.

Use Rechargeable Coin Cell Battery For SmartThings Smarthome Sensors | CR2450 To LIR2450
CR2450 Overview

CR2450 is a 3V Coin Cell Battery by Panasonic which delivers consistent and long-lasting power. It’s made of Lithium Manganese Dioxide (LiMnO2) and is ultra-compact in design. It has a capacity 620mAh and it’s not rechargeable. It’s one of the CR series of batteries of Panasonic. The CR series of Panasonic coin battery capacity ranges from 25mAh to 1000mAh.
LIR2450 Overview

LIR2450 is a coin cell, Lithium-Ion rechargeable battery. Physically the same size as CR2450, LIR2450 can be used as a rechargeable replacement to CR2450 in most cases. This little battery has a little over 100 mA/Hour capacity, with nominal 3.6 V output. This battery is perfect for powering a small project.
CR2450 vs LIR2450: Features
CR2450 Features
Lightweight, High Voltage, and High Energy Density
The battery voltage is 3V, almost double that of normal alkaline or manganese batteries. This means that the number of batteries required for equipment can be halved for maximum space-saving and weight reduction.
Excellent Discharge Characteristics
Voltage characteristics remain stable even for a long period of discharge, greatly improving the reliability of equipment that uses the battery. Such equipment is also maintenance-free (battery replacement is seldom required).
Excellent Leakage Resistance
The newly developed battery construction and electrolyte ensure maximum leakage resistance over a long span of time.
Excellent Long-Term Reliability
Carefully selected active materials are used for the active material as well as for the electrolyte. These materials are sealed by Murata's innovative technology to minimize battery self-discharge. The annual self-discharge rate at room temperature and normal humidity is less than 1% of the nominal capacity.
LIR2450 Features
Long Cycle Life: Under normal usage, the cycle life of the LIR2450 Lithium-Ion battery can be ≥500 circles while with a capacity of≥80%.
High Power Density: High power density makes the LIR2450 battery light in weight and small in dimension. It can be used in small devices.
Safe and Reliable: No floating metal lithium assures a safer usage.
High working voltage: Working voltage is up to 3.6V, approx. 3 times the voltage of NI-MH or NI-CD, which reduces the quantity of the battery needed in certain applications.
No memory effect: No memory effect assures a constant maximum application.
Low self-discharge rate: ≤5%/month
Good consistency is shown in LIR 2450 battery capacity, internal resistance, discharge platform, and capacity retention. A strict complete internal quality control is subject to the ISO9000 system
CR2450 vs LIR2450:Alternatives
CR2450 Alternatives
CR2025, CR-2450/VAN, CR-2450/F1AN, CR-2450/H1AN, CR-2450/G1AN
LIR2450 Alternatives
CR2450, 638179, CR-2450/BS, 6450101501
CR2450 vs LIR2450: Applications
CR2450 Applications
Automotive
Smart Key/Keyless entry
Door sill strip
IoT
Tracking devices
Sensors
Security
Medical
Thermometers
Others
Home electrical appliances/Multifunctional printer
Electronic price tags, POS systems
LIR2450 Applications
Laptop computers
PDA and IC cards
electric clocks and watches
Wearable electronics devices
Tracking units
Monitoring units
Remote control keys
Digital cameras
Sports Bluetooth headset batteries
RC toys.
LiR2450 vs CR2450 : Specifications
| PowerStream LiR2450 | Panasonic CR2450 | |
| Nominal Voltage | 3.7V | 3.0V |
| Nominal Capacity | 120 mAh | 620 mAh |
| Continuous Drain Current | 24 mA | 0.2 mA |
| Maximum Pulse Discharge Current | 200 mA | - |
| Operating Temperature | -20°C +60°C | -30°C +85°C |
Are LiR2450 and CR2450 Interchangeable?
The main differences between CR2450 and LiR2450 batteries in the voltage, capacity, and of course, rechargeable features.
Voltage difference - due to the voltage difference of ~0.6-0.7 volts, not all devices powered by the CR2450 battery will operate properly when powered by the LiR2450 battery. Actually, this voltage difference may even damage some more sensitive units.
Thus, unless the Owner's Guide of the device you have lists 3.6-3.7V LiR2450 batteries as supported battery type, do NOT replace the CR2450 battery with a LiR2450 battery.
Capacity difference - CR2450 battery features a much larger capacity than the LiR2450 battery. But, the LiR2450 battery may be recharged up to 500-1000 times, which is a lot.
Note: When charging LiR2450 batteries, be sure to use battery chargers specifically intended for such batteries.
Also, LiR2450 batteries feature a much larger self-discharge rate than CR2450 batteries and are usually 10-30% per year, sometimes even more.
Is LIR2450 the same as CR2450?
LIR2450 is a coin cell, Lithium-Ion rechargeable battery. Physically the same size as CR2450, LIR2450 can be used as a rechargeable replacement to CR2450 in most cases. This little battery has a little over 100 mA/Hour capacity, with nominal 3.6 V output. This battery is perfect for powering a small project.
Are Lithium coin cell rechargeable?
Largest on the list of power's smallest tools is the lithium coin cell. They are primary Lithium, meaning these single-use batteries are non-rechargeable.
What does CR in batteries mean?
CR is the generic designation that is used by the entire batteries maker but lithium batteries are also having chromium. All the batteries that have this chemical substance in their batteries can use this abbreviation CR. On the other DL is the short abbreviation of the battery-making company Duracell.
What is CR2450 used for?
The Lithium Coin CR2450 batteries have certain accomplishments for applications where traditional batteries cannot be used. Use them for calculators, digital watches, laser pens, car keys, medical devices like a clinical thermometer and a tensiometer, and fitness appliances.
Is a CR2450 battery the same as a DL2450?
DL2450 is a Duracell battery while CR2450 is an Energizer battery.
MB10S Bridge Rectifier: Circuit, Pinout, and Datasheet15 November 20217476
Top-Rated Suppliers of ADIS16209CCCZ Sensors07 June 2025214
ATMEGA8L-8PU 8-bit Microcontrollers - MCU 8kB Flash: Datasheet, Pinout, and Package information.21 February 20225051
Arduino Mega 2560 Rev3: Block Diagram, Features and Applications06 October 20238810
LM7810 Voltage Regulator: Circuit, Datasheet, Pinout28 December 202113987
DS1672 Binary Counter RTC: Pinout, Features and Datasheet14 April 20221152
LIS2DHTR Motion Sensor: 3-Axis, Application Hint, Datasheet PDF23 February 20221988
IRF9540 Power MOSFET: IRF9540 Datasheet, Pinout, Equivalent [FAQ&Video]17 December 202115195
Global Power Technology Authorized Distributor | UTMEL Electronics21 November 20234423
Kyoto University Successfully Demonstrates That SiC Can Also Work at 350°C26 March 2022925
Electrical Symbols & Electronic Symbols: A Practical Guide to Reading Circuit Diagrams17 June 2026766
What is an Inductive Sensor?31 October 202514058
The History of Microscope21 October 20218500
Semiconductor Sales Expected to Rebound in 2024, Driven by Innovation18 December 20235012
Buffer Amplifier Guide: How It Works, Key Specifications, Applications and Selection16 June 20261200
10 Details to Improve the Anti-Interference Ability of MCU29 December 20215708
Panasonic - BSG
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools