Enhancing Server Efficiency with BCM957412A4120AC Setup Tips

UTMEL

Published: 15 July 2025 | Last Updated: 15 July 2025

279

BCM957412A4120AC

BCM957412A4120AC

Broadcom Limited

ASSY,TOP,BCM957412A4120AC, CLOUD

Purchase Guide

ASSY,TOP,BCM957412A4120AC, CLOUD

Optimize server performance with BCM957412A4120AC. Learn setup tips, driver updates, and network settings to ensure high-speed, reliable connectivity.

Product Introduction

Enhancing
Image Source: pexels

In today’s IT environments, high-speed server connectivity plays a vital role in ensuring smooth operations. Faster connections allow you to handle larger data volumes, reduce latency, and improve overall system performance. By 2025, more than 60% of switch ports will operate at speeds of 100 Gbps or higher. Server connection speeds are also moving beyond 1/10 Gbps to 25 Gbps and above. This shift highlights the demand for reliable, high-speed solutions.

The BCM957412A4120AC offers a powerful way to achieve these goals. Its advanced design supports high-speed data transfer and ensures dependable connectivity. Implementing this solution can help you meet the growing demands of modern IT workloads.

Key Features of BCM957412A4120AC

Key
Image Source: unsplash

High-speed connectivity and bandwidth

The BCM957412A4120AC delivers exceptional network performance, making it ideal for modern IT environments. With support for PCI Express 3.0 x8, this network interface card (NIC) ensures fast data transfer rates. It features two ports and supports optical fiber media, enabling reliable and high-speed connectivity. Whether you need 10GBase-X or 1000Base-X network technology, this card provides the flexibility to meet your bandwidth requirements.

Here’s a quick overview of its technical specifications:

FeatureSpecification
Host InterfacePCI Express 3.0 x8
Total Number of Ports2
Expansion Slot TypeSFP+
Media Type SupportedOptical Fiber
Network Technology10GBase-X, 1000Base-X
Form FactorPlug-in Card
Device SupportedServer

These features ensure that your server can handle high-speed data transfers without bottlenecks.

Advanced hardware design

The advanced hardware design of the BCM957412A4120AC sets it apart from other NICs. It incorporates hardware acceleration engines that boost network performance significantly. Features like TruFlow™ allow you to increase virtual machine (VM) density by up to 50%, optimizing resource utilization. Additionally, the card supports on-chip tunneling protocol processing for Geneve, VXLAN, and NVGRE. This capability enhances throughput by up to 5X, making it a powerful choice for virtualized and cloud-based environments.

  • Hardware acceleration engines improve data handling efficiency.
  • TruFlow™ technology increases VM density, reducing server overhead.
  • On-chip tunneling protocol processing enhances throughput for modern networking protocols.

These design elements ensure that your server infrastructure remains robust and future-ready.

Energy efficiency

Energy efficiency is another standout feature of the BCM957412A4120AC. The card is engineered to minimize power consumption without compromising performance. By optimizing energy usage, it helps reduce operational costs and supports environmentally friendly IT practices. This makes it an excellent choice for organizations aiming to balance performance with sustainability.

Tip: Deploying energy-efficient hardware like the BCM957412A4120AC can significantly lower your data center's carbon footprint.

With its energy-saving design, this NIC not only boosts server efficiency but also aligns with green IT initiatives.

Support for modern networking protocols

Modern IT environments demand hardware that can handle advanced networking protocols. The BCM957412A4120AC excels in this area, offering robust support for protocols that are essential for virtualization, cloud computing, and high-speed data transfer.

Protocols Supported by BCM957412A4120AC

  • Geneve: This protocol simplifies network virtualization by encapsulating Layer 2 packets. It ensures seamless communication between virtual machines across different physical servers.
  • VXLAN: VXLAN enhances scalability in virtualized environments. It allows you to create thousands of isolated networks within a single infrastructure.
  • NVGRE: NVGRE optimizes network traffic by encapsulating Ethernet frames. It reduces overhead and improves data flow efficiency.

These protocols enable your server to handle complex workloads with ease. They also ensure compatibility with modern software-defined networking (SDN) solutions.

Note: Using hardware that supports these protocols can significantly improve your server's ability to manage virtualized workloads and cloud-based applications.

Benefits of Protocol Support

The BCM957412A4120AC’s protocol support offers several advantages:

  • Enhanced scalability: You can expand your network infrastructure without performance bottlenecks.
  • Improved efficiency: Protocol processing occurs directly on the card, reducing CPU workload.
  • Future-proofing: The card aligns with emerging networking standards, ensuring long-term usability.

Real-World Applications

Imagine running a data center with hundreds of virtual machines. The BCM957412A4120AC simplifies network management by processing protocols directly on its hardware. This reduces latency and boosts throughput, ensuring smooth operations even during peak workloads.

By leveraging its support for modern networking protocols, you can optimize your server infrastructure for today’s demanding IT environments.

Setting Up BCM957412A4120AC

Hardware installation

Installing the BCM957412A4120AC begins with ensuring the hardware is properly seated in your server. Start by identifying an available PCI Express 3.0 x8 slot on your motherboard. Carefully insert the card into the slot, applying even pressure until it clicks into place. Secure the card using the retention screw to prevent movement during operation.

For Linux-based systems, you may need to install prerequisite packages to ensure compatibility. Use your distribution's package manager to install these tools. For example, on Debian or Ubuntu systems, run the following command:

sudo apt install -y automake autoconf libtool libibverbs-dev ibverbs-utils infiniband-diags perftest ethtool

If you are using SuSE Linux with Secure Boot enabled, additional steps are required. You must import the Partner Linux Driver Program key to ensure the system recognizes the card. Refer to your distribution's documentation for detailed instructions.

Tip: Always handle the card by its edges to avoid damaging sensitive components. Use an anti-static wrist strap to protect the hardware from electrostatic discharge.

Configuring BIOS/UEFI settings

Once the hardware is installed, you need to configure your system’s BIOS or UEFI settings. Follow these steps to ensure the BCM957412A4120AC operates correctly:

  1. Verify that the card is properly seated in the PCIe slot. If the system does not detect the card, try reseating it.
  2. Check that the drivers for the card are installed and up to date. Visit Broadcom’s official website to download the latest drivers.
  3. Update your system BIOS/UEFI to the latest version. An outdated BIOS can sometimes prevent new hardware from being recognized.
  4. Test the card in a different PCIe slot if the current slot appears to be malfunctioning.
  5. If the card was previously functional but is no longer working, restart the system or clear the CMOS settings to reset the BIOS/UEFI configuration.

Note: Updating the BIOS/UEFI is a critical step. Manufacturers often release updates to improve hardware compatibility and performance.

Driver installation and updates

After configuring the BIOS/UEFI, the next step is to install the necessary drivers for the BCM957412A4120AC. Drivers act as the bridge between your operating system and the hardware, ensuring smooth communication.

For Windows systems, use the installation CD provided with the card or download the latest drivers from Broadcom’s website. Follow the on-screen instructions to complete the installation. On Linux systems, you may need to compile and install the drivers manually. Refer to the README file included with the driver package for specific commands.

Regular driver updates are essential for maintaining optimal performance. Updated drivers often include bug fixes, security patches, and performance enhancements. Set a reminder to check for updates periodically or enable automatic updates if your operating system supports this feature.

Tip: After installing the drivers, use the ethtool command on Linux or the Device Manager on Windows to verify that the card is functioning correctly.

Initial connectivity testing

Testing the initial connectivity of the BCM957412A4120AC ensures that your server is ready for high-speed data transfer. This step verifies that the hardware, drivers, and network settings are functioning correctly. Follow these steps to perform a thorough connectivity test:

  1. Verify physical connections
    Check the physical connections between the BCM957412A4120AC and your network infrastructure. Ensure that the optical fiber cables are securely attached to the card’s ports. Inspect the cables for any visible damage or loose connectors. A secure connection prevents signal loss and ensures reliable communication.

  2. Ping test for basic connectivity
    Use a ping test to confirm basic network communication. Open a terminal or command prompt on your server and run the following command:

    ping <destination_IP_address>
    

    Replace <destination_IP_address> with the IP address of another device on the network. If the ping test returns successful replies, the card is communicating with the network. If it fails, double-check the IP configuration and network settings.

  3. Check link status using diagnostic tools
    Use diagnostic tools like ethtool on Linux or the Device Manager on Windows to check the link status of the BCM957412A4120AC. For Linux systems, run:

    sudo ethtool <interface_name>
    

    Replace <interface_name> with the name of the network interface associated with the card. Look for the "Link detected" field. If it says "yes," the card is connected to the network. If it says "no," troubleshoot the connection further.

  4. Test data transfer speeds
    Conduct a speed test to measure the card’s performance. Use tools like iperf or netperf to test data transfer rates between your server and another device. For example, with iperf, you can run:

    iperf -c <destination_IP_address>
    

    This command initiates a speed test to the specified destination. Compare the results with the expected performance of the BCM957412A4120AC. If the speeds are lower than expected, review your network settings and ensure the card is configured correctly.

  5. Monitor network activity
    Observe network activity using monitoring tools like Wireshark or NetFlow analyzers. These tools help you identify any unusual traffic patterns or connectivity issues. They also provide insights into how the BCM957412A4120AC interacts with your network infrastructure.

Tip: If you encounter issues during testing, start by reviewing the card’s configuration settings. Small adjustments often resolve connectivity problems.

By completing these tests, you can confirm that the BCM957412A4120AC is functioning as intended. This ensures your server is prepared for high-speed operations and reliable data transfer.

Optimizing BCM957412A4120AC Performance

Optimizing
Image Source: unsplash

Adjusting network settings

Fine-tuning your network settings can significantly enhance the performance of the BCM957412A4120AC. Start by ensuring that your server’s network interface card (NIC) operates at its maximum capacity. Access your operating system’s network configuration tools to verify the link speed and duplex settings. For optimal performance, set the link speed to 10 Gbps or higher and ensure full-duplex mode is enabled.

You should also configure the Maximum Transmission Unit (MTU) size. Increasing the MTU size allows larger packets to be transmitted, reducing overhead and improving throughput. For most high-speed networks, an MTU size of 9000 bytes (jumbo frames) works well. Use the following command on Linux to adjust the MTU size:

sudo ifconfig <interface_name> mtu 9000

Replace <interface_name> with the name of your network interface. On Windows, you can modify the MTU size through the NIC’s advanced properties in the Device Manager.

Tip: Always test your network after making changes to ensure compatibility with your infrastructure. Some devices may not support jumbo frames, which could lead to connectivity issues.

Using QoS for traffic prioritization

Quality of Service (QoS) is a powerful tool for managing network traffic. By prioritizing critical data, you can ensure that essential applications receive the bandwidth they need. The BCM957412A4120AC supports advanced QoS features, allowing you to fine-tune traffic flow across your network.

To implement QoS, start by identifying the types of traffic that require prioritization. For example, real-time applications like video conferencing or VoIP often need higher priority than file transfers. Once identified, configure QoS rules on your network switches or routers. Assign higher priority levels to critical traffic and lower levels to less important data.

On Linux systems, you can use the tc (traffic control) command to set up QoS policies. Here’s an example of how to prioritize traffic on a specific interface:

sudo tc qdisc add dev <interface_name> root handle 1: htb default 10
sudo tc class add dev <interface_name> parent 1: classid 1:1 htb rate 1gbit

Replace <interface_name> with your NIC’s interface name. This configuration ensures that high-priority traffic receives a guaranteed bandwidth allocation.

Note: QoS settings must align with your overall network policies. Misconfigured rules can lead to bottlenecks or uneven traffic distribution.

Monitoring network performance

Regularly monitoring your network performance helps you identify potential issues and maintain optimal efficiency. The BCM957412A4120AC provides robust support for performance monitoring tools, enabling you to track key metrics and make data-driven adjustments.

Focus on metrics that provide actionable insights into your network’s health. Two critical metrics to monitor are throughput and latency. Throughput measures the amount of data transmitted per second, while latency tracks the time taken for transactions. Use tools like NetPerf to gather these metrics.

MetricDescription
NetPerf ThroughputMeasures the amount of data transmitted per second in Mb/s.
NetPerf LatencyMeasures the time taken for transactions in transactions/s.

To monitor throughput, run the following NetPerf command:

netperf -H <destination_IP_address> -t TCP_STREAM

Replace <destination_IP_address> with the IP address of the target device. For latency, use the TCP_RR test:

netperf -H <destination_IP_address> -t TCP_RR

These tests provide a clear picture of your network’s performance. If you notice a drop in throughput or an increase in latency, investigate potential causes such as hardware limitations or misconfigured settings.

Tip: Use monitoring tools like Wireshark to analyze traffic patterns and identify bottlenecks. These insights can guide you in optimizing your network further.

By adjusting network settings, leveraging QoS, and monitoring performance, you can unlock the full potential of the BCM957412A4120AC. These steps ensure your server operates at peak efficiency, meeting the demands of modern IT workloads.

Updating firmware regularly

Keeping the firmware of your BCM957412A4120AC up to date is essential for maintaining optimal performance and ensuring compatibility with modern IT environments. Firmware updates often include critical improvements, such as bug fixes, security patches, and performance enhancements. By updating regularly, you can unlock new features and extend the lifespan of your hardware.

Why firmware updates matter

Firmware acts as the bridge between your hardware and software. Outdated firmware can lead to performance bottlenecks, security vulnerabilities, or even hardware malfunctions. Manufacturers like Broadcom release updates to address these issues and adapt to evolving technology standards.

Tip: Always check for firmware updates when troubleshooting performance issues or after installing new hardware.

Steps to update the firmware

Updating the firmware of your BCM957412A4120AC is a straightforward process. Follow these steps to ensure a smooth update:

  1. Identify the current firmware version
    Start by checking the firmware version installed on your card. On Linux systems, use the ethtool command:

    sudo ethtool -i <interface_name>
    

    Replace <interface_name> with the name of your network interface. On Windows, you can find this information in the Device Manager under the card's properties.

  2. Download the latest firmware
    Visit Broadcom's official website to find the latest firmware for your card. Ensure that you download the version specifically designed for the BCM957412A4120AC. Verify the file's integrity by checking its checksum, which ensures the download is not corrupted.

  3. Backup your current configuration
    Before proceeding, back up your current settings. This step allows you to restore the previous configuration if the update encounters any issues. Use tools like ethtool or your operating system's network settings to save the configuration.

  4. Install the firmware update
    Use the firmware update utility provided by Broadcom. On Linux, you might need to use a command-line tool like fwupdate. For example:

    sudo fwupdate -i <firmware_file>
    

    Replace <firmware_file> with the path to the downloaded firmware file. Follow the on-screen instructions to complete the installation.

  5. Restart your server
    After the update, restart your server to apply the changes. This step ensures that the new firmware integrates seamlessly with your system.

  6. Verify the update
    Once the server restarts, check the firmware version again to confirm the update was successful. Use the same method you used in step one.

Note: Avoid interrupting the update process. A failed update can render your hardware inoperable.

Best practices for firmware updates

  • Schedule updates during maintenance windows: Perform updates during periods of low network activity to minimize disruptions.
  • Enable notifications: Subscribe to Broadcom's update alerts to stay informed about new firmware releases.
  • Test updates in a staging environment: If possible, test the firmware on a non-production server before deploying it to critical systems.

By updating the firmware regularly, you ensure that your BCM957412A4120AC operates at peak efficiency. This proactive approach helps you avoid potential issues and keeps your server infrastructure future-ready.

Ensuring Compatibility and Integration

Verifying server hardware compatibility

Before installing the BCM957412A4120AC, confirm that your server hardware supports it. Start by checking the server’s PCI Express slots. The card requires a PCI Express 3.0 x8 slot for optimal performance. Ensure the slot is available and not occupied by other components.

Next, review your server’s power supply capacity. The card is energy-efficient, but it still requires sufficient power to operate. Verify that your server can handle the additional load.

Finally, check the server’s operating system compatibility. The card supports major operating systems like Windows and Linux. However, ensure your specific version is compatible by consulting Broadcom’s documentation.

Tip: Always update your server’s firmware and drivers before installing new hardware. This step prevents compatibility issues.

Integrating with network infrastructure

Integrating the BCM957412A4120AC into your network infrastructure requires careful planning. Begin by assessing your existing network devices, such as switches and routers. Ensure they support the card’s high-speed capabilities, like 10GBase-X or 1000Base-X.

Next, configure your network settings to match the card’s specifications. For example, set the link speed to 10 Gbps or higher. Use high-quality optical fiber cables and transceivers to maintain reliable connections.

Finally, test the integration by running basic connectivity checks. Use tools like ping or ethtool to verify that the card communicates effectively with other devices.

Note: Proper integration ensures seamless data flow and maximizes the card’s performance.

Testing interoperability

Testing interoperability ensures the BCM957412A4120AC works well with other network components. Broadcom conducts extensive tests to validate compatibility. These tests cover cables, transceivers, and supported standards. The table below summarizes key interoperability tests:

Tested ComponentsDescription
Cables and TransceiversBroadcom tests a subset of cables and transceivers for compatibility with the BCM957412A4120AC.
Supported StandardsFirmware conforms to SNIA standards including SFF-8024, SFF-8472, SFF-8636, SFF-8665, and CMIS 4.0.
Compliance TestingContinuous testing with industry-compliant AOCs, optical modules, and DAC cables ensures ongoing interoperability.

Run your own tests to confirm compatibility with your specific setup. Use diagnostic tools to check link status and data transfer rates. If issues arise, consult Broadcom’s support resources for guidance.

Tip: Regular testing helps identify and resolve potential issues before they impact your network.

Addressing compatibility challenges

When integrating the BCM957412A4120AC into your server environment, you may encounter compatibility challenges. These issues can arise from mismatched hardware, outdated software, or unsupported configurations. Addressing them early ensures smooth operation and prevents downtime.

Common Compatibility Issues

  1. Hardware Limitations
    Some servers may lack the required PCI Express 3.0 x8 slot or sufficient power supply. Verify your server’s specifications before installation. If your server doesn’t meet the requirements, consider upgrading the hardware.

  2. Driver Conflicts
    Outdated or incompatible drivers can cause the card to malfunction. Always download the latest drivers from Broadcom’s official website. Avoid using generic drivers provided by the operating system.

  3. Network Infrastructure Mismatches
    The card supports high-speed connections like 10GBase-X. Ensure your switches, routers, and cables are compatible with these standards. Using older equipment may limit performance.

Steps to Resolve Compatibility Issues

  • Update Firmware and Drivers
    Regular updates improve compatibility with modern systems. Use tools like ethtool to check the current firmware version and update as needed.

  • Test with Certified Components
    Broadcom provides a list of tested cables and transceivers. Use these components to avoid interoperability issues.

  • Consult Documentation
    Broadcom’s user manuals and online resources offer detailed guidance. Refer to these materials for troubleshooting tips.

Tip: If you face persistent issues, contact Broadcom’s support team. They can provide expert assistance tailored to your setup.

By addressing these challenges proactively, you can ensure the BCM957412A4120AC integrates seamlessly into your server infrastructure. This approach minimizes disruptions and maximizes performance.

Troubleshooting BCM957412A4120AC Issues

Resolving hardware installation errors

Hardware installation errors can prevent the BCM957412A4120AC from functioning properly. Start by ensuring the card is securely seated in the PCIe slot. Apply even pressure during installation to avoid loose connections. If the card isn’t detected, test it in a different PCIe slot. This step helps identify potential issues with the slot itself.

Check the system BIOS or UEFI settings to confirm the card is recognized. Update the BIOS to the latest version if the card isn’t listed. Restarting the server or clearing the CMOS settings can also resolve detection problems. These actions reset the system configuration, allowing the hardware to initialize correctly.

Tip: Handle the card carefully during installation to avoid damaging sensitive components.

Fixing driver conflicts

Driver conflicts often disrupt the performance of the BCM957412A4120AC. Begin by verifying that the correct drivers are installed. Outdated or incompatible drivers can cause the card to malfunction. Visit Broadcom’s website to download the latest drivers specifically designed for this model.

Uninstall any conflicting drivers before installing new ones. On Windows, use the Device Manager to remove outdated drivers. For Linux systems, use the following command to uninstall drivers:

sudo apt remove <driver_package_name>  

After installing the updated drivers, restart the server to apply the changes. This step ensures the operating system communicates effectively with the card.

Note: Regularly updating drivers prevents conflicts and improves overall performance.

Addressing connectivity problems

Connectivity problems can arise due to improper configurations or physical issues. Start by inspecting the optical fiber cables connected to the BCM957412A4120AC. Ensure the cables are securely attached and free from damage. Loose or damaged cables often lead to signal loss.

Run a ping test to check basic network communication. Use the following command:

ping <destination_IP_address>  

Replace <destination_IP_address> with the IP address of another device on the network. If the test fails, review the card’s IP settings and network configuration. Tools like ethtool can help diagnose link status and identify connectivity issues.

Tip: Regularly monitor network activity to detect and resolve problems early.

When to seek professional help

Sometimes, despite your best efforts, resolving issues with the BCM957412A4120AC may require professional assistance. Knowing when to reach out can save you time and prevent further complications.

Situations that call for expert help:

  • Persistent hardware issues: If the card remains undetected after reseating it, testing different PCIe slots, or updating the BIOS, the problem might involve deeper hardware faults.
  • Complex driver conflicts: When driver updates or reinstallation fail to resolve errors, a professional can identify and fix underlying compatibility issues.
  • Network performance bottlenecks: If you notice unexplained drops in throughput or high latency, even after optimizing settings, an expert can analyze your network infrastructure for hidden inefficiencies.
  • Firmware update failures: Interruptions during firmware updates can render the card inoperable. Professionals have the tools to recover or reflash the firmware safely.
  • Interoperability challenges: If the card struggles to integrate with your existing network devices, a specialist can assess compatibility and recommend solutions.

Tip: Document all troubleshooting steps you’ve taken before contacting support. This information helps professionals diagnose the issue faster.

How to find the right help:

  • Manufacturer support: Broadcom offers technical support for their products. Visit their website to access resources or submit a support ticket.
  • Certified technicians: Look for IT professionals with experience in server hardware and networking. Certifications like CCNA or CompTIA Network+ indicate expertise.
  • Community forums: Online communities can provide valuable insights. However, rely on verified sources for critical issues.

Seeking professional help ensures that your BCM957412A4120AC operates at its full potential. Don’t hesitate to reach out when the situation demands it.


The BCM957412A4120AC offers a reliable solution for high-speed server connectivity. Its advanced features ensure faster data transfers, energy efficiency, and compatibility with modern networking protocols. By following proper setup steps, optimizing performance, and addressing issues promptly, you can maximize its potential. These practices not only improve server efficiency but also reduce downtime and operational costs.

Take action today by implementing these tips. Your server infrastructure will become more robust and ready to handle demanding workloads with ease.

FAQ

1. What operating systems are compatible with the BCM957412A4120AC?

The BCM957412A4120AC supports major operating systems like Windows and Linux. Check Broadcom’s documentation to confirm compatibility with your specific version. Keeping your OS updated ensures smooth operation.

2. How do you update the firmware for the BCM957412A4120AC?

Download the latest firmware from Broadcom’s website. Use tools like fwupdate on Linux or the provided utility on Windows. Restart your server after installation to apply changes.

3. Can you use the BCM957412A4120AC in virtualized environments?

Yes, the card supports protocols like VXLAN and Geneve, which optimize virtualized workloads. Its TruFlow™ technology increases VM density, making it ideal for cloud-based setups.

4. What should you do if the card isn’t detected after installation?

Reseat the card in the PCIe slot. Update your BIOS to the latest version. If the issue persists, test the card in another slot or contact Broadcom support.

5. How often should you update the drivers for the BCM957412A4120AC?

Check for updates monthly or enable automatic updates. Updated drivers improve performance, fix bugs, and ensure compatibility with new software.

Specifications

Broadcom Limited BCM957412A4120AC technical specifications, attributes, parameters and parts with similar specifications to Broadcom Limited BCM957412A4120AC.
  • Type
    Parameter
  • Factory Lead Time
    10 Weeks
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
0 Similar Products Remaining

Datasheet PDF

Download datasheets and manufacturer documentation for Broadcom Limited BCM957412A4120AC.
BCM957412A4120AC

Broadcom Limited

In Stock: 2314

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More