ESP32 vs ESP8266: Which is better?

UTMEL

Published: 01 December 2021 | Last Updated: 01 December 2021

27025

ESP-32

ESP-32

RF Solutions

2.4GHz~2.5GHz Bluetooth, WiFi -40°C~85°C 2.7V~3.6V ADC, GPIO, I2C, I2S, PWM, SDIO, SPI, UART 150Mbps 20.5dBm 802.11b/g/n, Bluetooth v4.2 + EDR, Class 1, 2 and 3 -97dBm Module

Purchase Guide

2.4GHz~2.5GHz Bluetooth, WiFi -40°C~85°C 2.7V~3.6V ADC, GPIO, I2C, I2S, PWM, SDIO, SPI, UART 150Mbps 20.5dBm 802.11b/g/n, Bluetooth v4.2 + EDR, Class 1, 2 and 3 -97dBm Module

The ESP32 and ESP8266 are cheap Wi-Fi modules perfectly suited for DIY projects in the Internet of Things (IoT) and Home Automation fields. So what is the difference between ESP32 and ESP8266? Should you use the ESP32 or the ESP8266 in your projects? It depends on what you want to do. In this article, we’ll compare the ESP32 with the ESP8266 and cover the pros and cons between them.

This video is about ESP32 vs ESP8266 Speed Comparison and Arduino Dual Core Speed.

ESP32 #60: ESP32 vs ESP8266 Speed Comparison and Arduino Dual Core Speed

Introduction

The ESP32 is a dual-core 160MHz to 240MHz CPU, whereas the ESP8266 is a single-core processor that runs at 80MHz.The ESP32 and ESP8266 are both fantastic Wi-Fi modules. When it comes to particular aspects, one is sometimes chosen above the other. The ESP8266 has a lower current consumption than that of its competitor however one has more digital pins than the other. As a result, you should select the appropriate option. Therefore, this article is going to discuss the pros and cons between ESP32 and ESP8266 and which one is better for your choice. I hope you found this post to be informative.


What is ESP32?

ESP32 is a low-cost, low-power Microcontroller with integrated Wi-Fi and Bluetooth. It is the successor to the ESP8266 which is also a low-cost Wi-Fi microchip albeit with limited vastly limited functionality.

It is an integrated antenna and RF balun, power amplifier, low-noise amplifiers, filters, and power management module. The entire solution occupies the smallest amount of space on the printed circuit board. This board is used with TSMC 40nm low power technology 2.4 GHz dual-mode Wi-Fi and Bluetooth chips, which have the best power and RF attributes, are safe, dependable, and scalable to a variety of applications.

 esp32.jpg

esp32 board.jpg

ESP32 Pinout



What is ESP8266?

The ESP8266 is a Wi-Fi SoC that integrates all the needed components to create a fully functional Wi-Fi device. The L106 is a custom 32-bit processor with 32KB of instruction space, 80KB of user data, 16 GPIO pins, and a variety of peripherals including a serial peripheral interface (SPI), inter-integrated circuit protocol (I2C), universal asynchronous receiver-transmitter (UART), and an analog-to-digital converter onboard the SoC. (ADC). Because the ESP8266 integrated circuit (IC) comes in a difficult-to-use maker package, most builders opt for the ESP-01, which includes the ESP8266, onboard flash memory, and other components.

esp8266.jpg

esp8266 board.jpg

ESP8266 Pinout

ESP32 vs. ESP8266: Specifications

CategoryESP8266ESP32Winner
Processor80MHz 32-Bit RISCUp to dual-core 240MHz 32-Bit   processorESP32
Memory32KB Instruction 80KB User Data520KM SRAMESP32
Peripherals16 GPIO, UART, I2C, I2S, ADC> 16 GPIO, UART, I2C, I2S, ADC,   DAC, CANESP32
Wi-FiYesYesNeither
BluetoothNoYesESP32
Hardware SecurityNoYesESP32
SSL SupportedYes – Not very wellYesESP32
PriceLowHighESP8266
ProgrammabilityNot EasyEasyESP32
Maker FriendlyNo – 8 Pin Device Not FriendlyYesESP32
Software SupportYes but   getting oldYes – Still relevantESP32


ESP32 vs. ESP8266: Arduino IDE

Let's compare the two modules using the Arduino IDE, which is mostly used to program the ESP32 and ESP8266 microcontrollers. Both boards can be programmed using the Arduino IDE, which is a benefit for individuals who are familiar with the platform. Both share the same library and command set. Some libraries are only compatible with the ESP32 or ESP8266 modules, and will not run on both. However, only a few changes are required.

 

How to program ESP32 on Arduino IDE

  • In your Arduino IDE, go to File> Preferences.

  • Open the Boards Manager. Go to Tools > Board > Boards Manager…

  • Search for ESP32 and press the install button for the “ESP32 by Espressif Systems“:

  • That's it. It should be installed after a few seconds.

 

Install ESP8266 Add-on in Arduino IDE

  • To install the ESP8266 board in your Arduino IDE, follow these next instructions:

  • In your Arduino IDE, go to File> Preferences

  • Enter http://arduino.esp8266.com/stable/package_esp8266com_index.json into the “Additional Boards Manager URLs” field as shown in the figure below. Then, click the “OK” button:

  • Open the Boards Manager. Go to Tools > Board > Boards Manager…

  • Search for ESP8266 and press the install button for the “ESP8266 by ESP8266 Community“:

  • That’s it. It should be installed after a few seconds.


ESP32 vs. ESP8266: Pros and Cons

ESP32 Pros:

  • ESP32 offers you dual-core 160MHZ to 240MHZ

  • You can control and monitor your device with the help of Wi-fi or Bluetooth at a very low price.

  • ESP32 offers you more GPIOs

  • ESP32 gives you a high speed of 150Mbps.

 

ESP32 Cons:

  • ESP32 is more expensive than the ESP8266

 

 

ESP8266 Pros:

  • ESP8266 Module gives you powerful onboard processing and storage capability, which allows it to integrate with sensors and other applications.

  • It has a high level of on-chip integration. The on-chip integration allows the user for very little external refer circuitry.

  • The ESP8266 goes with APSD for the Bluetooth and VoIP applications coexistence interfaces. It also contains a self-calibrated radio frequency (RF) that allows it to work with all the conditions of operating and does not require any radio frequency parts.

 

ESP8266 Cons:

  • ESP8266 does not have Bluetooth connectivity, whereas in ESP32 you can use this feature.

  • The GPIO is very less in ESP8266 compared to ESP32.


ESP32 vs. ESP8266: What are the applications?

  • Using Wi-Fi to triangulate a location

  • Automated outlets in various stores and workshops

  • Industrial security in home and business sectors

  • Wireless monitoring CCTV cameras and sensors that feed data

  • In the field of robotics for both academic and professional purposes


Why is ESP32 special?

The ESP8266 and ESP32 SoC microcontrollers both provide builders with an Internet communication device, but the ESP32 comes out on top. The Arduino IDE can program the ESP8266 directly, however it is frequently more difficult, whereas the ESP32 is simple to program. The ESP32's quicker processor and larger memory allow for far larger projects to be created on a single SoC, while the ESP32's robust security features make it a more secure device. Furthermore, the ESP32 is a dependable board, even though its firmware and attached peripherals can be flaky at times. Secure sockets layer (SSL) connections become increasingly viable as memory and processing power increase, which are critical criteria in a society where security is crucial.

In general, ESP32 devices have more GPIO to work with, making them more useful in complex applications. Because many ESP32 development boards have small cameras, the ESP32 appears to be a very capable device.

 


Which one is better ESP32 or ESP8266?

Choose ESP32 or ESP8266? It depends on what you want to do.

ESP32 is better than ESP8266 because ESP32 has extra features such as CPU core, Faster Wi-Fi, Bluetooth 4.0 (BLE), touch sensitivity pins, and built-in Hall Effect sensors and temperature sensors. The ESP32 has more GPIO pins as compared to the ESP8266. The ESP32 contains 10 capacitive GPROS that detect touch and can be used to trigger events. The trigger event is a circuit in which action is initiated by an input pulse e.g. as in a radar module.

The ESP8266 is a less expensive alternative to the ESP32. Although it lacks several features, it suffices for the majority of simple DIY IoT projects. However, the GPIO mapping has some limits, and there may not be enough pins for what you want to achieve. If that's the case, an ESP32 is the way to go.


Frequently Asked Questions

Is ESP32 the same as ESP8266?

The ESP32 is a dual-core 160MHz to 240MHz CPU, whereas the ESP8266 is a single-core processor that runs at 80MHz. These modules come with GPIOs that support various protocols like SPI, I2C, UART, ADC, DAC, and PWM.

Can ESP32 use ESP8266 library?

Different CPUs, different hardware, different CPU registers. Some libraries from the ESP8266 framework are converted to work on ESP32, but if you compare them you can see significant differences in how the lib accesses the hardware/OS layers. It's like you want a Windows program to run on Linux.

Is ESP8266 better than ESP32?

The ESP32 is much more powerful than the ESP8266, comes with more GPIOs with multiple functions, faster Wi-Fi, and supports Bluetooth. However, many people think that the ESP32 is more difficult to deal with than the ESP8266 because it is more complex.

How many cores are ESP8266?

ESP8266 is based on a Tensilica L106 32-bit RISC processor ref which is a single-core processor and thus you can't do real multiprocessing on it.

Can ESP32 connect to 5 GHz Wi-Fi?

The devices of the ESP32 Ethernet & Wi-Fi & BLE PLC controller family have an integrated 5 GHz Wi-Fi specific chip, called ISM43340. As you may know, the 5 GHz Wi-Fi band is an improved version of the previous ones, such as the 2.4GHz band, for example.

What is ESP8266 used for?

The ESP8266 WiFi Module is a self-contained SOC with an integrated TCP/IP protocol stack that can give any microcontroller access to your WiFi network. The ESP8266 is capable of either hosting an application or offloading all WiFi networking functions from another application processor.

What is ESP32 used for?

ESP32 can perform as a complete standalone system or as a slave device to a host MCU, reducing communication stack overhead on the main application processor. ESP32 can interface with other systems to provide Wi-Fi and Bluetooth functionality through its SPI / SDIO or I2C / UART interfaces.
ESP-32

RF Solutions

In Stock: 109

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More