IRF640 vs IRF640N: Datasheet, Specifications, and FAQ

Sophie

Published: 26 August 2022 | Last Updated: 05 November 2024

9840

IRF640

IRF640

STMicroelectronics

N-Channel Tube 180m Ω @ 9A, 10V ±20V 1560pF @ 25V 72nC @ 10V TO-220-3

Purchase Guide

N-Channel Tube 180m Ω @ 9A, 10V ±20V 1560pF @ 25V 72nC @ 10V TO-220-3

IRF640 and IRF640N are similar in their names. What are the differences between them? Magi will explain it in this passage. Please have a look. What’s more, Utmel has enough stock, welcome to order.

This is an introduction video about IRF640N.

IRF640N Power Amp DC 12v

IRF640 Description

The IRF640 is an N Channel MOSFET designed for fast switching. This high-speed switching capability can be extremely useful in applications where switching speed is critical, such as a UPS circuit or any other application where a user wants to change the load input power from one source to another.

The transistor can drive a load of up to 18A and has a maximum voltage of 200V with a minimum saturation voltage of 2V to 4V at its gate. The pulsed drain current of 72A indicates that this MOSFET can drive a load of up to 72A at short intervals or when the load is not continuously connected and is only connected for 300us (Microseconds) with a duty cycle of 1.5%.


IRF640N Description

The IR MOSFET series of power MOSFETs use proven silicon technologies to provide designers with a diverse device portfolio to serve a variety of applications including DC motors, inverters, SMPS, lights, load switches, and battery-powered applications. For ease of design, the devices come in a choice of surface mount and through-hole packaging with industry-standard footprints.


Parts with Similar Specs

IRF640 vs IRF640N: Pinout

640pinout.jpg       640n pinout.jpg

                     IRF640 Pinout                                                        IRF640N Pinout



IRF640 vs IRF640N: Applications

IRF640 Applications

  • Battery Chargers and BMS

  • Solar Power Supply Applications

  • Applications That Require Fast Switching

  • Motor Drivers

 

IRF640N Applications

  • DC motors

  • Inverters

  • SMPS

  • Lighting

  • Load switches

  • Battery powered applications


IRF640 vs IRF640N: Features / Technical Specifications


IRF640IRF640N
Package TypeTO-220-3TO-220-3
Transistor TypeN ChannelN Channel
Max Voltage Applied From Drain to Source400V200V
Max Gate to Source Voltage Should Be±20V±20V
Max Continuous Drain Current10A18A
Max Pulsed Drain Current40A72A
Max Power Dissipation125W150W
Minimum Voltage Required to Conduct2V to 4V2V to 4V
Max Storage & Operating temperature-55 to +150 ℃-55 to +175 ℃


IRF640 vs IRF640N: Equivalents

IRF640 Equivalents

YTA640, IRF641, IRF642, IRFB4620, IRFB5620, 2SK740, STP19NB20, YTA640, BUK455-200A, BUK456-200A, BUK456-200B, BUZ30A, MTP20N20E, RFP15N15, 2SK891, 18N25, 18N40, 22N20

 

IRF640N Equivalents

You can replace the IRF640N with the IRFB23N20D, IRFB260N, IRFB31N20D, IRFB38N20D, IRFB4127, IRFB4227, IRFB4229, IRFB4233, IRFB42N20D, IRFB4332


IRF640 vs IRF640N: Manufacturer

IRF640 Manufacturer

STMicroelectronics is a global independent semiconductor company and is a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology, and its products play a key role in enabling today's convergence trends.


 

IRF640N Manufacturer

International Rectifier was an American power management technology company manufacturing analog and mixed-signal ICs, advanced circuit devices, integrated power systems, and high-performance integrated components for computing. On 13 January 2015, the company became a part of Infineon Technologies.

IR's products, as a part of Infineon Technologies' overall semiconductor portfolio, continue to be used in many applications including lighting, automobile, satellite, aircraft, and defense systems; as well as key components in power supply systems in electronics-based products that include especially microcomputers, servers, networking, and telecommunications equipment.



Frequently Asked Questions

How does MOSFET work?

It works by varying the width of a channel along which charge carriers flow (electrons or holes). The charge carriers enter the channel at the source and exit via the drain. The width of the channel is controlled by the voltage on an electrode called a gate which is located between the source and drain.

What is IRF640?

IRF640 is an N Channel MOSFET designed for high-speed switching purposes. This high-speed switching capability can be very useful in applications where switching speed is crucial, for example in a UPS circuit or in any other application where a user wants to change the load input power from one source to another.

What is P channel Mosfet?

P-Channel MOSFET is a classification of Metal Oxide Semiconductor Device. This consists of the n-substrate in the middle with light doping concentration. 

What is the difference between N-channel and P-channel MOSFET?

Then the P-channel MOSFET is used to switch the positive supply to the motor for the forwarding direction (high-side switching) while the N-channel MOSFET is used to switch the negative supply to the motor for the reverse direction (low-side switching).

What is N channel Mosfet?

N-Channel MOSFET is a type of metal oxide semiconductor field-effect transistor that is categorized under the field-effect transistors (FET). MOSFET transistor operation is based on the capacitor. This type of transistor is also known as an insulated-gate field-effect transistor (IGFET).
IRF640

STMicroelectronics

In Stock: 4600

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More