web counter

S8550 PNP SILICON TRANSISTOR[Video+FAQ]: Pinout, Circuit, and Equivalents

Sophie

Published: 21 April 2022 | Last Updated: 21 April 2022

9805

S8550

S8550

Changjiang Electronics Tech (CJ)

S8550 datasheet pdf and Unclassified product details from Changjiang Electronics Tech (CJ) stock available at Utmel

Purchase Guide

The S8550 is a low voltage high current small signal PNP transistor, designed for Class B push-pull audio amplifiers and general-purpose applications.

This video will show you the simplest method to check trasistor 8050 and 8550 quite easily.

How To Check Transistor 8050 and 8550 Very EASILY

S8550 Overview

       S8550 is a PNP transistor hence the collector and emitter will be left open (Reverse biased) when the base pin is held at the ground and will be closed (Forward biased) when a signal is provided to the base pin. It has a maximum gain value of 300; this value determines the amplification capacity of the transistor normally S8550. Since it is very high it is normally used for amplification purposes.

 

      When this transistor is fully biassed then it can allow a maximum of 700mA to flow across the collector and emitter. This stage is called Saturation Region and the typical voltage allowed across the Collector-Emitter (V­CE) or Collector-Base (VCB) could be 20V and 30V respectively. When the base current is removed the transistor becomes fully off, this stage is called the Cut-off Region.


S8550 CAD Models

Symbol

symbol.jpg

Footprint

foot.jpg


S8550 Pinout and Configurations

pinout.jpg

S8550 Pin Configurations

Pin NumberPin NameDescription
1EmitterCurrent Drains out through emitter, normally connected to ground
2BaseControls the biasing of the transistor, Used to turn ON or OFF the transistor
3CollectorCurrent flows in through collector, normally connected to load


Specifications

Changjiang Electronics Tech (CJ) S8550 technical specifications, attributes, parameters and parts with similar specifications to Changjiang Electronics Tech (CJ) S8550.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    SOT-23(SOT-23-3)
  • Current-Collector (Ic) (Max)
    500mA
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • Power - Max

    Power - Max is a parameter that specifies the maximum amount of power that an electronic component can handle without being damaged. It is typically measured in watts and indicates the upper limit of power that can be safely supplied to the component. Exceeding the maximum power rating can lead to overheating, malfunction, or permanent damage to the component. It is important to consider the power-max rating when designing circuits or systems to ensure proper operation and longevity of the electronic components.

    300mW
  • Transistor Type

    Transistor type refers to the classification of transistors based on their operation and construction. The two primary types are bipolar junction transistors (BJTs) and field-effect transistors (FETs). BJTs use current to control the flow of current, while FETs utilize voltage to control current flow. Each type has its own subtypes, such as NPN and PNP for BJTs, and MOSFETs and JFETs for FETs, impacting their applications and characteristics in electronic circuits.

    PNP
  • Voltage - Collector Emitter Breakdown (Max)

    Voltage - Collector Emitter Breakdown (Max) is a parameter that specifies the maximum voltage that can be applied between the collector and emitter terminals of a transistor or other semiconductor device before it breaks down and allows excessive current to flow. This parameter is crucial for ensuring the safe and reliable operation of the component within its specified limits. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the device. Designers and engineers must carefully consider this parameter when selecting components for their circuits to prevent potential issues and ensure proper functionality.

    25V
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

S8550 Features

  • Low Voltage, High Current PNP Transistor

  • Continuous Collector current (IC) is 500mA

  • Collector-Emitter voltage (VCEO) is -25 V

  • Collector-Base voltage (VCB0) is -40V

  • Emitter Base Voltage (VBE0) is -5V

  • Current Gain (hFE), 85 to 300

  • Commonly used as Class B Push-pull transistors

  • Available in To-92 Package


S8550 Applications

  • Audio Amplification Circuits

  • Class B Amplifiers

  • Push-pull Transistors

  • Circuits where high gain is required

  • Low signal applications


S8550 PNP Complementary:

NPN Complementary of S8550 is S8050,


S8550 Equivalents

BC527, KSA708, MPS750


S8550 Alternative PNP Transistors

S8550 Circuit

 A simple circuit diagram of the Class B amplifier using the S8050 is shown below.

Circuit Diagram.jpg


Where to use S8550

     S8550 is a general-purpose transistor, therefore, you can use it at the output of your audio amplifier circuits to amplify the output audio signal to 1 watt, for example, it can be used in electronic doorbells circuits, mp3 audio amplifiers and in the output of buzzer circuits, etc. If you want to use it as a switch then you can easily drive big relays, many small LEDs at once, and one or two high-power LEDs around 10 to 20 watts, switching ON another portion or application in an electronic project/circuit, etc. Moreover, it can also be used as an alternative or equivalent to many other general-purpose transistors and it is also an ideal transistor to use in your hobby electronic projects, therefore it is a must to have transistors in your electronics lab.


S8550 Manufacturer

JCET Group Co., Ltd. is a public company headquartered in Jiangyin on China's eastern coast. It is the largest Outsourced Semiconductor Assembly and Test (OSAT) company in mainland China and the third-largest globally. JCET was formed in 1972 when Jiangyin converted a local factory to produce transistors. JCET went public on the Shanghai Stock Exchange in 2003 and continued to grow over time. JCET provides a range of semiconductor packaging, assembly, manufacturing, and testing products and services.


S8050 vs S8550

CharacteristicsS8050S8550 (PNP)
Collector to base voltage (VCB)30V-30V
Collector to emitter voltage (VCE)20V-20V
Emitter to base voltage (VEB)5V-5V
Collector current (IC)700mA-700mA
Power dissipation1W1W
Junction temperature (TJ)150°C150°C
Transition frequency (FT)100MHZ100MHZ
Noise (N)--
Gain (hFE)40 to 400hFE40to 400hFE
PackageTO-92TO-92


How to Safely Long Run in a Circuit

      Electronics components perform very well in a circuit for a long period of time if all the safety measures are taken into consideration at the time of designing and making the circuit, to make this transistor long run in your electronic application it is recommended to not use it in the circuit above 20V, and do not increase the output load from -700mA, always use a good current limiting resistor at the base of the transistor, and do not use it in the temperature above 150 centigrade and below -65 centigrade.


Trend Analysis

Parts with Similar Specs

Frequently Asked Questions

What is a S8550?

S8550 is a PNP transistor henceforth during reverse biasing both the collector and emitter will be open and during forward biasing these will be closed. It is produced in a flexible TO-92 casing.

What is the difference between PNP and NPN transistors?

 PNP sensors produce a positive output to your industrial controls input, while NPN sensors produce a negative signal during an “on” state.

What is S8050 transistor?

S8050 is an NPN Transistor with high current & low voltage capabilities. This transistor is a three-terminal component like an emitter, base & collector which are used for external connection through different circuits.

Which transistor can be used in place of S8050?

The transistor equivalent for the S8050 transistor will be S9013, S9014, 2n5551, 2n5830, mps6602, and mpsw01ag.

What does a transistor do?

A transistor is a semiconductor device used to amplify or switch electrical signals and power.
S8550

Changjiang Electronics Tech (CJ)

In Stock: 9008

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe