web counter

74LS00 Quad 2 Input NAND Gate: Datasheet, Pinout and Schematic

UTMEL

Published: 26 October 2021 | Last Updated: 26 October 2021

16456

74LS00

74LS00

ROCHESTER ELECTRONICS LLC

74LS00 datasheet pdf and Unclassified product details from ROCHESTER ELECTRONICS LLC stock available at Utmel

Purchase Guide

74LS00 is a quad 2 input NAND Gate. This post mainly covers pinout, datasheet, schematics, logic, circuit, and more details about the 74LS00 gate. Furthermore, there is a huge range of semiconductors, capacitors, resistors, and ICs in stock. Welcome your RFQ!

This video demonstrates Switch based NAND gate and 7400 integrated circuit IC.

Switch based NAND gate and 7400 integrated circuit IC demonstration beginner learning electronics

74LS00 Description

The 74LS00 is one of the most well-known and fundamental logic gates. AND, OR, and NOT are the three types of gates. Each of the three gates has a unique internal circuit and serves a different purpose in each device. Other gates such as NAND, NOR, XOR, and XNOR can be created by combining these three circuits. Transistors, resistors, and capacitors can be used to create all of these gates. When we construct these circuits, the size of a single gate exceeds our expectations.

74LS00 Pinout

74LS00  pinout.jpg

74LS00 Pinout

Pin NoPin Description
1A1-INPUT
2B1-INPUT
3Y1-OUTPUT
4A2-INPUT
5B2-INPUT
6Y2-OUTPUT
7GND
8Y3-OUTPUT
9A3-INPUT
10B3-INPUT
11Y4-OUTPUT
12A4-INPUT
13B4-INPUT
14VCC


74LS00 CAD Model

Footprint

74LS00  3d model.jpg

74LS00 Footprint

74LS00 Specifications

  • Operating voltage range: +4.75 to +5.25V

  • Maximum supply voltage: 7V

  • Maximum current allowed drawing through each gate output: 8mA

  • TTL outputs

  • Maximum ESD: 3.5KV

  • Typical Rise Time: 15ns

  • Typical Fall Time: 15ns

  • Operating temperature: 0°C to 75°C


74LS00 Features

  • It comes in a variety of packages, including SOIC, PDIP, and SOP.

  • It can be employed in systems with a high frequency.

  • This IC can be used as a NAND gate, but because of the NAND gate's universality, it can easily be transformed into other gates.

  • Because the IC's internal structure is based on TTL, its output is also TTL.


74LS00 Applications

  • General logic

  • Digital electronics

  • Computer and laptop

  • Server

  • ALU

  • Networking

  • Digital system


74LS00 Equivalents

Any two transistors can be modified to make a NAND gate, such as the SN54LS00, SN7400, or CD4011.


74LS00 Alternatives

74LS08, 74LS00CH,74LS00DC,74LS00J,74LS00N,74LS00NA,74LS00PC,74LS00W,901521-01,AMX3550,C74LS00P,DM74LS00N,EA33X8605,EAQ00-12100,ECG74LS00,GD74LS00,HD74LS00,HD74LS00P,HE-443-728


74LS00 Advantages

  • The IC features four NAND gates, each of which can be utilized for a different gate.

  • Because the NAND gate can be converted to a NOT gate by rearranging the pins, the 74LS00 can be utilized as an inverter.

  • The 74LS00 is one of the most affordable integrated circuits, making it more popular than other ICs.

  • Without the assistance of a microcontroller or processor, it could perform HIGH NAND speed operations in nanoseconds.


How to Use 74LS00

74LS00 2 input NAND Gate WORKING

The IC has four NAND gates; however, each NAND gate has two different types of internal structures. CMOS is the first, and PMOS is the second. When we observe the structure, it may appear to be changed, yet its primary function remains the same. Four transistors make up the CMOS NAND gate. The circuit is made up of transistors and a power source, and it produces the HIGH and LOW states depending on the input combinations. The NAND gate's internal construction is shown below.

74LS00 circuit.jpg

74LS00 Circuit


Q1 and Q2 will both be turned off. As a result, the total supply voltage is seen across transistors Q1 and Q2. Y1 will be HIGH because output Y1 is nothing but voltage across transistors Q1 and Q2.

When one of the inputs is HIGH, only the transistor closest to it will turn on, leaving the other off. The whole supply voltage appears across the transistor, which is in the OFF state, as a result of this. Y1 will be HIGH because output Y1 is the voltage across both transistors Q1 and Q2.

Both transistors will be ON when both inputs are HIGH, and the voltage across both of them will be zero.

Y1 will be LOW because output Y1 is the voltage across both transistors Q1 and Q2.

 


Examples with 74LS00 NAND Gate IC

74LS00 circuit2.jpg

74LS00 Circuit


Two inputs are connected to two buttons, while the output is connected to an LED. The ON and OFF states of this LED reveal the gate's output logic.

Both buttons are open and not pressed under usual conditions. Both of the gate's inputs will be LOW as a result. According to the truth table stated above, when both inputs are LOW, the output will be HIGH. The LED will light on since the output is high.

If one of the buttons is pressed. One of the inputs will be LOW, while the other will be HIGH. According to the truth table, the output will still be HIGH in this situation. The LED will light on since the output is high.

Only when both buttons are pressed will we get a LOW output, which will turn off the LED.

We discovered the truth table for chip NAND gate using these three scenarios. We can satisfy our needs by using all four gates in this manner.


74LS00 Package Dimension

74LS00  package dimension.jpg

74LS00 Package Dimension

74LS00 Manufacturer

Rochester Electronics ranks as a global leading semiconductor provider. Due to their products' characteristics of high quality and durability, these products are suitable for long-term production and maintenance in the fields of industry, transportation, and high-reliability markets. Their large inventory includes more than 100,000 products and 15 billion units, making them exceed other companies in terms of selection, capabilities, or solutions.


Frequently Asked Questions

74LS00 Manufacturer

74LS00 was used for performing the NAND function. The IC has four NAND gates in it. Each gate can be used separately.

What is the difference between 7400 and 74LS00?

The 74LS00 family improves technically on the 7400 families in two key areas: faster speed and lower power consumption. The only limitation of the 74LS00 family compared to the 7400 families is that the 74LS00 family can only source half as much current.

What is 74LS00 logic gates IC of digital electronics?

The 74LS00 is a TTL (Transistor to Transistor Logic) that uses low-power Shottky transistors to reduce the stored charge and get higher switching speeds than with conventional bipolar transistors. 74LS00 is a 14 pin IC that has four NAND gates each NAND gate has two inputs & one output.

How many 74ls00 NAND gate inputs can be driven by a 74ls00 NAND gate outputs?

The 74xxyy ICs are logic gates of digital electronics. 74LS00 IC has four NAND gates. Also, each gate has two inputs. Hence name QUAD TWO INPUT NAND GATE.
74LS00

ROCHESTER ELECTRONICS LLC

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe