D880 NPN Transistor: Datasheet, Pinout and Equivalent
D880A datasheet pdf and Unclassified product details from FeiHong stock available at Utmel









The D880 Transistor is a Low-Frequency Power Amplifier Transistor. This article enforces pinout, datasheet, equivalent, specifications, and more details about the D880 transistor. Furthermore, there is a huge range of semiconductors, capacitors, resistors, and ICs in stock. Welcome your RFQ!

Powerful Bass Amflifier Using D880 - How to Make Amplifier at Home
Overview of D880 Transistor
The D880 transistor is an NPN transistor with a TO-220 packaging. It's intended for audio frequency amplification, although it can be used for any general-purpose application that fits within its specifications. It can be used as a switch and can drive loads of up to 3A; with that much output current, it can drive motors, high-power transistors, and relays, for example. Because of its low saturation voltage, it can be used to drive a range of loads at the output of a variety of electrical platforms such as the Arduino and Raspberry Pi.
D880 Transistor Pinout
The D880 Transistor's pin configuration is shown below, along with its symbol. Each pin and its function are detailed below. This transistor has three terminals: E (emitter), B (base), and C (collector).

D880 Transistor Pinout
| Pin Number | Pin Name | Description |
| 1 | Base | Controls the biasing of the transistor, Used to turn ON or OFF the transistor |
| 2 | Collector | Current flows in through collector, normally connected to load |
| 3 | Emitter | Current Drains out through emitter, normally connected to ground |
D880 Transistor Features
Package Type: TO-220
Transistor Type: NPN
Max Collector Current(IC): 3A
Max Collector-Emitter Voltage (VCE): 60V
Max Collector-Base Voltage (VCB): 60V
Max Emitter-Base Voltage (VEBO): 7V
Max Collector Dissipation (Pc): 30 Watts
Max Transition Frequency (fT): 3 MHz
Minimum & Maximum DC Current Gain (hFE): 60 – 300
Max Storage & Operating temperature should be: -55 to +150 Centigrade
Specifications
- TypeParameter
- Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
TO-220 - Current-Collector (Ic) (Max)3A
- Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tube-packed - Power - Max
Power - Max is a parameter that specifies the maximum amount of power that an electronic component can handle without being damaged. It is typically measured in watts and indicates the upper limit of power that can be safely supplied to the component. Exceeding the maximum power rating can lead to overheating, malfunction, or permanent damage to the component. It is important to consider the power-max rating when designing circuits or systems to ensure proper operation and longevity of the electronic components.
30W - Voltage - Collector Emitter Breakdown (Max)
Voltage - Collector Emitter Breakdown (Max) is a parameter that specifies the maximum voltage that can be applied between the collector and emitter terminals of a transistor or other semiconductor device before it breaks down and allows excessive current to flow. This parameter is crucial for ensuring the safe and reliable operation of the component within its specified limits. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the device. Designers and engineers must carefully consider this parameter when selecting components for their circuits to prevent potential issues and ensure proper functionality.
60V - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
D880 Transistor Applications
DC-DC converts
Audio circuits
Amplifier circuits
Low voltage, medium current switching devices
D880 Transistor Equivalents
NTE152, SC1826, BD241, 2SB834, 2SC1060, 2SC1061, 2SC1173, 2SC1226, 2SC1226A, 2SC1418, 2SC1419, 2SC2236, 2SC2500, 2SC2075, 2SD1134, 2SD1274A, 2SC1985, 2SC1826, BDT31, BDT31A
Alternatives for D880
KSA1220, 2N5551, S8550, BD136, TIP32C
Where to Use D880 Transistor
The D880 transistor can be used in a wide range of applications. It can be used as a standalone amplifier to drive a speaker or for the construction of high-power audio amplifier circuits. Aside from that, it can be used as a switch and at the output of a variety of electronics platforms, ICs, and microcontrollers to drive loads such as motors, high-power relays, and lights, among other things.
How to Use D880 Transistor
We can achieve stable performance in a circuit by employing the D880 transistor. It is recommended that you use less than 20% of your total maximum ratings for this. Because the maximum collector current (Cc) is 3A, it cannot drive any load that consumes more than 2.4A. The maximum voltage from collector to emitter terminal is 60V thus do not drive any load above 48V. A suitable heat sink must be used in conjunction with a transistor, and the transistor must be operated at temperatures between -55 and +150 degrees Celsius at all times.

D880 Transistor Circuit
D880 Transistor Dimension Outline

D880 Transistor Dimension Outline
D880 Transistor Manufacturer
Feihong Machinery & Electrical Co, Ltd.(Tubemachines) is a leading heater machines factory in China. Our factory is located in Zhaoqing City, Guangdong Province, which is near Guangzhou, Foshan, and Shenzhen.
The heating machinery in Tubemachines is widely used in various heaters production. Such as machines for cartridge heaters, machines for hot runner heaters, machines for industrial heaters, machines for tubular heaters.
What is the use of D880 transistor?
The D880 Transistor is a Low-Frequency Power Amplifier Transistor. The transistor is often employed in amplifier circuits with a push-pull topology, such as class B amplifier circuits. A push-pull circuit, as we all know, necessitates the use of both NPN and complementary PNP transistors.
Can d882 and d880 be interchangeable?
D882: NPN; 30V; 7A; 10W; pin arrangement ECB; D880: NPN; 60V; 3A; 30W; pin arrangement BCE; If the actual working voltage does not exceed 30V and the current does not exceed 3A, they can be replaced with each other. If you want to replace under this condition, you can insert and weld the replaced transistor by rotating the text surface 180 degrees.
How to wire the d880 transistor?
The transistor is made of two PN junctions very close to each other on a semiconductor substrate. The two PN junctions divide the whole semiconductor into three parts. The middle part is the base area, and the two sides are the emitter and collector areas. The arrangement is PNP And NPN two kinds. The one with an arrow is the emitter (e), the one in the middle is the base (b) to the right of Q1, and the collector (c) to the far right is the collector (c).
24LC256 256K Serial EEPROM: Pinout, Equivalent and Datasheet17 December 20214449
STM32F070CBT6 Microcontroller: 48MHz,48-LQFP, Pinout and Features15 February 20222303
N76E003AT20 Microcontroller: Pinout, Datasheet and Programming27 October 202112970
AD9520-0BCPZ Clock Generators: Pinout, Feature, Specification14 August 2024614
TE Connectivity 1-968855-1 Terminal: Complete Automotive Wiring Guide28 August 2025244
STM32F051C6T7 Microcontroller: Datasheet, Pinout, Block Diagram13 September 20212441
M95512-R 512-Kbit serial SPI bus EEPROM: Pinout, Equivalent and Datasheet07 April 20225296
TCA6424ARGJR Expander: Features, Applications and Datasheet06 November 20231088
What is Network Topology?23 December 20214222
Classification and Characteristics of Microwave Filter14 December 20218990
The World's Top 10 Innovative LED Drivers12 February 20225160
800V HVDC Data Center Power: A Stage-by-Stage Component Shortlist for AI Racks18 August 2026346
Introduction to TTL and CMOS Logic Gate Circuits24 November 202523507
Humidity Sensor: Classification, Package and Application13 November 20255544
Top 10 IC Design Companies in China13 January 202210677
FPGA vs ASIC: Comprehensive Comparison Guide09 May 202515915
FeiHong
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools