web counter

ESP-12E Wi-Fi Module: Pinout, Datasheet and Power

UTMEL

Published: 18 September 2021 | Last Updated: 18 September 2021

21172

ESP-12S

ESP-12S

RF Solutions

2.412GHz~2.484GHz WiFi -20°C~85°C 3V~3.6V ADC, I2C, PWM, SPI, UART PCB Trace 54Mbps 16dBm 802.11b/g/n -90dBm Module

Unit Price: $7.655334

Ext Price: $7.66

Purchase Guide

2.412GHz~2.484GHz WiFi -20°C~85°C 3V~3.6V ADC, I2C, PWM, SPI, UART PCB Trace 54Mbps 16dBm 802.11b/g/n -90dBm Module

ESP-12E is a Wi-Fi Module featuring a highly competitive package size and ultra-low power technology. This article mainly covers pinout, datasheet, application, faq, and other details about ESP-12E. Furthermore, there is a huge range of Semiconductors, Capacitors, Resistors, and Ics in stock. Welcome RFQ!

In this video, I will explain how to prepare your Arduino IDE to upload sketches into the ESP8266 microcontroller and connect to an ESP-12E / ESP-12F board over USB.

Programming ESP-12E / ESP-12F / NodeMCU With Arduino IDE | Step by Step Guide

ESP-12E Pinout

esp-12e pinout .png

ESP-12E Pinout

PinNameDescription
1RSTReset Pin of the   module
2ADCAnalog Input Pin for   10-bit ADC (0V to1V)
3ENModule Enable Pin   (Active HIGH)
4GPIO16General Purpose Input   Output Pin 16
5GPIO14General Purpose Input   Output Pin 14
6GPIO12General Purpose Input   Output Pin 12
7GPIO13General Purpose Input   Output Pin 13
8VDD'+3.3V Power Input
9CS0Chip selection Pin of   SPI interface
10MISOMISO Pin of SPI   interface
11GPIO9General Purpose Input   Output Pin 9
12GPIO10General Purpose Input   Output Pin 10
13MOSIMOSI Pin of SPI   interface
14SILKClock Pin of SPI   interface
15GNDGround Pin
16GPIO15General Purpose Input   Output Pin 15
17GPIO2General Purpose Input   Output Pin 2
18GPIO0General Purpose Input   Output Pin 0
19GPIO4General Purpose Input   Output Pin 4
20GPIO5General Purpose Input   Output Pin 5
21RXD0UART0 RDX Pin
22TXD0UART0 TXD Pin


ESP-12E CAD Model

Symbol

esp12e symbol.png

Symbol


Footprint

esp12e footprint.png

Footprint


3D Model

esp12e 3d model.png

3D Model

What is ESP-12E?

ESP-12E is a Wi-Fi Module featuring a highly competitive package size and ultra-low power technology. ESP-12E can be widely used in a variety of networking, for home automation, industrial wireless control, baby monitors, wearable electronic products, wireless location sensing devices, wireless positioning system signals, and other networking applications. 


ESP-12E Block Diagram

esp12e block diagram.png

ESP-12E Block Diagram

Specifications

RF Solutions ESP-12S technical specifications, attributes, parameters and parts with similar specifications to RF Solutions ESP-12S.
  • Type
    Parameter
  • Factory Lead Time
    4 Weeks
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    Module
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -20°C~85°C
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    Not Applicable
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    3V~3.6V
  • Frequency

    In electronic components, the parameter "Frequency" refers to the rate at which a signal oscillates or cycles within a given period of time. It is typically measured in Hertz (Hz) and represents how many times a signal completes a full cycle in one second. Frequency is a crucial aspect in electronic components as it determines the behavior and performance of various devices such as oscillators, filters, and communication systems. Understanding the frequency characteristics of components is essential for designing and analyzing electronic circuits to ensure proper functionality and compatibility with other components in a system.

    2.412GHz~2.484GHz
  • Data Rate

    Data Rate is defined as the amount of data transmitted during a specified time period over a network. It is the speed at which data is transferred from one device to another or between a peripheral device and the computer. It is generally measured in Mega bits per second(Mbps) or Mega bytes per second(MBps).

    54Mbps
  • Protocol

    In electronic components, the parameter "Protocol" refers to a set of rules and standards that govern the communication between devices. It defines the format, timing, sequencing, and error checking methods for data exchange between different components or systems. Protocols ensure that devices can understand and interpret data correctly, enabling them to communicate effectively with each other. Common examples of protocols in electronics include USB, Ethernet, SPI, I2C, and Bluetooth, each with its own specifications for data transmission. Understanding and adhering to protocols is essential for ensuring compatibility and reliable communication between electronic devices.

    802.11b/g/n
  • Power - Output

    Power Output in electronic components refers to the amount of electrical power that a device can deliver to a load. It is typically measured in watts and indicates the effectiveness of the component in converting electrical energy into usable work or signal. Power Output can vary based on the component's design, operating conditions, and intended application, making it a critical factor in the performance of amplifiers, power supplies, and other electronic devices. Understanding the Power Output helps in selecting appropriate components for specific applications to ensure efficiency and reliability.

    16dBm
  • RF Family/Standard

    The parameter "RF Family/Standard" in electronic components refers to the specific radio frequency (RF) technology or standard that the component complies with or is designed for. RF technology encompasses a wide range of frequencies used for wireless communication, such as Wi-Fi, Bluetooth, cellular networks, and more. Different RF standards dictate the frequency bands, modulation techniques, data rates, and other specifications for communication systems. Understanding the RF family/standard of a component is crucial for ensuring compatibility and optimal performance in RF applications.

    WiFi
  • Antenna Type

    There are several different types of antennas in three broad categories: omni-directional, directional, and semi-directional.

    PCB Trace
  • Sensitivity

    Sensitivity in electronic components refers to the degree to which the output of a device responds to changes in input. It indicates how effectively a component translates a specific input signal into an observable output. High sensitivity means that even small variations in input can produce significant changes in output, making the device more responsive to signals. Sensitivity is crucial in applications where precise measurements or signal detection are required.

    -90dBm
  • Serial Interfaces

    A serial interface is a communication interface between two digital systems that transmits data as a series of voltage pulses down a wire. Essentially, the serial interface encodes the bits of a binary number by their "temporal" location on a wire rather than their "spatial" location within a set of wires.

    ADC, I2C, PWM, SPI, UART
  • Current - Transmitting

    Current - Transmitting is a parameter used to describe the maximum amount of electrical current that an electronic component can handle while in the transmitting mode. This parameter is crucial for components such as transistors, diodes, and integrated circuits that are involved in transmitting signals or power within a circuit. Exceeding the specified current transmitting rating can lead to overheating, component failure, or even damage to the entire circuit. Designers and engineers must carefully consider this parameter when selecting components to ensure the reliability and performance of the electronic system.

    11.1mA
  • Modulation

    In electronic components, modulation refers to the process of varying one or more properties of a periodic waveform, known as the carrier signal, in order to encode information. This modulation technique is commonly used in communication systems to transmit data efficiently over long distances. By modulating the carrier signal, information such as audio, video, or data can be embedded onto the signal for transmission and then demodulated at the receiving end to retrieve the original information. There are various types of modulation techniques, including amplitude modulation (AM), frequency modulation (FM), and phase modulation (PM), each with its own advantages and applications in different communication systems.

    64-QAM, BPSK, CCK
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

ESP-12E Features

  • The smallest 802.11b/g/n Wi-Fi SOC module

  • Low power 32-bit CPU, can also serve as the application processor

  • Up to 160MHz clock speed

  • Built-in 10 bit high precision ADC

  • Supports UART/HSPI/IIC/PWM/ADC

  • SMD-16 package for easy welding

  • Integrated Wi-Fi MAC/BB/RF/PA/LNA

  • Deep sleep current as low as 20uA

  • Embedded lwIP protocol stack

  • Supports STA/AP/STA + AP operation mode

  • Support Smart Config/AirKiss technology

  • UART baudrate up to 4Mbps

  • General AT commands can be used quickly

  • Supports remote firmware upgrade (FOTA)


ESP-12E Power Consumption

An ESP-12E module, for example, consumes an average of 70.5 mA when it is fully on (that is, when its WiFi modem and microcontroller are both on) even when the transceiver is inactive (neither receiving nor transmitting).


ESP-12E Applications

  • Weather station

  • IoT applications

  • Home appliances

  • Toys and Gaming applications

  • Wireless control systems

  • Home automation

  • Security ID tags


How to use ESP-12 E

esp-12e circuit.png

ESP-12E Circuit

Normally, to program the ESP8266-12E, you have to connect certain pins to each other, and to ground and VCC, and a few of the GPIO pins need to be connected correctly. You then connect the TX and RX pins to your USB-to-serial adapters like the FTDI or CP2102 or similar boards.


ESP-12E vs. ESP32

Both chips have a 32-bit processor. The ESP32 is a dual-core 160MHz to 240MHz CPU, whereas the ESP-12E is a single-core processor that runs at 80MHz.


ESP-12E Dimension

ESP-12E dimension.png

ESP-12E Dimension

ESP-12E Manufacturer

RF Solutions was founded in 2016 by experienced telecom professionals who wanted to use the best available technology and engineering services to make buildings safer and to protect critical infrastructure. Starting in the New York Metro area and branching out to adjoining states and beyond, we have received recognition for our leadership in the industry.


Datasheet PDF

Download datasheets and manufacturer documentation for RF Solutions ESP-12S.
Frequently Asked Questions

What is the function of ESP-12E chip?

ESP-12E is a miniature Wi-Fi module present in the market and is used for establishing a wireless network connection for a microcontroller or processor. The core of ESP-12E is ESP8266EX, which is a high integration wireless SoC (System on Chip).

Does ESP 12e have Bluetooth?

The Bluetooth connection is not necessary, but it allows the ESP/LDR to be placed out of the way on a shelf, not tethered to a laptop. Since there is only one dedicated Analog pin on the NODE boards, it is used for the LDR, and SoftwareSerial is used for the TX/RX Bluetooth pins.

How do I connect to ESP-12E?

Normally, to program the ESP-12E, you have to connect certain pins and to the ground and VCC, and a few of the GPIO pins need to be connected correctly. You then connect the TX and RX pins to your USB-to-serial adapters like the FTDI or CP2102 or similar boards.

Which pins are used for wifi esp 12e?

They are pin GND, GPIO15, GPIO2, and Flash.