web counter

rg6 vs rg11 Coaxials: What’s the Difference?

Sophie

Published: 31 March 2022 | Last Updated: 31 March 2022

58829

In choosing the correct coaxial cable to wire up an AV system, we often encounter the RG6 and RG11 designations. These cables are not the same and there are differences that need to be considered before choosing one over the other. So, Magi is here to tell you the difference between them.

This video is going to distinguish RG6 and RG11.

RG6 vs. RG11 - How Your Coaxial Cable Impacts TV Reception

Introduction

Coaxial cable types RG6 and RG11 are used to connect AVs, CCTVs, amplifiers, cellular signal boosters, and satellite TV systems. You'll come across these two cable classifications while looking for the proper cable. They're not the same, and there are several distinctions to consider while deciding between the two. When it comes to RG6 against RG11, here's what to expect.


What are RG coaxial cables?

RG Coaxial cables are the kind of coaxial cables utilized for efficient transmission solutions for Telecom systems that include Satellite communication, Marine, Mobile communication, AM, FM, Inbuilding, and Radar Communication systems, video, and more.


How is Coaxial Cable Constructed?

The center core of the coaxial cable is made of a single copper or copper-coated steel wire, which transmits the high-frequency signal. This wire is encased in a dielectric insulator, which is usually composed of plastic and keeps the distance between the center conductor and the following layer constant. A metal shield consisting of braided copper, aluminum, or another metal is wrapped around this insulator. Outside electromagnetic interference is canceled as a result of this. The final layer is a rubber wrapper that protects the entire setup.

 

With a few exceptions, the coaxial wire can be utilized in both indoor and outdoor applications. Outdoor use of coax needs additional insulation to keep the wires safe from the sun and rain. Outdoor-rated cables can be connected along the outside of your house to a satellite dish or a cable box on the corner. Whether exposed to the sun or buried in the ground, the cable must be sufficiently covered to ensure uninterrupted communications.


Rg6 Overview

RG6.jpg

RG6

RG6 is a type of coaxial cable with a protective sheath, an inner conductor surrounded by a cylindrical conducting shield, and a dielectric between the two. These cables are favored because of their long lifespan. RG6 cables are suitable for everyday networking and connecting requirements. Because it is thin, flexible, and requires less area to install.

 

RG6 is not good for long-range because the signal gets fluctuated and the originality is lost. RG6 is cheap and affordable. It is also preferred more by people for indoor connections. Lopping over other connections or cables is easy with RG6 cables because of their thinness. RG6 uses an F-type connector or a coaxial RF connector which is good for domestic connections. RG6 has a center conductor of 18 gauge wire.


Rg11 Overview

RG11.jpg

The RG11 cable is a coaxial radio guide cable with a protective wrapping around it. RG11 is a thicker version that covers a larger area. Because of its thickness, signal fluctuation is reduced, and the signal's authenticity is preserved. Long-range signal strength is favored with RG11, which is typically utilized for outdoor or unusual applications.

 

F-type connections are also used in RG11, which are good for signal strength. Because of its thickness, RG11 is not extremely flexible, making bending and looping difficult. When signal strength is the primary goal of installation, RG11 is the best option. Because of its rough and sturdy construction, RG11 is exceptionally durable and requires little care. The center conductor of RG11 is a 14 gauge wire.


Rg6 vs Rg11: Difference in Attenuation

RG6 has more signal loss compared to RG11. The RG11 cable will give you a better signal at its end compared to the end of the RG6 when given a specific length of cable. Meanwhile, noticeable attenuation will only happen to the RG11 cable once you start using longer RG11 cables since the signal travels longer distances, leading to attenuation.


Rg6 vs Rg11: Difference in Applications

Coaxial Cables, as the name implies, are electrical cables where the inner conductor & the outer conductor, share a common spatial axis and have dielectric insulation.

 

RG6 Coaxial Cable (nominal diameter - 7mm), finds its applications in Cable TV, Dish TV, TV Antenna, Broadband internet and can carry signals up to 450 meters.

 

RG11 Coaxial Cable (nominal diameter - 10mm), has similar applications as above but is used either in harsher environmental conditions and/or where signals need to be carried long distances up to 600 meters.


Rg6 vs Rg11: Difference in Price

The RG11 cable's most significant disadvantage is its greater price per meter. Because it is frequently utilized for long distances, the price increase can soon add up. The thickness of the cable and the conductor itself within the cable are the reasons for the greater pricing. A higher manufacturing cost is directly proportional to the number of materials used. The overall thickness of the RG6 cable is thinner because the conductor within is lower in diameter.


Rg6 vs Rg11: Difference in Flexibility

Another problem with the GR11 is the lack of flexibility, because of the thickness of the cable. As a result, RG11 cables are difficult, if not impossible, to utilize in conventional residential connections. The RG11 wire isn't designed to bend around bends or turn sharply. The RG6 is significantly better for this, which is why it is frequently used in residential setups. The RG11 coax cable is frequently used in backbone deployments when two sites separated by a significant distance must be connected.


Rg6 vs Rg11: Comparison Chart

CategoriesRG6RG11
UsesMostly used for satellite cablesOnly reserved for special uses
PriceLess expensiveMore expensive
ThicknessRG6 is0.375 inches.weak signal strengthRG11 is 0.75.  good signal strength.
FlexibilityMore flexible and less stiffLess flexible and stiffer
AttenuationMore signal lossLess signal loss
Center Conductor18AWG14AWG
Connector typesRG6 uses F-type connectors.RG11 also uses F-type connectors.


Conclusion

For various reasons, different wires or cables are required. As a result, there are many different types of cables on the market. When it comes to long-distance signal transmission, RG11 is favored. When it comes to indoor connections or wiring, however, RG6 is the standard. Because of its thick exterior covering and durability, RG11 is pricey. And in RG11, the signal strength or output quality is preserved.

 

RG6 is a flexible cable that may be looped over other connections with ease. Because RG6 cables are tiny and require less space for installation, they are commonly used for TV cables. Both RG6 and RG11 have a plastic jacket covering the outer layer, followed by a metallic shield, the center core, and a dielectric insulator barrier between the metallic shield and the center core. Because it delivers better signal strength and maintains the signal's uniqueness, RG11 is more expensive than RG6.


Frequently Asked Questions

When should I use RG11?

RG11 are thick cables used for special and long-distance signal purposes. It is mostly used in television connections, CCTV connections, and HTDV, etc. Because of its thickness, it does not bend easily or is not very flexible; therefore, indoor connections do not go easy with RG11.

What is RG6 used for?

The RG-6 is primarily used for cable and satellite signal transmission for residential or commercial installations. This coax cable is thin and easy to bend for wall or ceiling installations and remains the preferred choice to relay cable television signals.

What is RG11 cable used for?

RG11 Coaxial Cables are used for Wide Broadband with far signal transmission distance, often used as the main cable line in transmitting observing camera data, Cable Television, etc.

What coaxial cable is best for HDTV?

The best coaxial cable for HDTV is RG-11. This type of cable offers a higher gauge than others, which provides more space for signals to transfer. This makes the RG-11 cable adept at transferring strong HD signals at speed.

Does coax cable affect Internet speed?

Coax cable does not inherently slow down your Internet. In fact, because coax cable wiring is intentionally designed to carry extremely high-bandwidth data, you can harness this wiring using MoCA technology to transform and boost your Internet speeds.
RG6WR,TW

Belden Inc.

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More