web counter

SIM800L VS SIM900A[Video&FAQ]: How to differentiate them?

UTMEL

Published: 28 April 2022 | Last Updated: 28 April 2022

19251

SIM800L

SIM800L

SIMCom Wireless Solutions

SIM800L datasheet pdf and Unclassified product details from SIMCom Wireless Solutions stock available at Utmel

Purchase Guide

SIM800L and SIM900A all belong to the small cellular modules that can send and receive GPRS data, send and receive SMS, and make and receive voice calls. This article is going to talk about the pinout, features, application, and more detailed information about them.

This video demonstrates detailed information about Sim800L and sim900A, and interpret the differences between them.

Sim800L and sim900A Issues

Overview of SIM800L

  • The Mini GSM / GPRS breakout board is based on the SIM800L module, which supports a quad-band GSM/GPRS network and can send GPRS and SMS message data remotely. The board is small in size and consumes little power. In sleep mode, the current consumption is as low as 1mA thanks to the power conservation technology. It uses a UART port to interface with the microcontroller and supports commands such as 3GPP TS 27.007, 27.005 and SIMCOM improved AT Commands.

  • The SIM800L Component allows you to make phone calls, send text messages, and receive them. A UART bus must be used to link the device, which must support both receiving and transmitting lines. The UART bus must be set to the same speed as the module, which is 9600bps by default. +VCC, GND, RX, and TX are the needed connecting wires.


Overview of SIM900A

  • SIM900A Modem is based on SIMCOM's Dual Band GSM/GPRS SIM900A modem. It operates over the 900/ 1800 MHz band. SIM900A can automatically search these two bands. AT Commands can also be used to change the frequency bands. The baud rate can be changed from 1200-to 115200 using the AT command. The inbuilt TCP/IP stack on the GSM/GPRS modem allows you to connect to the internet through GPRS.

  • SIM900A is a wireless module that is both small and dependable. This is a complete GSM/GPRS module in SMT format, developed with a high-performance single-chip processor based on the AMR926EJ-Score, allowing for tiny dimensions and cost-effective solutions.


SIM800L VS SIM900A Features

SIM800L Features

  • Supports Quad-band: GSM850, EGSM900, DCS1800 and PCS1900

  • Connect onto any global GSM network with any 2G SIM

  • Make and receive voice calls using an external 8Ω speaker & electret microphone

  • Send and receive SMS messages

  • Send and receive GPRS data (TCP/IP, HTTP, etc.)

  • Scan and receive FM radio broadcasts

  • Transmit Power:

    -Class 4 (2W) for GSM850

    -Class 1 (1W) for DCS1800

  • Serial-based AT Command Set

  • FL connectors for cell antennae

  • Accepts Micro SIM Card

 

SIM900A Features

  • Single supply voltage: 3.4V – 4.5V

  • Power saving mode: Typical power consumption in SLEEP mode is 1.5mA

  • Frequency bands: SIM900A Dual-band: EGSM900, DCS1800. The SIM900A can search the two frequency bands automatically. The frequency bands also can be set by AT command.

  • GSM class: Small MS

  • GPRS connectivity:GPRS multi-slot class 10 (default) , GPRS multi-slot class 8 (option)

  • Transmitting power: Class 4 (2W) at EGSM 900, Class 1 (1W) at DCS 1800

  • Operating Temperature: -30ºC to +80ºC

  • Storage Temperature: -5ºC to +90ºC

  • DATA GPRS: download transfer max is 85.6KBps, Upload transfer max 42.8KBps

  • Supports CSD, USSD, SMS, FAX

  • Supports MIC and Audio Input

  • Speaker Input

  • Features keypad interface

  • Features display interface

  • Features Real-Time Clock

  • Supports UART interface

  • Supports single SIM card          

  • Firmware upgrade by debug port

  • Communication by using AT commands


SIM800L VS SIM900A Pinout

SIM800L Pinout.png

SIM800L Pinout


SIM900A Pinout.png

SIM900A Pinout

SIM800L VS SIM900A Dimensions

SIM800L Dimensions.png

SIM800L Dimensions


SIM900A Dimensions.png

SIM900A Dimensions

How to use the SIM800L?

The SIM800L is a GSM module with a serial interface. It can send and receive text messages and receive phone calls. It can also connect to the internet and receive FM signals. The SIM800L can be connected to a microcontroller using the serial UART interface, and in the example shown below, connected to an Arduino.

How to use the SIM800L.png

The module recognizes AT commands, which can be used to do things like check signal strength, get the SIM card number, check the network connection and battery state, in addition to reading texts, and making and receiving calls.


How to use the SIM900A?

How to use the SIM900A.png

The module is usually powered by a conventional +4.0V power source. It requires +4.5V regulated electricity to operate, and any greater voltage may cause harm to the module. Furthermore, the power source must be capable of delivering a peak current of 2A. The UART interface is set up as shown in the diagram. Simply connect the RXD of the module to the TXD of the Arduino, and the TXD to the RXD of the ARDUINO.

For voltage reference, the controller and module's ground must be linked. The MIC is connected to AUDIO IN, while the speaker or headset is connected to AUDIO OUT. Finally, we must attach a functional GSM SIM card to the module. On powering the module, the NET LIGHT LED will blink periodically to state a successful connection.


SIM800L VS SIM900A Equivalents

SIM800L Equivalents

 

SIM900A Equivalents


SIM800L VS SIM900A Applications

SIM800L Applications

  • Remote System Monitoring

  • Home Alarm System

  • Remote Controlling System

  • Security Access Control

  • Vehicle tracking

  • SMS Gateway

  • Pre-paid Electricity

 

SIM900A Applications

  • Cellular Communication

  • Robotics

  • Mobile Phone Accessories

  • Servers

  • Computer Peripherals

  • Automobile

  • USB Dongles


SIM800L VS SIM900A Specifications

SpecificationSIM800LSIM900A
Supply voltage3.4V to 4.4V3.4V to 4.4V
Bands supportedGSM850, EGSM900, DCS1800, PCS1900GSM850, EGSM900, DCS1800, PCS1900
Cellular network2G2G
Audio I/O8Ω speaker, electret micEarphone, electret mic
DataSMS, GPRS, FMSMS, GPRS, FM
Transmit powerClass 4 (2W) GSM850 Class 1 (1W) DCS1800Class 4 (2W) GSM850 Class 1 (1W) DCS1800
Communication with microcontrollerSerial based ATSerial based AT
AntennaFL connectorUFL, SMA connectors
SIM CardMicro SIMFull-size SIM


Major Differences Between SIM800L and SIM900A

SIM800LSIM900A
Newer moduleOlder module, nearing obsolescence
Support for Bluetooth and FMNo support for Bluetooth


Conclusion of SIM800L VS SIM900A

When comparing the SIM800L with SIM900A in many aspects, the major difference between them is that the SIM800L is a newer module, and the SIM900A is the older module. Additionally, the SIM800L Supports Bluetooth and FM, while the SIM900A does not support Bluetooth. The SIM800L is a newer and improved version of the SIM900A that includes more capabilities such as Bluetooth connectivity and FM reception, as well as greater signal reception and a lower price.


SIM800L VS SIM900A Datasheet

Popularity by Region

Frequently Asked Questions

What is a SIM800L?

The SIM800L is a small cellular module that can send and receive GPRS data, send and receive SMS, and make and receive voice calls. This module's low cost, small footprint, and quad-band frequency capabilities make it an ideal choice for any project requiring long-range connectivity.

What is a SIM900A?

The SIM900A GSM Module is the smallest and cheapest GPRS/GSM module available. In most embedded applications, Arduino and microcontroller are used. The module uses GPRS/GSM technology to communicate with a mobile sim card.

What are the differences between the SIM800L and SIM900A?

The SIM800L and SIM900A GSM modules are extremely identical, with the exception that the SIM800L model supports Bluetooth and has AT instructions for Bluetooth/FM.

Which is better SIM800 vs SIM900?

The SIM800C modem works with a supply voltage range of 3.4 to 4.4 volts (reduced operating range!). The SIM900 and SIM900A modules have a supply voltage range of 3.2V to 4.8V. The SIM800 has a pin for connecting to a Bluetooth Antenna. Apart from these distinctions, the hardware design is nearly identical.

Does SIM800L support 3G?

The SIM800 is a GSM/GPRS-only modem module. It can use either a 2G-only SIM or a 3G/4G USIM.
SIM800L

SIMCom Wireless Solutions

In Stock: 5

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe