SMAJ15A TVs Diodes: Features, Pinout, and Datasheet

Sophie

Published: 15 February 2022 | Last Updated: 15 February 2022

2905

SMAJ15A

SMAJ15A

Littelfuse Inc.

TVS DIODE 15V 24.4V DO214AC

Purchase Guide

TVS DIODE 15V 24.4V DO214AC

SMAJ15A is a Transient Voltage Suppression Diode. This article mainly introduces features, pinout, datasheet and other detailed information about Littelfuse Inc. SMAJ15A.

This video will show you how to create a surge protection circuit which is also known as a transient suppressor circuit using zener diodes and a fuse.

High Voltage Surge Protection Transient Suppressor Circuit Using Zener Diodes & Fuses

SMAJ15A Description

The SMAJ15A is created to protect sensitive electronic equipment against voltage transients such as those caused by lightning and other transient voltage events.

Surge and ESD protection is provided by the SMAJ series Transient Voltage Suppressor Diode  . The device has a working peak reverse voltage range of 5V to 495V, as well as a breakdown voltage range of 550V. From 0V to minimal breakdown voltage, typical quick response times for unidirectional devices are less than 1-picosecond and less than 5-picosecond for bidirectional devices. It complies with  JEDEC  requirements, is simple to handle with ordinary pick and place equipment, and its flat design reduces roll-away.


SMAJ15A Pinout

The following figure is SMAJ15A Pinout.

pinout.jpg

Pinout


SMAJ15A CAD Model

The following figures are SMAJ15A Symbol, Footprint and 3D Model.

symbol.png

Symbol

footprint.png

Footprint

3d model.jpg

3D Model


SMAJ15A Features

• 400W Power dissipation

• -55 to 150°C Operating temperature range

• 400W Peak pulse power capability at 10/1000µs waveform, repetition rate (duty cycle): 0.01%

• Excellent clamping capability

• Typical IR less than 1μA when VBR min>12V

• For surface mounted applications to optimize board space

• Low profile package

• Typical failure mode is short from over-specified voltage or current

• Whisker test is conducted based on  JEDEC 

JESD201A per its table 4a and 4c

• IEC-61000-4-2  ESD  30kV(Air), 30kV (Contact)

• ESD protection of data lines in accordance with  IEC  61000-4-2

• EFT protection of data lines in accordance with IEC 61000-4-4

• Built-in strain relief

• Fast response time: typically less than 1.0ps from 0 Volts to VBR min

• Glass passivated junction

• Low inductance

• High temperature to reflow soldering guaranteed: 260°C/40sec

• VBR @ TJ= VBR@25°C x (1+αT x (TJ - 25))(αT:Temperature Coefficient, typical value is 0.1%)

• Plastic package is flammability rated V-0 per  Underwriters Laboratories 

• Meet MSL level1, per J-STD-020, LF maximum peak of 260°C

• Matte tin lead–free Plated

• Halogen-free and  RoHS  compliant

• Pb-free E3 means 2nd level interconnect is Pb-free and the terminal finish material is tin(Sn) (IPC/JEDEC J-STD-609A.01)


Specifications

Littelfuse Inc. SMAJ15A technical specifications, attributes, parameters and parts with similar specifications to Littelfuse Inc. SMAJ15A.
  • Type
    Parameter
  • Factory Lead Time
    17 Weeks
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    Surface Mount
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    DO-214AC, SMA
  • Number of Pins
    2
  • Supplier Device Package

    The parameter "Supplier Device Package" in electronic components refers to the physical packaging or housing of the component as provided by the supplier. It specifies the form factor, dimensions, and layout of the component, which are crucial for compatibility and integration into electronic circuits and systems. The supplier device package information typically includes details such as the package type (e.g., DIP, SOP, QFN), number of pins, pitch, and overall size, allowing engineers and designers to select the appropriate component for their specific application requirements. Understanding the supplier device package is essential for proper component selection, placement, and soldering during the manufacturing process to ensure optimal performance and reliability of the electronic system.

    DO-214AC (SMA)
  • Breakdown Voltage / V
    16.7V
  • Number of Elements
    1
  • Reverse Stand-off Voltage
    15V
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -65°C~150°C TJ
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • Series

    In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.

    SMAJ
  • Published
    2009
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Termination

    Termination in electronic components refers to the practice of matching the impedance of a circuit to prevent signal reflections and ensure maximum power transfer. It involves the use of resistors or other components at the end of transmission lines or connections. Proper termination is crucial in high-frequency applications to maintain signal integrity and reduce noise.

    SMD/SMT
  • Type
    Zener
  • Max Operating Temperature

    The Maximum Operating Temperature is the maximum body temperature at which the thermistor is designed to operate for extended periods of time with acceptable stability of its electrical characteristics.

    150°C
  • Min Operating Temperature

    The "Min Operating Temperature" parameter in electronic components refers to the lowest temperature at which the component is designed to operate effectively and reliably. This parameter is crucial for ensuring the proper functioning and longevity of the component, as operating below this temperature may lead to performance issues or even damage. Manufacturers specify the minimum operating temperature to provide guidance to users on the environmental conditions in which the component can safely operate. It is important to adhere to this parameter to prevent malfunctions and ensure the overall reliability of the electronic system.

    -65°C
  • Composition

    Parameter "Composition" in electronic components refers to the specific materials and substances used in the construction of the component. It encompasses the chemical and physical elements that make up the component, influencing its electrical, thermal, and mechanical properties. The composition can affect the performance, reliability, and durability of the component in various applications. Understanding the composition is essential for optimizing the design and functionality of electronic devices.

    Zener
  • Applications

    The parameter "Applications" in electronic components refers to the specific uses or functions for which a component is designed. It encompasses various fields such as consumer electronics, industrial automation, telecommunications, automotive, and medical devices. Understanding the applications helps in selecting the right components for a particular design based on performance, reliability, and compatibility requirements. This parameter also guides manufacturers in targeting their products to relevant markets and customer needs.

    General Purpose
  • Power Rating

    The "Power Rating" of an electronic component refers to the maximum amount of power that the component can handle or dissipate without being damaged. It is typically measured in watts and is an important specification to consider when designing or selecting components for a circuit. Exceeding the power rating of a component can lead to overheating, malfunction, or even permanent damage. It is crucial to ensure that the power rating of each component in a circuit is sufficient to handle the power levels expected during normal operation to maintain the reliability and longevity of the electronic system.

    400W
  • Voltage - Rated DC

    Voltage - Rated DC is a parameter that specifies the maximum direct current (DC) voltage that an electronic component can safely handle without being damaged. This rating is crucial for ensuring the proper functioning and longevity of the component in a circuit. Exceeding the rated DC voltage can lead to overheating, breakdown, or even permanent damage to the component. It is important to carefully consider this parameter when designing or selecting components for a circuit to prevent any potential issues related to voltage overload.

    15V
  • Max Power Dissipation

    The maximum power that the MOSFET can dissipate continuously under the specified thermal conditions.

    3.3W
  • Operating Supply Voltage

    The voltage level by which an electrical system is designated and to which certain operating characteristics of the system are related.

    15V
  • Polarity

    In electronic components, polarity refers to the orientation or direction in which the component must be connected in a circuit to function properly. Components such as diodes, capacitors, and LEDs have polarity markings to indicate which terminal should be connected to the positive or negative side of the circuit. Connecting a component with incorrect polarity can lead to malfunction or damage. It is important to pay attention to polarity markings and follow the manufacturer's instructions to ensure proper operation of electronic components.

    Unidirectional
  • Number of Channels
    1
  • Leakage Current

    Leakage current is a term used in electronics to describe the small amount of current that flows through a component when it is supposed to be in a non-conductive state. This current can occur due to imperfections in the materials used to manufacture the component, as well as other factors such as temperature and voltage. Leakage current can lead to power loss, reduced efficiency, and potential reliability issues in electronic devices. It is important to consider and minimize leakage current in electronic components to ensure proper functionality and performance.

    1μA
  • Element Configuration

    The distribution of electrons of an atom or molecule (or other physical structure) in atomic or molecular orbitals.

    Single
  • Power Dissipation

    the process by which an electronic or electrical device produces heat (energy loss or waste) as an undesirable derivative of its primary action.

    400W
  • Power Line Protection

    During fault, the only circuit breaker closest to the fault point should be tripped. The operating time of relay associated with protection of line should be as minimum as possible in order to prevent unnecessary tripping of circuit breakers associated with other healthy parts of power system.

    No
  • Voltage - Breakdown (Min)

    Voltage - Breakdown (Min) is a parameter used to specify the minimum voltage level at which an electronic component, such as a diode or capacitor, will break down and allow current to flow through it uncontrollably. This breakdown voltage is a critical characteristic that determines the maximum voltage the component can withstand before failing. It is important to ensure that the applied voltage does not exceed this minimum breakdown voltage to prevent damage to the component and maintain proper functionality. Manufacturers provide this specification to help engineers and designers select components that are suitable for their intended applications and operating conditions.

    16.7V
  • Power - Peak Pulse

    Power - Peak Pulse refers to the maximum transient power level that an electronic component, such as a diode or a transzorber, can safely dissipate during a short-duration pulse. This parameter is critical in determining the component's ability to withstand voltage spikes or surges without failure. It is typically expressed in watts and is measured over a specific duration, usually in microseconds or nanoseconds, to reflect the component's performance under peak conditions. Understanding this parameter helps designers select appropriate components for applications where transient conditions are expected.

    400W
  • Current - Peak Pulse (10/1000μs)

    The parameter "Current - Peak Pulse (10/1000μs)" in electronic components refers to the maximum current that a device can handle during a transient overvoltage event with a specific waveform, typically a 10/1000μs pulse. This parameter is important for surge protection devices such as transient voltage suppressors (TVS) and varistors, as it indicates the device's ability to divert excess current away from sensitive components and protect them from damage. A higher peak pulse current rating signifies better surge protection capability, making the component more suitable for applications exposed to high-voltage transients or lightning strikes. Designers should carefully consider this parameter when selecting surge protection components to ensure reliable operation and protection of their electronic circuits.

    16.4A
  • Max Reverse Leakage Current

    Max Reverse Leakage Current refers to the maximum amount of current that can flow through a semiconductor device, such as a diode or transistor, when it is reverse biased. This current is an important parameter as it indicates the level of unintended current that can flow when the device is not conducting in the forward direction. High values of reverse leakage current can lead to power loss, reduced efficiency, and may affect the performance and reliability of electronic circuits. It is particularly critical in applications where precise current control and low power consumption are necessary.

    1μA
  • Voltage - Clamping (Max) @ Ipp

    Voltage - Clamping (Max) @ Ipp refers to the maximum voltage that a component, such as a transient voltage suppressor or diode, can clamp when subjected to a specific peak current (Ipp). It indicates the upper limit of voltage that the component will allow to pass through, effectively protecting sensitive circuits from overvoltage conditions. This parameter is crucial for ensuring that devices are safeguarded against voltage spikes without being damaged. Designers use this specification to select appropriate components for overvoltage protection in their applications.

    24.4V
  • Clamping Voltage

    Clamping voltage is a term used in electronic components, particularly in devices like diodes and transient voltage suppressors. It refers to the maximum voltage level at which the component can effectively limit or clamp the voltage across its terminals. When the voltage across the component exceeds the clamping voltage, the component conducts and effectively limits the voltage to that level, protecting the circuit from overvoltage conditions. Clamping voltage is an important parameter to consider when selecting components for applications where voltage spikes or surges may occur, as it determines the level at which the component will start to protect the circuit.

    24.4V
  • Voltage - Reverse Standoff (Typ)

    Voltage - Reverse Standoff (Typ) refers to the maximum reverse voltage that a semiconductor device, such as a diode or a transient voltage suppressor, can withstand without entering into breakdown. It is typically specified as a nominal value and indicates the voltage level at which the device transitions from its non-conducting state to a conducting state when reverse-biased. Exceeding this voltage can lead to permanent damage or failure of the component. This parameter is crucial for ensuring the safe operating limits of electronic circuits, particularly in protecting sensitive components from voltage spikes.

    15V
  • Peak Pulse Current

    The peak pulse power rating of a TVS diode is defined as the instantaneous power dissipated by a device for a given pulse condition, and is a measure of the power that is dissipated in the TVS junction during a given transient event.

    16.4A
  • Max Surge Current

    Surge current is a peak non repetitive current. Maximum (peak or surge) forward current = IFSM or if(surge), the maximum peak amount of current the diode is able to conduct in forward bias mode.

    16.4A
  • Peak Pulse Power

    Peak Pulse Power is a parameter used to specify the maximum amount of power that an electronic component can handle during a transient event, such as a surge or spike in voltage or current. It indicates the maximum power dissipation capability of the component for a short duration. This parameter is important for protecting electronic circuits from damage caused by sudden high-energy events. Peak Pulse Power is typically expressed in watts and is crucial for selecting components that can withstand transient overloads without failing. It helps ensure the reliability and longevity of electronic systems in various applications.

    400W
  • Direction

    In electronic components, the parameter "Direction" refers to the orientation or alignment in which the component is designed to operate effectively. This parameter is particularly important for components such as diodes, transistors, and capacitors, which have specific polarity or orientation requirements for proper functionality. For example, diodes allow current flow in one direction only, so their direction parameter indicates the correct orientation for current flow. Similarly, polarized capacitors have a positive and negative terminal, requiring proper alignment for correct operation. Understanding and adhering to the direction parameter is crucial for ensuring the reliable and efficient performance of electronic components in a circuit.

    Unidirectional
  • Test Current

    Test Current refers to a specified amount of electrical current applied to an electronic component during testing to evaluate its performance and characteristics. This current is typically defined by manufacturers to ensure that the component operates within its designed parameters. By measuring how the component reacts to this test current, engineers can determine its reliability, efficiency, and suitability for specific applications.

    1mA
  • Unidirectional Channels

    Unidirectional channels in electronic components refer to pathways that allow the flow of electrical current in only one direction. These channels are essential in devices like diodes, which permit current to pass through while blocking any reverse flow. Their primary function is to control and direct the flow of electricity, ensuring that circuit operation remains efficient and protects components from potential damage due to reverse currents. Unidirectional channels are commonly used in power supply circuits, signal rectification, and various electronic applications where controlled current flow is crucial.

    1
  • Reverse Breakdown Voltage

    Reverse Breakdown Voltage is the maximum reverse voltage a semiconductor device can withstand before it starts to conduct heavily in the reverse direction. It is a critical parameter in diodes and other components, indicating the threshold at which the material's insulating properties fail. Beyond this voltage, the device may enter a breakdown region, leading to potential damage if not properly managed. This parameter is essential for ensuring safe operation and reliability in electronic circuits.

    16.7V
  • Max Breakdown Voltage

    The "Max Breakdown Voltage" of an electronic component refers to the maximum voltage that the component can withstand across its terminals before it breaks down and allows current to flow uncontrollably. This parameter is crucial in determining the operating limits and safety margins of the component in a circuit. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the component. It is typically specified by the manufacturer in datasheets to guide engineers and designers in selecting the appropriate components for their applications.

    18.5V
  • Number of Unidirectional Channels
    1
  • Max Junction Temperature (Tj)

    Max Junction Temperature (Tj) refers to the maximum allowable temperature at the junction of a semiconductor device, such as a transistor or integrated circuit. It is a critical parameter that influences the performance, reliability, and lifespan of the component. Exceeding this temperature can lead to thermal runaway, breakdown, or permanent damage to the device. Proper thermal management is essential to ensure the junction temperature remains within safe operating limits during device operation.

    150°C
  • Height
    2.29mm
  • Length
    4.5mm
  • Width
    2.79mm
  • REACH SVHC

    The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.

    No SVHC
  • Radiation Hardening

    Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.

    No
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
  • Lead Free

    Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.

    Lead Free
0 Similar Products Remaining

Parts with Similar Specs

The three parts on the right have similar specifications to Littelfuse Inc. & SMAJ15A.

SMAJ15A Functional Diagram

The following figure is SMAJ15A Functional Diagram.

Functional Diagram.png

Functional Diagram


SMAJ15A Part Numbering System

The following figure is SMAJ15A Part Numbering System.

Part Numbering System.png

Part Numbering System


SMAJ15A Part Marking System

The following figure is SMAJ15A Part Marking System.

Part Marking System.png

Part Marking System


SMAJ15A Alternatives

Part NumberDescriptionManufacturer
SMAJ15A-GDIODESTrans Voltage Suppressor Diode, 400W, 15V V(RWM), Unidirectional, 1 Element, Silicon, DO-214AC, LEAD FREE, PLASTIC, SMA, 2 PINSangdest Microelectronics (Nanjing) Co Ltd
SMAJ15A-GT3DIODESTrans Voltage Suppressor Diode, 400W, 15V V(RWM), Unidirectional, 1 Element, Silicon, DO-214AC, LEAD FREE, PLASTIC, SMA, 2 PINSangdest Microelectronics (Nanjing) Co Ltd
SMAJ15A-13DIODESTrans Voltage Suppressor Diode, 400W, 15V V(RWM), Unidirectional, 1 Element, Silicon, PLASTIC, SMA, 2 PINDiodes Incorporated
SMAJ15AHE3/5ADIODESDIODE 400 W, UNIDIRECTIONAL, SILICON, TVS DIODE, DO-214AC, ROHS COMPLIANT, PLASTIC, SMA, 2 PIN, Transient SuppressorVishay Semiconductors
SMAJ15AE3/TR13DIODESTrans Voltage Suppressor Diode, 400W, 15V V(RWM), Unidirectional, 1 Element, Silicon, DO-214AC, ROHS COMPLIANT, PLASTIC, SMA, 2 PINMicrosemi Corporation
SMAJ15A-7DIODESTrans Voltage Suppressor Diode, 400W, 15V V(RWM), Unidirectional, 1 Element, Silicon, PLASTIC, SMA, 2 PINDiodes Incorporated
SMAJ15A/11DIODESTrans Voltage Suppressor Diode, 400W, Unidirectional, 1 Element, Silicon, DO-214AC, PLASTIC, SMA, 2 PINVishay Semiconductors
SMAJ15AHE3_A/HDIODESTrans Voltage Suppressor Diode,Vishay Intertechnologies
SMAJ15A/61DIODESTrans Voltage Suppressor Diode, 15V V(RWM), Unidirectional,Vishay Intertechnologies
SMAJ15AHM3/HDIODESTrans Voltage Suppressor Diode,Vishay Intertechnologies


SMAJ15A Applications

• The Protection of I/O Interfaces

• VCC Bus and Other Vulnerable Circuits Used in Telecom

• Industrial

• Consumer Electronic Applications

• Communications & Networking

• Computers & Computer Peripherals

• Imaging

• Video & Vision


SMAJ15A Package

The following figure is SMAJ15A Package.

package.png

Package


SMAJ15A Manufacturer

Littelfuse, Inc. is an electronic manufacturing company situated in Chicago, Illinois. The company's major focus is circuit protection, although it also develops electronic switches and car sensors. Littelfuse first opened its doors in 1927. In addition to its world headquarters in Chicago, Illinois, Littelfuse has more than 40 sales, distribution, production, and engineering offices throughout the Americas, Europe, and Asia.


Datasheet PDF

Download datasheets and manufacturer documentation for Littelfuse Inc. SMAJ15A.
Frequently Asked Questions

How does a transient voltage suppressor diode work?

Transient Voltage Suppressor Diode is a clamping device, so whenever the induced voltage exceeds the avalanche breakdown voltage, it absorbs the excess energy of the overvoltage event, and then it automatically resets after overvoltage condition.

Which diode that is used for transient voltage suppression?

The Transient Voltage Suppressor diode (also known as a TVS Diode) is a protection diode designed to protect electronic circuits against transients and overvoltage threats such as EFT (electrically fast transients) and ESD (electro-static discharge).

Where should a TVS diode be placed?

Place TVs diode near the edge of the PCB. To enable the excessive surge current to be channeled to the chassis ground before damaging the transceiver, the placement of the TVS diode is also important. It is a good practice to place TVS diodes as close to the edge of the board as possible.
SMAJ15A

Littelfuse Inc.

In Stock: 19271

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More