SR621SW VS SR626SW[Video]: Are they interchangeable?
MURATA 364 BATTERY SR 1.55V 6.8M
SR621SW and SR626SW are all coin batteries with a voltage of 1.55. This article is going to talk about the detailed information about SR621SW and SR626SW, and interpret the differences between them.

memilih baterai jam tangan | kualitas tahan lama
Overview of SR621SW
The SR621SW is a Silver-Oxide cell with a 5-year shelf life that is extensively used in clocks. Other applications include calculators, film cameras, medical tools, cash registers, and financial instruments (measuring instruments, onboard microcomputers, sensors). This is an "SW" battery with a low drain. Low-drain batteries are perfect for devices like analog timepieces, TV remote controls, and alarm clocks that require a small quantity of power over a lengthy period of time. High-drain batteries, on the other hand, are used in devices that have a steady low power consumption with occasional high peaks, such as analog and digital watches with additional functions (backlight, alarm), pocket calculators, electronic games, cameras, and so on.
Overview of SR626SW
The SR626SW is a silver oxide watch battery that can be used to replace obsolete batteries or to change the chemistry of coin cells currently in use. Coin cells, which use a silver oxide chemistry, offer a lower self-discharge and a more steady output voltage, making them ideal for powering low-draining, continuous-use devices. Watches, calculators, heart-rate monitors, glucometers, small electronic toys, and keyless remote entry systems for cars and homes are all good candidates for a Murata 377-sized battery. Because these batteries are a specialty size that isn't one-size-fits-all, be sure your equipment is compatible before purchasing.
SR621SW VS SR626SW Dimensions

SR621SW Dimension

SR626SW Dimension
SR621SW VS SR626SW Characteristics

SR621SW Characteristics

SR626SW Characteristics
SR621SW VS SR626SW Applications
SR621SW Applications
Timepieces
TV remote controls
Alarm clocks
Pocket calculators
Electronic games
Cameras
SR626SW Applications
Watch battery
Pagers
Memory backup
Security devices
Hand-held electronic devices
SR621SW VS SR626SW Equivalents
SR621SW VS SR626SW Specifications
| Model | SR621SW 364 | SR626SW | |
| Nominal Voltage | 1.55V | 1.55V | |
| Nominal Capacity | 23mAh [cov:1.20V] | 28mAh [cov:1.20V] | |
| Standard Discharge Current | 40μA | 40μA | |
| Operating Temperature Range | -10 to +60 (deg. C) | -10℃~+60℃ | |
| Weight | 0.32g | 0.39g | |
| Dimensions | Diameter | 6.8㎜ | 6.80㎜ |
| Height | 2.15㎜ | 2.60㎜ | |
| Images | ![]() | ![]() | |
Conclusion of SR621SW VS SR626SW
The major differences between the SR621SW and SR626SW are nominal capacity and dimension. The nominal capacity of SR626SW is higher than SR621SW. The nominal capacity of SR621SW is 23mAh, while the nominal capacity of SR626SW is 28mAh, which means SR621SW can deliver more amps in an hour than SR626SW and can last longer than the SR621SW. Additionally, the height of SR621SW and SR626SW is different. The height of SR621SW is 2.15 mm, and the height of SR626SW is 2.6 mm. So they are not interchangeable and the application of they are applied in different places.
SR621SW VS SR626SW Datasheet
SR621SW Manufacturer
Seiko Instruments Inc. (SII) was founded in 1937 as the Seiko Group's primary watch manufacturer. The company provides micro mechatronics products and services, such as watch and HDD components, semiconductors, FPD and electronic devices, network solutions systems, nanotechnology equipment, scientific instruments, and large-format inkjet printers, based on sophisticated micro mechatronics and nanotechnology techniques developed through decades of experience in precision machinery manufacturing and low-power consumption technologies.
Parts with Similar Specs
Popularity by Region
Can you replace SR621SW with SR626SW?
The SR626SW and SR621SW batteries are only 0.5 mm apart in height, which isn't much; nonetheless, battery compartments designed for SR626SW cells may take smaller SR621SW batteries.
What battery replaces SR621SW?
SR621SW, SR60, SR621, SB-AG/DG, 280-34, T, V364, D364, 602, S621E, GP364, AG1, AG-1, 364, L621, LR621, SG1, LR60, LR620, SW621, GP164, 364X, 364A, AG1/364A, SB-AG, E364 batteries are all direct replacements.
What battery can replace SR626SW?
The Energizer 377/376 is a multi-drain 1.55 Volt silver oxide button cell battery. Primarily used as watch batteries, 377 376 replaces SR626W and SR626SW batteries.
How long do SR621SW batteries last?
SR621SW runs 5 years.
What are the differences between the SR621SW with SR626SW?
The nominal capacity and dimension are the main variations between the SR621SW and SR626SW. SR626SW has a higher nominal capacity than SR621SW. The SR621SW has a nominal capacity of 23mAh, whereas the SR626SW has a nominal capacity of 28mAh, implying that the SR621SW can deliver more amps per hour and last longer than the SR626SW. Furthermore, the heights of SR621SW and SR626SW differ. SR621SW has a height of 2.15 mm, whereas SR626SW has a height of 2.6 mm.
CD4071 Dual Input OR Gate IC: Datasheet, Pinout and Equivalents23 October 20215850
2N2646 PN Unijunction Transistor: Datasheet, Pinout and Equivalent21 October 202121012
STM32F103RCT6 Microcontroller: 72MHz, 64-LQFP, Pinout and Datasheet07 February 20226158
TL431 Shunt Regulator: How to Test and Replace?26 April 202220021
LM317 Voltage Regulator[Video+FAQ]: Pinout, Circuit, LM317 VS LM7805 and Datasheet27 April 202213263
TPS2553DBVR Power-Distribution Switch: Layout, Pinout, and Datasheet25 March 20224234
DS1090 Clock Generator: Pinout, Equivalent and Datasheet21 February 2022584
DS1820 Digital Thermometer: Pinout, Datasheet and Comparison04 August 20215690
Stanford Engineer Sheds Light on Semiconductors: Their Importance, Challenges, and Future22 September 20231865
What is an Inverting Amplifier?25 April 20259710
All About Video Connectors and Their Uses in Today’s Technology02 July 20252573
What is Mini LED?08 December 20205806
What is a Delay Circuit? 6 Types of Delay Circuits Explained28 March 202548934
Reverse Voltage Protection for Battery Chargers29 March 20224378
Introduction to Inductive Reactance16 April 202112591
What is Solenoid Valve? How to Choose a Solenoid Valve?06 January 20223190
Murata
In Stock