web counter

TP4056 Standalone Linear Li-Lon Battery Charger: Datasheet, Schematics and Current

UTMEL

Published: 18 October 2021 | Last Updated: 18 October 2021

40281

TP4056

TP4056

TPOWER

TP4056 datasheet pdf and Unclassified product details from TPOWER stock available at Utmel

Purchase Guide

TP4056 is a 1A standalone linear Li-Lon battery charger with thermal regulation in sop-8. This article enforces the datasheet, battery, current, schematic, module, and more details about the TP4056 charger. Furthermore, there is a huge range of semiconductors, capacitors, resistors, and Ics in stock. Welcome your RFQ!

This TP4056 or TC4056  1000mA USB Lithium battery charger first explained, the wiring is shown , then connected via external 5V sources battery charge is tested.

TC4056 TP4056 USB 18650 Lithium Battery Protection Charger Review

What is TP4056?

The TP4056 module is a lithium-ion battery linear charger. This module is capable of charging single-cell batteries. Most importantly, it offers to charge modes with constant current and constant voltage. The TP4056 is also a battery charger with a 4.2-volt set charge voltage.


TP4056 Pinout

TP4056 PINOUT.jpg

TP4056 Pinout

No:Pin NameDescription
1OUT +These pins output the positive voltage from the battery. It should be connected to the circuit which   has to be powered by the battery
2B +Outputs positive voltage from the USB cable to charge to the battery. It should be connected to the   positive of the battery
3B -Outputs negative voltage from USB cable for charging the battery. It should be connected to the negative of the battery
4OUT -This pin outputs negative voltage from the battery. It should be connected to the ground of the circuit which has to be powered by the battery
5IN +Should provide +5V,   can be used if charge cable not available
6IN -Should provide the ground   of the +5V supply, can be used if charge cable not available
7LED RedThis LED turns on   while the battery is charging
8LED GreenThis LED turns on   after the battery is fully charged


Specifications

TPOWER TP4056 technical specifications, attributes, parameters and parts with similar specifications to TPOWER TP4056.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    ESOP-8
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

TP4056 Features

  • This module can charge and discharge Lithium batteries safely

  • Suitable for 18650 cells and other 3.7V batteries

  • Charging current – 1A (adjustable)

  • Input Voltage: 4.5V to 5.5V

  • Full charge voltage 4.2V

  • Protects battery from overcharging and over-discharging

  • No verse polarity protection


TP4056 Equivalents

TP4056A (only charging), TP541


TP4056 Applications

  • Solar Chargers

  • Digital Cameras

  • Portable Home Appliances

  • Cell Phones & Tablets

  • Charge and Discharge Lithium cells

  • Commonly used with 18650 Li-ion batteries

  • Power banks

  • Used with 5V booster for powering Arduino projects


TP4056 Typical Applications

The charging current of the module is set to 1A by default. However, it can be changed by altering the resistor RPROG (R3 on the module) in the circuit diagram. The datasheet for the TP4056 datasheet may be seen below for more information.

TP4056 typical application.jpg

TP4056 Application Circuit

 

The module will automatically stop charging after the Lithium battery is fully charged, and the Red LED will turn off and the Green LED will turn on to signal completion. As illustrated in the pin diagram above, the circuit can now be connected to the Circuit (Load) that must be powered by this battery. The voltage of the battery will be monitored as it is consumed by the circuit by the module (load). When it falls below the crucial level (3.7V), the module will separate your battery from the load and safeguard it from over-discharge.


Where to Use TP4056

It is ideal for charging 18650 cells and other 3.7V batteries because of its capacity to supply 4.2V. Because it only requires a few external components, it can be used in portable applications. Mobile phones, tablets, laptops, cameras, power banks, and a variety of other electronic gadgets all consume batteries; hence this module is used to charge them. This module can also be utilized with a USB port and a wall adaptor.


How to use TP4056

The TP4056 module is powered by a 5V supply from a micro USB cable or the IN+ and IN- solder pads. For the charger to correctly charge a battery connected at the output terminals, a current of at least 1A is necessary. Connect the B+ and B- connections to the cell you want to charge. The battery's power is supplied through the OUT+ and OUT- pads. As a result, if you're running a load, you can attach it to these two pads. But remember to disconnect the load from the module if you're charging a cell.

TP4056 connection diagram.jpg

TP4056 Connection Schematic


TP4056 Dimension

TP4056 dimension.jpg

TP4056 Dimension

TP4056 Manufacturer

Frequently Asked Questions

What does a TP4056 do?

The TP4056 chip is a lithium-Ion battery charger for a single cell battery, protecting the cell from over and undercharging. It has two status outputs indicating charging in progress and charging complete. You can use it to charge batteries directly from a USB port since the working input voltage range is 4V ~ 8V.

How does TP4056 module work?

The charge voltage is fixed at 4.2V, and the charge current can be programmed externally with a single resistor. The TP4056 automatically terminates the charge cycle when the charge current drops to 1/10th the programmed value after the final float voltage is reached.

How many batteries can a TP4056 charge?

You can connect two lithium battery cells in parallel to form an equivalent single cell battery with a total capacity of twice that of the individual single cells, but we do not recommend connecting more than two cells at a time to this module.

What is output voltage of TP4056?

Output voltage: DC 4.2V. 4 chips, with a reasonable turn-off voltage, the charging circuit for each chipset 750mA, total 3A. Input connected two 5A Schottky diodes, 5V standard voltage input chip heat ideal (3.8V battery test). 

Can TP4056 charge multiple batteries?

Don't. Just use one TP4056 and connect both cells in parallel after balancing them first. Don't connect batteries with more than 0.2V difference in parallel as this can risk fire and explosions (excessive charging current from one to another).
TP4056

TPOWER

In Stock: 4254

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe