1N4148 VS 1N4007 VS 1N5819: Brief introduction of 1N4148, 1N5819 and 1N4007 diodes
Standard Diode Rectifier Small Signal =< 200mA (Io), Any Speed 1V @ 10mA -65°C~175°C 5μA @ 75V Cut Tape (CT) DO-204AH, DO-35, Axial Through Hole









Standard Diode Rectifier Small Signal =< 200mA (Io), Any Speed 1V @ 10mA -65°C~175°C 5μA @ 75V Cut Tape (CT) DO-204AH, DO-35, Axial Through Hole
1N4148, 1N5819, and 1N4007 are all semiconductor diodes. This article is going to talk about the detailed information about the 1N4148, 1N5819, and 1N4007, and interpret the difference between them.
- What is the diode?
- Overview of 1N4148
- Overview of 1N4007
- Overview of 1N5819
- 1N4148 VS 1N4007 VS 1N5819 Features
- 1N4148 VS 1N4007 VS 1N5819 Pinout
- 1N4148 VS 1N4007 VS 1N5819 Specifications
- 1N4148 VS 1N4007 VS 1N5819 Applications
- 1N4148 VS 1N4007 VS 1N5819 Equivalents
- 1N4148 VS 1N4007 VS 1N5819 Datasheet
- Conclusion of 1N4148 VS 1N4007
- Conclusion of 1N4148 vs 1N5819
- Popularity by Region
What is the diode?
A diode is a two-terminal electrical device that enables just one direction of electricity to flow. The diode is also renowned for its unidirectional current feature, which allows electricity to flow in only one direction. In radio detectors and power supplies, a diode is used to rectify waveforms in theory. They can also be employed in a variety of electrical and electronic circuits that require a 'one-way' diode outcome. The majority of diodes are composed of semiconductors such as Si (silicon), but Ge (germanium) is also utilized in a few circumstances.
There are several types of diodes and those are available for use in electronics design, such as Laser diode, Light emitting diodes, crystal diode, PN Junction, Shockley diode, Zener diode, and many others.
Overview of 1N4148
A diode is a semiconductor device that only enables current to flow in one direction. The current must always flow from the anode to the cathode. A grey bar, as illustrated in the figure above, identifies the cathode terminal.
The IN4148 Diode can endure peaks of up to 2A and has a maximum current carrying capacity of 300mA. Because of its quick recovery time of 8ns at a forward current of 10mA, this diode is employed in applications that require fast switching.
Overview of 1N4007
A diode is a semiconductor device that allows just one direction of electricity to flow. The current has to flow from the anode to the cathode at all times. The cathode terminal can be identified by a grey bar, as shown in the image above.
The 1N4007 Diode has a maximum current carrying capacity of 1A and can sustain peaks of up to 30A. As a result, it can be used in circuits requiring less than 1A. At 5uA, the reverse current is negligible. The power dissipation of this diode is 3W.
Overview of 1N5819
In a large area metal-to-silicon power diode, 1N5819 uses the Schottky Barrier principle. Chrome barrier metal, epitaxial structure with oxide passivation, and metal overlap contact are all part of the state-of-the-art geometry. Ideal for usage as rectifiers, free-wheeling diodes, and polarity protection diodes in low voltage, high-frequency inverters.
1N4148 VS 1N4007 VS 1N5819 Features
1N4148 Features
High Reliability
Low Current Leakage
Metallurgical Bonded Construction
Moisture Sensitivity Level 1
Marking: Cathode band and type number
Lead-Free Finish/Rohs Compliant (Note1) ("P" Suffix designates Compliant. See ordering information)
1N4007 Features
Halogen-free is available upon request by adding the suffix "-HF"
Low Current Leakage and Low Cost
Lead-Free Finish/RoHS Compliant
Epoxy meets UL 94 V-0 flammability rating
Moisture Sensitivity Level 1
1N5819 Features
Extremely Low VF
Low Stored Charge, Majority Carrier Conduction
Low Power Loss/High Efficiency
These are Pb−Free Devices*
1N4148 VS 1N4007 VS 1N5819 Pinout

1N4007 Pinout

1N4148 Pinout

1N5819 Pinout
1N4148 VS 1N4007 VS 1N5819 Specifications
| 1N4148 | 1N4007 | 1N5819 | |
| Voltage - Forward (Vf) (Max) @ If | 1V @ 10mA | 1.1V @ 1A | 600mV @ 1A |
| Voltage - DC Reverse (Vr) (Max) | 75V | 1000V | 40V |
| Package / Case | DO-204AH, DO-35, Axial | DO-204AL, DO-41, Axial | DO-204AL, DO-41, Axial |
| Operating Temperature | -65°C~175°C | -55°C~175°C | ‘-65°C~125°C |
| Current - Reverse Leakage @ Vr | 5μA @ 75V | 5μA @ 1000V | 500μA @ 40V |
| Current - Average Rectified | 150mA | 1A | 1A |
1N4148 VS 1N4007 VS 1N5819 Applications
1N4148 Applications
Extreme fast switches
High-frequency signal circuits
Industrial control circuits
Computer boards
Communication
1N4007 Applications
Rectification of power supplies
Inverters
Converters
Freewheeling diodes application
1N5819 Applications
Inverters
DC-DC converters
1N4148 VS 1N4007 VS 1N5819 Equivalents
1N4148 VS 1N4007 VS 1N5819 Datasheet
Conclusion of 1N4148 VS 1N4007
IN4148 is a low-current inductive load commonly used in buzzers and other low-current inductive loads. However, heavy current loads, such as industrial loads (relays) and power supply loads, frequently employ 1N4007. The current, voltage and response speed are the most significant differences between them. The 1N4148 is a switching diode with a voltage of 100V and a current of 150mA. It features a low nS level and a fast reversal speed. The 1N4007 is a common rectifier diode with a reverse recovery time of uS and can withstand 1000V and 1A current. Only low-frequency circuits are suited for its use.
1N4007 can, in my opinion, replace 1N4148 as long as the response speed isn't too fast. Only low-current inductive loads with weak current should be used with 1N4148. If you're replacing a 1N4148 with a 1N4007, pay special attention to the reaction time.
Conclusion of 1N4148 vs 1N5819
1N5819 has a high switching speed (low switching loss), a low forward voltage drop (low voltage loss), and a low reverse withstand voltage (typically less than 60V), making it ideal for low-voltage (no more than 12V) switching power supplies. The reverse characteristic of the 1N5819 diode can also be used to stabilize the voltage. As a result, when the withstand voltage is low and the current is low, a Zener tube can be used instead. The 1N4148 is a high-speed, low-current, high-frequency switching diode with a working current of only 150 milliamperes. It is commonly employed in circuits with higher signal frequencies.
The 1N4148 is a high-speed, low-current, high-frequency switching diode with a working current of only 150 milliamperes. It is commonly employed in circuits with higher signal frequencies. Although the reverse leakage of the 1N5819 tube is rather significant, it possesses small capacitance and high speed. However, it is not as fast as the 1N4148; after all, the 1N4148 is designed for high-frequency detection rather than rectification.
Popularity by Region
What is the difference between 1N4148 and 1N4007?
The 1N4148 is a 100V, 150mA switching diode. It is of the nS level and has a quick reverse recovery speed. The 1N4007 is a low-frequency rectifier diode that can tolerate 1000V, 1A current, and has a reverse recovery time of uS.
What is the 1N4148 diode used for?
The 1N4148 diode is a tiny, high-speed switching diode with quick switching. Single supply isolation for high-frequency signal circuits, industrial control circuits, computer boards, communication, TV, and other applications are among its most common uses.
Can I use 1N4007 instead of 1N4148?
In some ways, 1N4007 can replace 1N4148 as long as the response speed isn't too high; 1N4148 is only suitable for low-current inductive loads with the weak current.
What are the differences between the 1N4148 vs 1N5819?
The reverse leakage of 1N5819 tube is relatively large, but it has the characteristics of small capacitance and high speed. But it is not as fast as 1N4148, after all, the purpose of 1N4148 is high frequency detection, not rectification.
PIC10F200/202/204/206 Microcontrollers: Technical Insights29 February 2024291
MIC5205 150mA Low-Noise LDO Regulator: Pinout, Datasheet pdf and Circuit25 November 20213320
2SJ162 P-Channel MOSFET: 2SJ162 MOSFET, Price, Datasheet [Video]24 December 20214063
What you need to know about using C1740 [FAQ]31 March 20228949
ATSAMD21G18AAUT Microcontroller: Technical Overview29 February 2024222
Xilinx XC2C512-10FT256I CPLD: Ultra-Low Power Design Solutions for Battery-Operated Embedded Systems07 June 2025369
LP2951 Voltage Regulator: Pinout, Equivalent and Datasheet23 October 20213840
STM32F318K8U6 Microcontroller: Technical Analysis and Overview28 February 2024291
Optocouplers Guide: Understanding Types, Applications, and Circuit Design Tutorial06 June 20254986
‘6G Networks’ - Pioneering the Next Era of Connectivity And Innovation18 March 20243922
STMicroelectronics: The European Powerhouse in Silicon Carbide Semiconductor Technology05 October 20233560
RF Technology: Complete Guide to Specifications, Frequency Bands, Components, and Applications22 June 2026790
Introduction to Step-up Transformer01 March 20216914
What is the Difference between an Integrated Circuit and a Chip04 August 202620223
Resistor Symbols: From Circuit Diagrams to PCB Design06 June 202620407
Clock&Timing - Application Specific: A Dedicated Chip That Helps Produce Signals on the Circuit Board22 February 20232325
Micro Commercial Co
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools