DS18S20 Temperature Sensor: Datasheet, Pinout and Comparison

UTMEL

Published: 01 November 2021 | Last Updated: 01 November 2021

2621

DS18S20

DS18S20

Maxim Integrated

Bulk Digital, Local 3V~5.5V Through Hole -55°C~125°C 1-Wire® ±0.5°C (±2°C) 8 b 1 (Unlimited)

Purchase Guide

Bulk Digital, Local 3V~5.5V Through Hole -55°C~125°C 1-Wire® ±0.5°C (±2°C) 8 b 1 (Unlimited)

DS18S20 is a high-precision 1-wire digital thermometer. This post enforces pinout, datasheet, applications, features, comparison, and other details about the DS18S20 temperature sensor. Furthermore, there is a huge range of semiconductors, capacitors, resistors, and ICs in stock. Welcome your RFQ!

In this video discussed about DS18S20 One Wire Bus supported temperature Sensor and how to interface the sensor to Arduino Uno Board.

DS18S20 One Wire Bus Temperature Sensor Interfacing to Arduino Board

What is a DS18S20 Temperature Sensor?

The DS18S20 digital thermometer measures temperatures in 9-bit Celsius and offers a nonvolatile alarm function with user-programmable upper and lower trigger points. Furthermore, the DS18S20 may get power directly from the data line ("parasitic power"), removing the need for an external power supply.


DS18S20 Pinout

ds18s20 pinout.jpg

DS18S20 Pinout

DS18S20 CAD Model

ds18s20 symbol.jpg

DS18S20 Symbol


ds18s20 footprint.jpg

DS18S20 Footprint


ds18s20 3d model.jpg

DS18S20 3D Model


Specifications

Maxim Integrated DS18S20 technical specifications, attributes, parameters and parts with similar specifications to Maxim Integrated DS18S20 .
  • Type
    Parameter
  • Factory Lead Time
    6 Weeks
  • Contact Plating

    Contact plating (finish) provides corrosion protection for base metals and optimizes the mechanical and electrical properties of the contact interfaces.

    Tin
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    PCB, Through Hole
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Through Hole
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    TO-226-3, TO-92-3 (TO-226AA)
  • Number of Pins
    3
  • Test Conditions
    -10°C ~ 85°C (-55°C ~ 125°C)
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -55°C~125°C
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Bulk
  • Published
    2003
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e3
  • Pbfree Code

    The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.

    yes
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    3
  • Termination

    Termination in electronic components refers to the practice of matching the impedance of a circuit to prevent signal reflections and ensure maximum power transfer. It involves the use of resistors or other components at the end of transmission lines or connections. Proper termination is crucial in high-frequency applications to maintain signal integrity and reduce noise.

    SMD/SMT
  • Connector Type

    Connector Type in electronic components refers to the specific design and configuration of the connector used to establish electrical connections between different devices or components. This parameter describes the physical shape, size, and layout of the connector, as well as the number and arrangement of pins or contacts. Common connector types include USB, HDMI, RJ45, and D-sub connectors, each serving different purposes and applications. Understanding the connector type is crucial for ensuring compatibility and proper functionality when connecting electronic devices together.

    Solder
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    3V~5.5V
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    DS18S20
  • Output Type

    The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.

    1-Wire®
  • Interface

    In electronic components, the term "Interface" refers to the point at which two different systems, devices, or components connect and interact with each other. It can involve physical connections such as ports, connectors, or cables, as well as communication protocols and standards that facilitate the exchange of data or signals between the connected entities. The interface serves as a bridge that enables seamless communication and interoperability between different parts of a system or between different systems altogether. Designing a reliable and efficient interface is crucial in ensuring proper functionality and performance of electronic components and systems.

    Serial
  • Operating Supply Current

    Operating Supply Current, also known as supply current or quiescent current, is a crucial parameter in electronic components that indicates the amount of current required for the device to operate under normal conditions. It represents the current drawn by the component from the power supply while it is functioning. This parameter is important for determining the power consumption of the component and is typically specified in datasheets to help designers calculate the overall power requirements of their circuits. Understanding the operating supply current is essential for ensuring proper functionality and efficiency of electronic systems.

    1mA
  • Nominal Supply Current

    Nominal current is the same as the rated current. It is the current drawn by the motor while delivering rated mechanical output at its shaft.

    1mA
  • Output Current

    The rated output current is the maximum load current that a power supply can provide at a specified ambient temperature. A power supply can never provide more current that it's rated output current unless there is a fault, such as short circuit at the load.

    4mA
  • Number of Bits
    9
  • Resolution

    Resolution in electronic components refers to the smallest increment of measurement or change that can be detected or represented by the component. It is a crucial specification in devices such as sensors, displays, and converters, as it determines the level of detail or accuracy that can be achieved. For example, in a digital camera, resolution refers to the number of pixels that make up an image, with higher resolution indicating a greater level of detail. In analog-to-digital converters, resolution is the number of discrete values that can be represented in the digital output, determining the precision of the conversion process. Overall, resolution plays a significant role in determining the performance and capabilities of electronic components in various applications.

    8 b
  • Sensor Type

    In electronic components, the parameter "Sensor Type" refers to the specific type of sensor technology used in a particular component to detect and measure physical phenomena such as light, temperature, pressure, motion, or proximity. Different sensor types utilize various principles and mechanisms to convert the detected input into an electrical signal that can be processed by the electronic component. Common sensor types include photodiodes, thermistors, accelerometers, and proximity sensors, each designed for specific applications and environments. Understanding the sensor type is crucial for selecting the right component for a given task and ensuring accurate and reliable sensing capabilities in electronic systems.

    Digital, Local
  • Max Supply Voltage (DC)

    The parameter "Max Supply Voltage (DC)" in electronic components refers to the maximum voltage that can be safely applied to the component without causing damage. This specification is crucial for ensuring the reliable operation and longevity of the component within a given circuit. Exceeding the maximum supply voltage can lead to overheating, breakdown of internal components, or even permanent damage. It is important to carefully adhere to this specification when designing or using electronic circuits to prevent potential failures and ensure the safety of the components.

    5.5V
  • Min Supply Voltage (DC)

    The parameter "Min Supply Voltage (DC)" in electronic components refers to the minimum voltage level required for the component to operate properly. It indicates the lowest voltage that can be safely applied to the component without causing damage or malfunction. This parameter is crucial for ensuring the reliable and stable operation of the component within its specified operating range. It is important for designers and engineers to adhere to the specified minimum supply voltage to prevent potential issues such as erratic behavior, reduced performance, or permanent damage to the component.

    3V
  • Housing

    Housing in electronic components refers to the physical enclosure that protects the internal circuitry and components from environmental factors such as dust, moisture, and mechanical damage. It provides structural support and electrical insulation while facilitating heat dissipation. The design and materials used for housing are crucial for the reliability and performance of the electronic device, as they impact factors like thermal management, electromagnetic interference, and overall aesthetics.

    PLASTIC
  • Accuracy - Highest (Lowest)

    In electronic components, "Accuracy - Highest (Lowest)" refers to the range within which the actual value of a parameter can deviate from the ideal or specified value. The term "Highest" indicates the upper limit of this range, while "Lowest" indicates the lower limit. For example, if a component has an accuracy of ±5%, the highest accuracy would mean that the actual value could be within 5% above the specified value, while the lowest accuracy would mean it could be within 5% below the specified value. This parameter is crucial for ensuring the reliability and performance of electronic devices by determining how closely the component's output matches the desired value.

    ±0.5°C (±2°C)
  • Sensing Temperature - Local

    Sensing Temperature - Local refers to the capability of an electronic component to measure the temperature in its immediate environment or vicinity. This parameter is crucial for applications that require monitoring of temperature for performance, safety, or stability purposes. It often involves temperature sensors integrated within components like microcontrollers, power regulators, or other integrated circuits. The local sensing allows for accurate temperature readings that help in adjusting operational conditions, ensuring optimal performance, and preventing thermal-related failures.

    -55°C~125°C
  • Accuracy-Max

    Accuracy-Max refers to the maximum permissible error in the output of an electronic component or system, typically expressed as a percentage of the nominal value. It indicates the extent to which the measured or calculated value can deviate from the true value under specified conditions. This parameter is crucial for ensuring reliable performance, especially in applications where precision is critical. A lower Accuracy-Max signifies better accuracy and higher quality in measurement and control processes.

    0.5 Cel
  • Features

    In the context of electronic components, the term "Features" typically refers to the specific characteristics or functionalities that a particular component offers. These features can vary depending on the type of component and its intended use. For example, a microcontroller may have features such as built-in memory, analog-to-digital converters, and communication interfaces like UART or SPI.When evaluating electronic components, understanding their features is crucial in determining whether they meet the requirements of a particular project or application. Engineers and designers often look at features such as operating voltage, speed, power consumption, and communication protocols to ensure compatibility and optimal performance.In summary, the "Features" parameter in electronic components describes the unique attributes and capabilities that differentiate one component from another, helping users make informed decisions when selecting components for their electronic designs.

    Programmable Limit, Standby Mode
  • Height
    4.95mm
  • Length
    4.95mm
  • Width
    3.94mm
  • REACH SVHC

    The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.

    Unknown
  • Radiation Hardening

    Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.

    No
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
  • Lead Free

    Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.

    Lead Free
0 Similar Products Remaining

DS18S20 Features and Advantages

  • Unique 1-Wire® Interface Requires Only One Port Pin for Communication

  • Maximize System Accuracy in Broad Range of Thermal Management Applications

    • Measures Temperatures from -55°C to +125°C (-67°F to +257°F)

    • ±0.5°C Accuracy from -10°C to +85°C

    • 9-Bit Resolution

    • No External Components Required

  • Parasite Power Mode Requires Only 2 Pins for Operation (DQ and GND)

  • Simplifies Distributed Temperature-Sensing Applications with Multidrop Capability

    • Each Device Has a Unique 64-Bit Serial Code Stored in On-Board ROM

  • Flexible User-Definable Nonvolatile (NV) Alarm Settings with Alarm Search Command Identifies Devices with Temperatures outside Programmed Limits

  • Available in 8-Pin SO (150 mils) and 3-Pin TO-92 Packages



DS18S20 Block Diagram

ds18s20 block diagram.jpg

DS18S20 Block Diagram

DS18S20 Applications

Thermostatic Controls

Industrial temperature controller

Consumer Products

Thermometers

Thermally Sensitive Systems

Liquid temperature measurement

Buildings temperature controller

Digital thermometers


DS18S20 Equivalent

DS18B20


DS18S20 Alternatives

TMP100, LM75, DHT11, SHT15, LM35DZ, TPA81, D6T


Parts with Similar Specs

The three parts on the right have similar specifications to Maxim Integrated & DS18S20 .

Where to Use DS18S20

DS18S20 is a high-precision 1-wire digital thermometer. It's commonly used to detect the temperature in harsh settings like chemical solutions, mines, and soil, among other things. The sensor's construction is tough, and it may also be ordered with a waterproof variant, making installation simple. It has a good accuracy of 5°C and can measure a wide range of temperatures from -55°C to +125°C. Each sensor has its address and only uses one MCU pin to transport data, making it an excellent choice for sensing temperature at various locations without sacrificing too many of your microcontroller's digital pins.


DS18s20 interfacing with PIC16F877A microcontroller

The circuit diagram for the DS18S20 interface is shown below. In parasite power mode, it isn't used. As a result, 5-volt electricity is supplied externally. The DS18S20 is connected to port D's pin zero. PORT D pin zero is used to communicate with a digital thermometer over a single wire. Temperature is displayed on a 162 LCD. Temperature is displayed using an LCD connected to a pic microcontroller.

ds18s20 interfacing with PIC16F877A.jpg

DS18S20 interfacing with PIC16F877A


DS18S20 Dimensions

ds18s20 dimensions.jpg

DS18S20 Dimensions

DS18S20 Manufacturer

To shorten the time to market and keep up with the development of the market, you need a complete integration from the chip to the supply chain. Maxim Integrated can provide you with integrated solutions in the industrial, medical, consumer, automotive, energy, computing, and communications fields. With our superior solutions, you can easily meet design and architectural challenges. Maxim Integrated products are widely used in power supplies, interfaces, and even digital products in the analog world. It is our honor to be able to meet the needs of reference designs, tools, technical documents, packaging, etc. Our latest simulation integration products look forward to your exploration.


Trend Analysis

Frequently Asked Questions

What is DS18S20 used for?

DS18S20 is used for temperature measurement. These work on a supply in the range of 3 to 5.5V, and can also work on parasitic power. The DS1820 was a digital thermometer IC that worked on 1 – wire technology.

How does ds18s20 temperature sensor work?

The sensor works by reading and converting the temperature and storing this value in scratchpad memory. The scratchpad memory is then read via the One-wire bus by the Dallas library. The power-on value in the scratchpad memory is 85 °C.

How accurate is DS18S20?

Meanwhile, after the calibration using the proposed method, the DS18S20 sensor has a smaller mean error of ± 0.85 %, so that obtained a more accurate sensor and it can be used for testing of Grashof Portable Incubator made by the University of Indonesia. Temperature is one of the main parameters in a baby incubator.
DS18S20

Maxim Integrated

In Stock
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
Related Parts More