MLX90614 Infra Red Thermometer: Pinout, Datasheet and Applications

UTMEL

Published: 30 July 2021 | Last Updated: 30 July 2021

8142

MLX90614ESF-BCH-000-TU

MLX90614ESF-BCH-000-TU

Melexis Technologies NV

Tube Digital, Infrared (IR) 2.6V~3.6V Through Hole -40°C~85°C PWM, SMBus ±0.5°C (±4°C) 16 b 1 (Unlimited)

Unit Price: $24.087981

Ext Price: $24.09

Purchase Guide

Tube Digital, Infrared (IR) 2.6V~3.6V Through Hole -40°C~85°C PWM, SMBus ±0.5°C (±4°C) 16 b 1 (Unlimited)

The MLX90614 is an Infra Red thermometer for noncontact temperature measurements. This article mainly covers pinout, datasheet, schematic, features and other details about MLX90614.

We examine how to use contactless temperature sensor mlx90614 with an arduino.

Non-contact temperature sensor mlx90614 with arduino tutorial

MLX90614 Pinout

mlx90614 Pinout .png

mlx90614 pin configuration.png

MLX90614 Description

The MLX90614 is an Infra Red thermometer for noncontact temperature measurements. Both the IR sensitive thermopile detector chip and the signal conditioning ASSP are integrated in the same TO-39 can.

Thanks to its low noise amplifier, 17-bit ADC and powerful DSP unit, a high accuracy and resolution of the thermometer is achieved.


MLX90614 CAD Model

Symbol

mlx90614 symbol.png

Footprint

mlx90614 footprint.png

3D Model

mlx90614 3d model.png

MLX90614 Block Diagram

mlx90614 block diagram.png

Specifications

Melexis Technologies NV MLX90614ESF-BCH-000-TU technical specifications, attributes, parameters and parts with similar specifications to Melexis Technologies NV MLX90614ESF-BCH-000-TU.
  • Type
    Parameter
  • Factory Lead Time
    20 Weeks
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Through Hole
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    TO-205AD, TO-39-4 Modified Metal Can
  • Surface Mount

    having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.

    NO
  • Test Conditions
    0°C ~ 60°C (120°C ~ 380°C)
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -40°C~85°C
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube
  • Published
    2012
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    4
  • HTS Code

    HTS (Harmonized Tariff Schedule) codes are product classification codes between 8-1 digits. The first six digits are an HS code, and the countries of import assign the subsequent digits to provide additional classification. U.S. HTS codes are 1 digits and are administered by the U.S. International Trade Commission.

    8542.39.00.01
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    2.6V~3.6V
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    BOTTOM
  • Peak Reflow Temperature (Cel)

    Peak Reflow Temperature (Cel) is a parameter that specifies the maximum temperature at which an electronic component can be exposed during the reflow soldering process. Reflow soldering is a common method used to attach electronic components to a circuit board. The Peak Reflow Temperature is crucial because it ensures that the component is not damaged or degraded during the soldering process. Exceeding the specified Peak Reflow Temperature can lead to issues such as component failure, reduced performance, or even permanent damage to the component. It is important for manufacturers and assemblers to adhere to the recommended Peak Reflow Temperature to ensure the reliability and functionality of the electronic components.

    NOT SPECIFIED
  • Number of Functions
    1
  • Supply Voltage

    Supply voltage refers to the electrical potential difference provided to an electronic component or circuit. It is crucial for the proper operation of devices, as it powers their functions and determines performance characteristics. The supply voltage must be within specified limits to ensure reliability and prevent damage to components. Different electronic devices have specific supply voltage requirements, which can vary widely depending on their design and intended application.

    3V
  • Time@Peak Reflow Temperature-Max (s)

    Time@Peak Reflow Temperature-Max (s) refers to the maximum duration that an electronic component can be exposed to the peak reflow temperature during the soldering process, which is crucial for ensuring reliable solder joint formation without damaging the component.

    NOT SPECIFIED
  • JESD-30 Code

    JESD-30 Code refers to a standardized descriptive designation system established by JEDEC for semiconductor-device packages. This system provides a systematic method for generating designators that convey essential information about the package's physical characteristics, such as size and shape, which aids in component identification and selection. By using JESD-30 codes, manufacturers and engineers can ensure consistency and clarity in the specification of semiconductor packages across various applications and industries.

    O-MBCY-T4
  • Output Type

    The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.

    PWM, SMBus
  • Supply Voltage-Max (Vsup)

    The parameter "Supply Voltage-Max (Vsup)" in electronic components refers to the maximum voltage that can be safely applied to the component without causing damage. It is an important specification to consider when designing or using electronic circuits to ensure the component operates within its safe operating limits. Exceeding the maximum supply voltage can lead to overheating, component failure, or even permanent damage. It is crucial to adhere to the specified maximum supply voltage to ensure the reliable and safe operation of the electronic component.

    3.6V
  • Supply Voltage-Min (Vsup)

    The parameter "Supply Voltage-Min (Vsup)" in electronic components refers to the minimum voltage level required for the component to operate within its specified performance range. This parameter indicates the lowest voltage that can be safely applied to the component without risking damage or malfunction. It is crucial to ensure that the supply voltage provided to the component meets or exceeds this minimum value to ensure proper functionality and reliability. Failure to adhere to the specified minimum supply voltage may result in erratic behavior, reduced performance, or even permanent damage to the component.

    2.6V
  • Analog IC - Other Type

    Analog IC - Other Type is a parameter used to categorize electronic components that are integrated circuits (ICs) designed for analog signal processing but do not fall into more specific subcategories such as amplifiers, comparators, or voltage regulators. These ICs may include specialized analog functions such as analog-to-digital converters (ADCs), digital-to-analog converters (DACs), voltage references, or signal conditioning circuits. They are typically used in various applications where precise analog signal processing is required, such as in audio equipment, instrumentation, communication systems, and industrial control systems. Manufacturers provide detailed specifications for these components to help engineers select the most suitable IC for their specific design requirements.

    ANALOG CIRCUIT
  • Resolution

    Resolution in electronic components refers to the smallest increment of measurement or change that can be detected or represented by the component. It is a crucial specification in devices such as sensors, displays, and converters, as it determines the level of detail or accuracy that can be achieved. For example, in a digital camera, resolution refers to the number of pixels that make up an image, with higher resolution indicating a greater level of detail. In analog-to-digital converters, resolution is the number of discrete values that can be represented in the digital output, determining the precision of the conversion process. Overall, resolution plays a significant role in determining the performance and capabilities of electronic components in various applications.

    16 b
  • Sensor Type

    In electronic components, the parameter "Sensor Type" refers to the specific type of sensor technology used in a particular component to detect and measure physical phenomena such as light, temperature, pressure, motion, or proximity. Different sensor types utilize various principles and mechanisms to convert the detected input into an electrical signal that can be processed by the electronic component. Common sensor types include photodiodes, thermistors, accelerometers, and proximity sensors, each designed for specific applications and environments. Understanding the sensor type is crucial for selecting the right component for a given task and ensuring accurate and reliable sensing capabilities in electronic systems.

    Digital, Infrared (IR)
  • Sensing Method

    The sensing method in electronic components refers to the technique or mechanism used to detect and measure physical phenomena such as temperature, pressure, light, or motion. This includes a variety of technologies such as resistive, capacitive, inductive, and optical sensing methods. The choice of sensing method affects the accuracy, response time, and application suitability of the electronic component. It plays a crucial role in determining how effectively a device can interact with and interpret its environment.

    Infrared (IR)
  • Accuracy - Highest (Lowest)

    In electronic components, "Accuracy - Highest (Lowest)" refers to the range within which the actual value of a parameter can deviate from the ideal or specified value. The term "Highest" indicates the upper limit of this range, while "Lowest" indicates the lower limit. For example, if a component has an accuracy of ±5%, the highest accuracy would mean that the actual value could be within 5% above the specified value, while the lowest accuracy would mean it could be within 5% below the specified value. This parameter is crucial for ensuring the reliability and performance of electronic devices by determining how closely the component's output matches the desired value.

    ±0.5°C (±4°C)
  • Sensing Temperature - Local

    Sensing Temperature - Local refers to the capability of an electronic component to measure the temperature in its immediate environment or vicinity. This parameter is crucial for applications that require monitoring of temperature for performance, safety, or stability purposes. It often involves temperature sensors integrated within components like microcontrollers, power regulators, or other integrated circuits. The local sensing allows for accurate temperature readings that help in adjusting operational conditions, ensuring optimal performance, and preventing thermal-related failures.

    -40°C~85°C
  • Sensing Temperature - Remote

    Sensing Temperature - Remote refers to the capability of electronic components to measure temperature at a location that is distant from the main control unit or sensor. This parameter typically involves the use of external temperature probes or sensors that are connected to a monitoring device, allowing for accurate temperature readings in environments that are difficult to access. Remote sensing is crucial in applications like HVAC systems, industrial processes, and environmental monitoring, where precise temperature data is needed from various locations.

    -70°C~380°C IR
  • Features

    In the context of electronic components, the term "Features" typically refers to the specific characteristics or functionalities that a particular component offers. These features can vary depending on the type of component and its intended use. For example, a microcontroller may have features such as built-in memory, analog-to-digital converters, and communication interfaces like UART or SPI.When evaluating electronic components, understanding their features is crucial in determining whether they meet the requirements of a particular project or application. Engineers and designers often look at features such as operating voltage, speed, power consumption, and communication protocols to ensure compatibility and optimal performance.In summary, the "Features" parameter in electronic components describes the unique attributes and capabilities that differentiate one component from another, helping users make informed decisions when selecting components for their electronic designs.

    Sleep Mode
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
  • Lead Free

    Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.

    Lead Free
0 Similar Products Remaining

MLX90614 Benefits and Features

  • Small size, low cost

  • Easy to integrate

  • Factory calibrated in wide temperature range:

       -40°C…+125˚C for sensor temperature and

       -70°C…+380˚C for object temperature.

  • High accuracy of 0.5°C in a wide temperature range (0°C…+50°C for both Ta and To)

  • High (medical) accuracy calibration

  • Measurement resolution of 0.02°C

  • Single and dual zone versions

  • SMBus compatible digital interface

  • Customizable PWM output for continuous reading

  • Available in 3V and 5V versions

  • Simple adaptation for 8V…16V applications

  • Sleep mode for reduced power consumption

  • Different package options for applications and measurements versatility

  • Automotive grade


MLX90614 Functional Diagram

mlx90614 functional diagram.png

MLX90614 Alternative

MLX90615, ZTP115, TPIS 1S


MLX90614 Applications

  • High precision non-contact temperature measurements

  • Thermal Comfort sensor for Mobile Air Conditioning control system

  • Temperature sensing element for residential, commercial and industrial building air conditioning

  • Windshield defogging

  • Automotive blind angle detection

  • Industrial temperature control of moving parts

  • Temperature control in printers and copiers

  • Home appliances with temperature control

  • Healthcare

  • Livestock monitoring

  • Movement detection

  • Multiple zone temperature control – up to 127 sensors can be read via common 2 wires

  • Thermal relay / alert

  • Body temperature measurement


MLX90614 Application Circuit

Use of the MLX90614 thermometer in SMBus configuration

mlx90614 application circuit.png

Where to use MLX90614

The key feature of MLX90614 is that it is a contactless IR temperature sensor with high accuracy. Therefore, it can be used in industries to measure the temperature of moving objects like a rotating motor shaft. With its high accuracy and precision, it is also used in a wide range of commercial, health care, and household applications like room temperature monitoring, body temperature measurement, etc.


How to use MLX90614

The MLX90614 Temperature sensor is manufactured by a company called Melexis. The sensor is factory calibrated and hence it acts like a plug and play sensor module for speeding up development processes.


MLX90614 Dimension Outline

The MLX90614 is available in the standard TO-39 package making it easy to mount on a breadboard. The dimensions of MLX90614 is shown below.

mlx90614 DIMENSION.png

MLX90614 Manufacturer

Combining a passion for technology with truly inspired engineering, Melexis designs, develops and delivers innovative micro-electronic solutions that enable designers to turn ideas into applications that support the best imaginable future. The company’s advanced mixed-signal semiconductor sensor and actuator components address the challenges of integrating sensing, driving and communication into next-generation products and systems that improve safety, raise efficiency, support sustainability and enhance comfort. Melexis is headquartered in Belgium and employs over 1,500 people in 19 locations worldwide. The company is publicly traded on Euronext Brussels (MELE).


Datasheet PDF

Download datasheets and manufacturer documentation for Melexis Technologies NV MLX90614ESF-BCH-000-TU.
Frequently Asked Questions

After I put the MLX90614 in the dashboard I start getting errors larger than specified in spite that the module was working properly before that. Why?

Any object present in the FOV of the module provides IR signal. It is actually possible to introduce error in the measurements if the module is attached to the dashboard with an opening that enters the FOV. In that case portion of the dashboard opening will introduce IR signal in conjunction with constraining the effective FOV and thus compromising specified accuracy. Relevant opening that takes in account the FOV is a must for accurate measurements. Note that the basic FOV specification takes 50% of IR signal as threshold (in order to define the area, where the measurements are relevant), while the entire FOV at lower level is capable of introducing lateral IR signal under many conditions.

How do I program my MLX90614?

1.Connect GND to common power/data ground.
2.Connect PWR to the power supply, for the 3V sensor this is about 3.3V. For the 5V version, use about 5VDC.
3.Connect the SDA pin to the I2C data SDA pin on your Arduino. ...
4.Connect the SCL pin to the I2C clock SCL pin on your Arduino.

How does MLX90614 infrared temperature sensor work?

The working principle of infrared sensor MLX90614 is to transform the infrared radiation signal collected from objects and bodies into electrical signals, send the electrical signal into converter after noise amplification processing by amplifier, then the electrical signal is converted to digital signals and store the ...

What is the range of MLX90614?

The object temperature measurements can range from -70 to 382.2 °C (-94 to 719.96 °F), while the ambient temperature reading ranges from -40 to 125 °C. Both the ambient temperature and object temperatures have a resolution of 0.02 °C.

How do I calibrate my MLX90614 sensor?

Calibration procedure for correct object temperature reading is also explained.
1.Before coding , we need to install the required libraries for Arduino. ...
2.Search for MLX and select ADAFRUIT MLX90614 Library to install.
3.Next search for GFX and install ADAFRUIT GFX Library , which is graphic support library for displays.
MLX90614ESF-BCH-000-TU

Melexis Technologies NV

In Stock: 600

Minimum: 1 Multiples: 1

Qty

Unit Price

Ext Price

  • 1

    $24.087981

    $24.09

  • 10

    $22.724510

    $227.25

  • 100

    $21.438217

    $2,143.82

  • 500

    $20.224733

    $10,112.37

  • 1000

    $19.079937

    $19,079.94

Not the price you want? Send RFQ Now and we'll contact you ASAP.

Inquire for More Quantity

Related Parts More