CR2032 VS DL2032, CR2032 VS CR2016, CR2032 VS CR2025[video+FAQ]
BATTERY LITHIUM 3V COIN 20MM
CR2032 is one of the most popular batteries. This passage is going to introduce the difference between CR2032 and DL2032, the difference between CR2032 and CR2016, and the difference between CR2032 and CR2025. If you are interested in it, please have a look.

How to Measure a CR2032 Coin cell battery
CR2032 VS DL2032

Both of these batteries have a diameter of 20mm and a thickness of 3.2mm. They're both 3-volt batteries using Lithium Manganese Dioxide as the primary component (Li-MnO2). They can also operate at temperatures ranging from -20 to +60 degrees Celsius.
CR2032 Overview
The CR2032 battery has a high energy density and can run continuously. This battery has outstanding leak-proof qualities and discharges evenly. The battery will then conserve a lot of power while in use.
Furthermore, CR2032 is noted for having a long-lasting, consistent power source that outlasts standard dry batteries.
DL2032 Overview
The Dl2032 battery is a type of battery that is used to extend the battery life of devices with a voltage of 3V. This sort of battery contains a large number of energy sources, making it ideal for compact electronic devices such as calculators, watches, and medical equipment.
Furthermore, when compared to CR2032, DL2032 has a higher energy density and discharge rate power. As a result, the Dl2032 maintains a constant current exceeding the CR limit under intermittent or continuous discharge situations.
CR2032 VS DL2032: Differences
1. Battery Maker
The manufacturer is the key distinction between these two batteries. Any Li-MnO2 coin battery that begins with the letter CR is a general IEC prefix. This is a technique that most manufacturers now employ. Duracell, on the other hand, makes a battery that starts with the letter DL.
2. Battery Capacity
In comparison to the CR2032, the DL2032 battery has a substantially higher capacity. A CR2032 battery has a capacity of 220 mAh, whereas a DL2032 has a capacity of 240 mAh. This prolongs the life of the Duracell battery and reduces the frequency with which it must be replaced.
3. Dimension and weight
CR2032 has a usual weight of 3.0g, whereas DL2032 has an average weight of 8g, with a diameter of 20mm and a thickness of 0.86mm. Due to increased demand, manufacturers are attempting to shrink these cells even further while maintaining great performance. This is why DL2032 is slightly thicker than CR2032, albeit only by a few millimeters.
Conclusion
Both CR2032 and DL2032 batteries are suitable for your devices. They are extremely adaptable and useful in a variety of situations. Both of these batteries were created for use in compact devices and can power a wide range of devices, including watches, calculators, and more.
CR2032 VS CR2016

The CR2016 battery is a fraction of the thickness of the CR2032 battery. The CR2016 battery has a thickness of 1.6 mm, whereas the CR2032 battery has a thickness of 2.0 mm. They're both the same size and produce the same 3 volts.
CR2016 Overview
CR2016 batteries are commonly used in calculators, digital watches, memory backup, laser pens, car key remotes, calculators, toys, fitness appliances, and medical devices like a clinical thermometer and a tensiometer. It has a proven track record for appliances where conventional batteries cannot be used.
CR2032 VS CR2016: Differences
1. Cell Numbers
The identification numbers on these two batteries are different. Each of their numerals has a specific meaning. The first two numerals represent the diameter of the battery in millimeters, while the latter two digits represent its thickness in millimeters.
CR2016 has a diameter of 20 mm and a thickness of 1.6 mm, whereas CR2032 has a diameter of 20 mm and a thickness of 3.2 mm. In other words, the CR2032 has double the thickness of the CR2016 but has the same diameter.
2. Capacity
The capacity of a typical CR2016 battery is roughly 90 mAh. It indicates that if you use this battery with a 15 mA load, it will last about six hours.
The capacity of the CR2032 battery is approximately 240 mAh. If you use this battery with a 24 mA load, it will last roughly 10 hours.
3. Thickness
For the CR2016 battery, the thickness is 1.6 mm. And the thickness of the CR2032 battery is 3.2 mm, double that of the CR2016.
Conclusion
What is the difference between CR2016 and CR2032? The diameter of the CR2016 and the CR2032 is the same, at 20 mm. Their thickness is a big difference. The CR2016 battery has a thickness of 1.6 mm, whereas the CR2032 battery has a thickness of 2.0 mm.
Both batteries are capable of producing 3 volts. However, you can't use them interchangeably because they're not the same thickness. You can't use two CR2016s to replace a single CR2032. If you do it, you'll end up with 6 volts, which will destroy whatever device you're using.
CR2032 VS CR2025

CR2025 Overview
CR2025 is a coin cell battery. Coin cell batteries like CR2025 have many uses, they are usually used for small portable electronics devices such as:
wristwatches
pocket calculators
automobile keyless entry transmitter
hearing aids
They are generally of a compact size, 5-25mm in diameter and 1-6mm in height. The name defines the size of the battery as for CR2025, the first two digits are for the diameter and the second for the height or thickness of tenths of mm. Therefore, 20mm is the diameter of CR2025, and 2.5mm is the thickness.
CR2032 VS CR2025: Differences
The thickness of the two battery types is the most evident distinction. The CR2032 has a thickness of 3.2mm, while the CR2025 has a thickness of 2.5mm. The CR2032 has a bigger capacity (mAh) to deliver electricity to the load since it is 0.7mm thicker than the CR2025. A common CR2032 battery can deliver 225mAh, but a typical CR2025 battery can only deliver 160mAh. Because the slimmer battery has a lower capacity, it may not last as long and will need to be replaced sooner.
Conclusion
CR2025 and CR2032 have a lot in common. Both have the same voltage (3V), diameter, and application in devices like watches and calculators. They are not, however, identical, so be sure you know which one you need before you buy.
Is the cr2450 the same as the cr2032?
The CR2450 battery is based on the same storage technology as the CR2032 type. Therefore, the energy density is the same, but the CR2450 cell offers more capacity due to its larger size.
Are the cr2016 and cr2032 batteries interchangeable?
Since CR2032 and CR2016 have the same voltage and diameter, it can be tempting to think that the batteries are replaceable. If it fits into the battery compartment of the device and makes a good electrical connection, a CR2016 can replace a CR2032 but will last less than half the life of the CR2032.
Is there a battery replacement for CR2032?
CR2032 is a type of lithium battery that has been used in many electronic devices such as watches, calculators, and hearing aids. CR2025 is another alternative option to replace your CR2032 as it is also a coin-cell battery and has a slightly higher capacity.
What are the benefits of using a CR2032 over a CR2016 battery?
A CR2032 battery lasts about four times as long as a CR2016, and because it's larger, it doesn't have much snap, which makes it safer for toys and some children's devices.
How long does a CR2032 battery last?
There are factors that can affect how long the battery will last. The thing to remember is, that whether you get one with ten years or three months shelf life depends on where it's stored and what time period it was manufactured in. If they were made recently, there should be no reason your batteries couldn't have up to ten years of shelf life.
Guide to Reading the Toshiba 74HC245D Datasheet18 August 2025301
AON7403 P-Channel MOSFET: 30V 11A 8DFN, AON7403 Datasheet and Equivalents21 February 20227451
74HC02 Quad 2-Input NOR Gate: 74HC02, Datasheet, Pinout14 December 202110927
A Comprehensive Guide to LTC6946IUFD-1 Clock/Frequency Synthesizer06 March 2024343
BMP085 Pressure Sensor: Datasheet, Pinout, BMP085 vs.BMP18001 November 20213222
STM32F072RBT6 Microcontroller: 48MHz, 64-LQFP, Pinout and Datasheet14 February 20223843
PIC10F200/202/204/206 Microcontrollers: Technical Insights29 February 2024279
AD9520-5 Output Clock Generator: Pinout, Equivalent and AD9520 PLL12 January 20221173
VRAM (Video RAM) Explained03 June 202110506
What is UWB (Ultra-wideband)?04 June 20218669
How to make an Obstacle Avoiding Robot?29 August 202316167
Top Batteries That Can Replace LR4409 June 20253619
Ceramic Capacitors vs Film Capacitors: A Comprehensive Comparison Guide14 May 20257440
Introduction to Inductive Reactance16 April 202115267
Fuse Design and Selection Points01 July 20227939
What is Vacuum Circuit Breaker?12 October 202110493
Panasonic - BSG
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools