2N3904 VS 2N2222 NPN Transistor: What’s the Differences?
Whenever you search for 2N3904, Google will suggest that 2N3904 vs 2N2222 as a popular search. So this article will show you the difference between 2N3904 and 2N2222 in detail.

Breadboard gain test and multimeter hFE test of 2n2222 and 2N3904 NPN bipolar transistors
- Introduction
- Overview of 2N3904
- Overview of 2N2222
- 2N3904 VS 2N2222 NPN Transistor: Difference in Pinout
- 2N3904 VS 2N2222 NPN Transistor: Difference in Applications
- 2N3904 VS 2N2222 NPN Transistor: Difference in Package
- 2N3904 VS 2N2222 NPN Transistor: Difference in Complementary PNP
- 2N3904 VS 2N2222 NPN Transistor: Difference in Equivalent
- 2N3904 VS 2N2222
- Conclusion
Introduction
The two most common NPN bipolar junction transistors on the market are the 2N3904 and 2N2222. Furthermore, 2N3904 and 2N2222 have a similar look.
As a result, some individuals may wonder why 2N3904 is so popular yet 2N2222 isn't constantly utilized. If you're undecided about which one to use or which is superior, read on. We'll compare the chip properties and pin schematics of these two transistors in this article.
Overview of 2N3904

2N3904 transistor
The 2N3904 is a common NPN bipolar junction transistor used for general purpose low power amplification or switching applications. It is designed for low current and low power, medium voltage operation at moderate speeds.
Overview of 2N2222

2N2222 transistor
The 2N2222 is a typical NPN bipolar junction transistor (BJT) that is used for low-power amplification and switching. It's made to run at moderate speeds with low to medium current, low power, and medium voltage. It was designed to work with TO-18 metal cans, as illustrated in the diagram.
The 2N2222 is a highly common transistor that is used to illustrate an NPN transistor. It is still a small general-purpose transistor that is frequently employed as a small signal transistor.
2N3904 VS 2N2222 NPN Transistor: Difference in Pinout

| Pin Number | Pin Name | Description |
| 1 | Base | Controls the biasing of transistor |
| 2 | Collector | Current flows in through collector |
| 3 | Emitter | Current Drains out through emitter |
2n2222 pinout

| Pin Number | Pin Name | Description |
| 1 | Emitter | Current Drains out through emitter |
| 2 | Base | Controls the biasing of transistor |
| 3 | Collector | Current flows in through collector |
2n3904 pinout
2N3904 VS 2N2222 NPN Transistor: Difference in Applications
2n3904 transistor applications
Module driving circuits
LED driving
Relay driving
Amplifier circuits
Amplifier modules
Used at television
Used at almost all home appliances
2n2222 transistor applications
Amplifier circuits
Complementary transistor amplifier circuits
Used as switch
PWM
Embedded systems
Automation systems
Inverter circuits
Rectifier circuits
Speed control systems
High current circuits
2N3904 VS 2N2222 NPN Transistor: Difference in Package
2n3904 Package
The 2n3904 transistor has a TO-92 package, the external covering is made with plastic and epoxy of suitable size. The main advantage of the TO92 package is the compatibility and the less expensive. The TO92 package can’t withstand higher temperatures.
2n2222 Package
The 2n2222 transistor had a TO-18 package, the external covering of the transistor is built with metal.
Using the TO-18 package, the 2n2222 had so many advantages, such as it can handle higher values of current and also can have the ability to handle a high amount of temperature. In other words, the TO-18 package acts as a heat sink.
2N3904 VS 2N2222 NPN Transistor: Difference in Complementary PNP
2n2222 complementary PNP
The 2n2222 transistor is an NPN type device, in some circuits they need a perfect complementary PNP transistor.
For applications like siren circuits, amplifier circuits, and flash circuits, a combination of NPN-PNP is needed. For the 2n2222 NPN transistor, we have 2n2907 PNP.
2n3904 complementary PNP
The 2n3904 NPN transistor needs PNP complementary transistor.
The most common PNP transistor used with 2n3904 is the 2n3906.
2N3904 VS 2N2222 NPN Transistor: Difference in Equivalent
2n2222 Equivalent
The equivalent transistors for the 2n2222 on a circuit are, 2n2219, 2n1613, 2n2792, and 2n2218.
Other than these transistors, 2n2222 had a more possible equivalent, this is because the 2n2222 is a general-purpose transistor
The only thing we need to consider before replacing the 2n2222 is the pin configuration.
2n3904 equivalent
The equivalent transistors for 2n3904 are, 2n3055 and BC548
The 2n3904 is a general-purpose transistor.
2N3904 VS 2N2222
| 2n2222 | 2n3904 | |
| Collector to base voltage (VCB) | 60v | 60v |
| Collector to emitter voltage (VCE) | 30 | 40 |
| Emitter to base voltage (VEB) | 5v | 6v |
| Collector current (IC) | 800mA | 200mA |
| Power dissipation | 500mw | 625mw |
| Junction temperature (TJ) | 200°C | 150°C |
| Transition frequency (FT) | 250MHZ | 300MHZ |
| Noise (N) | 4db | 10db |
| Gain (hFE) | 30 – 300 hFE | 30 – 300 hFE |
| Package | TO-18 | TO-92 |
Conclusion
As a result, the decision is ultimately based on the amount of current required. The 2N3904 or 2N2222 will suffice if you require less than 200mA. The 2N2222 is the one to choose if you require more than 200mA but not more than 1A. If you need more than 1 amp at the output, you can use a Darlington transistor like the TIP122, which can take up to 5 amps of amplified current. If you want a higher current, the TIP3055 can deliver up to 15A.
However, unless you work in power electronics, you will almost never require this much amperage when dealing with electronics. These are truly harsh circumstances.
For most circuits, a 2N3904 would suffice, however, if you need more above 200mA, a 2N2222 should be used instead.
What is the difference between 2N2222 and 2n2222A?
The 2n2222A is a slight bit better in terms of Vceo, Vcbo, Vebo. But if you are not planning on stressing the part (higher voltages, etc) both will work well, especially for simple switching and logic circuits. The 2n2222 part is the older style part which might be the reason they are being offered at a low price.
What is the difference between 2N3904 and 2N3906?
The 2N3906 has a 200 mA collector current, 40 V collector-base and collector-emitter voltages, and a 300 mW power dissipation. The 2N3904 is a complementary NPN transistor to the 2N3906. Motorola Semiconductor registered both variants in the mid-1960s.
What is the gain of a 2N2222?
The gain value of the 2N2222A is 110 to 800, which controls the transistor's amplification capacity. Because the maximum amount of current that can flow through the Collector pin is 800mA, we can't use this transistor to connect loads that need more than 800mA.
What is the difference between 2N3904 and 2N4401?
In every way, the 2N3904 and 2N4401 look to be quite similar parts. The 2N4401 has a greater current rating, but otherwise, they appear to be similar in pricing and other aspects. Given that both pieces are manufactured by different companies, it's difficult to give a uniform response.
What is difference between BC547 and 2N2222 transistor?
The 2N2222A transistor is very similar to the BC547 NPN transistor, which is widely used. However, there are two key differences between the two. When compared to BC547, 2N2222A has a collector current of up to 800mA and a power dissipation of 652mW, allowing it to drive larger loads.
Comprehensive Guide to STM32L431CBT6 for Developers24 July 20253037
ATTINY88-MU 8-bit Microcontroller: Pinout, Equivalent and Datasheet25 March 20223025
BMC150 ECompass: Features, Specifications and Datasheet14 August 2024456
AD4004 16-Bit 1 MSPS SAR ADC: Datasheet, Performance, and Integration Deep Dive20 March 2026303
2N5458 JFET: Alternatives, Datasheet, Pinout07 October 20218930
Xilinx XC7Z030-2FBG676I SoC Review09 June 2025307
AD7606 16-Bit 8-Channel ADC: Datasheet Analysis, Pinout, and Performance Review10 February 20263087
STM32F303CBT6TR Microcontroller: 32-Bit, 48-LQFP, Pinout and Datasheet11 January 2022478
Solid State Relay Basics: Working, Features and Structure17 September 202010602
Parallel Plate Capacitor: Features, Working Principle and Applications30 January 20219310
An Overview of Linear Integrated Circuits23 October 202513281
Basic Introduction to System on a Chip02 December 20205292
Introduction to TVS Diodes07 August 202014210
A Hybrid SiC and GaN-Based DC-DC Converter for EVs20 September 20243143
Basic Introduction to Hall Effect Sensors13 November 202513115
Introduction to TRIAC and TRIAC Dimmer10 September 202010910
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools