BMI088 IMU: BMI088 Datasheet, Pinout, BMI088 vs. MPU6050
BMI088 Series 3.6 V 6 Axis Digital Output Accelerometer Motion Sensor - LGA-16
Unit Price: $4.879292
Ext Price: $4.88









BMI088 Series 3.6 V 6 Axis Digital Output Accelerometer Motion Sensor - LGA-16
BMI088 is an inertial measurement unit (IMU) for the detection of movements and rotations in 6 degrees of freedom(6DoF). This article mainly covers its datasheet, pinout, feature, comparison, and more details about BMI088
BMI088 Pinout

BMI088 Pinout
BMI088 CAD Model
Symbol

BMI088 Symbol
Footprint

BMI088 Footprint
3D Model

BMI088 Footprint
BMI088 Description
BMI088 is an inertial measurement unit (IMU) for the detection of movements and rotations in 6 degrees of freedom(6DoF). It combines the functionality of two inertial sensors in one device: an advanced triaxial 16 -bit gyroscope and a versatile, leading-edge triaxial 16 -bit accelerometer.
BMI088 is designed to meet all requirements for high-performance consumer applications in harsh vibration environments such as those encountered in drones and robotics applications. The IMU is designed to effectively suppress vibrations above a few hundred Hz that could occasionally occur due to resonances on the PCB or the structure of the total system. The sensor has an extended measurement range of up to +24 g to avoid signal clipping under strong signal exposure.
BMI088 Feature
Noise density (typ.) | (A): 175 μg/√Hz |
Bandwidths (progr.) | 5 Hz … 523Hz |
Selectable output data rates | 12.5 Hz ... 2 kHz |
Digital inputs/outputs | |
Supply voltage (VDD) | 2.4 ~3.6 V |
I/0 supply voltage (VDDIO) | 1.2 ~3.6 V |
Temperature range | -40 ~+85°C |
Current consumption (full operation) | 5.15 mA |
LGA package | 3 x 4.5 x 0.95 mm³ |
BMI088 Application
Drones
Robotics
BMI088 Block Diagram
BMI088 SPI and I2C Connection

Connection diagram SPI

Connection diagram I2C
The BMI088 supports two serial digital interface protocols for communication as a slave with a host
device: SPI and I2C. The active interface is selected by the state of the Pin#07 (PS) 'protocol select pin:
PS = 'VDDIO' selects I2C
PS = 'GND' selects SPI
BMI088 Package

BMI088 Package
BMI088 Manufacturer
Bosch Sensortec GmbH is a fully owned subsidiary of Robert Bosch GmbH dedicated to the world of consumer electronics; offering a complete portfolio of micro-electro-mechanical systems (MEMS) based sensors and solutions that enable mobile devices to feel and sense the world around them. Bosch Sensortec develops and markets a broad portfolio of MEMS sensors, solutions and systems for applications in smartphones, tablets, wearable devices, and various products within the IoT (Internet of Things).
The more Bosch hit parts ' related articles:
BMP280 Sensor: Pinout, Application, Circuit and Comparison
BMP180 Digital Pressure Sensor: Datasheet, Pinout, Application
BMP085 Pressure Sensor: Datasheet, Pinout, BMP085 vs.BMP180 and etc.
Specifications
- TypeParameter
- Factory Lead Time14 Weeks
- Mounting Type
The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.
Surface Mount - Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
16-VFLGA Module - Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
-40°C~85°C - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tape & Reel (TR) - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Output Type
The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.
I2C, SPI - Sensor Type
In electronic components, the parameter "Sensor Type" refers to the specific type of sensor technology used in a particular component to detect and measure physical phenomena such as light, temperature, pressure, motion, or proximity. Different sensor types utilize various principles and mechanisms to convert the detected input into an electrical signal that can be processed by the electronic component. Common sensor types include photodiodes, thermistors, accelerometers, and proximity sensors, each designed for specific applications and environments. Understanding the sensor type is crucial for selecting the right component for a given task and ensuring accurate and reliable sensing capabilities in electronic systems.
Accelerometer, Gyroscope, 6 Axis - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
ROHS3 Compliant
Parts with Similar Specs
Datasheet PDF
- Datasheets :
- Environmental Information :
In what degree of freedom does BMI088 detect movements and rotations?
6 degrees of freedom.
How many inertial sensors does BMI088 combine?
Two.
What types of applications are BMI088 designed to meet?
Drones and robotics applications.
What is the measurement range of the BMI088 sensor?
+24 g.
What does the temperature stability of the BMI088 help on a system level?
Reducing design efforts and costs.
A Comprehensive Guide to LTC6605IDJC-7#TRPBF Active Filter Interface06 March 2024193
ADG1204 Multiplexer: Pinout, Features and Datasheet14 February 20221599
BME280 Sensor: Datasheet, Pinout and Applications08 July 202116864
W77L516A 8-BIT Microcontroller: Technical Specifications and Applications29 February 2024220
Cypress MB95F778MPMC1GSNE2 Microcontroller: Technical Overview29 February 2024164
SG3524N IC REG CTRLR MULT TOPOLOGY 16DIP: Datasheet, Circuit, Pinout and Equivalents16 February 202211668
Murata BLM18PG471SN1D: Datasheet, Application, and Alternatives11 February 2022489
MIC2560 PCMCIA Switch: Pinout, Equivalent and Datasheet24 February 20221056
What Are Buck-Boost Converters?07 June 20251265
Introduction to Step-up Transformer01 March 20216753
What is Inertial Measurement Unit (IMU)?15 October 202510961
Elon Musk: The Neuralink Brain Chip Developed By Its Company Could Help Treat Morbid Obesity24 April 20222858
Introduction to Wireless Router17 June 20214200
Everything You Need to Know about Connectors07 September 20218765
Nickel-Cadmium Battery: Construction, Features and Working Principle19 March 202633762
What causes the Noise of Electronic Equipment when it is Running?01 August 20223324
Bosch Sensortec
In Stock: 6145
Minimum: 1 Multiples: 1
Qty
Unit Price
Ext Price
1
$4.879292
$4.88
10
$4.603106
$46.03
100
$4.342553
$434.26
500
$4.096748
$2,048.37
1000
$3.864856
$3,864.86
Not the price you want? Send RFQ Now and we'll contact you ASAP.
Inquire for More Quantity


Product
Brand
Articles
Tools