web counter

cr2 vs cr123:Which battery do you prefer?

Sophie

Published: 29 March 2022 | Last Updated: 29 March 2022

27018

CR-2

CR-2

Panasonic - BSG

BATTERY LITHIUM 3V CR2

Purchase Guide

BATTERY LITHIUM 3V CR2

CR2 and CR123 batteries are among the most cost-effective options available. You may be familiar with one of these batteries if you own a camera, film-making equipment, shutter remotes, or a small flashlight. Despite the fact that both batteries perform well, there are several key distinctions that make one preferable to the other. This article compares and contrasts the two products, as well as which one you should choose based on your needs. Let's get started!

This video is about review of the handy Watson Rapid Battery Charger for CR123A and CR2 Lithium Batteries.

Charger for CR123A and CR 2 Recharable Batteries Review

Introduction

Today, it appears like practically everything needs a battery to function. When it comes to more specialized equipment, however, the standard AA  and AAA batteries are insufficient. And we're stumped as to which batteries to utilize in our gear.

 

When we see battery types like the CR2  or the CR123, we know it's for tactical gear and other specialist items. But how should these batteries be utilized and what is the difference between them?


What does the CR stand for?

The prefix CR is used by the International Electrotechnical Commission (IEC) to show that the battery uses lithium chemistry, specifically LiMnO2 (Lithium-Ion Manganese Oxide).

The C denotes Lithium, and R means the batteries are round. The numbers that follow describe the size of the battery. 123A stands for one battery that’s two-thirds the size of a standard A battery. Some manufacturers simply omit the A at the end. 


Overview of CR2

CR2.jpg

The CR2 battery is a compact battery that is about half the size of a typical AA battery. It's commonly found in cameras and photographic equipment. Its compact profile, on the other hand, makes it easy to fit into smaller equipment.

 

The battery's entire length is 27 mm, and its diameter is 15.6 mm. This battery will outlive other options in terms of charge due to its low discharge. The CR123 will, however, have a longer charge life.


Overview of CR123

CR123.jpg

The CR123 is the larger of the two alternatives, with much greater power than the CR2. The CR123 is nearly 34% the length of a typical AA battery but slightly wider, measuring 35.4 mm long with a diameter of 17 mm.

 

Despite its smaller size than the CR2, the CR123 produces much more power and has a longer charge life than the CR2.


CR2 VS CR123, what’s the similarities?

1. They are 3-volt.

The first thing that these two batteries have in common is that they are both 3-volt batteries. A 3-volt battery must be replaced with another 3-volt battery. If you don't, higher-voltage batteries can cause serious damage to the gadget you're using them in.

2. They are lithium batteries.

The second similarity between these two is that they are both formed of lithium. Lithium is an extremely light metal with the highest energy density of any battery currently available.

3. They are non-rechargeable.

Thirdly, they share the same technology and are not rechargeable. These batteries have a long run time as they have a lower discharge rate.

These, on average, will lose around 5% of their charge each month. In turn, this helps to provide them with a longer run time compared to comparably sized batteries.


CR2 VS CR123, what’s the differences?

1. Size & Dimensions

comparing-CR2-to-123-battery-1024x1024.jpg

The CR123 battery is 34.5mm long and 17mm wide, whereas the CR2 battery is 27mm long and 15.6mm wide. As a result, replacing a CR2 battery with a CR123 may be impossible.

2. Capacity

Between CR2 and CR123, there is a significant capacity variation. Both products' capacity is measured in milliamperes. CR2 has a capacity of 600-900mAH, whereas CR123 has a capacity of 700-1700mAH.

As a result, CR2 would provide power for a shorter period of time than CR123. Their capacity has no bearing on their effectiveness. Instead, it has a lot to do with how long these batteries can last before they need to be recharged.


Is it possible to use CR2 and CR123 interchangeably?

Many individuals are perplexed and believe that CR2 and CR123 batteries are interchangeable. Both are common in handheld devices like flashlights, camera flashlights, and gaming console controllers.

 

Both of these batteries have a lot of power and may discharge it for a long time. However, you should be aware that, although being 3-volt batteries, their sizes fluctuate. It's possible that you won't be able to replace a CR2 with a CR123.


CR123 Batteries vs. CR2 Batteries: Which Is Better?

Many individuals believe a CR123 battery is superior to a CR2. They say this because this battery is not only somewhat larger in size, but it also has more energy in it. The CR123 battery has 60% greater power than the CR2 battery on average.

 

The CR123 is also superior to the CR2 due to its significantly higher current draw. In other words, it will give the device extra juice. If your flashlight uses CR123 batteries, for example, the light it emits will be much brighter.

 

If the device requires smaller batteries, you should use CR2 batteries.


What Uses CR2 Batteries?

Military, industrial, medical, and consumer applications all use the CR2 battery. The CR2 battery is utilized in weapons lights, optics, laser rangefinders, laser designators, and communications devices in military settings. Alarm batteries and power for various devices are among the medical applications of the CR2 battery. Lights, alarms, cameras, and memory backup applications are examples of industrial and consumer applications.


What Uses CR123 Batteries?

Known for being cold-resistant, CR123 lithium batteries are often used for tactical flashlights, pocket flashlights, LED headlamps and lanterns to name a few. Because of the use of lightweight materials, the Panasonic CYLINDRICAL LITHIUM CR123 batteries are perfect for small cameras as well as portable lighting systems. The batteries can also be used in safety equipment, security sensors, and smoke detectors.


Conclusion

Batteries are a form of expendable that can be used right away. You will always acquire the correct sort of battery if you know the size your device requires. The issue arises when it comes to the type of equipment you want or desire.

 

What you choose will be influenced by the power output, the device's footprint and storage, and the storage or type of battery you'll need to use. It's not always about how much power it produces; it's about why you need that power and what your device's requirements are.


Frequently Asked Questions

Is it possible to use CR2 and CR123 batteries interchangeably?

While both CR123 and CR2 batteries have the same voltage and are created as lithium batteries, CR2 batteries are NOT the same as CR123A batteries and CAN NOT be used interchangeably due to size variations.

What Battery Is Equivalent To The CR123A Battery?

Direct replacements and equivalents for the CR2 battery could be, DLCR2, KCR2, ECR2 1CR2, and 5046LC. These batteries are all direct replacements for the CR2 battery and are all considered primary or non-rechargeable batteries. 

How Long Do CR2 Batteries Last?

 How long a CR2 battery lasts depends greatly on the manufacturing quality and the application of the battery. Assuming that the battery is fresh and purchased from a reliable source, there is still a large range of service life depending on the usage. For a frequent application that requires large amounts of energy, such as for a high lumen flashlight, a CR2 battery could last less than a month. For more passive usage, such as in a home security alarm panel, service life can be over a year with the right conditions. 

Are C2 and CR2 batteries the same?

Although the CR2 battery is not commonly referred to as a C2, several small manufacturers do offer C2 batteries that are identical to the CR2. The CR2 battery is commonly designated by the majority of major manufacturers. Additionally, certain retail packaging for C cell batteries may cause some misunderstanding. The top of certain retail packs of two C batteries may state C 2 at the top of the box. This does not imply that it is the same as a C2 (CR2) battery, but rather that the pack contains two C cells.

What is a CR2 Battery?

The CR2 Battery is a cylindrical cell battery that has lithium chemistry. In simple terms, the CR2 battery looks like a smaller version of a D Cell Battery, or for simpler reference almost like a can.
CR-2

Panasonic - BSG

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More