CR2016 vs. CR2032: Specifications, Applications, Differences
BATTERY LITHIUM 3V COIN 20MM
The CR2032 and CR2016 are coin-type batteries with the same voltage and appearance. The power capabilities and sizes of these two batteries are substantially different. This article is going to discuss the difference between CR2032 and CR2016 batteries to help customers to use these two batteries appropriately. Also, a huge range of products is in stock. Welcome your RFQ!

CR2032 vs. CR2016 – What is the Difference between These Batteries
Introduction
Although the CR2016 and CR2032 batteries appear to be very similar, there is a minor difference between them. The CR2032 and the CR2016 are coin-type batteries that look similar and provide the same voltage. The significant difference between these two batteries is their power capacities and sizes.
These two-cell batteries can be found in a wide range of electronic devices, including watches, calculators, diabetes meters, and computers. While the CR2016 and CR2032 batteries have the same diameter and may deliver the same amount of volts, they are not interchangeable due to their different thicknesses. One physical explanation is that the battery holder size for one may differ from that of the other.
Continue reading to learn more about the differences between the CR2016 and the CR2032, as well as their commonalities, applications, and service lives.
What is CR2016 Battery?
Lithium coin CR2016 battery is frequently used in fitness appliances, digital watches, car key remotes, calculators, toys, and more. The CR2016 provides long-lasting reliable power in various devices.

CR2016 Pinout
Features & Benefits
Good pulse capability
High discharge characteristics
Stable voltage level during discharge
Long-term reliability
Specifications
Nominal Capacity: 90 mAh
Nominal Voltage: 3V
Operating Temperature: -30°C - +60°C
Diameter: 20 mm
Weight: 1, 7 g
Shelf Life: 10 years
Where to Use CR2016 Battery?

Small PDA devices
Wireless doorbell for house
Electronic Toys
Portable electronics
Digital thermometers
Digital altimeter
Cyclocomputers
Heart rate monitors
How long does CR2016 Run?
The shelf life of CR2016 batteries is usually six years. However, one battery company says that its single-use silver-zinc battery would last for ten years. According to watch manuals, a CR2016 can run the device for two years, especially those from G-Shock watches.
Some others believe they are merely a conservative approximation. The battery in your watch could survive seven years or more if you don't utilize the auto EL light function, the hourly chime, or the alarm. This is based on real-world experiences of users who use CR2016 batteries in their electronic timepieces.
What is CR2032 Battery?
The CR2032 battery is a coin-type lithium-ion battery with a 3-volt output. The CMOS (complementary metal-oxide-semiconductor) battery is the most common name for it. These batteries can also be used to power a computer's BIOS or the computer's real-time clock.

CR2032
Features & Benefits
Good pulse capability
High discharge characteristics
Stable voltage level during discharge
Long-term reliability
Specifications
Nominal Capacity: 225 mAh
Nominal Voltage: 3V
Operating Temperature: -30°C - +60°C
Diameter: 20 mm
Weight: 3, 1 g
Shelf Life: 10 years
Where to Use CR2032 Battery?
Lithium Coin CR2032 has certain achievements for devices where traditional batteries cannot be used. This battery can be used for memory backup, digital watches, car keys, laser pens, fitness appliances, and medical devices such as tensiometers and clinical thermometers.
How long does CR2032 Battery Run?
When used in computers and other electrical equipment, it can often last up to two years before dying. You can figure out how long a CR2032 battery will last by dividing its entire charge in mAh by its current consumption.
A CR2032 can survive ten years if the gadget draws 1 microamp or less consistently. This is feasible in cases where the CR2032 has only been used to power the computer's BIOS. In most cases, however, the battery is asked to provide additional current in pulses or even continuously.
CR2016 vs. CR2032: Interchangeability
Capacity
CR2032 Battery
A typical CR2032 battery has a capacity of 240 mAh. The button battery will last for about 10 hours when using it with an average load of 24 mA.
CR2016 Battery
A typical CR2016 battery has a capacity of 90 mAh. The button battery will last for about 6 hours when using it with an average load of 15 mA
Voltage
CR2032 Battery
The typical CR2032 battery is a 3-volt lithium coin battery.
CR2016 Battery
Likewise, the typical CR2016 battery is a 3-volt lithium coin battery.
Thickness
CR2032 Battery
The CR2032 battery has a thickness of 3.2 mm.
CR2016 Battery
The CR2016 battery has a thickness of 1.6 mm.
Although the thickness of the CR2016 and CR2032 differs, they are identical in many aspects. Both are 3-volt types that aren't rechargeable. It's vital to remember, however, that their capacities differ. The CR 2032 has a 240 mAh capacity, but the CR2016 only has a 90 mAh capacity. The CR2032 may last up to 10 hours; however, the CR2016 only lasts approximately six hours, depending on the power you're using.
Both batteries are capable of producing 3 volts. However, you can't use them interchangeably because they're not the same thickness. You can't use two CR2016s to replace a single CR2032, If you do it, you'll end up with 6 volts. which will destroy whatever device you're using.
CR2016 vs. CR2032: Conclusion
Is it possible to use CR2016 and CR2032 interchangeably? The thicker CR2032 battery will not fit into the CR2016 battery compartment in most devices that use a single CR2016 cell. In contrast, your gadget may get by with two stacked CR2016 coin-type batteries instead of one CR2032, The size may be correct, but the voltage is incorrect. It is not recommended of stacking two CR2016s yields 6V (3V+3V) rather than the 3V provided by a single CR2032.
What is a CR2016 battery used for?
Panasonic Lithium coin CR2016 batteries provide long-lasting reliable power in various devices. The CR2016 is frequently used in fitness appliances, digital watches, car key remotes, calculators, toys, and more.
Are the cr2016 and cr2032 batteries interchangeable?
Since CR2032 and CR2016 have the same voltage and diameter, it can be tempting to think that the batteries are replaceable. If it fits into the battery compartment of the device and makes a good electrical connection, a CR2016 can replace a CR2032 but will last less than half the life of the CR2032.
Is Cr1620 the same as cr2032?
A CR2032 has a diameter of 20mm (0.787in) and a thickness of 3.2mm (0.126in), while a CR2016 has the same diameter (20mm) but only half the thickness, only 1.6 mm (0.063 inches). A CR1620, on the other hand, has a diameter of 16mm and a thickness of 2.0mm.
What Battery is Equivalent to CR1632?
CR1632 Battery Equivalents are as follows: BR1632, BR 1632, BR1612-1W, CR1632, CR 1632, DL1632, DL1612B, ECR1632, E-CR1632, KCR1632, KECR1632, KL1632, L1632, LITH34, LITH-34 Good for Car remotes, Watches, Cameras, Calculators, Car Security Alarm, Organizers, Glucometer, Computer Equipment and so on.
4N28 Phototransistor Optocoupler IC: Circuit, Datasheet and Pinout26 October 20214919
EP4CE6F17C8N Altera: Specifications, Features and Applications08 April 2025781
MPSA92 PNP High Voltage Transistor: Datasheet, Pinout and Equivalent13 October 20215093
AD4005 16-Bit 1 MSPS SAR ADC: Eliminating High-Speed Drivers with Easy Drive Technology06 May 2026313
MC33079DG Operational Amplifier: Datasheet, Pinout, Alternatives03 January 20234106
ADS1220 Sensors: Price, Package and Datasheet17 August 202110145
SMAJ15A TVs Diodes: Features, Pinout, and Datasheet15 February 20224010
ESP32 Microcontroller: Datasheet, Pinout and Programming08 September 202117458
The Ultimate Guide to AI Noise Reduction Translation Earbuds24 September 202610558
LLC Converter with Planar Matrix Transformer for High-Current-High-Power Applications15 March 20245522
What is 3D XPoint?09 November 20215832
Semiconductor Inspection System Market Expected to Reach US$ 8,380.01 Million By 203015 September 20233915
Classification and Working Principle of Ballast Resistor18 November 20208446
7 Common Functions of MOSFET Gate Circuits22 January 20227878
PMIC - Gate Drivers: A Purpose-Built Integrated Circuit22 February 20234427
LDO VS DC to DC Converter11 March 202212417
Panasonic - BSG
In Stock: 100
Minimum: 1 Multiples: 1
Qty
Unit Price
Ext Price
1
$0.251676
$0.25
10
$0.237430
$2.37
100
$0.223990
$22.40
500
$0.211312
$105.66
1000
$0.199351
$199.35
Not the price you want? Send RFQ Now and we'll contact you ASAP.
Inquire for More Quantity


Product
Brand
Articles
Tools