DS1307N Real-Time Clock: Circuit, Pinout, and Datasheet
8 Terminations 5V 8 Pin DS1307 Real Time Clocks 0.032MHz
The DS1307N serial real-time clock (RTC) is a low-power clock/calendar with complete binary-coded decimal (BCD) and 56 bytes of NV SRAM. This article mainly introduces circuit, pinout, datasheet and other detailed information about Maxim Integrated DS1307N.

How to use DS1307 Real Time Clock with Arduino code
DS1307N Description
The DS1307N serial real-time clock (RTC) is a low-power clock/calendar with complete binary-coded decimal (BCD) and 56 bytes of NV SRAM. An I2C bidirectional bus is used to transport address and data serially.
The clock/calendar displays information such as seconds, minutes, hours, days, dates, months, and years. For months with fewer than 31 days, the end of the month date is automatically modified, including leap year corrections. The clock has an AM/PM indicator and works in either a 24-hour or 12-hour mode. The DS1307N includes a built-in power sensor circuit that detects power outages and switches to the backup source automatically. While the part is running on the backup supply, the timekeeping operation continues.
DS1307N Pinout
The following figure is DS1307N Pinout.

Pinout
| Pin Number | Pin Name | Description |
| 1 | X1 | Standard 32.768kHz Quartz Crystal Connections The internal oscillator circuitry is set up to work with a crystal that has a load capacitance (CL) of 12.5pF. The oscillator's input, X1, can be connected to an external 32.768kHz oscillator if desired. If an external oscillator is attached to X1, the output of the internal oscillator, X2, is floating. |
| 2 | X2 | |
| 3 | VBAT | Any standard 3V lithium cell or other energy source can be used as a backup supply. For proper operation, battery voltage must be kept within the minimum and maximum limits. Between the battery and the VBAT pin, there may be diodes in series that prohibit correct operation. VBAT must be grounded if a backup source is not required. Internal circuitry sets the nominal power-fail trip point (VPF) voltage at which access to the RTC and user RAM is disallowed as 1.25 x VBAT nominal. In the absence of power, a lithium battery with 48mAh or more will power the DS1307 for more than 10 years at +25°C. When utilized with a lithium battery, it is UL recognized to prevent reverse charging current. |
| 4 | GND | Ground. |
| 5 | SDA | Input/output of serial data. SDA is the I2 C serial interface's data input/output port. The SDA pin is open drain and requires a pullup resistor externally. Regardless of the voltage on VCC, the pullup voltage can be up to 5.5V. |
| 6 | SCL | Input for a serial clock. The I2 C interface's clock input, SCL, is used to synchronize data movement on the serial interface. Regardless of the voltage on VCC, the pullup voltage can be up to 5.5V. |
| 7 | SQW/OUT | Output Driver (Square Wave). The SQW/OUT pin outputs one of four square-wave frequencies when the SQWE bit is set to 1. (1Hz, 4kHz, 8kHz, 32kHz). The SQW/OUT pin is an open drain pin that requires a pullup resistor externally. SQW/OUT can be used with either VCC or VBAT. Regardless of the voltage on VCC, the pullup voltage can be up to 5.5V. This pin can be left floating if not in use. |
| 8 | VCC | The source of primary energy. The device becomes fully accessible and data can be written and read when voltage is provided within typical limits. Reads and writes are disabled when a backup supply is attached to the device and VCC falls below VTP. The reduced input voltage has no effect on the timekeeping function, though. |
DS1307N CAD Model
The following figures are DS1307N Symbol, Footprint and 3D Model.

Symbol

Footprint

3D Model
DS1307N Features
• Completely Manages All Timekeeping Functions
o Real-Time Clock Counts Seconds, Minutes, Hours, Date of the Month, Month, Day of the Week, and Year with Leap-Year Compensation Valid Up to 2100
o 56-Byte, Battery-Backed, General-Purpose RAM with Unlimited Writes
o Programmable Square-Wave Output Signal
• Simple Serial Port Interfaces to Most Microcontrollers
o I2C Serial Interface
• Low Power Operation Extends Battery Backup Run Time
o Consumes Less than 500nA in Battery Backup Mode with Oscillator Running
o Automatic Power-Fail Detect and Switch Circuitry
• 8-Pin DIP and 8-Pin SO Minimizes Required Space
• Optional Industrial Temperature Range: -40°C to +85°C Supports Operation in a Wide Range of Applications
• Underwriters Laboratories ® (UL) Recognized
Specifications
- TypeParameter
- Factory Lead Time6 Weeks
- Contact Plating
Contact plating (finish) provides corrosion protection for base metals and optimizes the mechanical and electrical properties of the contact interfaces.
Tin - Mount
In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.
Through Hole - Mounting Type
The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.
Through Hole - Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
8-DIP (0.300, 7.62mm) - Number of Pins8
- Weight930.006106mg
- Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
-40°C~85°C - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tube - Published2000
- JESD-609 Code
The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.
e3 - Pbfree Code
The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.
yes - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Number of Terminations8
- ECCN Code
An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.
EAR99 - TypeClock/Calendar
- Voltage - Supply
Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.
4.5V~5.5V - Terminal Position
In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.
DUAL - Peak Reflow Temperature (Cel)
Peak Reflow Temperature (Cel) is a parameter that specifies the maximum temperature at which an electronic component can be exposed during the reflow soldering process. Reflow soldering is a common method used to attach electronic components to a circuit board. The Peak Reflow Temperature is crucial because it ensures that the component is not damaged or degraded during the soldering process. Exceeding the specified Peak Reflow Temperature can lead to issues such as component failure, reduced performance, or even permanent damage to the component. It is important for manufacturers and assemblers to adhere to the recommended Peak Reflow Temperature to ensure the reliability and functionality of the electronic components.
260 - Supply Voltage
Supply voltage refers to the electrical potential difference provided to an electronic component or circuit. It is crucial for the proper operation of devices, as it powers their functions and determines performance characteristics. The supply voltage must be within specified limits to ensure reliability and prevent damage to components. Different electronic devices have specific supply voltage requirements, which can vary widely depending on their design and intended application.
5V - Terminal Pitch
The center distance from one pole to the next.
2.54mm - Time@Peak Reflow Temperature-Max (s)
Time@Peak Reflow Temperature-Max (s) refers to the maximum duration that an electronic component can be exposed to the peak reflow temperature during the soldering process, which is crucial for ensuring reliable solder joint formation without damaging the component.
30 - Base Part Number
The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.
DS1307 - Pin Count
a count of all of the component leads (or pins)
8 - Operating Supply Voltage
The voltage level by which an electrical system is designated and to which certain operating characteristics of the system are related.
5V - Power Supplies
an electronic circuit that converts the voltage of an alternating current (AC) into a direct current (DC) voltage.?
5V - Interface
In electronic components, the term "Interface" refers to the point at which two different systems, devices, or components connect and interact with each other. It can involve physical connections such as ports, connectors, or cables, as well as communication protocols and standards that facilitate the exchange of data or signals between the connected entities. The interface serves as a bridge that enables seamless communication and interoperability between different parts of a system or between different systems altogether. Designing a reliable and efficient interface is crucial in ensuring proper functionality and performance of electronic components and systems.
I2C, 2-Wire Serial - Memory Size
The memory capacity is the amount of data a device can store at any given time in its memory.
56B - Clock Frequency
Clock frequency, also known as clock speed, refers to the rate at which a processor or electronic component can execute instructions. It is measured in hertz (Hz) and represents the number of cycles per second that the component can perform. A higher clock frequency typically indicates a faster processing speed and better performance. However, it is important to note that other factors such as architecture, efficiency, and workload also play a significant role in determining the overall performance of a component. In summary, clock frequency is a crucial parameter that influences the speed and efficiency of electronic components in processing data and executing tasks.
0.032MHz - Logic Function
In electronic components, the term "Logic Function" refers to the specific operation or behavior of a component based on its input signals. It describes how the component processes the input signals to produce the desired output. Logic functions are fundamental to digital circuits and are used to perform logical operations such as AND, OR, NOT, and XOR.Each electronic component, such as logic gates or flip-flops, is designed to perform a specific logic function based on its internal circuitry. By understanding the logic function of a component, engineers can design and analyze complex digital systems to ensure proper functionality and performance. Different logic functions can be combined to create more complex operations, allowing for the creation of sophisticated digital devices and systems.
Clock - Number of Timers1
- Time Format
Time is based on a 24 hour system. This is frequently referred to as "military time". The 24 hour system is the default format.
HH:MM:SS (12/24 hr) - Date Format
The international standard recommends writing the date as year, then month, then the day:?YYYY-MM-DD.
YY-MM-DD-dd - Current - Timekeeping (Max)
The parameter "Current - Timekeeping (Max)" in electronic components refers to the maximum current that a device can draw while performing timekeeping functions. Timekeeping functions typically involve maintaining accurate time and date information within a device, such as in a real-time clock (RTC) or a microcontroller with a built-in clock. The maximum current specified for timekeeping is important for determining the power consumption of the device when it is in standby or low-power modes, as excessive current draw can drain the battery quickly. Designers need to consider this parameter when selecting components for battery-powered devices to ensure efficient power management and longer battery life.
200μA @ 5V - Time-Min
Time-Min is a parameter in electronic components that refers to the minimum amount of time required for a specific operation or function to be completed. This parameter is crucial in determining the speed and efficiency of the component's performance. It is often specified in datasheets and technical documentation to provide users with information on the component's timing characteristics. Understanding the "Time-Min" parameter is essential for designing and integrating electronic components into circuits to ensure proper functionality and timing synchronization.
SECONDS - Interrupt Capability
Returns the number of interrupts available for a specified hardware device and interrupt type.
N - Voltage - Supply, Battery
Voltage - Supply, Battery refers to the nominal voltage level provided by a battery to power electronic components or circuits. It indicates the standard voltage output that a battery can deliver under typical operating conditions. This parameter is crucial for ensuring compatibility between the battery and the electronic device, as it affects performance and functionality. The voltage supply rating helps in selecting the appropriate battery for specific applications, ensuring that the device operates efficiently and safely.
2V~3.5V - Volatile
In the context of electronic components, the term "Volatile" refers to a type of memory or storage that requires power to maintain the stored data. When power is removed or lost, the data stored in volatile memory is also lost. This is in contrast to non-volatile memory, which retains data even when power is turned off.Volatile memory is commonly used in devices like RAM (Random Access Memory) in computers, where data needs to be quickly accessed and modified. However, it is not suitable for long-term storage of important data as it requires continuous power supply to retain information.Overall, the volatile nature of this type of memory makes it fast and efficient for temporary data storage and processing, but it is not ideal for permanent data storage due to its dependency on power supply.
YES - Information Access Method
Information Access Method refers to the techniques and protocols used to retrieve, manage, and manipulate data stored in electronic systems. It encompasses various approaches such as direct memory access, polling, interrupts, and data buses, enabling efficient communication between different components within a system. This method is crucial for optimizing data retrieval speed and ensuring effective interaction between hardware and software in electronic devices.
I2C - Features
In the context of electronic components, the term "Features" typically refers to the specific characteristics or functionalities that a particular component offers. These features can vary depending on the type of component and its intended use. For example, a microcontroller may have features such as built-in memory, analog-to-digital converters, and communication interfaces like UART or SPI.When evaluating electronic components, understanding their features is crucial in determining whether they meet the requirements of a particular project or application. Engineers and designers often look at features such as operating voltage, speed, power consumption, and communication protocols to ensure compatibility and optimal performance.In summary, the "Features" parameter in electronic components describes the unique attributes and capabilities that differentiate one component from another, helping users make informed decisions when selecting components for their electronic designs.
Leap Year, NVSRAM, Square Wave Output - Height4.45mm
- Length9.91mm
- Width7.87mm
- REACH SVHC
The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.
Unknown - Radiation Hardening
Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.
No - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
ROHS3 Compliant - Lead Free
Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.
Lead Free
DS1307N Functional Block Diagram
The following figure is DS1307N Functional Block Diagram.

Functional Block Diagram
DS1307N Typical Operating Circuit
The following shows DS1307N Typical Operating Circuit.

Typical Operating Circuit
DS1307N Alternatives
| Part Number | Description | Manufacturer |
| DS1307NMICROCONTROLLERS AND PROCESSORS | Real Time Clock, Volatile, 1 Timer(s), CMOS, PDIP8, DIP-8 | Dallas Semiconductor |
| DS1307INDUCTORS | General Purpose Inductor, | Falco Electronics |
| DS1307+MICROCONTROLLERS AND PROCESSORS | Real Time Clock, Volatile, 1 Timer(s), CMOS, PDIP8, 0.300 INCH, ROHS COMPLIANT, PLASTIC, DIP-8 | Maxim Integrated Products |
DS1307N Applications
• Backup Supply
• AM/PM Indicator
DS1307N Package
The following figure is DS1307N Package.

Package
DS1307N Manufacturer
Analog Devices' Maxim Integrated designs, manufactures and sells analog and mixed-signal integrated circuits for automotive, industrial, communications, consumer, and computing applications. Power and battery management ICs, sensors, analog ICs, interface ICs, communications solutions, digital ICs, embedded security, and microcontrollers are all part of Maxim's product line. The company includes design centers, manufacturing facilities, and sales offices all around the world, with its headquarters in San Jose, California.
Trend Analysis
Datasheet PDF
- Datasheets :
- Environmental Information :
- Application Notes :
- Other Related Documents :
- ConflictMineralStatement :
What is the difference between DS1307 and DS3231?
The main difference between the DS3231 and DS1370 is the accuracy of time-keeping. DS1307 comes with an external 32kHz crystal for time-keeping whose oscillation frequency is easily affected by external temperature. This usually results in the clock being off by around five or so minutes per month.
What is the purpose of DS1307 pin 3?
Battery input for any standard 3V lithium cell or other energy sources. Battery voltage should be between 2V and 3.5V for suitable operation. The nominal write-protect trip point voltage at which access to the RTC and user RAM is denied is set by the internal circuitry as 1.25 x VBAT nominal.
Is DS3231 compatible with DS1307?
Although the notes and functions in the sketch refer only to the DS3231, the code also works with the DS1307. There may be a lot of code, however, it breaks down well into manageable parts.
How many bytes of NV SRAM is the DS1307N serial real-time clock?
56 bytes.
What is used to transport address and data serially?
An I2C bidirectional bus.
In what mode does the DS1307N clock work?
24-hour or 12-hour.
What does the DS1307N include?
A built-in power sensor circuit.
What happens when the part is running on the backup supply?
The timekeeping operation continues.
FDG6335N N-Channel MOSFET: Diagram, Pinout, and Datasheet [Video&FAQ]28 April 20222797
LM393M Comparators: Pinout, Datasheet16 March 20222826
25AA160D 16K SPI Bus Serial EEPROM: Pinout, Equivalent and Datasheet21 April 20221681
S8050 NPN Silicon Transistors: Datasheet, Pinout and Equivalent30 August 2021133964
LM386 Low Voltage Audio Power Amplifier: Features, Specifications, Applications10 May 20212110
EL817 Optocoupler: Package, Pinout, and Datasheet [Video&FAQ]18 October 202113107
43025-0800 Micro-Fit 3.0 Receptacle Housing Dual Row: Drawing, Datasheet, and Equivalents11 February 20222523
STM32F401RET6 vs GD32 Microcontrollers Key Differences24 July 20251631
What is an Operational Amplifier?27 March 20253808
Intel Launches First-of-its-Kind Semiconductor Technician Certificate Program to Address Workforce Shortage28 September 20233582
Introduction to DDIC (Display Driver IC)07 January 202632039
What is PCB Reflow? High-Speed Signal Reflow Path Analysis24 November 20214500
LDR/Light Dependent Resistor: Working Principle, Types and Applications19 January 202632638
What is a Fiber Optic Connector?27 October 20257856
What is 4G Router?27 September 20217519
What are the Types and Dielectric of Ceramic Capacitors?16 October 202512580
Maxim Integrated
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools