RS232 VS DB9: Disadvantages and advantages of RS232 and DB9, Differences between the RS232 and DB9

UTMEL

Published: 23 February 2022 | Last Updated: 23 February 2022

23173

DB9

DB9

Tripp Lite

SURGE SUPPRESSOR RS-232 DB9M/F

Purchase Guide

SURGE SUPPRESSOR RS-232 DB9M/F

RS232 and DB9 are all data connectors. This article is going to talk about the advantages, disadvantages of RS232 and DB9, and introduce the differences between RS232 VS DB9.

This video demonstrates detailed information about RS232 and DB9.

RS 232 DB9 Connector by Prof.Sachin Sambhaji Patil

What is RS232 Protocol?

In RS232, ‘RS’ stands for Recommended Standard. It defines serial communication using DTE and DCE signals. Here, DTE refers to Data Terminal Equipment and DCE refers to Data Communication Equipment. An example of a DTE device is a computer and DCE is a modem. Formally, it is specified as the interface between DTE equipment and DCE equipment using serial binary data exchange.

The DTE (computer) transmits the information serially to the other end equipment DCE (modem). In this case, DTE sends binary data “11011101” to DCE and DCE sends binary data “11010101” to the DTE device. RS232 describes the common voltage levels, electrical standards, operation mode, and a number of bits to be transferred from DTE to DCE. This standard is used for the transmission of information exchange over telephone lines.

RS232 Protocol.jpg

How RS232 Works?

The working of RS-232 can be understood by the protocol format. As RS-232 is a point-to-point asynchronous communication protocol, it sends data in a single direction. Here, no clock is required for synchronizing the transmitter and receiver. The data format is initiated with a start bit followed by 7-bit binary data, parity bit, and stop bit which are sent one after another.

The transmission begins by sending a Start bit ‘0’. This is succeeded by 7 bits of ASCII data. The parity bit is appended to this data for the receiver validation. The data sent from the transmitter should match the receiver. Finally, the transmission is halted using a stop bit and it is represented by the binary ‘1’. Generally, 1 or 2 stop bits can be sent. In the above diagram, ASCII character ‘A’ is sent using a serial binary stream of ‘1’s and ‘0’s. While sending data, there should be a certain delay between each bit. This delay is considered as inactive time and the RS232 line is at a negative logic state (-12V).

Protocol Format.jpg

What is a DB9 Connector?

The term "DB9" refers to a common connector type, one of the D-Subminiature or D-Sub types of connectors.  DB9 has the smallest "footprint" of the D-Subminiature connectors and houses 9 pins (for the male connector) or 9 holes (for the female connector).

DB9 Connector.jpg

Where are DB9 Connectors used?

DB9 connectors were once very common on PCs and servers.  DB9 connectors are designed to work with the EIA/TIA 232 serial interface standard, which determined the function of all nine pins as a standard so that multiple companies could design them into their products.  DB9 connectors were commonly used for serial peripheral devices like keyboards, mice, joysticks, etc. Also, they are used on DB9 cable assemblies for data connectivity.

Today, the DB9 has mostly been replaced by more modern interfaces such as USB, PS/2, Firewire, and others.  However, there are still many legacy devices that use the DB9 interface for serial communication.


RS232 VS DB9 3D Model

RS232  3D Model

RS232 Symbol.jpg

RS232 Symbol

RS232 Footprint.jpg

RS232 Footprint

DB9  3D Model

DB9 Symbol.jpg

DB9 Symbol

DB9 Footprint.jpg

DB9 Footprint

RS232 VS DB9 Features

RS232 Features

  • Features molded hoods and thumbscrews that enable a snug fit when making connections.

  • All nine pins are wired straight through.

 

DB9 Features

  • DB9 protects 9 pin serial connections for data line surge suppression of data terminal, data communications equipment and PCs, printers, modems, and more

  • Reversible for use with male or female captive DB9 ports

  • Offers protection on all 9 data lines, plus D shell chassis

  • Surge suppression utilizing high-speed avalanche diodes divert excess energies on the network to

  • Ground


Advantages and Disadvantages of RS232

RS232 Advantages

  • RS232 interface is supported in many compatible legacy devices due to its simplicity. It is widely used for point-to-point connections between DTE and DCE devices.

  • It supports long distances of about 50 feet (for low baud rates) and with error correction capabilities.

  • RS232 is immune to noise due to the use of +/-5 Volts or higher for binary logic 0 and logic 1.

  • RS232 is a low-cost interface.

  • Converters or adaptors are available at cheaper rates for conversion from RS232 to RS485/USB/Ethernet etc.



RS232 Disadvantages

  • It is suitable for system-to-system communications. It is not suitable for chip to chip or chip to sensor device communications.

  • Supports lower speed for long distances. Higher speed (i.e. 115200 baud) can be achieved for short distances only.

  • RS232 interface requires separate transceiver chips which will add cost to the system.

  • It is used for single master and single slave configuration and not for single master-multiple slaves mode.

  • It is an unbalanced transmission.


Advantages and Disadvantages of DB9

DB9 Advantages

DB9 connectors have several advantages. You can easily customize them with 9 individual pins to carry serial data. Although the speed of these connectors is low as compared to other standards like USB, the length of these cables is quite long. For eg, USB has a five-meter length limit, but RS-232, which is the most commonly used standard for serial data doesn’t have a particularly defined length limit. RS-422 has been used at length which is hundreds of meters long with special equipment.

In case you have an old device having DB9 connectors on it, you will find several options for conversions. Converters from other standards like USB, Ethernet, etc also enable you to make use of your device on any computer.

 

DB9 Disadvantages

As the connectors are large, it becomes difficult to connect and disconnect them in small spaces. The pins of these cables are usually exposed so there are more chances for them to get damaged or break. Although you can mate the connector without any thumbscrew hardware, there are fewer chances that it will hold on to the equipment. On the other hand, if you use thumbscrews, the connector will take a long time to get plugged and unplugged.

And as mentioned before, serial communication is a slow and old way of exchanging data. So the speed is quite slow when there are cables of long length. This also causes breaks in communication and makes the software of PC freeze. Due to such issues, other standards gained more popularity over DB9 cables.

But this in no way means that DB9 connectors aren’t used. If you use right-angle adapters, they can help you solve the tight space issue without causing any damage to the connector. You can attach the connectors with D-Subminiature plug and jack covers which can protect pins from getting damaged when not being used.

Before you make a buy for DB9 connectors, make sure you precisely know what your needs are. If there is a smart alternative for DB9 cables, you can go for that as well!


What is the difference between DB9 and RS232?

The serial interface is defined by RS232, which includes things like signal voltage and duration. The 9-pin connector is known as DB9. These connectors are commonly used for RS232 connections, but there is also a 25-pin connector. RS232 is the definition of the serial interface, e.g. the signal voltage and duration. DB9 is the 9-pin connector. RS232 connections are frequently implemented using these connectors, but there is a 25-pin connector also. But of course, you can solder the cable to the devices directly also, without a DB9 or DB25 connector.


DB9 Manufacturer

Outstanding product reliability and exceptional service have been Tripp Lite's trademarks for over 95 years. Tripp Lite manufactures over 4,000 products to power and connect the computers, networking equipment, and electronic devices that form the foundation of our connected world. On the desktop, in the data center, wherever power and information flow, products and services that solve customers' problems and meet their highest expectations are the hallmarks of a Tripp Lite solution. Headquartered in Chicago, Illinois, Tripp Lite maintains a global presence with offices and partners worldwide.


RS232 and DB9 Datasheet

Popularity by Region

Parts with Similar Specs

Frequently Asked Questions

Is DB9 same as RS-232?

RS232 is the definition of the serial interface, e.g. the signal voltage and duration. DB9 is the 9 pin connector. RS232 connections are frequently implemented using these connectors, but there is a 25 pin connector also.

What computer cable has 9 pins?

DB9

What is the difference between DB9 and DB25?

DB9 was a 9 pin connector and DB25 was a 25 pin connector. They were used for peripherals such as serial printers, mice, game controllers, and modems. We always called them RS-232 ports or a COM port.

What is a RS-232 cable?

RS232 is a standard protocol used for serial communication, it is used for connecting computers and its peripheral devices to allow serial data exchange between them. ... These connectors are known as the DB-9 Connector as a serial port and they are of two type's Male connectors (DTE) & Female connector (DCE).

How do I connect my DB9 to my laptop?

Plug the serial DB-9 end of the console cable into the serial DB-9 port on your laptop. If your laptop has no serial DB-9 port, plug the serial DB-9 end of the console cable into the serial DB-9 end of a USB to serial DB-9 adapter and then into a USB port on your laptop.
DB9

Tripp Lite

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More