2SC2240 NPN Transistor: Datasheet pdf, Equivalent, and Pinout
2SC2240 datasheet pdf and Unclassified product details from Foshan Blue Rocket Elec stock available at Utmel









The 2SC2240 is a bipolar junction transistor that belongs to the NPN transistor family. This article mainly covers pinout, datasheet pdf, equivalent, specifications, and other details about the 2SC2240 transistor.

Power Transistor for Amplifier 2SC3133, 2SC2240, 2SC3264, 2SC2238, 2SC1969, 2SC2312
2SC2240 Transistor Description
The 2SC2240 is a bipolar junction transistor that belongs to the NPN transistor family. The transistor 2SC2240 is designed for low-frequency and low-noise applications. This device is intended to reduce noise figures and pulse noise in the low signal source impedance range.
2SC2240 Pinout
The 2SC2240 is packaged in a TO-92 plastic casing. The emitter, collector, and base leads emerge from the transistor from left to right when looking at the flat side with the leads oriented downward.
The 2SC2240 pinout diagram for this transistor can be seen in the image below.

2SC2240 Pinout
| Pin Number | Pin Name | Description |
| 1 | Emitter | Current Drains out through emitter, normally connected to ground |
| 2 | Collector | Current flows in through collector, normally connected to load |
| 3 | Base | Controls the biasing of the transistor, Used to turn ON or OFF the transistor |
Specifications
- TypeParameter
- Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
TO-92 - Current-Collector (Ic) (Max)100mA
- Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tape & Reel (TR) - Power - Max
Power - Max is a parameter that specifies the maximum amount of power that an electronic component can handle without being damaged. It is typically measured in watts and indicates the upper limit of power that can be safely supplied to the component. Exceeding the maximum power rating can lead to overheating, malfunction, or permanent damage to the component. It is important to consider the power-max rating when designing circuits or systems to ensure proper operation and longevity of the electronic components.
300mW - Transistor Type
Transistor type refers to the classification of transistors based on their operation and construction. The two primary types are bipolar junction transistors (BJTs) and field-effect transistors (FETs). BJTs use current to control the flow of current, while FETs utilize voltage to control current flow. Each type has its own subtypes, such as NPN and PNP for BJTs, and MOSFETs and JFETs for FETs, impacting their applications and characteristics in electronic circuits.
NPN - Voltage - Collector Emitter Breakdown (Max)
Voltage - Collector Emitter Breakdown (Max) is a parameter that specifies the maximum voltage that can be applied between the collector and emitter terminals of a transistor or other semiconductor device before it breaks down and allows excessive current to flow. This parameter is crucial for ensuring the safe and reliable operation of the component within its specified limits. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the device. Designers and engineers must carefully consider this parameter when selecting components for their circuits to prevent potential issues and ensure proper functionality.
120V - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
2SC2240 Electronics Characteristic
Type: NPN
Collector-Emitter Voltage: 120 V
Collector-Base Voltage: 120 V
Emitter-Base Voltage: 5 V
Collector Current: 0.1 A
Collector Dissipation: 0.3 W
DC Current Gain (hfe): 200 to 700
Transition Frequency: 100 MHz
Operating and Storage Junction Temperature Range: -55 to +125 °C
Package: TO-92
Replacements and Equivalents for 2SC2240
You can replace the 2SC2240 with the 2SA970, 2SC2459, 2SC3200, 2SC3201, 2SC3245, 2SC3245A or KTC3200.
2SC2240 Applications
Audio preamplifier
Audio amplifier
Switching loads under 100mA
Darlington pairs
Different types of signal amplification
Where and How to Use 2SC2240
The 2SC2240 transistor is designed for low noise audio applications, but it may also be used as a switch and can drive up to 100mA of current. It can also be utilized for any form of signal amplification and in radio and RF applications around the 100MHz frequency range. The transistor is used in the same way as any other NPN BJT transistor.
2SC2240 Working
The transistor's action is controlled by the base. When voltage is added to the base terminal, the device is biased, and current flows from the collector to the emitter terminal.
Because this is an NPN transistor, current will flow from the collector to the emitter, whereas current will flow from the emitter to the collector in a PNP transistor.

2SC2240 Circuit
2SC2240 Dimensions

2SC2240 Dimensions
2SC2240 Manufacturer
Foshan Blue Rocket Electronics Co., Ltd. which is a Guangdong High-Tech Enterprise is professional in researching, developing, and manufacturing semiconductor devices in China.
Its former is No.4 Electronics Factory of Foshan which was founded in the early 1970s. In 1998 it transformed into a limited liability company and renamed FOSHAN BLUE ROCKET ELECTRONICS CO., LTD. by finishing share reform in 2012. Now its annual capacity reaches 10 billion pieces. It is one of the main manufacturing bases of semiconductor devices in south china.
What is the use of 2SC2240?
The 2SC2240 is a transistor for low frequency and low noise applications. This device is designed to lower the noise figures in the region of low signal source impedance and to lower the pulse noise. This is recommended for the first stages of Equalizer amplifiers.
How does 2SC2240 work?
This is an NPN transistor so here current will flow from the collector to the emitter side and in the case of the PNP transistor current will flow from the emitter to the collector side. These bipolar devices are not symmetrical.
Which transistor can replace the c2240?
2SC2362K、 2SC2014 、2SC1845、 2SC1708.
Kintex-7 XC7K410T Series: An Evergreen Mainstream Solution in FPGA14 January 20261702
MAX3243IPW Transceiver: Pinout,Specification, and Datasheet06 July 2021809
74LS107 Dual JK Flip-Flops: Flip-Flops Datasheet pdf, Pinout and Diagram20 December 20216574
TPS27081ADDCR High-Side Load Switch: Diagram, Pinout, and Datasheet26 March 20222625
LP5912-3.3DRVT LDO Regulator Pos, 1.8V 0.5A 6-Pin WSON EP T/R and 500mA Low-Noise14 February 20222431
MCF532x ColdFire® Microprocessor Datasheet Overview29 February 2024195
MAX30003 Integrated Biopotential AFE: Circuit, Pinout, MAX30003 vs AD8232 [Video&FAQ]09 May 202219791
73S1215F System-on-Chip: Technical Specifications and Applications29 February 2024238
Smart Sensors: Definition, Structures and Applications04 July 20226151
How to Increase Laptop Battery Life03 July 20213700
Analysis of Resistors in Series and Parallel12 June 202622225
Semiconductor Market Poised for Strong Rebound in 2024, Predicts WSTS11 December 20235403
Four Proximity Sensors PK, Who can Win?08 April 20222500
How to Select the Most Accurate Shunt Resistor for Your Circuit06 June 20254925
800G Optical Transceivers: The Guide for AI Data Centers21 August 202615733
JSCJ Authorized Distributor | UTMEL Electronics21 November 20234375
Foshan Blue Rocket Elec
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools