UF5408 Rectifier Diode: Package, Pinout, and Datasheet

Sophie

Published: 25 October 2021 | Last Updated: 25 October 2021

5316

UF5408-TP

UF5408-TP

Micro Commercial Co

Standard Diode Rectifier Fast Recovery =< 500ns, > 200mA (Io) 1.7V @ 3A -55°C~150°C 10μA @ 1000V 2-Termination Tape & Reel (TR) DO-201AD, Axial Through Hole

Purchase Guide

Standard Diode Rectifier Fast Recovery =< 500ns, > 200mA (Io) 1.7V @ 3A -55°C~150°C 10μA @ 1000V 2-Termination Tape & Reel (TR) DO-201AD, Axial Through Hole

UF5408 is an ultra-fast recovery rectifier tube, diode, which is mainly used for internal high-frequency rectification and freewheeling of switching power supplies. This article mainly introduces package, pinout, datasheet and other detailed information about Micro Commercial Components UF5408.

This video will show you the application of UF5408.

Diyot ile 220 Volt Kademeli Hız Ayarı - UF5408 Kademeli Hız Ayarı - Diyot İle 2 Kademeli Hız Ayarı

UF5408 Description

UF5408 is an ultra-fast recovery rectifier tube, diode, which is mainly used for internal high-frequency rectification and freewheeling of switching power supplies. With a current of 3A, a voltage of 1000V, a voltage drop of 1.7V, and a recovery time of 75ns (nanoseconds) packaged DO-27. The more prominent feature is that the recovery time is very fast.

The plastic rectifier features a glass passivated pallet chip junction, high forward surge capability, low switching losses and high efficiency. Color band denotes cathode end polarity.


The rectifier diode is a semiconductor device that converts AC power into DC power. Usually, it contains a PN junction with two terminals, a positive electrode and a negative electrode. The most important characteristic of a diode is its unidirectional conductivity. In a circuit, current can only flow in from the anode of the diode and flow out of the cathode. 


The rectifier diode, one end with a silver circle on the picture is the negative electrode. Rectifier diodes are generally planar silicon diodes, which are used in various power rectifier circuits.


UF5408 Pinout

pinout.jpg

Pinout


UF5408 CAD Model

symbol.png

Symbol

footprint.png

Footprint

3D Model.jpg

3D Model


UF5408 Features

• Lead-Free Finish/RoHS Compliant("P" Suffix Designates RoHS Compliant. See Ordering Information)

• Epoxy Meets UL 94 V-0 Flammability Rating

• Low Forward Voltage Drop and Low Leakage

• Moisture Sensitivity Level 1

• Ultra Fast Switching Speed For High Efficiency

• Halogen Free Available Upon Request by Adding The Suffix "-HF"


Specifications

Micro Commercial Co UF5408-TP technical specifications, attributes, parameters and parts with similar specifications to Micro Commercial Co UF5408-TP.
  • Type
    Parameter
  • Factory Lead Time
    8 Weeks
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Through Hole
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    DO-201AD, Axial
  • Surface Mount

    having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.

    NO
  • Diode Element Material

    The parameter "Diode Element Material" refers to the specific semiconductor material used in the construction of a diode. This material determines the electrical characteristics and performance of the diode, including its forward voltage drop, reverse breakdown voltage, and switching speed. Common diode element materials include silicon, germanium, and gallium arsenide, each offering different advantages for various applications. The choice of material impacts the diode's efficiency, thermal stability, and overall suitability for specific electronic circuits.

    SILICON
  • Number of Elements
    1
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • Published
    2000
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e3
  • Pbfree Code

    The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.

    yes
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Obsolete
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    2
  • ECCN Code

    An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.

    EAR99
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Matte Tin (Sn)
  • Applications

    The parameter "Applications" in electronic components refers to the specific uses or functions for which a component is designed. It encompasses various fields such as consumer electronics, industrial automation, telecommunications, automotive, and medical devices. Understanding the applications helps in selecting the right components for a particular design based on performance, reliability, and compatibility requirements. This parameter also guides manufacturers in targeting their products to relevant markets and customer needs.

    EFFICIENCY
  • Additional Feature

    Any Feature, including a modified Existing Feature, that is not an Existing Feature.

    LOW LEAKAGE CURRENT
  • HTS Code

    HTS (Harmonized Tariff Schedule) codes are product classification codes between 8-1 digits. The first six digits are an HS code, and the countries of import assign the subsequent digits to provide additional classification. U.S. HTS codes are 1 digits and are administered by the U.S. International Trade Commission.

    8541.10.00.80
  • Terminal Form

    Occurring at or forming the end of a series, succession, or the like; closing; concluding.

    WIRE
  • Peak Reflow Temperature (Cel)

    Peak Reflow Temperature (Cel) is a parameter that specifies the maximum temperature at which an electronic component can be exposed during the reflow soldering process. Reflow soldering is a common method used to attach electronic components to a circuit board. The Peak Reflow Temperature is crucial because it ensures that the component is not damaged or degraded during the soldering process. Exceeding the specified Peak Reflow Temperature can lead to issues such as component failure, reduced performance, or even permanent damage to the component. It is important for manufacturers and assemblers to adhere to the recommended Peak Reflow Temperature to ensure the reliability and functionality of the electronic components.

    NOT SPECIFIED
  • Reach Compliance Code

    Reach Compliance Code refers to a designation indicating that electronic components meet the requirements set by the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation in the European Union. It signifies that the manufacturer has assessed and managed the chemical substances within the components to ensure safety and environmental protection. This code is vital for compliance with regulations aimed at minimizing risks associated with hazardous substances in electronic products.

    not_compliant
  • Time@Peak Reflow Temperature-Max (s)

    Time@Peak Reflow Temperature-Max (s) refers to the maximum duration that an electronic component can be exposed to the peak reflow temperature during the soldering process, which is crucial for ensuring reliable solder joint formation without damaging the component.

    NOT SPECIFIED
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    UF5408
  • Pin Count

    a count of all of the component leads (or pins)

    2
  • JESD-30 Code

    JESD-30 Code refers to a standardized descriptive designation system established by JEDEC for semiconductor-device packages. This system provides a systematic method for generating designators that convey essential information about the package's physical characteristics, such as size and shape, which aids in component identification and selection. By using JESD-30 codes, manufacturers and engineers can ensure consistency and clarity in the specification of semiconductor packages across various applications and industries.

    O-PALF-W2
  • Qualification Status

    An indicator of formal certification of qualifications.

    Not Qualified
  • Configuration

    The parameter "Configuration" in electronic components refers to the specific arrangement or setup of the components within a circuit or system. It encompasses how individual elements are interconnected and their physical layout. Configuration can affect the functionality, performance, and efficiency of the electronic system, and may influence factors such as signal flow, impedance, and power distribution. Understanding the configuration is essential for design, troubleshooting, and optimizing electronic devices.

    SINGLE
  • Speed

    In electronic components, "Speed" typically refers to the rate at which data can be processed or transferred within the component. It is a measure of how quickly the component can perform its functions, such as executing instructions or transmitting signals. Speed is often specified in terms of frequency, such as clock speed in processors or data transfer rate in memory modules. Higher speed components can perform tasks more quickly, leading to improved overall performance in electronic devices. It is an important parameter to consider when designing or selecting electronic components for specific applications.

    Fast Recovery =< 500ns, > 200mA (Io)
  • Diode Type

    In electronic components, the parameter "Diode Type" refers to the specific type or configuration of a diode, which is a semiconductor device that allows current to flow in one direction only. There are various types of diodes, each designed for specific applications and functions. Common diode types include rectifier diodes, zener diodes, light-emitting diodes (LEDs), and Schottky diodes, among others. The diode type determines the diode's characteristics, such as forward voltage drop, reverse breakdown voltage, and maximum current rating, making it crucial for selecting the right diode for a particular circuit or application. Understanding the diode type is essential for ensuring proper functionality and performance in electronic circuits.

    Standard
  • Current - Reverse Leakage @ Vr

    Current - Reverse Leakage @ Vr is a parameter that describes the amount of current that flows in the reverse direction through a diode or other semiconductor component when a reverse voltage (Vr) is applied across it. This leakage current is typically very small, but it is important to consider in electronic circuits as it can affect the overall performance and reliability of the component. The reverse leakage current is influenced by factors such as the material properties of the semiconductor, temperature, and the magnitude of the reverse voltage applied. Manufacturers provide this parameter in datasheets to help engineers and designers understand the behavior of the component in reverse bias conditions.

    10μA @ 1000V
  • Voltage - Forward (Vf) (Max) @ If

    The parameter "Voltage - Forward (Vf) (Max) @ If" refers to the maximum voltage drop across a diode when it is forward-biased and conducting a specified forward current (If). It indicates the maximum potential difference the diode can withstand while allowing current to flow in the forward direction without breaking down. This value is crucial for designing circuits as it helps determine how much voltage will be lost across the diode during operation. Higher Vf values can lead to reduced efficiency in power applications, making this parameter essential for optimizing circuit performance.

    1.7V @ 3A
  • Case Connection

    Case Connection refers to the method by which an electronic component's case or housing is connected to the electrical circuit. This connection is important for grounding purposes, mechanical stability, and heat dissipation. The case connection can vary depending on the type of component and its intended application. It is crucial to ensure a secure and reliable case connection to maintain the overall performance and safety of the electronic device.

    ISOLATED
  • Operating Temperature - Junction

    Operating Temperature - Junction refers to the maximum temperature at which the junction of an electronic component can safely operate without causing damage or performance degradation. This parameter is crucial for determining the reliability and longevity of the component, as excessive heat can lead to thermal stress and failure. Manufacturers specify the operating temperature range to ensure that the component functions within safe limits under normal operating conditions. It is important for designers and engineers to consider the operating temperature - junction when selecting and using electronic components to prevent overheating and ensure optimal performance.

    -55°C~150°C
  • Output Current-Max

    Output Current-Max is a parameter in electronic components that specifies the maximum amount of current that can be safely drawn from the output of the component without causing damage. It is an important specification to consider when designing circuits to ensure that the component can handle the required current without overheating or failing. Exceeding the maximum output current can lead to performance issues, component damage, or even complete failure of the circuit. It is crucial to adhere to the specified maximum output current to ensure the reliable operation of the electronic component and the overall circuit.

    3A
  • Voltage - DC Reverse (Vr) (Max)

    Voltage - DC Reverse (Vr) (Max) is a parameter in electronic components that specifies the maximum reverse voltage that the component can withstand without breaking down. This parameter is crucial for components like diodes and transistors that are often subjected to reverse voltage during operation. Exceeding the maximum reverse voltage can lead to the component failing or getting damaged. Designers need to consider this parameter when selecting components to ensure the reliability and longevity of their circuits.

    1000V
  • Current - Average Rectified (Io)

    The parameter "Current - Average Rectified (Io)" in electronic components refers to the average value of the rectified current flowing through the component. This parameter is important in determining the average power dissipation and thermal considerations of the component. It is typically specified in datasheets for diodes, rectifiers, and other components that handle alternating current (AC) and convert it to direct current (DC). Understanding the average rectified current helps in selecting the appropriate component for a given application to ensure reliable operation and prevent overheating.

    3A
  • Number of Phases
    1
  • Reverse Recovery Time

    Reverse Recovery Time is a key parameter in semiconductor devices, particularly diodes and transistors. It refers to the time taken for a diode or transistor to switch from conducting in the forward direction to blocking in the reverse direction when the polarity of the voltage across the device is reversed. This parameter is crucial in applications where fast switching speeds are required, as a shorter reverse recovery time allows for quicker response times and improved efficiency. Reverse Recovery Time is typically specified in datasheets for electronic components and is an important consideration in circuit design to ensure optimal performance and reliability.

    75ns
  • Rep Pk Reverse Voltage-Max

    Rep Pk Reverse Voltage-Max refers to the maximum reverse voltage that an electronic component, such as a diode, can withstand during a specified period of time without failing. This parameter is crucial in determining the safe operating limits of components in circuits where reverse voltage conditions may occur. Exceeding this value can lead to breakdown or permanent damage to the component. It is typically expressed in volts and is a key specification in signal and power applications.

    1000V
  • Capacitance @ Vr, F

    Capacitance @ Vr, F refers to the capacitance value of a capacitor measured at a specified rated voltage (Vr). It indicates how much electrical charge the capacitor can store per volt when subjected to this voltage. This parameter is essential for understanding the behavior of capacitors in circuits, particularly under different voltage conditions, and ensures that the component operates within its safe limits. The unit of measurement is Farads (F), which quantifies the capacitor's ability to hold an electrical charge.

    50pF @ 4V 1MHz
  • Non-rep Pk Forward Current-Max

    Non-rep Pk Forward Current-Max refers to the maximum forward current that a semiconductor device, such as a diode or LED, can handle in a pulsed or non-repetitive manner without being damaged. This parameter is essential for designers to ensure that the component operates reliably under specific conditions, particularly during transient events like switching or fault conditions. Exceeding this limit can lead to overheating or failure of the device.

    150A
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

UF5408 vs 1N5408

UF5408 is an ultra-fast recovery rectifier tube, diode, which is mainly used for internal high-frequency rectification and freewheeling of switching power supplies. With a current of 3A, a voltage of 1000V, a voltage drop of 1.7V, and a recovery time of 75ns (nanoseconds) packaged DO-27. The more prominent feature is that the recovery time is very fast.

 

1N5408 is a low-frequency rectifier tube, diode, which is mainly used for rectification of mains (50/60Hz),  current 3A, voltage 1000V, voltage drop 1.0V, package DO-27, its main function is to rectify alternating current into direct current.


Reference:  1N5408 Power Diode: Pinout, Price, Datasheet

UF5408 Alternatives

Part NumberDescriptionManufacturer
UF3007DIODESRectifier Diode, 1 Element, 3A, 1000V V(RRM)Silitek Corp
UF5408-E3DIODESDIODE 3 A, 1000 V, SILICON, RECTIFIER DIODE, DO-201AD, LEAD FREE, PLASTIC PACKAGE-2, Rectifier DiodeVishay Semiconductors
UF5408-GT3DIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD, LEAD FREE, PLASTIC PACKAGE-2Sensitron Semiconductors
UF5408GP-BPDIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD, ROHS COMPLIANT, PLASTIC PACKAGE-2Micro Commercial Components
UF5408-T3DIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD, PLASTIC PACKAGE-2Won-Top Electronics Co Ltd
UF5408GPDIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD,Microsemi Corporation
UF5408GP-TPDIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD, ROHS COMPLIANT, PLASTIC PACKAGE-2Micro Commercial Components
UF5408-BPDIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD, ROHS COMPLIANT, PLASTIC PACKAGE-2Micro Commercial Components
UF3007-TDIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD, ROHS COMPLIANT, PLASTIC PACKAGE-2Diodes Incorporated
UF5408-TPDIODESRectifier Diode, 1 Phase, 1 Element, 3A, 1000V V(RRM), Silicon, DO-201AD, ROHS COMPLIANT, PLASTIC PACKAGE-2Micro Commercial Components


UF5408 Applications

• High-Frequency Rectification

• Freewheeling Application in Switching Mode Converters

• Inverters for Consumer

• Telecommunication

• Power Management

• Consumer Electronics

• Computers & Computer Peripherals

• Communications & Networking


UF5408 Package

Package.png

package1.png

Package


UF5408 Manufacturer

Founded in 1991, Micro Commercial Components Corp. (MCC) is a manufacturer of high-quality discrete semiconductors to the consumer markets. It provides diodes, rectifiers, transistors, MOSFETs, voltage regulators and protection devices.

 

MCC has extensive experience in the manufacturing and delivery of high-quality products, including extensive marketing and sales network throughout the world; Americas, EMEA, APAC

 

Headquarter is located in Simi Valley, CA., engineering and technical support office in Suzhou, China, warehouse and logistic offices in California, Suzhou, and Taipei, and main front and backend manufacturing facility in Yangzhou, China.

 

Their mission is to surpass their customer's expectations in quality, cost, and delivery through superior customer service and continuous product improvement.


Datasheet PDF

Download datasheets and manufacturer documentation for Micro Commercial Co UF5408-TP.
Frequently Asked Questions

1.Can 10A10 replace UF5408?

UF5408 belongs to ultra-fast recovery diode, package DO-27/DO-201AD, its more prominent feature is that the reverse recovery time is short, 10A10 belongs to rectifier diode, package R-6, they can not be replaced, the performance is not good.

2.Can UF5408 replace HER307? What are the differences in specific parameters?

The maximum peak current and voltage of the two are different, the other two are the same, the two can be replaced, just check the data manually for specific parameters.

3.Can diode UF4005 be replaced by UF5408?

Yes. UF4005 is a very fast rectifier diode, which can be replaced by UF4006, UF4007, or UF5406, UF5407, UF5408.
UF5408-TP

Micro Commercial Co

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More